nF Capacitors: Definition, Conversion, Circuit Applications, and Selection
Quick answer
An nF capacitor is simply a capacitor whose capacitance is expressed in nanofarads. The prefix nano means 10-9, so 1 nF equals 0.000000001 F, 1,000 pF, or 0.001 µF. The notation tells you the capacitance value, not the dielectric, package, voltage rating, tolerance, or intended circuit function.
For fast conversion, move by a factor of 1,000 between adjacent common units: pF to nF to µF. For example, 47 nF = 47,000 pF = 0.047 µF, and 100 nF = 100,000 pF = 0.1 µF. When selecting the actual part, check the manufacturer datasheet for voltage, dielectric, tolerance, effective capacitance under bias and temperature, impedance, package, and safety approvals.
What is an nF capacitor?
The farad, symbol F, is the SI unit of capacitance. Most electronic capacitors are much smaller than one farad, so prefixes keep the numbers readable. The official SI prefix symbols are case-sensitive: milli is m, micro is µ, nano is n, and pico is p.
| Unit | Symbol | Factor relative to 1 F | Relationship |
|---|---|---|---|
| Millifarad | mF | 10-3 F | 1 mF = 1,000 µF |
| Microfarad | µF | 10-6 F | 1 µF = 1,000 nF |
| Nanofarad | nF | 10-9 F | 1 nF = 1,000 pF |
| Picofarad | pF | 10-12 F | 1 pF = 0.001 nF |
The term "nF capacitor" does not define a special component family. A 10 nF part could be ceramic, film, silicon, or another technology. It could be surface-mount or leaded, low-voltage or high-voltage, general-purpose or safety-approved. Two capacitors with the same nominal nF value may behave very differently in the circuit.
How to convert pF, nF, and µF
Each step between pF, nF, and µF is a factor of 1,000:
pF to nF: divide by 1,000.
nF to pF: multiply by 1,000.
nF to µF: divide by 1,000.
µF to nF: multiply by 1,000.

| Nominal value | In pF | In nF | In µF |
|---|---|---|---|
| 1 nF | 1,000 pF | 1 nF | 0.001 µF |
| 2.2 nF | 2,200 pF | 2.2 nF | 0.0022 µF |
| 10 nF | 10,000 pF | 10 nF | 0.01 µF |
| 47 nF | 47,000 pF | 47 nF | 0.047 µF |
| 100 nF | 100,000 pF | 100 nF | 0.1 µF |
| 220 nF | 220,000 pF | 220 nF | 0.22 µF |
| 470 nF | 470,000 pF | 470 nF | 0.47 µF |
| 1 µF | 1,000,000 pF | 1,000 nF | 1 µF |
A calculator can verify arithmetic, but preserve enough significant digits for the design. For example, 3.3 nF is 0.0033 µF, not 0.003 µF. Utmel also provides a capacitance conversion tool.
How to read nF capacitor codes
Capacitor marking is not universal. Some leaded ceramic and film capacitors use a three-character capacitance code, some print the value directly, and many small surface-mount MLCCs are unmarked. IEC 60062 defines marking and designation methods, but the manufacturer datasheet and reel label remain the authoritative identification sources for a specific part.
Three-digit capacitance code
Where a manufacturer uses the common three-digit capacitance code, the first two digits are the significant figures and the third digit is the power-of-ten multiplier. The resulting value is expressed in picofarads:
Code ABC = AB × 10C pF

| Code | Calculation | Capacitance | Equivalent nF value |
|---|---|---|---|
| 102 | 10 × 102 pF | 1,000 pF | 1 nF |
| 222 | 22 × 102 pF | 2,200 pF | 2.2 nF |
| 103 | 10 × 103 pF | 10,000 pF | 10 nF |
| 473 | 47 × 103 pF | 47,000 pF | 47 nF |
| 104 | 10 × 104 pF | 100,000 pF | 100 nF |
| 224 | 22 × 104 pF | 220,000 pF | 220 nF |
| 474 | 47 × 104 pF | 470,000 pF | 470 nF |
Some code systems use R as a decimal marker, but the unit and exact interpretation still depend on the manufacturer's marking specification. Do not assume that every three-character string printed on a capacitor is a capacitance value; it may be a date, lot, voltage, tolerance, series, or safety-approval code.
Direct value marking
Larger parts may show values such as 10n, 47n, 100n, 0.1µF, or 100 nF. The micro symbol may appear as µ, and plain-text systems often use u instead. Letter tolerance codes can appear on the body or in the part number. For example, J, K, and M commonly indicate ±5%, ±10%, and ±20% in manufacturer coding systems, but verify the applicable data sheet rather than decoding a detached part by convention alone.
Why an SMD capacitor may have no marking
Small MLCCs are frequently supplied unmarked because the body is too small for a legible, durable code. KEMET data sheets, for example, explicitly list unmarked reel options. Identify these parts from the reel label, approved vendor list, bill of materials, placement record, or controlled inventory. A capacitance meter can help sort parts, but it cannot recover voltage rating, dielectric, tolerance, qualification, or lot traceability.
Which capacitor technologies use nF values?
Nanofarad values occur across several capacitor technologies. The correct choice follows the circuit requirement, not the unit notation.
| Technology | Useful characteristics | Points to verify | Common nF roles |
|---|---|---|---|
| C0G or NP0 ceramic | Stable capacitance, low loss, minimal DC-bias effect | Available capacitance, voltage, package, tolerance | Precision filters, oscillators, RF matching, timing |
| X7R ceramic | Higher capacitance density and broad availability | DC bias, temperature change, aging, AC voltage, package stress | Decoupling, bypassing, general filtering |
| Film | Low loss and useful pulse or AC options in suitable series | Dielectric type, package size, pulse current, dv/dt, voltage | Signal paths, filters, timing, pulse networks |
| Silicon or other specialty capacitor | Technology-specific stability, integration, or high-frequency behavior | Supplier model, voltage, frequency data, cost, mounting | RF, precision, high-temperature, integrated applications |
C0G and NP0 are Class 1 ceramic temperature characteristics. TDK lists C0G at 0 ±30 ppm/°C over -55°C to +125°C in applicable product tables. X7R is a Class 2 characteristic with capacitance change within ±15% over -55°C to +125°C under the defined test conditions. That temperature code does not include all other effects: an X7R part can lose effective capacitance under DC bias, and the amount is part-specific.
Parameters that matter beyond the nF value
A useful selection process starts with the circuit requirement and ends with the exact manufacturer part number. The nominal nF value is only one input.

Rated voltage and waveform
Do not apply one universal 1.5× or 2× voltage rule to every capacitor technology. Use the manufacturer data sheet, reliability guidance, and equipment standard. Account for DC bias, AC peak-to-peak voltage, ripple, switching overshoot, startup and shutdown transients, and temperature. Murata specifies that the relevant applied voltage, including abnormal transient voltage, must remain within the rated-voltage conditions for the applicable ceramic capacitor.
Effective capacitance
Class 2 MLCC capacitance can change with DC bias, temperature, aging, and AC measurement conditions. Murata notes that X5R, X6S, X7R, and similar high-dielectric-constant ceramics may show reduced capacitance under applied DC voltage, while C0G temperature-compensating types do not show the same DC-bias characteristic. Check the vendor's curves for the exact part number and conditions.
Tolerance and stability
A ±20% capacitor may be acceptable for supply bypassing but unsuitable for a filter pole, oscillator, or timing interval that needs tight accuracy. Calculate the combined tolerance of the resistor, capacitor, source, load, temperature, and other relevant effects instead of assigning all error to the nominal capacitor tolerance.
Impedance, ESR, ESL, and self-resonance
A real capacitor is not purely capacitive. Equivalent series resistance and inductance shape impedance versus frequency. Below self-resonance, the capacitive term generally dominates; around self-resonance, impedance reaches a minimum; above it, inductive behavior becomes important. TI's PCB design guidance shows that different values and layouts produce different impedance profiles, so "smaller capacitance means faster" is not a reliable selection rule.
Package, mounting, and environment
Verify dimensions, land pattern, terminal construction, mounting method, board flex exposure, vibration, humidity, operating temperature, and qualification level. Physical size is not determined by capacitance unit alone. The same 100 nF value can be offered in several case sizes and voltage ratings, and a smaller high-capacitance MLCC can show stronger DC-bias loss than a larger alternative.
Safety classification
A capacitor connected to the AC mains, protective earth, or another safety-critical location may require an approved X or Y safety class. Nominal capacitance and voltage alone do not authorize a general-purpose capacitor for that position. Use the class, subclass, approvals, impulse rating, and equipment-standard requirements specified by the design.
Typical nF capacitor applications
Decoupling and bypassing
Values such as 10 nF and 100 nF are common in decoupling networks, but no single value is correct for every IC. Follow the IC data sheet or validated reference design. Placement and current-loop geometry matter: the capacitor, supply pin, and return path should form a low-inductance loop. Multiple values may be used when the target impedance spans different frequencies, but the combined network should be checked for resonances rather than assembled by habit.

RC filters and timing networks
An nF capacitor and a resistor can set a filter corner or time constant. For an ideal first-order RC network:
τ = RC
fc = 1 / (2πRC)
These equations establish the ideal target. Source impedance, load impedance, component tolerances, leakage, dielectric behavior, and parasitic elements can shift the real result. For timing circuits, verify input thresholds and leakage from the actual IC data sheet.

AC coupling and signal shaping
A series capacitor can block DC while passing part of an AC signal. Its corner frequency depends on the resistance seen by the capacitor, not on capacitance alone. Check signal amplitude, bias voltage, distortion, leakage, and dielectric absorption. Precision or low-distortion paths may favor C0G, film, or another technology over a high-capacitance-density Class 2 ceramic.
EMI suppression, snubbers, and pulse circuits
Nanofarad values are also used in EMI and transient-control networks. These applications can impose high pulse current, repetitive voltage, dv/dt, or mains safety requirements. Select from a series explicitly rated for the waveform and application. A general-purpose 10 nF or 100 nF capacitor is not automatically suitable for a snubber or mains-connected circuit.
Worked examples
Example 1: convert 4.7 nF
Multiply by 1,000 to convert to pF: 4.7 nF = 4,700 pF. Divide by 1,000 to convert to µF: 4.7 nF = 0.0047 µF.
Example 2: decode 473
In a series that uses the three-digit pF code, 473 means 47 × 103 pF = 47,000 pF = 47 nF = 0.047 µF.
Example 3: calculate an RC corner frequency
For an ideal 10 kΩ resistor and 47 nF capacitor, RC = 0.00047 s. The ideal corner frequency is approximately 339 Hz:
fc = 1 / (2π × 10,000 × 47 × 10-9) ≈ 339 Hz
The real corner moves with resistor and capacitor tolerance, source and load impedance, temperature, bias, and parasitic elements.
Example 4: ideal capacitive reactance
For an ideal 10 nF capacitor at 1 MHz:
XC = 1 / (2πfC) ≈ 15.9 Ω
This is the ideal capacitive term. Use the vendor's impedance or S-parameter data for real high-frequency behavior because ESR, ESL, package, mounting, and self-resonance matter.
Testing and troubleshooting nF capacitors
De-energize the equipment, follow the applicable stored-energy procedure, and confirm a safe state before handling or measuring a capacitor. In-circuit capacitance readings can be distorted by parallel components, semiconductor junctions, and residual voltage. Remove or isolate the component only when the service procedure permits it.
A capacitance reading near nominal does not prove that the part is suitable or healthy under operating conditions. Depending on the technology and circuit, diagnosis may require leakage, insulation resistance, dissipation factor, ESR, impedance-versus-frequency, or operation under controlled voltage and temperature. Replace a damaged part only with one meeting the complete electrical, mechanical, environmental, and safety requirements.
For an unknown unmarked SMD capacitor, measurement can estimate capacitance, but it cannot identify the original voltage rating, dielectric, qualification, or traceability. If the BOM or controlled records are unavailable, treat the identification as unresolved rather than guessing.
nF capacitor selection checklist
Define the circuit function and target nominal capacitance.
Calculate the required tolerance and effective capacitance range.
Identify DC, AC, ripple, surge, pulse, and startup voltage conditions.
Select the dielectric or capacitor technology for stability, loss, and waveform duty.
Check DC-bias, temperature, aging, and frequency curves for the exact part.
Verify ESR, ESL, impedance, self-resonance, ripple, and self-heating where relevant.
Confirm case size, land pattern, mounting process, board flex, and environment.
Apply the required safety class, qualification, and regulatory approvals.
Validate the selected part in the real circuit and operating range.
Frequently asked questions
Is 100 nF the same as 0.1 µF?
Yes. 100 nF = 0.1 µF = 100,000 pF. The notation changes, but the nominal capacitance is the same.
What does 104 mean on a capacitor?
If the applicable manufacturer marking system uses the common three-digit pF code, 104 means 10 × 104 pF = 100,000 pF = 100 nF = 0.1 µF. Confirm the component series before applying the rule.
Is an nF capacitor polarized?
The unit does not determine polarity. Common ceramic and film capacitors are non-polar, while some other capacitor technologies can be polarized. Check the exact data sheet and body markings.
Can I replace 100 nF with 0.1 µF?
The nominal capacitance is equivalent, but that alone does not establish interchangeability. Voltage rating, dielectric, tolerance, effective capacitance, ESR, ESL, package, temperature range, pulse or ripple capability, and safety approval must also satisfy the circuit.
Why does a 100 nF MLCC measure below 100 nF in operation?
Possible causes include tolerance, DC bias, temperature, aging, measurement frequency and amplitude, or the surrounding circuit. Review the exact part's characteristic curves and measure under defined conditions.
Why is there no code on my SMD capacitor?
Many small MLCCs are intentionally supplied unmarked. Use the reel label, BOM, placement record, or controlled inventory to identify them. A meter cannot reconstruct all missing part specifications.
Official sources
AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 CapacitorsUTMEL02 June 20264003Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.
Read More
MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNsUTMEL07 August 20261021Facing 2026 MLCC lead times of up to 24 weeks driven by AI server demand, hardware engineers are substituting multi-layer ceramic capacitors with conductive polymer tantalum capacitors. While Class II MLCCs suffer severe DC bias capacitance loss and acoustic noise, polymer tantalums offer voltage stability and low ESR. Implementing a division-of-labor strategy—using polymer tantalums for bulk decoupling and MLCCs for point-of-load—optimizes PDN performance and bypasses supply bottlenecks.
Read More
Sourcing Silicon Capacitors and MLCCs in the AI Hardware EraUTMEL13 August 2026863Modern AI hardware requires a hybrid Power Delivery Network (PDN) to maintain low-voltage stability under extreme transient currents. Deep Trench Silicon Capacitors (DTCs) integrate directly into advanced packages to deliver ultra-low ESL and stable performance for high-frequency transient suppression. Meanwhile, Multilayer Ceramic Capacitors (MLCCs) provide essential bulk energy storage on the motherboard, making both technologies complementary across the AI power stack.
Read More
AI-Grade High-Capacitance MLCC Shortage Outlook for 1H 2027: Supply Bifurcation, Derating Risks, and Dual-Source RFQ ChecklistUTMEL06 November 2026519While consumer MLCC spot prices softened in late 2026, AI inference servers, DDR5 RDIMMs, and 800G/1.6T optical modules keep high-capacitance Class II and copper-electrode Class I High-Q capacitors supply-constrained through 1H 2027. This engineering and procurement guide explains DC bias and thermal derating risks, separates High-Q RF specs from power decoupling, and provides a 10-field parametric RFQ checklist to dual-qualify alternates before 1Q 2027 price talks.
Read More
MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component SelectionUTMEL11 September 20261039Class II ceramic capacitors suffer significant capacitance loss under DC voltage due to ferroelectric domain saturation and high electric field intensity. This comprehensive engineering guide explains how to calculate true worst-case effective capacitance by compounding DC bias, temperature, tolerance, and aging. It provides multi-vendor simulation workflows, benchtop impedance measurement techniques, and practical guidelines to maintain power supply stability and avoid costly design failures.
Read More
Subscribe to Utmel !
BBCAnalog Devices
NUTINY-SDK-M0564Nuvoton
CORE1553BBC-ARMicrochip
![ZOPT3100KITV1P0]()
![ZSSC313XMCREFBV1P0]()
![ZSSC5101KITV1P1]()
MT9J003I12STCUH-GEVBAptina
MAX17506EVKITBE#Maxim
MAX17536EVKITBE#Maxim
453-8Essentra Components


Product
Brand
Articles
Tools