web counter

DC Bias Characteristic of a Capacitor: Why MLCC Capacitance Drops Under Voltage

Published: 28 July 2022 | Last Updated: 03 July 202613071
A multilayer ceramic capacitor (MLCC) marked 10 uF does not always behave like 10 uF on a live rail. Put a working DC voltage across many ceramic parts and the usable capacitance falls, sometimes dramatically. Engineers who size decoupling, bulk, and filter capacitors from the nameplate value alone can end up with a smaller reservoir, more ripple, and a filter that no longer sits where the math said it would. This guide explains the characteristic, its physics, the capacitor types it affects, how to read a derating curve, and how to design around it.
This video explains the influence of an applied voltage on ceramic filter capacitors of a LC-filter with two different filter boards.

#askLorandt explains: Influence of DC-Bias on Ceramic Filter Capacitors

MLCC <a href='https://www.utmel.com/blog/categories/capacitors'><strong>capacitor</strong></a> marked 10 uF showing reduced effective capacitance under <a href='https://www.utmel.com/blog/categories/capacitors/what-is-the-dc-bias-characteristic-of-a-capacitor'><strong>DC bias</strong></a> on a live voltage rail..png

An MLCC’s marked capacitance is measured under benign test conditions, but its effective capacitance can drop significantly once DC voltage is applied.

Catalog

What the DC Bias Characteristic Is

The DC bias characteristic describes how the capacitance of a ceramic capacitor changes as a steady DC voltage is applied across its terminals. As that bias voltage rises toward the rated voltage, the effective capacitance of a Class II ceramic part drops below its marked value. The part is not faulty and nothing has broken; this is a normal, measurable, and reversible property of the dielectric material.

The reason the nameplate and the operating value diverge comes down to how parts are measured. A capacitor is characterized at a small AC test signal with little or no DC bias applied, which is the value printed on the reel and in the part number. Your circuit, by contrast, holds the capacitor at a real operating voltage. Once that bias is present, the measured AC capacitance the circuit actually sees can be substantially lower than the catalog figure. The gap is widest for high-capacitance-density parts operating near their rated voltage, and it is the single most common reason a ceramic capacitor underperforms expectations.

The practical takeaway is simple: treat the marked value as a starting point measured under benign conditions, not as the capacitance delivered on a biased rail. The real number for a specific part comes from that part's derating curve.

The Mechanism: Ferroelectric Class II Dielectrics Under Field

Class II ceramic dielectrics are built on ferroelectric materials, typically barium-titanate-based ceramics chosen because they pack an enormous amount of capacitance into a small volume. That high permittivity is exactly what makes them sensitive to bias. In a ferroelectric material the effective permittivity is not constant; it depends on the strength of the internal electric field. As applied voltage drives the field higher, the dielectric domains become progressively harder to polarize further, the effective permittivity falls, and capacitance falls with it.

Field strength, not voltage alone, is what the dielectric responds to. Field is voltage divided by the thickness of each dielectric layer, so two parts at the same applied voltage can experience very different fields depending on how their layers are built. This is why the mechanism and the cure are linked: anything that lowers the field for a given working voltage softens the loss.

Cross-section of a <a href='https://www.utmel.com/blog/categories/capacitors/what-are-the-types-and-dielectric-of-ceramic-capacitors'><strong>multilayer ceramic capacitor</strong></a> showing thinner dielectric layers creating higher electric field and stronger DC bias capacitance loss..png

DC-bias loss is driven by electric field inside the dielectric, so thinner high-density MLCC layers can lose more capacitance at the same applied voltage.

Crucially, the effect is reversible. When the bias is reduced, the permittivity rises again and the capacitance recovers. Nothing is permanently consumed; the dielectric simply delivers less capacitance while it is held under field. That distinguishes DC-bias loss from aging, which is a slow, separate drift discussed later.

Why thinner, higher-density parts derate harder

The race for ever-smaller, higher-value MLCCs is won by making the internal dielectric layers thinner and stacking more of them. Thinner layers raise capacitance density, but for the same working voltage they also raise the field across each layer, which is precisely the condition that drives more loss. As a result, two parts with the same marked capacitance and rated voltage can derate quite differently if one achieves its value in a smaller case with thinner layers. The manufacturer curve for the exact ordering part is the only reliable way to see how far that trade has been pushed.

Class I vs Class II: C0G/NP0 Barely Moves While X7R, X5R, and Y5V Drop

Ceramic dielectrics split into two families with very different bias behavior. Class I dielectrics, of which C0G (also labeled NP0) is the best known, are paraelectric and essentially linear. Their permittivity barely changes with field, so they are stable under DC bias and over temperature. The trade-off is low capacitance density: a C0G part is physically large for its value.

Class II dielectrics such as X7R, X5R, and Y5V are the ferroelectric, high-density materials described above. They offer far more capacitance per unit volume but trade that for sensitivity to both bias and temperature. The sensitivity broadly increases as you move from X7R toward Y5V; the more aggressively a dielectric chases capacitance density, the more it tends to give up under field and heat.

The design cue follows directly from the table. When the application needs a value that must hold steady, such as a timing network, a precision RC filter, or a resonant tank, Class I earns its larger footprint. When the job is bulk decoupling and the budget is board area, Class II is the practical choice, provided the bias loss is accounted for rather than ignored.

Where DC Bias Loss Bites: Decoupling, DC-DC Output, and RC Filters

The loss matters wherever a design depends on a capacitor actually holding its rated value while biased. Three places show it most clearly.

In decoupling and bulk energy storage, the effective capacitance on the rail can sit well under the nameplate, which means the charge reservoir buffering load transients is smaller than the schematic implies. A bank sized purely from marked values may sag more than expected during current spikes.

On a DC-DC converter output, lower effective output capacitance raises output ripple and can shift the control loop's behavior, because the compensation was likely designed around an assumed output capacitance. Less capacitance than planned can erode phase margin and degrade transient response.

In RC and signal filters, capacitance sets the cutoff frequency. If the real biased capacitance is lower than the marked value, the corner frequency moves upward, so a filter intended to roll off at one frequency rolls off higher. The direction is always the same: less effective capacitance pushes the filter toward letting more through. The size of the shift depends entirely on the specific part and its operating point, which is why the next step is reading the curve rather than assuming a figure.

How to Read a DC-Bias Derating Curve

Every Class II MLCC series that matters comes with a DC-bias derating curve, and reading it is straightforward once you know the layout. The horizontal axis is the applied DC voltage, sometimes shown as an absolute voltage and sometimes as a percentage of rated voltage. The vertical axis is the change in capacitance, usually as a percentage relative to the value at zero bias.

To use it, enter the curve at your circuit's operating voltage on the horizontal axis, read up to the line for your exact part, and read across to the capacitance change. That value, applied to the marked capacitance, is the bias-derated capacitance you should design with. The curve is specific to the part: case size, rated voltage, and dielectric all change its shape, so a curve for one ordering code does not transfer to another even at the same nominal value.

For numbers you can trust, the most reliable route is the manufacturer's own characteristic viewer or simulation tool, where you select the exact part and the tool plots effective capacitance versus bias for that device. Murata's SimSurfing and the KEMET/YAGEO K-SIM tool both do this. Pull the curve for your exact ordering part and read the value at your real rail voltage.

DC bias derating curve showing how to read effective capacitance from operating voltage for an MLCC capacitor..png

To estimate usable capacitance, read the manufacturer’s DC-bias curve at the circuit’s real operating voltage, then apply the percentage loss to the marked value.

Stacking the Deratings: Bias Plus Temperature, Aging, and Tolerance

DC bias is only one of several effects that reduce real capacitance, and worst-case design has to combine them rather than treat bias in isolation. Temperature changes the capacitance of Class II parts according to their temperature characteristic. Aging causes Class II ceramics to lose capacitance slowly over time as the crystal structure relaxes after manufacture, a drift that resets if the part is heated above its Curie point and then begins again. Initial tolerance sets how far the part can start from its nominal value before any of these effects apply.

The effective capacitance your circuit can rely on is the marked value reduced by all of these together at the relevant operating point, not by bias alone. A part that looks comfortable on the bias curve can still fall short once temperature, aging, and tolerance are stacked on top.

FactorDirection of effectReversible?Where to find the number
DC biasReduces capacitance as voltage risesYes, recovers when bias fallsPart-specific DC-bias derating curve
TemperatureShifts capacitance per the temperature codeYes, follows temperatureTemperature characteristic curve for the series
AgingSlow downward drift over timeResets only by heating above Curie pointAging rate in the series datasheet
Initial toleranceSets starting spread around nominalFixed at manufactureTolerance code in the part number

The practical workflow is to read the bias-derated value from the curve, then layer on the temperature characteristic for your operating range, the aging loss over the design life, and the tolerance band, to land on a defensible worst-case effective capacitance.

Mitigation: Case Size, Rated Voltage, Dielectric, and More Devices

DC-bias loss cannot be eliminated from Class II parts, but several levers reduce it, each with a trade-off worth weighing against board area and cost in space.

A larger case size for the same value generally derates less, because the dielectric layers can be thicker and the field per layer lower at the same voltage. A higher rated-voltage part moves the operating point further down its own curve, so the percentage of rated voltage in use is smaller and the loss is gentler. Switching to a lower-k dielectric or to Class I (C0G/NP0) trades density for stability and largely sidesteps the problem where the value is small enough to be practical. Finally, placing more devices in parallel raises the combined effective capacitance and rebuilds the margin lost to bias.

OptionWhy it helpsTrade-off
Larger case sizeThicker layers lower the field for the same voltageConsumes more board area
Higher rated voltageOperating point sits lower on the derating curveOften larger and lower density for the value
Lower-k or Class I dielectricFar less bias sensitivity, stable valueMuch lower capacitance density
More devices in parallelRebuilds effective-capacitance marginMore placements and board space

The exact gain from any of these is part-specific, so confirm the improvement on the candidate part's curve or tool rather than assuming a fixed benefit. The same nominal value in a different case size or voltage rating can behave very differently under bias, which is exactly the lever these options exploit.

Frequently Asked Questions

Does C0G/NP0 also lose capacitance under DC bias?
Effectively no. Class I dielectrics like C0G/NP0 are paraelectric and nearly linear, so their capacitance is stable under bias. That stability is the reason to choose them for timing and precision filters, at the cost of much lower capacitance density.

Why does my circuit simulator not show this capacitance loss?
A standard simulator treats a capacitor as an ideal component with a fixed value and does not model the dielectric's bias dependence. To see the real behavior, use a manufacturer characteristic viewer or simulation tool that includes the part's measured DC-bias data, such as Murata SimSurfing or KEMET K-SIM.

Does choosing a higher voltage rating eliminate the problem?
It reduces it but does not remove it. A higher-rated part operates at a smaller fraction of its rated voltage, which places it lower on the derating curve, so the loss is gentler. The part is usually larger or lower density for the same value, and you should still confirm the result on its curve.

Is a larger case size always better for DC-bias performance?
For the same value and dielectric, a larger case generally derates less because the layers can be thicker and the field lower. It is not free, since it costs board area, and the actual difference depends on the specific parts, so compare their curves before deciding.

How much capacitance do I actually lose at my operating voltage?
That depends entirely on the exact part, its case size, rated voltage, and dielectric. There is no universal figure to apply. Read the loss from the manufacturer's derating curve for your ordering part at your operating voltage, or plot it in the manufacturer's tool.

Is the loss permanent, or does the capacitance come back?
It is reversible. The capacitance falls only while the bias is applied and recovers when the voltage is reduced. This is distinct from aging, which is a slow, separate drift over time.

Does the DC bias characteristic apply to film, tantalum, or aluminum electrolytic capacitors?
The strong voltage-dependent loss described here is a property of Class II ceramic dielectrics. Film capacitors are very stable with bias, and tantalum and aluminum electrolytics have their own voltage and frequency behaviors that differ from this ferroelectric mechanism, so do not assume a ceramic curve applies to them.

How can I confirm the effective capacitance for my rail before finalizing the design?
Find the derating curve or open the manufacturer tool for the exact part, enter the operating voltage to get the bias-derated value, then combine that with the temperature characteristic for your range, the aging loss over life, and the initial tolerance to reach a worst-case effective capacitance.

Sources and Further Reading

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. What is the definition of DC bias voltage?

The DC bias voltage refers to the voltage that should be set between the base-emitter and the collector-base when the transistor is in the amplifying state in the transistor amplifier circuit.

2. What is the relationship between ceramic capacitor capacity and DC bias voltage?

The capacitance of Y5V dielectric ceramic capacitors varies greatly with the DC bias voltage. When the capacitance decreases from 100% of the unbiased capacitance to the DC bias voltage under the rated voltage, the percentage of the rated capacitance cannot be obtained. Twenty-five, that is to say, the capacitance of 10μF is only less than 2.5μF at rated voltage. At high temperature, since the capacitance has dropped to a very low level, the capacitance at this time does not change much with the DC bias voltage.
Although the capacitance of X7R dielectric ceramic capacitors varies greatly with DC bias voltage, it is much better than Y5V.

3. What is bias voltage what is forward bias voltage?

Considering the voltage as the coordinate axis, there is no offset when Y=0,
The voltage is greater than 0 volts, and Y is positive, called forward bias.
Voltage is less than 0 volts, and Y is negative, called reverse bias.
Related Articles

  • AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    AI Server MLCCs: Why NVIDIA Rubin Racks Require Over 600,000 Capacitors
    UTMEL02 June 20263604

    Next-generation AI servers like NVIDIA's Rubin architecture require over 600,000 MLCCs per rack due to extreme power densities exceeding 120kW. This transition from GB300 demands high-capacitance, low-ESR capacitors with X7R/X7S dielectrics to handle intense transient responses and thermal loads, forcing procurement teams to navigate extended 24-week lead times for these specialized components.

    Read More
  • MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    MLCC vs Polymer Tantalum Capacitors: Overcoming 2026 Shortages in AI Server PDNs
    UTMEL07 August 2026776

    Facing 2026 MLCC lead times of up to 24 weeks driven by AI server demand, hardware engineers are substituting multi-layer ceramic capacitors with conductive polymer tantalum capacitors. While Class II MLCCs suffer severe DC bias capacitance loss and acoustic noise, polymer tantalums offer voltage stability and low ESR. Implementing a division-of-labor strategy—using polymer tantalums for bulk decoupling and MLCCs for point-of-load—optimizes PDN performance and bypasses supply bottlenecks.

    Read More
  • Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    Sourcing Silicon Capacitors and MLCCs in the AI Hardware Era
    UTMEL13 August 2026651

    Modern AI hardware requires a hybrid Power Delivery Network (PDN) to maintain low-voltage stability under extreme transient currents. Deep Trench Silicon Capacitors (DTCs) integrate directly into advanced packages to deliver ultra-low ESL and stable performance for high-frequency transient suppression. Meanwhile, Multilayer Ceramic Capacitors (MLCCs) provide essential bulk energy storage on the motherboard, making both technologies complementary across the AI power stack.

    Read More
  • MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    MLCC DC Bias Derating: How to Calculate and Compare Effective Capacitance Before Component Selection
    UTMEL11 September 2026661

    Class II ceramic capacitors suffer significant capacitance loss under DC voltage due to ferroelectric domain saturation and high electric field intensity. This comprehensive engineering guide explains how to calculate true worst-case effective capacitance by compounding DC bias, temperature, tolerance, and aging. It provides multi-vendor simulation workflows, benchtop impedance measurement techniques, and practical guidelines to maintain power supply stability and avoid costly design failures.

    Read More
  • Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments
    UTMEL13 July 2026434

    Explore how the transition from traditional air-cooling to liquid cooling (direct-to-chip and immersion) in high-density AI server racks alters component thermal profiles. Focus on why design engineers are increasingly specifying Class 2 MLCCs (X7R and X7S dielectrics) over standard X5R variants to prevent thermal degradation near the liquid cooling microchannels. Explain how these capacitors mitigate acoustic noise and voltage bias degradation under heavy workloads. Provide sourcing advice for high-reliability passives via UTMEL during this high-demand memory and passive component super-cycle.

    Read More

Subscribe to Utmel !

Featured Parts More