web counter

Understanding the Flight Sensing Modules of Drones

Published: 06 September 2021 | Last Updated: 06 September 20212269
Body movement state sensing, surrounding environment state sensing of drones, and ways to improve measurement accuracy are introduced in the article.
Let's learn the complete flight dynamics of the drones in this video.

Drones | The complete flight dynamics

 

Topics covered in this article:

Purposes of the flight sensing technology of drones

Body movement sensing modules

Surrounding environment sensing modules

Ways to improve measurement accuracy

 

Purposes of the flight sensing technology of drones

The flight sensing modules of drones are mainly used for two purposes. One is to provide the flight control system. Since the main function of the flight control system is to control the drone to reach the desired attitude and spatial position, this part of the sensing technology mainly measures state-related physical quantities. The modules involved include gyroscopes, accelerometers, magnetic compasses, barometers, GNSS modules, and optical flow modules.

the drone.jpg

the drone

Another purpose is to provide autonomous navigation systems for drones, that is, path and obstacle avoidance planning systems. So it needs to perceive the state of the surrounding environment, such as the location of obstacles. Related modules include ranging modules, object detection, and tracking modules, etc...

Body movement sensing modules

Gyroscopes

At present, MEMS technology gyroscopes are commonly used in commercial drones because of their small size and low price. They can be packaged in the form of ICs. MEMS gyroscopes are used to measure the angular rate of the body rotating around its own axis. Commonly used models are 6050A (Invensense) and ADXRS290 (ADI). The indicators for measuring gyroscope performance include measurement range, sensitivity, and stability (drift) and the signal-to-noise ratio, and so on.

the test results of the temperature drift of the gyroscope.jpg

test results of the temperature drift of the gyroscope

The above is a graph of the test results of the temperature drift of the gyroscope. The test environment is heated from 25°C to 50°C. The gyroscope is kept still during the whole process, and the accurate output of the gyroscope should be a fixed value. But judging from the results, the actual output of the two sensors is affected by temperature changes. In comparison, the output value of ADXRS290 (ADI) has a small change range, basically around 0.5.

Accelerometer

The accelerometer measures the linear acceleration of the body's motion. Due to the gravity of the earth, the measured value will also include the gravitational acceleration component, which needs to be subtracted in some use cases. Commonly used MEMS accelerometer sensor models are 6050A (Invensense) and ADXL350 (ADI). In order to improve chip integration, some sensor manufacturers package gyroscopes and accelerometers together, called six-axis sensors, such as 6050A (Invensense).

Magnetic compass

The physical quantity measured by the magnetic compass is the component of the earth's magnetic field strength along the axis of the airframe, and the heading angle of the airframe is calculated based on this. Commonly used MEMS magnetic compass sensor models are HMC5983L (Honeywell) and QMC5883L (Silicon Core), both of which have similar performance. The former has been discontinued. The main performance parameters of the magnetic compass include sensitivity, stability (drift), etc.

Barometer

The physical quantity measured by the barometer is the atmospheric pressure value, from which the absolute altitude can be calculated. Commonly used barometer sensor models include MS5611 (MEAS), MS5607 (MEAS), and BMP180 (Bosch) [check this product's detail]. The problem with the barometer is that when flying near the ground, the "ground effect" will cause the air pressure distribution around the aircraft to be different from the atmosphere at rest, making it impossible to use the barometer to measure altitude. The usual solution is to use other sensors during takeoff or landing, such as ultrasonic sensors or laser rangefinders.

GNSS module

The physical quantities measured by the GNSS module are relatively rich, mainly including geographic coordinates (latitude and longitude), altitude, linear velocity, and heading angle (RTK system). Commonly used GNSS module manufacturers include U-BLOX of Switzerland and NOVATEL of Canada. When using the GNSS module, the placement of the satellite signal receiving antenna needs to avoid the shielding of electromagnetic interference. Some powerful complete machine manufacturers will customize the satellite signal receiving antenna according to the aircraft model.

Optical flow module

The optical flow module is a special module that can be used to sense the motion state of the body, such as measuring the displacement speed in the horizontal direction, or it can be used to sense the surrounding environment for obstacle avoidance purposes. The more common optical flow module is the open-source PX4FLOW. Optical flow modules are usually used indoors, mainly to solve the problem of poor indoor satellite signals. In addition, a certain texture pattern is required for the ground to be photographed.

Surrounding environment sensing modules

Ranging module

Here are five commonly used ranging modules: ultrasonic, infrared TOF, lidar, millimeter-wave radar sensor, and depth-sensing camera. 


Ultrasonic measurementInfrared ToFLaser measurementDepth-sensing cameraMillimeter-wave radar
Measurement distanceshortshortlongmediumlong
Measurement accuracyhighhighhighlowlow
Anti-interferenceweakweakweakweakstrong
Module volumesmallsmalllargemediumlarge

Ultrasonic and infrared TOF have similar performance in all aspects. For example, the measurement distance is relatively close. The distance for ultrasonic measurement is generally about 4 meters. In addition, the use range of these two sensors is easily limited by the actual environment. For example, infrared TOF emits red light to the surface of the measured object and reflects it. If it encounters an object with low red light reflectivity like glass, it will fail. But these two kinds of sensors have one of the biggest advantages of low cost, and the module size is relatively small, so they have been widely used in consumer drones.

The measurement distance of lidar ranging is far enough. Most products can reach more than 100 meters, but the weather environment of heavy rain and fog will affect its measurement results. Another disadvantage is that the cost is relatively high: Velodyne is the strongest in the lidar industry. Its VLP-16, a miniaturized product suitable for drones, has also reached a price of more than $1,000. The cost is still relatively high.

Depth-sensing cameras can be divided into three types according to measurement technology. ①Stereo cameras are also called binocular vision technology. The representative product of this technology is DJI's Wizard 4. ②Structured light technology. It represents Microsof’s Kinect. ③ Time of flight technology (TOF). Because there are fewer manufacturers and higher costs, there are few applications on UAVs.

Depth-sensing cameras also have limitations when used. The disadvantage of binocular vision technology is that it cannot work normally in low-light environments, while structured light technology, on the contrary, cannot work normally under strong light. Therefore, some manufacturers combine the two technologies to make up for each other's shortcomings and expand the scope of their applicable environment.

Ways to improve measurement accuracy

Sensor calibration

Sensor calibration, including fine calibration and rough calibration. The fine calibration is better, but it requires expensive calibration equipment; the rough calibration does not need to rely on external equipment, only the sensor itself can be operated.

Taking the rough calibration of a magnetic compass as an example, since the geomagnetic field intensity at any position on the earth can be regarded as constant over a long time span when the magnetic compass is rotated, it can be assumed that the magnetic compass is fixed according to the relative motion. The geomagnetic field vector rotates accordingly, and the trajectory of the vector endpoint in space should be a standard sphere. However, due to the error of the sensor, the actual measured data is not strictly on the surface of the sphere. At this time, it needs to be based on the measured data. The numerical value and the known accurate value are used to calculate the conversion relationship between the two, which is the error model of the magnetic compass. When using this magnetic compass in the future, the measured value can be processed according to the error model obtained from the rough calibration, so that the error of the measured value is reduced.

Magnetic compass calibration (SGB sbgcenter).jpg

Magnetic compass calibration (SGB sbgcenter)

Multiple sensor data fusion

There are many different types of sensor data fusion methods. The most common method used in the industry is EKF, which is the extended Kalman filter.

Taking the fusion method of calculating the aircraft attitude angle as an example, the EKF update process is mainly divided into two parts, prediction update and measurement update. The forecast update mainly uses the gyroscope to update the forecast state quantity, and at the same time calculates the covariance matrix of the state quantity. In the measurement update, the filter gain is calculated first, and then the filter gain is used to fuse the data of the predicted state quantity, accelerometer, and magnetic compass to become a fusion state quantity. At the same time, the covariance matrix of the fusion state quantity is calculated, which will be calculated in the next update cycle.

 Fusion method flow for calculating attitude angle.jpg

Fusion method flow for calculating attitude angle

Sensor redundancy design

The sensor redundancy design mainly combines multiple sensors of the same type. The processing method is to first remove the sensors with abnormal data, and then perform sensor fusion. The redundant design can not only improve the measurement accuracy but also improve the reliability of the entire system. When a certain sensor fails, the entire system can continue to work normally.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.How Many Sensors are in a Drone, And What do they Do?

Accelerometers.

Inertial Measurement Units.

Tilt Sensors

Current Sensors.

Magnetic Sensors.

Engine Intake Flow Sensors.

2.What is flight control module in drones?

The flight controller is the brain of a drone. A small box filled with intelligent electronics and software, which monitors and controls everything the drone does. And just like the brains of different organisms, flight controllers also vary in sizes and complexity.

3.What are the different types of drones?

Single-Rotor Drones.

Multi-Rotor Drones.

Fixed-Wing Drones.

Fixed-Wing Hybrid Drones.

Small Drones.

Micro Drones.

Tactical Drones.

Reconnaissance Drones.
Related Articles

  • The Key Role of Electronic Components in IoT Devices
    The Key Role of Electronic Components in IoT Devices
    UTMEL01 September 20236514

    The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.

    Read More
  • Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    UTMEL25 June 20261505

    A practical accelerometer sensor guide covering working principles, MEMS and piezoelectric types, datasheet specifications, circuit design, mounting, applications, and selection.

    Read More
  • 2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    UTMEL18 July 20261618

    Automotive cleanroom assembly integrating advanced driver assistance systems. The automotive industry faces a structural semiconductor deficit in 2026, driven not by pandemic-era demand shocks but by AI data centers absorbing global foundry capacity on legacy nodes (40nm-90nm) where 95% of automotive-grade components are manufactured. Video demonstrations of these systems show a "machine view" overlay with red crosshairs tracking pedestrian movement and sudden cut-ins before traditional collision thresholds are triggered.

    Read More
  • Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    UTMEL21 August 2026950

    This guide compares Hall effect, AMR, and TMR magnetic sensors for position detection in motor control and robotics. It explains their physical principles, key performance metrics, and selection criteria. Hall effect suits low-cost commutation, AMR offers high-speed angle sensing, and TMR provides maximum precision and low power, with practical integration advice.

    Read More
  • Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    UTMEL17 August 2026802

    This comprehensive selection guide compares thermocouples, platinum RTDs, and semiconductor ICs across measurement range, accuracy limits, and signal conditioning complexity. It covers fundamental operating physics, mathematical transfer functions, lead-wire compensation topologies, and power budgets. Engineers will find practical design checklists, benchtop multimeter diagnostic techniques, and an architectural decision workflow to optimize system performance and bill-of-materials cost.

    Read More

Subscribe to Utmel !

Featured Parts More