web counter

What is IMU: Definition, Features and Prospects

Published: 12 April 2022 | Last Updated: 12 April 20224390
Hello everyone, I am Rose. Today I want to introduce IMU to you. IMU (Inertial Measurement Unit), the inertial measurement unit, is used to measure the three-axis attitude angle (or angular rate) and acceleration of the object.
This video will show you what is inertial measurement unit.

Intro to Inertial Measurement Units (IMU)

Topics covered in this article:
Ⅰ. IMU technology
Ⅱ. Features of Inertial Navigation Technology
Ⅲ. The Development Prospect of Inertial Navigation Technology
Ⅳ. Points to note
Ⅴ. How to avoid major difficulties caused by IMU offline?


As autonomous driving technology becomes more popular, related technologies are evolving at a rapid pace. By leaps and bounds, several high-precision positioning, sensing, and other technologies have been developed. IMU  technology, for example, is a rising star among them. The development of this technology compensates for the lack of GPS location, and the two work together to provide the most accurate positional information to autonomous vehicles.

In reality, ignore the IMU  technology, which appears to be quite new. In reality, IMU  is used in our everyday phones, vehicles, planes, and even rockets and spaceships that we utilize when traveling. The cost and accuracy are the key differences.、

 

Ⅰ. IMU technology

When driving a car on unfamiliar roads and following GPS  or Beidou navigation instructions, the navigation system can still offer us driving data such as direction, speed, mileage, time, and other driving data when passing the tunnel. How does the navigation system work? We're astounded at the signal reception that isn't connected to the satellite system. Inertial measuring technology keeps us moving in this way.

The inertial measurement unit (IMU) is a device that consists of three single-axis accelerometers and three single-axis gyroscopes. After processing these data in relation to the navigation coordinate system's angular velocity signal, the object's attitude can be computed.

Figure. 1.jpg

Figure. 1

It's worth mentioning that the IMU only offers relative positioning information; its purpose is to measure the journey relative to the beginning point object, not your precise location. As a result, it's frequently used in conjunction with GPS,  When the GPS signal is weak in some areas, the IMU can step in and help the car maintain absolute position information so it doesn't "get lost."

Inertial technology is a method of controlling the trajectory and attitude of moving objects. Inertial instruments, inertial stabilization, inertial systems, inertial guidance, and inertial measurement are all examples of related technology. Physics, mathematics, mechanics, optics, materials science, confidential mechanics, electronic technology, computer technology, control technology, measurement technology, simulation technology, manufacturing and process technology, and so on are all covered by inertial technology. It's a technology that spans multiple disciplines. Inertial devices and systems are widely employed in aviation, aerospace, land navigation and geodetic mapping, drilling and tunneling, geological research, robotics, vehicles, medical equipment, and other fields, as well as cameras. In mobile phones, toys, and other fields, sensitive objects' motion posture and trajectory, location, and orientation are all critical.

Modern precision navigation, guiding, and control systems rely on inertial technology as their primary source of data. In the process of implementing the composite development of military equipment mechanization and informatization, inertial technology plays an indispensable supporting role in the establishment of a five-dimensional integrated information system of land, sea, air, space, and electricity (magnetic).

Figure. 2.gif

Figure. 2

 

Ⅱ. Features of Inertial Navigation Technology

In comparison to other navigation systems, the inertial navigation system has important features like comprehensive information, complete autonomy, high concealment, real-time and continuous information, and is not limited by time, geography, or human interference (see Table 1), and can be used in the air, water, underground, and other environments.

The inertial system is used in missile, rocket, airplane, and other carriers' navigation, guidance, and control (GNC) systems that need maneuvering and high-speed operation due to its measurement frequency bandwidth and high data frequency (up to hundreds of hertz or more). For example, pure inertial guidance surface-to-surface missiles have a short measurement delay (less than 1 ms), are easy to digitalize and have become the core information source for  GNC  systems to achieve fast and precise guidance and control, and their performance plays a key role in guidance accuracy. The accuracy of the inertial system is responsible for more than 70% of hit accuracy.

At the same time, inertial technology encourages the application of advanced control theories in engineering, such as optimal filtering technology. Inertial technology is the foundation for the realization of the functions of  GNC systems on various modern carriers, and it is a guided weapon. It is a critical national military technology strictly blocked by developed countries. Or the weapon platform's supporting critical technology.

Inertial technology is widely employed in civilian industries such as geodetic surveying, oil drilling, tunnel engineering, geological research, robotics, intelligent transportation, medical equipment, cameras, mobile phones, toys, and so on, in addition to military applications. As a result, inertial technology can be used in any situation requiring real-time sensitivity or monitoring of object motion information.

The fundamental downside of inertial navigation systems is that they acquire navigation mistakes over time and are rather expensive. Researchers have expressed concern about the future prospects of inertial navigation technology as competing navigation technologies, particularly satellite navigation systems such as GPS.  mature and become more commonly utilized.

However, the emergence of electronic warfare, navigation warfare, and systematic combat modes in several high-tech local wars have demonstrated that almost only inertial navigation systems can work continuously and stably in extremely harsh environments with strong electromagnetic interference, bolstering the inertial system's irreplaceable position in weapons and equipment.

 

Ⅲ. The Development Prospect of Inertial Navigation Technology

1. Development prospects of inertial sensors

In terms of the current state of development, existing inertial sensors are capable of meeting the precision requirements of a variety of current navigation activities. In the future, the key goal is to minimize the device's cost, volume/weight, and power consumption, which includes the following aspects:

①Materials and methods: Inertial sensors are made using low-labor-intensive production models and batch processing technologies, as well as novel materials such as silicon wafers, quartz, or optoelectronic materials (such as lithium niobate).

② Cost: includes the purchase price of the product as well as the costs of operation and maintenance. The cost of inertial sensors is falling drastically as a result of mass production.

③ Volume: Inertial measurement sensors are continually improving in terms of light weight, miniaturization, and miniaturization; certain new inertial sensors, such as  NEMS  (Nano-Electro-Mechanical System) and optical NEMS, will not be visible to the naked eye in the future.

④hotspots for research: On the one hand, it focuses on improving the performance and packing of miniaturized MEMS  inertial devices, while on the other, it focuses on optical sensors, particularly FOG with integrated optics research.

⑤ Expectation: Inertial sensors of all levels of precision are small and affordable. The development and deployment of inertial navigation systems are directly influenced by the development and application of inertial sensors. Inertial sensors' cost, volume, and power consumption have an impact on the characteristics of inertial navigation systems. As a result, when developing inertial measurement sensors, the following variables must be considered: accuracy, consistency, dependability, cost, volume/weight, and power consumption.

2. The development direction of inertial navigation technology

The following are the most important things to consider when designing and developing inertial navigation systems: (1) It must be directed at and fit the needs of the application, with navigation performance (particularly accuracy) and price cost being the two fundamental characteristics indicators. The price comprises the system's original cost, as well as maintenance and service life costs. As a result, a fair price is still at the top of the application requirements for many navigation applications. Navigation performance encompasses navigation accuracy, continuity, integrity, and simplicity of use (which refers to the system's ease of use and maintenance, as well as its autonomy). ②The most difficult difficulty is the real application environment. The inertial navigation system's size, power consumption, dependability, and availability will all influence whether it can be employed in a certain application scenario. ③ Expand the application field of the inertial navigation system by increasing its adaptability.

The development and technological progress of inertial navigation systems present the following characteristics:

(1) High-performance autonomous  INS  still serves an indispensable role in applications that cannot receive  GNSS  signals or require high navigation reliability.

(2) Due to the rapid advancement and development of  GNSS technology, some old  INS application domains will be phased out. Raytheon Anschütz, for example, created a GPS compass that uses GPS and solid-state rate sensors to attain a heading accuracy of 0.5°. (RMS). Under the conditions of a 1m baseline, the GPS attitude measuring apparatus developed by Shanghai Jiao Tong University's  Institute of Navigation, Guidance, and Control can achieve a 2-D attitude measurement accuracy of greater than 0.2°.

(3) The use of INS in conjunction with other navigational aids, particularly the GNSS/INS integrated navigation system, has gotten a lot of attention.

(4) Civil markets, such as ground vehicle navigation, are quickly developing, and low-cost integrated, miniaturized, and multi-mode integrated navigation equipment have emerged as three key market development directions. The development of inertial navigation systems is both an opportunity and a challenge.

(5) For the ship navigation system's design and development: (1) In order to increase the system's performance and reliability, the inertial navigation system's integration degree must be continually improved; it must also provide a flexible interface with the ship's other operational controls or navigation equipment.

②Second, many academics strive to employ low- and medium-precision inertial measurement sensors or MEMS devices to achieve adequate accuracy index H by refining the navigation system's configuration and combining it with other navigation methods in order to reduce system cost. ③ It's worth noting that INS is first merged with GNSS, and then with other navigation systems like sonar and pictures to produce a ship-integrated integrated navigation system, which is the most hotly debated research topic and development path.

In summary, compact and inexpensive MEMS inertial sensors, as well as high-precision, high-performance FOG, will continue to be the center of attention in inertial device research in the future. The platform-based navigation system will be replaced by the strap-down inertial navigation system, which will be influenced by the rapid growth of current computer technology.

 

Ⅳ. Points to note

Check to see if the power supply is stable. The IMU  may be disconnected if the power supply voltage fluctuates significantly.

Ensure physical safety; on-field collisions/projectile hits may cause the IMU  to shift or drop.

Check the gyroscope range; if the hit creates a large angular velocity outside of the gyroscope range, gimbal offset may occur.

Ensure that the line is connected and that the communication connection is in good working order, especially if the hardware solution requires rather long traces.

Temperature has an impact on IMU,  If you wish to move the robot outside in the winter, keep in mind that certain insulating measures must be taken (such as heating resistors)

 

Ⅴ. How to avoid major difficulties caused by IMU offline?

After detecting that the  IMU is offline, prepare a motor closed-loop solution and switch to motor encoder feedback automatically or manually.

Mount many IMUs on the gimbal, and when one goes offline, swap the feedback source to another.

It is less risky to use the  IMU incorporated on the official development board/self-developed development board than it is to use a standalone IMU module.

Inertial technology has evolved into one of the most important symbols of a country's advanced technological level, and its advanced level and application level are linked to the level of informatization and automated control of many industries in the country. Inertial technology is currently evolving in the directions of downsizing, digitalization, intelligence, low cost, high reliability, and multi-field applications, and new applications and products are being developed at a rapid pace. The application domains of inertial technology will continue to increase in the future as the national economy and technological level develop.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. What does IMU mean?

IMU refers to Inertial Measurement Unit. IMUs are mostly used in devices that require motion control, such as cars and robots. It is also used in occasions where precise displacement estimation with attitude is required, such as inertial navigation equipment for submarines, aircraft, missiles and spacecraft.

2. In SLAM, what is the role of the IMU unit?

IMU is only a sensor of SLAM, and it needs to be combined with other sensors to get better results, such as IMU+camera, IMU+GPS, etc.

3. What does an IMU inertial measurement unit consist of?

The IMU inertial measurement unit is composed of a three-axis gyroscope and a three-axis accelerometer, which is used to measure and output the three-axis angular rate and three-axis acceleration of the carrier, and can measure the speed and position information of the carrier.
Related Articles

  • The Key Role of Electronic Components in IoT Devices
    The Key Role of Electronic Components in IoT Devices
    UTMEL01 September 20236305

    The article discusses the pivotal role of electronic components in Internet of Things (IoT) devices. IoT devices work by capturing real-world data using sensors, processing it through a microcontroller, and then sending it to the cloud for further analysis.

    Read More
  • Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    Accelerometer Sensors Guide: Working Principle, Circuit Design, Specifications, and Applications
    UTMEL25 June 20261134

    A practical accelerometer sensor guide covering working principles, MEMS and piezoelectric types, datasheet specifications, circuit design, mounting, applications, and selection.

    Read More
  • 2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    2026 ADAS Sensors: Supply Outlook and Alternative Sourcing
    UTMEL18 July 20261276

    Automotive cleanroom assembly integrating advanced driver assistance systems. The automotive industry faces a structural semiconductor deficit in 2026, driven not by pandemic-era demand shocks but by AI data centers absorbing global foundry capacity on legacy nodes (40nm-90nm) where 95% of automotive-grade components are manufactured. Video demonstrations of these systems show a "machine view" overlay with red crosshairs tracking pedestrian movement and sudden cut-ins before traditional collision thresholds are triggered.

    Read More
  • Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    Magnetic Sensors for Position Detection: Hall Effect vs. AMR vs. TMR Engineering Guide
    UTMEL21 August 2026660

    This guide compares Hall effect, AMR, and TMR magnetic sensors for position detection in motor control and robotics. It explains their physical principles, key performance metrics, and selection criteria. Hall effect suits low-cost commutation, AMR offers high-speed angle sensing, and TMR provides maximum precision and low power, with practical integration advice.

    Read More
  • Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    Temperature Sensor Types Comparison: Thermocouple, RTD, and Semiconductor IC Selection Guide
    UTMEL17 August 2026573

    This comprehensive selection guide compares thermocouples, platinum RTDs, and semiconductor ICs across measurement range, accuracy limits, and signal conditioning complexity. It covers fundamental operating physics, mathematical transfer functions, lead-wire compensation topologies, and power budgets. Engineers will find practical design checklists, benchtop multimeter diagnostic techniques, and an architectural decision workflow to optimize system performance and bill-of-materials cost.

    Read More

Subscribe to Utmel !

Featured Parts More