web counter

2SC458 Silicon NPN Transistor: Datasheet pdf, Equivalent and Pinout

UTMEL

Published: 01 December 2021 | Last Updated: 01 December 2021

4976

2SC458

2SC458

HITACHI LTD

2SC458 datasheet pdf and Unclassified product details from HITACHI LTD stock available at Utmel

Purchase Guide

The 2SC458 transistor is an NPN BJT transistor with a TO-92 packaging. This article will mainly cover pinout, equivalents, datasheet pdf, features, and other details about the 2SC458 transistor.

This video demonstrates the 2SC458 HITACHI MARZAP300 TRANSISTORES.

2SC458 HITACHI MARZAP300 TRANSISTORES MULTI COMERCIAL PRE PHONO AMILSOM

What is 2SC458?

The 2SC458 transistor is an NPN BJT transistor with a TO-92 packaging. The transistor is designed for use in low-frequency amplifiers, but it can also be utilized in a wide range of other applications. Because the transistor's maximum collector current is 100mA, it can also be utilized to drive a 100mA load with a load voltage of less than 30V. The DC gain ranges from 100 to 500, with a maximum collector dissipation of 200mW. The transistor has a low noise figure of 4 to 10 dB, making it appropriate for a range of low-level audio and other signal amplification applications. Because the transistor's maximum transition frequency is 230MHz, it can be employed in a wide range of RF applications below that frequency.


2SC458 Pinout

2sc458 pinout.jpg

2SC458 Pinout

2SC458 Features

  • Collector-Emitter Volt (Vceo): 30V

  • Collector-Base Volt (Vcbo): 30V

  • Collector Current (Ic): 0.1A

  • hfe: 100-500 @ 2mA

  • Power Dissipation (Ptot): 200mW

  • Current-Gain-Bandwidth (ftotal): 230MHz

  • Type: NPN


Specifications

HITACHI LTD 2SC458 technical specifications, attributes, parameters and parts with similar specifications to HITACHI LTD 2SC458.
  • Type
    Parameter
  • Surface Mount

    having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.

    NO
  • Number of Terminals
    3
  • Operating Temperature (Max.)
    150°C
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e0
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Tin/Lead (Sn/Pb)
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    BOTTOM
  • Terminal Form

    Occurring at or forming the end of a series, succession, or the like; closing; concluding.

    THROUGH-HOLE
  • JESD-30 Code

    JESD-30 Code refers to a standardized descriptive designation system established by JEDEC for semiconductor-device packages. This system provides a systematic method for generating designators that convey essential information about the package's physical characteristics, such as size and shape, which aids in component identification and selection. By using JESD-30 codes, manufacturers and engineers can ensure consistency and clarity in the specification of semiconductor packages across various applications and industries.

    O-PBCY-T3
  • Qualification Status

    An indicator of formal certification of qualifications.

    Not Qualified
  • Configuration

    The parameter "Configuration" in electronic components refers to the specific arrangement or setup of the components within a circuit or system. It encompasses how individual elements are interconnected and their physical layout. Configuration can affect the functionality, performance, and efficiency of the electronic system, and may influence factors such as signal flow, impedance, and power distribution. Understanding the configuration is essential for design, troubleshooting, and optimizing electronic devices.

    Single
  • Polarity/Channel Type

    In electronic components, the parameter "Polarity/Channel Type" refers to the characteristic that determines the direction of current flow or the type of signal that can be accommodated by the component. For components like diodes and transistors, polarity indicates the direction in which current can flow through the component, such as forward bias or reverse bias for diodes. For components like MOSFETs or JFETs, the channel type refers to whether the component is an N-channel or P-channel device, which determines the type of charge carriers that carry current through the component. Understanding the polarity or channel type of a component is crucial for proper circuit design and ensuring that the component is connected correctly to achieve the desired functionality.

    NPN
  • JEDEC-95 Code

    JEDEC-95 Code is a standardized identification system used by the Joint Electron Device Engineering Council to categorize and describe semiconductor devices. This code provides a unique alphanumeric identifier for various memory components, ensuring consistency in documentation and communication across the electronics industry. The format includes information about the type, capacity, and technology of the device, facilitating easier specification and understanding for manufacturers and engineers.

    TO-92
  • Transition Frequency

    Transition Frequency in electronic components refers to the frequency at which a device can transition from one state to another, typically defining the upper limit of its operating frequency. It is a critical parameter in determining the speed and performance of active components like transistors and integrated circuits. This frequency is influenced by factors such as capacitance, resistance, and the inherent characteristics of the materials used in the component's construction. Understanding transition frequency is essential for optimizing circuit designs and ensuring reliable signal processing in various applications.

    230MHz
  • Power Dissipation-Max (Abs)

    Power Dissipation-Max (Abs) refers to the maximum amount of power that an electronic component can dissipate without undergoing thermal damage or degradation. This value is crucial for ensuring reliable operation, as exceeding it can result in overheating and failure. It is typically specified in watts and serves as a critical parameter for designers to determine proper heat management strategies in circuits. Properly managing the power dissipation is essential for the longevity and performance of electronic devices.

    0.2W
  • Collector Current-Max (IC)

    The parameter "Collector Current-Max (IC)" in electronic components refers to the maximum amount of current that can safely flow through the collector terminal of a transistor without causing damage to the component. It is an important specification that indicates the upper limit of current that the transistor can handle under normal operating conditions. Exceeding this maximum current rating can lead to overheating and potentially result in the failure of the transistor. Designers must ensure that the collector current does not exceed this specified limit to prevent damage to the component and ensure reliable operation of the circuit.

    0.1A
  • DC Current Gain-Min (hFE)

    The parameter "DC Current Gain-Min (hFE)" in electronic components refers to the minimum value of the DC current gain of a bipolar junction transistor (BJT). It is a measure of how much the transistor amplifies the input current to produce the output current. The hFE value indicates the ratio of the output current to the input current when the transistor is operating in the active region. A higher hFE value signifies a higher current gain and better amplification capabilities of the transistor. It is an important parameter to consider when designing and analyzing transistor circuits for various electronic applications.

    100
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    Non-RoHS Compliant
0 Similar Products Remaining

2SC458 Applications

  • Audio Preamplifier Circuits

  • Audio Amplifier Circuits

  • Audio Preamplifiers Stages

  • Driving or Switching Loads under 100mA

  • Amplification of any low gain signal

  • RF Circuits


2SC458 Equivalents

2SA1029, 2N3708, 2SC1815, 2SC2458, 2SC2960, 2SC3114, 2SC3198, 2SC3199, 2SC3330, 2SC3331, 2SC3382, 2SC3383, 2SC3916, 2SC3917, 2SC3918, 2SC3919, 2SC3920, 2SC3921, 2SC3922, 2SC3923


Where and How to use 2SC458

The 2SC458 can be utilized in a wide range of applications. When used as a switch, it can drive up to 100mA of current, which can be used to power relays, LEDs, ICs, high-power transistors, and many other components in your circuit. Other than that, it can be used to amplify extremely low gain signals to high gain with noise filtration, for example, it can be used to amplify very low gain audio to high gain, RF signals, and any other sort of low level or low gain signal.


2SC458 Dimensions

2SC458 dimensions.jpg

2SC458 Dimensions

2SC458 Manufacturer

The Hitachi Group, with about 335,000 workers globally, is a global leader in the Social Innovation Business. Hitachi provides solutions to clients in a wide variety of industries, including Power / Energy, Industry / Distribution / Water, Urban Development, and Finance / Government & Public / Healthcare, via collaborative development.


Frequently Asked Questions

What type is the 2SC458?

The 2sc458 is a silicon NPN transistor.

What is the complementary of 2SC458?

The PNP Complementary of 2SC458 is 2SA1029
2SC458

HITACHI LTD

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe