BNO080 Sensor: Datasheet, Pinout and Circuit
IMU ACCEL/GYRO/MAG I2C 32BIT
The BNO080 is a System in Package (SiP) that integrates a triaxial accelerometer, triaxial gyroscope, magnetometer, and a 32-bit ARM® Cortex™-M0+ microcontroller running Hillcrest’s SH-2 firmware. This article enforces datasheet, features, circuit, and other details about BNO080.

BNO080 or BNO085 with USB to Serial Cable
BNO080 Pinout


BNO080 Description
The BNO080 is a System in Package (SiP) that integrates a triaxial accelerometer, triaxial gyroscope, magnetometer, and a 32-bit ARM® Cortex™-M0+ microcontroller running Hillcrest’s SH-2 firmware. The BNO080 is integrated into a single 28 pin LGA 3.8mm x 5.2mm x 1.1mm package. It is compatible with Android and provides a turn-key sensor hub solution, eliminating the complexity and investment associated with a discrete design.
BNO080 Block Diagram

Specifications
- TypeParameter
- Factory Lead Time6 Weeks
- Mounting Type
The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.
Surface Mount - Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
28-TFLGA Module - Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
-40°C~85°C - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tape & Reel (TR) - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Output Type
The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.
I2C, SPI, UART - Sensor Type
In electronic components, the parameter "Sensor Type" refers to the specific type of sensor technology used in a particular component to detect and measure physical phenomena such as light, temperature, pressure, motion, or proximity. Different sensor types utilize various principles and mechanisms to convert the detected input into an electrical signal that can be processed by the electronic component. Common sensor types include photodiodes, thermistors, accelerometers, and proximity sensors, each designed for specific applications and environments. Understanding the sensor type is crucial for selecting the right component for a given task and ensuring accurate and reliable sensing capabilities in electronic systems.
Accelerometer, Gyroscope, Magnetometer, 9 Axis - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
BNO080 CAD Model
Symbol

Footprint

BNO080 Features
Motion Engine 9-Axis and 6-Axis Sensor Fusion: Provides raw, calibrated, and fused sensor orientation data with best in class accuracy and stability.
Application Based Fusion: Sensor fusion is tuned for the specific needs of AR, VR, and Robotics applications.
Intelligent Power Management: Manages sensor states to conserve power without sacrificing the quality of motion data.
Calibration: Support both Dynamic and Factory-Based calibration to deliver the highest performance.
Control via Ic, Spi, or Uart Interfaces: Freedom to optimize overall circuit design requirements.
Secondary Ic Interface: Allows attachment of additional environment sensors.
Always-On Capabilities: Includes software to enable low power, high accuracy step counter, and gesture recognition.
Android Compatible: Provides support for sensors defined in Android 5.x and 6.0, but can be used with any operating system.
BNO080 Operating Circuit

What can be BNO080 used for?
The BNO080 can be used in many applications, but is tuned specifically for use in Virtual Reality, Augmented Reality, and Robotics applications. The BNO080 provides a head tracking solution for head-mounted displays (HMD).
BNO085 vs. BNO080
The BNO080/BNO085 is the successor to the BNO070 and provides additional features and performance improvements. The BNO085 is an optimized version of the BNO080 that allows for the use of add-on libraries for use in VR controllers and other specialized applications.
BNO080 Breakout
The BNO080 was designed to be implemented in Android-based cellular phones to handle all the computations necessary for virtual reality goggles using only your phone. The sensor is quite powerful, and with power comes a complex interface.

BNO080 Package


BNO080 Manufacturer
CEVA TECHNOLOGIES - CEVA Technologies (NASDAQ: CEVA), is a leading global supplier of software, components, and intellectual property to enable the intelligent use of sensors in consumer electronics and IoT devices. For more than 10 years, Hillcrest Labs and Freespace? sensor processing technology has powered advanced motion controllers in a wide variety of products including Smart TVs, set-top boxes, PCs, and game consoles. Today, CEVA Hillcrest Labs products are used in the development of devices in virtual reality (VR), augmented reality (AR), robotics, TV, and motion remote control segments. Their proprietary and patented Freespace technology transforms human and machine movement into high-quality, application-ready information which enables developers and manufacturers to create everyday products that work with precision.
Datasheet PDF
- Datasheets :
What is BNO080?
The BNO08 is a 9-axis System in Package (SiP) that enables the rapid development of sensor-enabled Augmented Reality (AR), Virtual Reality (VR), Robotics, and IoT devices. The first such library provides additional advanced capabilities for use with VR controllers.
What can be BNO080 used for?
The BNO080 can be used in many applications, but is tuned specifically for use in Virtual Reality, Augmented Reality, and Robotics applications. The BNO080 provides a head tracking solution for head-mounted displays (HMD).
DS3232 RTC: Pinout, Datasheet and DS3232 vs. DS323128 March 20246015
RFP30N06LE Power MOSFET: Equivalent, Circuit, and Datasheet12 August 20216362
PC817 Photocoupler : Application, Pinout and Datasheet30 July 202117338
A Comprehensive Overview of the AD390 Digital to Analog Converter (DAC)06 March 2024323
1N5822 Schottky Diode: Pinout, Datasheet, and Applications06 August 20267995
74HC373 Octal D-type Transparent Latch: Datasheet pdf, Schematics and Pinout18 December 20218329
MIC2548 Programmable Current-Limit High-Side Switch: Pinout, Equivalent and Datasheet04 March 2022763
LM338K Voltage Regulator: Datasheet, Circuit, Alternatives16 September 20216183
Towards an Optoelectronic Chip That Mimics the Human Brain20 April 20221087
What is a Hard Disk Drive (HDD)?31 May 20216165
What is FIR Filter?24 September 202018755
GlobalFoundries Unveils $4 Billion Expansion in Singapore to Meet Rising Chip Demand13 September 20234190
What are Proximity Sensors?24 October 20259013
Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments13 July 2026486
Basic Introduction to Memristor12 January 202112943
What is an Encoder?20 October 20207749
Hillcrest Laboratories, Inc.
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools