web counter

How to Use MQ4 Gas Sensor?

UTMEL

Published: 10 November 2021 | Last Updated: 10 November 2021

11962

MQ-4

MQ-4

Zhengzhou Winsen Elec Tech

MQ-4 datasheet pdf and Unclassified product details from Zhengzhou Winsen Elec Tech stock available at Utmel

Purchase Guide

This MQ4 Gas Sensor module is useful for gas leakage detection. It is suitable for detecting Methane, Propane, Butane, and other combustible gas. The sensitivity of the sensor can be adjusted by a potentiometer. In this post, we will see an introduction to the MQ4 methane gas sensor, it's working, interfacing with Arduino, and applications.

This video demonstrates MQ4 methane gas detector.

Arduino, MQ4 methane gas detector

Overview of MQ4 Gas Sensor

The MQ4 methane gas sensor is a MOS (metal oxide semiconductor) type sensor that detects methane gas concentration in the air at home or in the workplace and gives an analog voltage output when read. The concentration range for sensing, in this case, is 300 pm – 10,000 ppm, which is suitable for detecting a leak.

The main component of this gas sensor is a detecting element made of aluminum oxide (Al2O3) ceramic covered with Tin dioxide (SnO2) and organized within a stainless-steel mesh.


MQ4 Gas Sensor Pinout

The pin configuration of the MQ4 methane gas sensor is shown below. 

MQ4..jpg

mq4 pin..jpg

MQ4 Pinout

Pin NameFunction
VCCPositive power supply   pin
GNDReference potential   pin
AOAnalog output pin. It generates a signal proportional to the intensity of methane.
DODigital Output pin.   It also produces a digital signal whose limit can be set using a   potentiometer.


MQ4 Gas Sensor Features

  • Good sensitivity to a wide range of combustible gas

  • High sensitivity to Natural gas

  • Stable and long life

  • Small sensitivity to alcohol, smoke

  • Fast response Stable and long life


MQ4 Gas Sensor Specifications

  • Power requirements: VCC - 5V±0.1

  • DO output: TTL digital 0 and 1 (0.1 and 5V)

  • AO output: 0.1-0 .3 V (relative to pollution), the maximum concentration of a voltage of about 4V

  • Detection Gas: Natural gas/Methane

  • Operating temperature: 14 to 122 °F (-10 to 50°C)

  • RH Related humidity less than 95%Rh

  • O2 Oxygen concentration is 21% (standard condition) - Oxygen concentration can affect sensitivity

  • Load resistance: 20KΩ

  • Sensing Resistance Rs: 10KΩ- 60KΩ (1000ppm CH4)

  • Preheat time:Over 24 hour

  • Detection Concentration: 200-10000ppm (Natural gas / Methane)

  • Interface: 1 TTL compatible input (HSW), 1 TTL compatible output (ALR)

  • Heater consumption: less than 750mw


Working Principle of MQ4 Gas Sensor

The power LED illuminates as soon as the module is turned on. The MQ-4 detects the presence of methane in the atmosphere. The sensor's analog pin then produces an analog signal proportional to the amount of CH4 in the air. An ADC microcontroller can be used to measure a sensor's analog output.

Most microcontrollers nowadays include an ADC peripheral that can be used to read the analog output of sensors like the MQ4. The methane gas sensor's analog output signal is read by the microcontroller, which then performs signal conditioning to transform the observed analog voltage into methane concentration in the air. When methane gas is detected, the digital pin turns HIGH and the built-in LED for the Digital output illuminates. This digital pin can also be used to control other operations using a microcontroller.

 


Digital Output of MQ4 Gas Sensor

When there is methane gas present, the D0 pin creates a high (equal to VCC) signal and a low (equivalent to about 0.1 V) signal. The trimmer pot on the circuit can be used to calibrate this "digital" output.

mq4 digital output circuit.jpg

MQ4 Digital Output Circuit

 

The D0 pin is connected to the Arduino's digital pin 2. The Arduino sketch below uses an interrupt to ensure that the MQ-4 is always detected first by the microcontroller.

mq4 arduino data.jpg

MQ4 Arduino Data


Analog Output of MQ4 Gas Sensor

  • Determining PPM Equation

    mq4 sensitivity curve.jpg

Sensitivity curve of the MQ-4

This graph, taken from the device datasheet, depicts the MQ-4's sensitivity to gases. It's especially sensitive to CH4, the molecular term for methane, as shown above. Propane and butane gases are not included in the curve, even though they are both known components of LPG (which is second to methane in this curve).

The graph depicts the relationship between RS/R0 and gas concentration in parts-per-million on a log-log scale (PPM). The ratio of sensor resistance at target gas (RS) to sensor resistance in clean air (R0) is RS/R0 (R0). As a result, knowing RS/R0 allows us to calculate the gas concentration in PPM.

 

To derive a formula, we take two points on this graph. Later on, we'll use this formula in our Arduino sketch.

When RS/R0 = 1 and PPM = 1000, the most evident point appears. When RS/R0 is around 0.58 and PPM = 5000, the second point is reached. The formula begins with:

 formula1.jpg

From the first point, we'll assign Y1 = 1, X1 = 1000, and from the second point, Y2 = 0.58, X2 = 5000. Substituting these values into the previous equation:

 formula 2.jpg

Changing Y to RS/R0 and X to PPM and solving for PPM:

 formula 3.jpg

 

  • Methane PPM Output Arduino Diagram

In the presence of methane, the sensor resistance is RS, while in clean air, the sensor resistance is R0. R0 would be the simplest to figure out of the two. Using an ohmmeter, we measure the resistance of electrodes 1-6 or 4-3.

mq4 arduino.jpg

MQ4 Arduino Diagram

 

As can be seen, Aout is connected to one of the electrodes and a resistor RL in parallel. This indicates that the electrode resistance generates a voltage divider with RL, resulting in the following voltage at Aout:

 mq4 ppm.jpg

The resistance of our target electrode, RS, fluctuates depending on the amount of methane present.

RL is an SMD resistor with the designation 102, by the way. This is equivalent to a 1k resistance.

So we apply this formula to get RS.

 


Equivalents for MQ4 Gas Sensor

MQ 214, MQ306A, MQ-5, MQ306A & MQ-2


Alternatives for MQ4 Gas Sensor

MQ2, 3, 4, 5, 6, 7, 8, 9, 131, 135, 136, 137, 138, 214, 216, 303A, 306A, 307A, 309A


MQ4 Gas Sensor Dimension

mq4 dimensions.jpg

MQ4 Gas Sensor Dimension

Frequently Asked Questions

What is the use of MQ-4 gas sensor?

MQ-4 gas sensor has a high sensitivity to Methane, also to Propane and Butane. The sensor could be used to detect different combustible gas, especially Methane, which is with low cost and suitable for different applications.

How does MQ-4 gas sensor work?

The MQ-4 works by sensing the methane concentration in the air. The analog pin of the sensor then generates an analog signal proportional to the amount of CH4 in the air. We can measure the analog output of a sensor with an ADC microcontroller.

What is the output of MQ4 sensor?

The MQ4 can detect natural gas concentrations anywhere from 200 to 10000 ppm. This sensor has selective digital or analog output capability which can be measured easily with SPDuino or any other microcontroller.

What is the range of MQ sensor?

The concentration sensing range of 300 ppm to 10,000 ppm is suitable for leak detection. For example, the sensor could detect if someone left a gas stove on but not lit. The sensor can operate at temperatures from -10 to 50°C and consumes less than 150 mA at 5 V.
MQ-4

Zhengzhou Winsen Elec Tech

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe