AD8367 500 MHz Variable Gain Amplifier: Datasheet, Pinout, and AGC Design Analysis

UTMEL

Published: 17 March 2026 | Last Updated: 17 March 2026

346

Amplifier

Explore the AD8367 45 dB Variable Gain Amplifier. Features 500 MHz bandwidth and X-AMP architecture for AGC loops. View specs and optimize your RF design today.

Executive Summary: What is the AD8367?

The AD8367 is a high-performance 45 dB variable gain amplifier (VGA) designed for linear-in-dB gain control in applications ranging from low frequencies up to 500 MHz. It utilizes Analog Devices’ proprietary X-AMP® architecture to provide precise gain scaling and high-speed operation.

  • Market Position: High-performance, industry-standard VGA for RF/IF signal chains.

  • Top Features: 45 dB dynamic range (-2.5 dB to +42.5 dB), 500 MHz bandwidth, and an integrated square-law detector for AGC loops.

  • Primary Audience: Ideal for RF design engineers, telecommunications infrastructure developers, and broadband equipment manufacturers.

  • Supply Status: Active; widely available through major electronics distributors.

1. Technical Specifications & Performance Analysis

The AD8367 is a dictionary-style example of a Variable Gain Amplifier (VGA) designed for IF (Intermediate Frequency) stages in wireless receivers.

1.1 Core Architecture (X-AMP)

{{SECTION_1_OVERVIEW}} The AD8367 is built on the X-AMP (Exponential Amplifier) architecture. Unlike traditional VGAs that vary the gain of the active stage, the X-AMP uses a precision 200 Ω passive resistive attenuator followed by a fixed-gain feedback amplifier. This ensures that the amplifier always operates with a constant bandwidth and high linearity across the majority of its control range.

1.2 Key Electrical Characteristics

Engineers must account for the following power and performance metrics during the BOM selection process:

  • Gain Range: Total of 45 dB (-2.5 dB to +42.5 dB).

  • Bandwidth: A robust 500 MHz (3 dB cutoff), making it suitable for high-speed data I/O and broadband access.

  • Operating Voltage: Single-supply operation from 2.7 V to 5.5 V, facilitating integration into both legacy 5V systems and modern low-power 3.3V rails.

  • Current Consumption: Typically 26 mA quiescent current, balancing performance with thermal efficiency.

  • Linearity: Output Third Order Intercept (OIP3) of +20 dBV at 100 MHz, ensuring minimal signal distortion in crowded spectrums.

1.3 Interfaces and Connectivity

The device features a "Linear-in-dB" control interface. The gain is controlled by an analog voltage applied to the GAIN pin, scaled at 20 mV/dB. It also includes a MODE pin that allows the user to toggle between "Gain Up" (positive slope) and "Gain Down" (negative slope) control, providing flexibility for different feedback loop polarities.


2. Pinout, Package, and Configuration

The AD8367's layout is optimized for high-frequency signal integrity, keeping input and output pins separated by ground pins to minimize crosstalk.

2.1 Pin Configuration Guide


  • VIN (Pin 13): Resistive ground-referenced input with a nominal 200 Ω impedance.

  • VOUT (Pin 5): High-speed output signal.

  • GAIN (Pin 11): Analog gain control input.

  • DETO (Pin 4): Output of the integrated square-law detector; used to drive the GAIN pin in AGC applications.

  • MODE (Pin 12): Sets the gain slope (High for positive, Low for negative).

  • VPOS / COMM: Power supply and ground pins.

2.2 Naming Convention & Ordering Codes

The most common ordering code is the AD8367ARUZ, where "ARU" designates the TSSOP package and "Z" indicates a RoHS-compliant (lead-free) part. Procurement managers should verify the suffix to ensure compatibility with automated pick-and-place moisture sensitivity levels (MSL).

2.3 Available Packages

Package TypeDimensionsCommon Use Case
TSSOP-144.4mm x 5.0mmStandard PCB assembly; compact footprint for base stations.

Note: The TSSOP-14 package is machine-assembly friendly but can be hand-soldered by experienced technicians using fine-tip irons or hot air stations.

3. Design & Integration Guide (For Engineers & Makers)

Pro Tip: Always use a solid ground plane. At 500 MHz, even a small parasitic inductance in the ground path can lead to instability.

3.1 Hardware Implementation

  • Bypass Capacitors: Use a combination of a 0.1 µF ceramic capacitor for low-frequency decoupling and a 100 pF capacitor placed as close as possible to the VPOS pin to filter high-frequency noise.

  • Input Matching: Since the input impedance is 200 Ω, matching networks (such as a 4:1 balun or LC network) may be required when interfacing with standard 50 μV RF systems.

  • Thermal Management: With a 26 mA draw at 5V, the device dissipates roughly 130 mW. While it does not usually require a dedicated heatsink, ensure sufficient copper area is connected to the COMM pins for heat dissipation.

3.2 Common Design Challenges

  • Issue: Noise Figure Degradation at Low Gain.

    • Fix: Because the X-AMP architecture attenuates the input before amplifying, the noise figure increases as gain decreases. To maintain a high SNR, place a Low-Noise Amplifier (LNA) before the AD8367.

  • Issue: Self-Excitation and Instability.

    • Fix: This often occurs near maximum control voltage. Ensure strict power supply decoupling and avoid long traces on the GAIN control line which can pick up stray EMI.

  • Issue: Cascading Gain Mismatch.

    • Fix: If +42.5 dB is too high for your second stage, use a fixed attenuator (e.g., 6 dB) between stages to keep the amplifiers within their linear operating regions.

4. Typical Applications & Use Cases

4.1 Real-World Example: Automatic Gain Control (AGC)

In a Cellular Base Station, the incoming signal strength varies wildly. The AD8367 is used as a "Complete IF AGC Amplifier." By connecting the DETO (Detector Output) pin back to the GAIN pin through a simple low-pass filter, the AD8367 automatically adjusts its gain to maintain a constant output power level, protecting the subsequent Analog-to-Digital Converter (ADC) from clipping.


5. Alternatives and Cross-Reference Guide

If the AD8367 is unavailable or does not meet specific requirements, consider these alternatives:

  • Direct Replacements (Analog Devices):

    • AD603: A classic VGA, though it has a lower bandwidth (90 MHz) compared to the AD8367.

    • AD8330: Offers a wider gain range and differential inputs, ideal for low-frequency applications.

  • Competitor Options (Texas Instruments):

    • VCA821: A wideband, voltage-controlled amplifier offering high bandwidth and similar gain-control characteristics.

    • LMH6515: A digital-controlled VGA if your design requires SPI/Parallel control instead of analog voltage.

6. Frequently Asked Questions (FAQ)

Q: What is the difference between AD8367 and AD603?A: The AD8367 supports up to 500 MHz and includes an integrated square-law detector, whereas the AD603 is limited to 90 MHz and requires external components for power detection.

Q: Can AD8367 be used in Automotive applications?A: While it is high-performance, check the specific "Automotive Qualified" status in the datasheet (typically denoted by a /V suffix) if your project requires AEC-Q100 compliance.

Q: Where can I find the datasheet and library files for AD8367?A: Detailed datasheets, S-parameters, and CAD symbols are available on the Analog Devices official website and major distributor portals like Mouser or Digi-Key.

Q: Is AD8367 suitable for battery-operated devices?A: Yes, its ability to operate down to 2.7 V and its relatively low 26 mA current draw make it suitable for portable RF test equipment.

Q: How do I program/configure the AD8367?A: The AD8367 is an analog-controlled device. You do not "program" it with code; instead, you provide a DC voltage between 0V and 1V to the GAIN pin to set the amplification level.

7. Resources

  • Evaluation Boards: AD8367-EVALZ

  • Software Tools: ADI DiffAmpCalc™ (for calculating signal chain performance)

  • Application Note: AN-620 (Detailed AGC loop design with the AD8367)


Specifications

Datasheet PDF

Download datasheets and manufacturer documentation for Analog Devices AD8367ARUZ-REEL7.
AD8367ARUZ-REEL7

Analog Devices

In Stock: 9000

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More