web counter

RG8 VS LMR400[FAQ]: Differentiate the differences between them.

UTMEL

Published: 24 April 2022 | Last Updated: 12 June 2024

23549

LMR-400

LMR-400

Amphenol Times Microwave Systems

COAXIAL CABLE, ANTENNA, RG8, 50 OHM, BCC

Purchase Guide

COAXIAL CABLE, ANTENNA, RG8, 50 OHM, BCC

RG8 and LMR400 all coax cables. This article is going to talk about the detailed information about RG8 and LMR400, and interpret the differences between them.

This video demonstrates detailed information about LMR400 and RG8, and interpret the differences between them.

PL259 install RG8 - LMR400 - RG213

Overview of LMR400

Times Microwave's LMR®-400 is designed for adaptability, low loss, RF shielding, and wearability. The LMR-400 has the narrowest bend radius of any cable of comparable size and performance due to its cable architecture. The cable has the lowest loss of any comparable cable. This cable offers 90 dB of RF shielding and is ideal for EMI-prone environments. The LMR-400 is suitable for both indoor and outdoor use. Use Times Microwave's LMR-400 cable for any application that necessitates a low-loss, conveniently routed RF cable (e.g. WLL, GPS, LMR, WLAN, WISP, WiMax, SCADA, Mobile Antennas). The LMR-400 cable can be used in place of an RG-8 cable.

Note: LMR® is a registered trademark of Times Microwave Systems.

Overview of RG8

Pasternack's RG8 product number refers to a flexible RG8 coax cable. The RG8 flexible coax cable from Pasternack is 50 Ohm and features a PE dielectric. Our RG8 coax has a PVC jacket with a thickness of 0.405. (NC). The shield count on RG8 coax is one, and the maximum frequency for this Pasternack wire is one GHz. At 1 GHz, the RG8 coax cable has an attenuation of 8 dB and a maximum power of 190 watts.

Over 40,000 RF, microwave, and millimeter-wave components are made up of Pasternack RG8 coax cables. RG8 cables and other RF components are available for same-day shipping anywhere in the world. Custom RF cable assemblies using RG8 or another coax can be built and shipped the same day as well.


RG8 VS LMR400 Features

LMR400 Features

  • Priced Per Foot

  • Cable Type: LMR-400

  • Impedance: 50 ohm

  • Center Conductor: Bare Copper Covered Aluminum (BCCAI)

  • Jacket: Polyethylene (PE)

  • Outer Diameter: .405 inch

  • Indoor/Outdoor Rated

  • Drop-in replacement for RG-8

  • Attenuation @ 900 MHz/100 ft: 3.9dB/100ft

  • Attenuation @ 2.4 GHz/100 ft: 6.65dB/100ft

  • Any application (e.g. WLL, GPS, LMR, WLAN, WISP, WiMax, SCADA, Mobile Antennas) requiring an easily routed, low loss RF cable

  • Max Continuous Length: 1000 FT

 

RG8 Features

  • Conductor: Bare Copper

  • Insulation: Solid Low-Density Polyethylene

  • Shielding: Bare Copper Shield

  • Jacket: PVC (contaminating) Type 1 per MIL-C-17

  • Jacket Color: Black

  • 12 AWG stranded copper center conductor

  • 95% bare copper braid shielding

  • PVC Jacket

  • 50 Ohm

  • UL Listed

  • Sold per ft.

  • Max Continuous Length: 1000 FT


RG8 VS LMR400 Applications

LMR400 Applications

  • Wireless communication systems

  • Drop-in replacement for RG8/9913 air-dielectric type cable

  • Short antenna

  • Feeder runs

  • Easily routed, low loss RF cable.

 

 

RG8 Applications

  • Carrying radio transmission signals

  • Audio control rooms

  • Radio stations

  • Connections for external radio antennas.


Comparison between the LMR400 and RG8 of Attentuation VS Frenquency

LMR400 Attentuation VS Frenquency.png

LMR400  Attentuation VS Frequency


RG8 Attentuation VS Frenquency.png

RG8 Attentuation VS Frequency

LMR400 VS RG8 Specifications

Generic NameLMR-400RG8
Flex TypeFlexibleFlexible
Impedance50 Ohm50 Ohm
Dielectric TypePE (F)PE
Velocity of Propagation85%66%
Jacket Diameter0.405 in0.405 in
Jacket MaterialPEPVC (NC)
No. of Shields21
Attenuation at 1 GHz.4.25 dB8 dB
Frequency, Max6 GHz1 GHz
Max Operating Temperature85 deg C80 deg C
Center Conductor TypeSolidStranded
Inner Conductor, Number of Strands17
Coax TypeCoaxCoax


Conclusion of LMR400 VS RG8

Although LMR400 cable has low loss, it is thicker and less flexible than RG58 or LMR240 cable, making it more difficult to work with. Meanwhile, the impedances of LMR400 and RG8 are both 50 Ohm. The major differences between the LMR400 and RG8 are the attenuation and frequency. The Attenuation at 1 GHz of LMR400 is 4.25 dB, while the Attenuation at 1 GHz of RG8 is 8 dB. Additionally, the maximum frequency of  LMR400 is 6 GHz, while the maximum frequency of RG8 is 1 GHz. What’s more, the maximum operating temperature of LMR400 is 85 deg C, while the maximum operating temperature of RG8 is 80 deg C. LMR-400 was designed to replace low-quality RG-8 wires because it offers greater flexibility, a simpler connection, and the lowest signal loss. In general, the LMR-400 can be utilized in any application where low signal loss is required.


LMR400 VS RG8 Datasheet

LMR400 Manufacturer

Times Microwave Systems is a pioneer in the development and manufacture of coaxial transmission lines. For military, aerospace, wireless communications, and industrial applications, they offer a wide range of RF and microwave transmission line solutions. In the industry, its engineering competence and range of manufacturing capabilities are well acknowledged. They can serve both specialist applications with extremely demanding performance requirements and high volume commercial applications at frequencies ranging from a few kHz to 110 GHz, thanks to production sites in the United States and China. Since 2009, Times Microwave Systems has had access to the resources of Amphenol, one of the world's largest makers of interconnect components. Amphenol Corporation is a manufacturer of electrical, electronic, and fiber-optic connectors, as well as connection systems and coaxial and specialized cable.


Popularity by Region

Frequently Asked Questions

Is LMR-400 the same as RG-58?

Although LMR400 cable has low loss, it is thicker and less flexible than RG58 or LMR240 cable, making it more difficult to work with. It comes in lengths ranging from 2' to 100' and is designed to be used with antennas and amplifiers that don't come with cabling.

What is LMR-400 cable used for?

LMR400 is designed as a drop-in replacement for RG8/9913 air-dielectric type cable and short antenna, feeder runs in wireless communication systems. It's also appropriate for applications that demand a low-loss, conveniently routed RF connection.

What is better than LMR400?

RG-8, RG 213, and RG 214 coaxial cables are the same physical size as LMR-400, but their attenuation is up to 40% higher and their RF shielding performance is much worse.

What is RG8 used for?

RG8 is a type of coaxial cable that can be used to transmit radio transmissions. They're mostly seen in audio control rooms, radio stations, or as radio antenna hookups.

Which is better RG8 vs RG-58?

RG8. RG8 is a thicker 50-ohm cable, with a 12 AWG wire gauge, than RG58, and can carry a stronger signal. It is mostly used for amateur radio transmissions. A variation known as RG8X is also available, which is thinner at 16 AWG but delivers equivalent signal quality.
LMR-400

Amphenol Times Microwave Systems

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More