LMR240 VS LMR400[Video]: Which one is better?

UTMEL

Published: 11 April 2022 | Last Updated: 12 June 2024

14437

LMR-400

LMR-400

Amphenol Times Microwave Systems

COAXIAL CABLE, ANTENNA, RG8, 50 OHM, BCC

Purchase Guide

COAXIAL CABLE, ANTENNA, RG8, 50 OHM, BCC

LMR240 and LMR400 all coax cables. This article is going to talk about the detailed information about LMR240 and LMR400, and interpret the differences between them.

This video demonstrates detailed information about LMR400 and LMR240, and interpret the differences between them.

Helium Hotspot Miner - LMR-240 & LMR-400 - MPD Digital - Lightning Arrester - 8 dbi antenna

Overview of LMR400

Times Microwave's LMR®-400 is designed for adaptability, low loss, RF shielding, and wearability. The LMR-400 has the narrowest bend radius of any cable of comparable size and performance due to its cable architecture. The cable has the lowest loss of any comparable cable. This cable offers 90 dB of RF shielding and is ideal for EMI-prone environments. The LMR-400 is suitable for both indoor and outdoor use. Use Times Microwave's LMR-400 cable for any application that necessitates a low-loss, conveniently routed RF cable (e.g. WLL, GPS, LMR, WLAN, WISP, WiMax, SCADA, Mobile Antennas). The LMR-400 cable can be used in place of an RG-8 cable.


LMR400 Coaxial Cable Structure Figure

LMR400 Coaxial Cable Structure Figure.png

LMR400 Chart.png

Overview of LMR-240

Pasternack's LMR-240 part number refers to a flexible LMR-240 coax cable. The 50 Ohm Pasternack LMR-240 flexible coax cable has a PE (F) dielectric. Our LMR-240 coax has a PE jacket with a thickness of 0.24. This Pasternack cable features a shield count of two, RF shielding of 90 dB, and a maximum frequency of 5.8 GHz. At 1 GHz, the attenuation of the LMR-240 coax cable is 8 dB.

Over 40,000 RF, microwave, and millimeter-wave components are made up of Pasternack LMR-240 coax cables. LMR-240 cables and other RF components are available for same-day shipping anywhere in the world. Custom RF cable assemblies made from LMR-240 or other types of coax can also be constructed and dispatched on the same day.


LMR240 Coaxial Cable Structure Figure

LMR240 Coaxial Cable Structure Figure.png

LMR240 Chart.png

LMR240 VS LMR400 Features

LMR400 Features

  • Priced Per Foot

  • Cable Type: LMR-400

  • Impedance: 50 ohm

  • Center Conductor: Bare Copper Covered Aluminum (BCCAI)

  • Jacket: Polyethylene (PE)

  • Outer Diameter: .405 inch

  • Indoor/Outdoor Rated

  • Drop-in replacement for RG-8

  • Attenuation @ 900 MHz/100 ft: 3.9dB/100ft

  • Attenuation @ 2.4 GHz/100 ft: 6.65dB/100ft

  • Any application (e.g. WLL, GPS, LMR, WLAN, WISP, WiMax, SCADA, Mobile Antennas) requiring an easily routed, low loss RF cable

  • Max Continuous Length: 1000 FT

 

LMR240 Features

  • Priced Per Foot

  • Cable Type: LMR-240

  • Impedance: 50 ohm

  • Center Conductor: Bare Copper (BC)

  • Jacket: Polyethylene (PE)

  • Outer Diameter: .240 inch

  • Indoor/Outdoor Rated

  • Drop-in replacement for RG-8X

  • Attenuation @ 900 MHz/100 ft: 7.6dB/100ft

  • Attenuation @ 2.4 GHz/100 ft: 12.1dB/100ft

  • Any application (e.g. WLL, GPS, LMR, WLAN, WISP, WiMax, SCADA, Mobile Antennas) requiring an easily routed, low loss RF cable

  • Max Continuous Length: 1000 FT


Comparison between LMR240 and LMR400 of Attenuation vs Frequency

LMR400 Attenuation vs Frequency.png

LMR400 Attenuation vs Frequency

LMR240 Attenuation vs Frequency.png

LMR240 Attenuation vs Frequency

LMR240 VS LMR400 Specifications

Product Code201-202201-402
SeriesLMR-240LMR-400
Inner ConductorSolid BCSolid BCCAI
Inner ConductorSolid BCSolid BCCAI
DielectricFoam PEFoam PE
Outer ConductorAluminum TapeAluminum Tape
Outer ConductorAluminum TapeAluminum Tape
Overall BraidTinned CopperTinned Copper
CableLMR-240LMR-400
Outer JacketPEPE
Dia Inner Conductor1.422.74
Dia Dielectric3.817.24
Dia Outer Conductor3.947.39
Dia Overall Braid4.528.13
Dia Over Jacket6.110.29
Max Frequency3116.2
Velocity8485
DC Breakdown15002500
Peak Power Rating5.616
Jacket Spark50008000
Capacitance79.478.4
Inductance0.20.2
Operating TempMinus 40 to Plus 85Minus 40 to Plus 85
Min Bending Radius19.125.4
Cable Weight0.050.1
Attenuation 30 MHz4.42.2
Attenuation 50 MHz5.72.9
Attenuation 150 MHz9.95
Attenuation 220 MHz126.1
Attenuation 450 MHz17.38.9
Attenuation 900 MHz24.812.8
Attenuation 1500 MHz32.416.8
Attenuation 1800 MHz35.618.6
Attenuation 2000 MHz37.719.6
Attenuation 2500 MHz42.422.2


Conclusion of LMR240 VS LMR400

LMR®240 is also a 50 Ohm impedance outdoor rated flexible low loss communications cable. It's developed for short feeder runs in applications like GPS, WLAN, and mobile antennas. The flexible communications coax LMR®400 has a 50 Ohm impedance.

LMR400 cable has a lower loss than LMR240 cable, but it is thicker and less flexible, making it more difficult to work with. It is available in lengths ranging from 2' to 100' and is intended for use with antennas and amplifiers that do not include wiring. Although LMR240 is half the size and has twice the attenuation loss of LMR400, the difference does not appear to be significant, and both appear to be the highest quality and lowest loss alternatives for marine coax. The DB (waterproof) version is also available. I'm leaning toward the LMR240 because of its smaller diameter, and I'd use a messenger line to run the wire up.


LMR400 VS LMR240 Datasheet

LMR400 Manufacturer

Times Microwave Systems is a pioneer in the development and manufacture of coaxial transmission lines. For military, aerospace, wireless communications, and industrial applications, they offer a wide range of RF and microwave transmission line solutions. In the industry, its engineering competence and range of manufacturing capabilities are well acknowledged. They can serve both specialist applications with extremely demanding performance requirements and high volume commercial applications at frequencies ranging from a few kHz to 110 GHz, thanks to production sites in the United States and China. Since 2009, Times Microwave Systems has had access to the resources of Amphenol, one of the world's largest makers of interconnect components. Amphenol Corporation is a manufacturer of electrical, electronic, and fiber-optic connectors, as well as connection systems and coaxial and specialized cable.


Note: LMR® is a registered trademark of Times Microwave Systems.


Popularity by Region

Frequently Asked Questions

What is LMR-240 cable?

The maximum operating frequency of the LMR-240 flexible 50 Ohm coax cable with PE jacket is 5.8 GHz. With a double shield count and RF shielding of 90 dB, this 50 Ohm 0.24 inch diameter and low-loss flexible coax cable is meant to last.

What is the difference between LMR 400 and LMR-240 RF cable?

LMR®240 is also a 50 Ohm impedance outdoor rated flexible low loss communications cable. It's developed for short feeder runs in applications like GPS, WLAN, and mobile antennas. The flexible communications coax LMR®400 has a 50 Ohm impedance.

What is LMR-400 cable used for?

In wireless communication systems, the LMR400 is designed to be a drop-in replacement for RG8/9913 air-dielectric type cable and short antenna, feeder runs. It's also suitable for applications that require a low-loss, easily routed RF link.

What is better than LMR400?

RG-8, RG 213, and RG 214 coaxial cables are the same physical size as LMR-400, but their attenuation is up to 40% higher and their RF shielding performance is much worse.
LMR-400

Amphenol Times Microwave Systems

In Stock: 5135

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More