web counter

Facial Recognition: Features, Working and Applications

Published: 02 September 2021 | Last Updated: 02 September 20219624
The broad sense of facial recognition includes a series of technologies for building a facial recognition system, including face image acquisition, face positioning, facial recognition preprocessing, identity confirmation, and identity search, etc… The narrow sense of facial recognition refers specifically to the adoption of the system for confirming or finding the identity of a human face.
Watch our video to learn how this biometric technology works.

How does facial recognition work?


Topics covered in this article:

What is facial recognition?

Features of facial recognition

Working process of facial recognition

Three key technologies of facial recognition

Products based on facial recognition

Controversies

 

What is facial recognition?

Face recognition is a type of biometric recognition technology that uses information about a person's facial features to identify them. This technology collects photos or video streams including human faces using a video camera or camera. It then automatically recognizes and tracks human faces in the images, performing a sequence of face-related technologies on the detected human faces. Traditional facial recognition is mainly based on visible light images, which is also a familiar recognition method. Simply put, it is a process of making the computer recognize you.

facial recognition.jpg

facial recognition

Features of facial recognition

The traditional facial recognition technology is mainly based on visible light image facial recognition, which is also the most familiar recognition method. It has a research and development history of more than 30 years. This system, however, has insurmountable flaws. When the ambient light changes, the recognition effect drops dramatically, leaving the system unable to achieve its requirements. Solutions to the lighting problem include three-dimensional image facial recognition and thermal imaging facial recognition. But these two technologies are far from mature, and the recognition effect is not satisfactory.

A rapidly developing solution is the multi-light source facial recognition technology based on active near-infrared images. It can overcome the influence of light changes and has achieved excellent recognition performance. The overall system performance in terms of accuracy, stability, and speed exceeds that of 3D image facial recognition. This technology has developed rapidly in the past two to three years, making facial recognition technology gradually practical.

The human face is innate like other biological characteristics of the human body (fingerprints, iris, etc.). Its uniqueness and good characteristics provide the necessary prerequisites for identity authentication.

Compared with other types of biometrics, facial recognition has the following characteristics:

Non-mandatory: The user does not need to specifically cooperate with the face acquisition equipment. It can obtain face images almost unconsciously.
Non-contact: Without making physical touch with the device, the user can obtain facial images.
Concurrency: In real-world circumstances, it is feasible to sort, judge, and recognize many faces.

Working process of facial recognition

The facial recognition system mainly includes four components, namely: face image acquisition and detection, face image preprocessing, face image feature extraction, and face image matching and recognition.

Face image collection and detection

Face image collection: The camera lens can collect different face images, such as static images, dynamic images, different positions, different expressions, etc… When the user enters the capture device's shooting range, the gadget will automatically look for and capture the user's face image.

Face detection: In practice, face detection is mainly used for preprocessing facial recognition, that is, to accurately calibrate the position and size of the face in the image. Histogram features, color features, template features, structural features, and Haar features are just a few of the pattern features in face photos. Face detection is the process of extracting usable information and putting it to use in order to detect faces.

face image feature.jpg

face image feature

The Adaboost learning algorithm is used in the standard face identification approach, which is based on the above attributes. The Adaboost algorithm is a classification method. It combines a number of weaker classification methods to create a new, more powerful classification approach.
The Adaboost method is used in the face identification process to select several rectangle characteristics (weak classifiers) that best depict the face. Then the weak classifier is constructed into a strong classifier according to the weighted voting method. And several strong classifiers obtained by training A cascade structure of stacked classifiers are connected in series to effectively improve the detection speed of the classifier.

Face image preprocessing

Face image preprocessing: It is based on the face detection result, and the image is treated before being used in the feature extraction process. Due to diverse situations and random interference, the system's original image is frequently not directly utilized. In the early stages of image processing, it must be pre-processed using grayscale correction and noise filtering. Light compensation, gray scale transformation, histogram equalization, normalization, geometric correction, filtering, and sharpening of the face picture are all part of the preprocessing process for face images.

Face image feature extraction

Face image feature extraction: The features that can be used in a facial recognition system are usually divided into visual features, pixel statistical features, face image transformation coefficient features, and face image algebra features. Facial feature extraction is based on certain features of the human face. Face feature extraction, also known as face representation, is the process of feature modeling of human faces. Two categories of methods of facial feature extraction: one is the representation method based on knowledge; the other is the representation method based on algebraic features or statistical learning.

Face image matching and recognition

Face image matching and recognition: The facial recognition system searches and matches the feature data of the extracted face image with the feature template stored in the database, and sets a threshold. The matching result is output when the similarity surpasses this threshold. The face features to be recognized are compared with the obtained face feature templates, and the identity information of the face is judged according to the degree of similarity. There are two steps in this procedure: confirmation and identification. Confirmation is a one-to-one picture comparison process, while identification is a one-to-many image matching and comparison process.

Three key technologies of facial recognition

Face detection based on features

It is performed by using color, contour, texture, structure, or histogram features.

Face detection based on template matching

The face template is extracted from the database, and then a certain template matching strategy is adopted to match the captured face image with the image extracted from the template library. The face size and position information are determined by the level of correlation and the size of the matched template.

Face detection based on statistics

Through a large collection of "face" and "non-face" images to form a positive and negative sample library of human faces, statistical methods are used to strengthen the training of the system, so as to realize the detection and classification of the patterns of human faces and non-human faces.

Products based on facial recognition

Digital camera

Face autofocus and smile shutter technology: The first is facial capture. It judges according to the position of the human head. First, the head is determined, and then the head features such as eyes and mouth are judged. Through the comparison of the feature library, the face is captured. Then autofocus with the face as the focus, which can greatly improve the clarity of the photos taken.

mobile phone 3D facial recognition.jpg

mobile phone 3D facial recognition

Smile shutter technology is based on face recognition to complete facial capture. It judges the degree of mouth bend and the degree of eye bend to judge whether it is a smile. All the above captures and comparisons are done under the condition of comparing the feature library. Therefore, the feature library is the basis, which contains various typical facial and smile feature data.

Access control system

The security-protected area can recognize the identity of the intruder through face recognition. Facial recognition technology can be utilized for security and management in both businesses and homes.

Face recognition access control

Face recognition access control is an access control product based on advanced face recognition technology, combined with mature ID card and fingerprint recognition technology. The product adopts a split design. It has the functions of collection of face, fingerprint, and ID card information, and biometric information recognition. The system adopts network information encryption transmission and supports remote control and management. It can be widely used in access control security control in key areas such as banks, the military, public security agencies, and intelligent buildings.

Identification

E-passport and ID card. The International Civil Aviation Organization has determined that from April 1, 2010, its 118 member countries and regions must use machine-readable passports. Face recognition technology is the first recognition mode. This regulation has become an international standard. The United States has required countries that have visa-free access agreements with it to use an electronic passport system that incorporates facial fingerprints and other biometrics before October 26, 2006. By the end of 2006, more than 50 countries had implemented such a system. The Transportation Security Administration plans to promote a biometric-based domestic travel document throughout the United States. Many countries in Europe are also planning or implementing similar programs to identify and manage passengers with biometric documents.

Face recognition can monitor people in public places such as airports, stadiums, and supermarkets. For example, surveillance systems can be installed at airports to prevent terrorists from boarding the plane. If the user's card and password are stolen from the bank's ATM, they will be taken by others as cash. At the same time, the application of face recognition will prevent this from happening. Find out whether there is the basic information of key populations in the database by querying the target portrait data. For example, install systems at airports or stations to catch fugitives.

Internet applications

Use face recognition to assist credit card network payment to prevent non-credit card owners from using credit cards, etc. Such as computer login, e-government, and e-commerce. In e-commerce, all transactions are completed online, and many approval procedures in e-government have also been moved online. At present, the authorization of transactions or approvals is achieved by passwords. Security cannot be assured if the password is taken. The digital identity and real identity of parties on the Internet can be unified if biometrics are employed. As a result, the reliability of e-commerce and e-government systems is considerably improved.

Entertainment applications

You'll find many applications of face recognition technologies in daily life, such as camera shooting, picture comparison, etc.

With the rise of the mobile Internet, some face recognition technology developers apply the technology to the entertainment field, such as applying happy celebrity faces. It is based on the contour, skin color, texture, texture, color, light, and other characteristics of the face to calculate the similarity between the protagonist and the celebrity in the photo.

Controversies

In the United States, facial recognition software has attracted criticism from privacy and civil rights organizations. For example, this technology has a low recognition rate for people of color. Republican and Democratic lawmakers in the United States called for supervision of this technology at the hearing, saying that the use of this technology may violate constitutional rights and legal procedures. For retailers, sometimes use facial recognition technology to filter customers, shut out those who are considered shoplifters, and instead give preferential treatment to those who spend money.

In 2021, more than 35 American civil rights organizations called on retailers to stop using facial recognition technology to screen shoppers. These civil rights organizations, including public citizens and the National Bar Association, joined the boycott and urged retailers such as Albertson and Macy's not to use facial recognition technology to screen employees and customers. The coalition of civil rights organizations said in a statement that this technology will be abused by retailers, leading to privacy issues. The alliance also stated that it plans to use social media to appeal to retailers who use these tools. The civil rights group "Fight for the Future" stated that this technology may facilitate the exclusion of low-income shoppers and the exploitation of workers.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.How does facial recognition work?

Facial recognition uses computer-generated filters to transform face images into numerical expressions that can be compared to determine their similarity. These filters are usually generated by using deep “learning,” which uses artificial neural networks to process data.

2.What can facial recognition detect?

Facial recognition is a way of identifying or confirming an individual's identity using their face. Facial recognition systems can be used to identify people in photos, videos, or in real-time. Facial recognition is a category of biometric security.

3.What is bad about facial recognition?

As with any technology, there are potential drawbacks to using facial recognition, such as threats to privacy, violations of rights and personal freedoms, potential data theft and other crimes. There's also the risk of errors due to flaws in the technology.
Related Articles

  • Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators
    Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators
    Saumitra Jagdale19 November 20243344

    There is a huge growth in demand for self-sustaining electronic devices, as the traditional power-generating devices fail in remote and harsh environments due to the periodic requirement of battery changes. Also, these devices are frequency specific; some work only in high frequency and some in low frequency. Triboelectric nanogenerators (TENGs) provide a promising solution by efficiently converting mechanical energy into electricity as they are versatile, compact, and cheap, making them a popular choice.

    Read More
  • Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy Generation
    Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy Generation
    Saumitra Jagdale19 November 20243179

    Presently, power companies are moving towards renewable energy systems. Conventional energy sources are more expensive because they require a vast network to be maintained and huge human resources. Also, they harm the environment by releasing several harmful gases. As the industry’s focus shifts toward renewable energy sources, energy systems powered by Proton Exchange Membrane Fuel Stacks (PEMFS) are gaining traction.

    Read More
  • VSC Light Meaning, Causes, and Step-by-Step Diagnostics
    VSC Light Meaning, Causes, and Step-by-Step Diagnostics
    UTMEL19 May 20264823

    A VSC (Vehicle Stability Control) light indicates the system is disabled, often as a fail-safe triggered by unrelated engine faults like a loose gas cap. While the stability system prevents lateral skidding, it shuts down when sensor data is unreliable. Proper diagnosis requires an ABS-capable OBD2 scanner. Resolving the root engine code, checking wheel speed sensors, or performing a zero-point calibration usually restores system function.

    Read More
  • What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component Buyers
    What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component Buyers
    UTMEL29 July 2026635

    ​Summary: When JEDEC published JEP203 and JEP204 on June 3, 2026[1], most coverage treated them as an announcement. They are better understood as the first shared language the silicon carbide industry has had for two problems that have quietly consumed engineering hours since the first commercial SiC MOSFETs shipped: short-circuit evaluation that produces numbers you can compare across suppliers, and a consolidated reference of stress procedures so qualification engineers stop reinventing test plans from scratch. This article explains what changes on Monday morning and what to ask suppliers for now.

    Read More
  • 2nm vs 3nm Chips: What the Latest Process Nodes Mean for Performance
    2nm vs 3nm Chips: What the Latest Process Nodes Mean for Performance
    UTMEL19 August 20262342

    The shift from 3nm to 2nm process nodes marks a fundamental change in transistor architecture, moving from FinFET to Gate-All-Around (GAA) nanosheets. This transition delivers meaningful improvements in performance, power, and density, but also introduces new challenges like SRAM scaling limits, thermal density, and backside power delivery. The article compares TSMC, Samsung, and Intel approaches, offering a practical decision framework for engineering teams.

    Read More

Subscribe to Utmel !

Featured Parts More