SR44 vs LR44 Which Battery Should You Use
You might wonder if you can swap SR44 and LR44 batteries. In most cases, you can use either one, but SR44 usually performs better. If you want longer battery life and stronger performance, choose SR44. For simple devices, LR44 can work, but it may not last as long. When you look at sr44 vs lr44, you see SR44 gives more value for demanding devices. Always check your device’s instructions before making a decision. The sr44 vs lr44 debate often comes down to your device’s needs, but SR44 wins for most users. Remember, sr44 vs lr44 is about picking the right battery for your situation.
SR44 vs LR44 Overview
SR44 Battery
You will find the SR44 battery in many precision devices. This button cell battery uses silver oxide as its main chemical component. The positive electrode contains silver oxide, and the negative electrode uses zinc. Potassium hydroxide acts as the electrolyte. This chemistry gives the SR44 a flat discharge curve, so your device gets steady voltage until the battery runs out. You can rely on the SR44 for high energy density and long-lasting power. Many people choose the SR44 battery for devices that need consistent performance, such as medical instruments and advanced calculators. The SR44 is also known as the 357 battery, and you may see it listed as an equivalent to other button cell models like AG13 or A76.
| Battery Type | Main Chemical Composition | Energy Density |
|---|---|---|
| LR44 | Alkaline: Zinc and Manganese Dioxide | Lower |
| SR44 | Silver Oxide | Higher |
LR44 Battery
The LR44 battery is an alkaline button cell. It uses manganese dioxide as the positive electrode and zinc as the negative electrode, with potassium hydroxide as the electrolyte. The LR44 battery has a sloping discharge curve, so the voltage drops as you use it. This makes it less ideal for devices that need stable voltage. However, the LR44 battery is more affordable and works well in low-drain devices. You will often see the LR44 in basic calculators, toys, and small LED lights. The LR44 is also called the 357 battery in some cases, and it serves as an equivalent for many button cell applications. The LR44 battery is popular because it is easy to find and cost-effective.
Common Uses
You will see both SR44 and LR44 batteries in many everyday devices. The SR44 battery is common in high-end watches, medical tools like blood glucose monitors, and scientific calculators. The LR44 battery fits well in digital watches, remote controls, and small flashlights. Both batteries are button cell types, and you may find them listed as equivalents for the 357 battery, AG13, or A76. The table below shows typical applications for each type:
| Battery Type | Common Applications in Consumer Electronics |
|---|---|
| SR44 (Silver Oxide) | High-end watches, medical instruments, advanced calculators, cameras, hearing aids, digital thermometers |
| LR44 (Alkaline) | Basic calculators, digital watches, toys, remote controls, small LED lights, digital thermometers |
Tip: When you buy SR44 batteries in bulk, you can save money. The chart below shows how the price per SR44 battery drops as you buy more units.
You should always check your device’s manual to see if it needs a specific type of button cell battery. The sr44 vs lr44 comparison matters most for devices that need steady voltage or long life. If you need a 357 battery or its equivalents, look at your device’s requirements before choosing between SR44 and LR44.
Key Differences
Chemistry & Voltage
You will notice that the main difference between the SR44 and LR44 batteries comes from their chemistry. The SR44 battery uses silver oxide chemistry, while the LR44 battery uses alkaline chemistry. This difference affects how each battery delivers power to your devices.
| Battery Type | Chemistry | Standard Nominal Voltage |
|---|---|---|
| LR44 | Alkaline | 1.5 V |
| SR44 | Silver Oxide | 1.55 V |
The SR44 battery provides a nominal voltage of 1.55 volts. The LR44 battery gives you a nominal voltage of 1.5 volts. This small difference in voltage output can make a big impact on sensitive devices. Silver oxide batteries like the SR44 keep their voltage output steady throughout most of their life. The LR44 battery starts at 1.5 volts, but its voltage output drops as you use it. You will see this difference in devices that need a constant voltage output, such as watches and medical tools.
Note: Major brands like Duracell and Energizer confirm these voltage ratings for both the SR44 and LR44 batteries.
Capacity & Lifespan
When you compare the SR44 and LR44 batteries, you should look at their capacity and how long they last. The SR44 battery usually has a capacity of around 150 mAh. The LR44 battery ranges from 90 to 150 mAh, depending on the brand and quality.
| Battery Type | Chemistry | Typical Capacity (mAh) | Voltage (V) |
|---|---|---|---|
| SR44 | Silver Oxide | Around 150 | 1.55 |
| LR44 | Alkaline | 90 to 150 | 1.5 |
Silver oxide batteries like the SR44 battery hold their charge longer when you store them. The self-discharge rate for the SR44 battery is lower than for the LR44 battery. This means you can keep an SR44 battery in storage for years and still expect it to work. The SR44 battery can last up to 5 years at room temperature, and sometimes even longer under perfect conditions. The LR44 battery does not last as long in storage because it loses its charge faster.
If you use a 357 battery in a device that sits unused for long periods, you will get better results with the SR44 battery. The longer shelf life and higher capacity of silver oxide batteries make them a better choice for devices you do not use every day.
Performance
You will see the biggest difference between the SR44 and LR44 batteries when you look at performance in real devices. The SR44 battery gives you a flat voltage output for most of its life. This means your device gets steady power until the battery is almost empty. The LR44 battery starts strong, but its voltage output drops as you use it. This can cause problems in devices that need a constant voltage output.
The SR44 battery works best in devices that need reliable, steady voltage output. These include watches, medical instruments, hearing aids, cameras, and precision tools.
The LR44 battery fits better in less demanding devices, such as toys, flashlights, and simple remote controls.
If you use an LR44 battery in a high-drain device, you may notice short battery life, corrosion, or even leakage. The 357 battery, when made with silver oxide chemistry, will outperform an alkaline 357 battery in every way. You should always pick the SR44 battery for devices that need consistent voltage output and long life.
Tip: If your device manual asks for a 357 battery, check if it needs silver oxide chemistry. Using the right battery will help your device last longer and work better.
Silver oxide batteries like the SR44 battery give you more stable voltage output, higher energy density, and longer lifespan. The LR44 battery is cheaper, but it cannot match the performance of the SR44 battery in demanding devices. For most precision electronics, the SR44 battery is the best choice.
Interchangeability
Device Compatibility
You might notice that SR44 and LR44 batteries look almost identical. Both fit in the same battery compartment and share the same size as the 357 battery. This physical similarity often leads you to believe that you can swap them without any problems. In many cases, you can use either battery as a replacement, especially for devices that do not require precise voltage or long-lasting power.
However, compatibility goes beyond just size. The chemistry inside each battery makes a big difference. The SR44 uses silver oxide, while the LR44 uses alkaline chemistry. The SR44 provides a steady 1.55V output, but the LR44 starts at 1.5V and drops as you use it. Devices that need stable voltage, like medical instruments, high-end watches, or scientific calculators, work best with the SR44 or a silver oxide 357 battery. If you use an LR44 in these devices, you may see performance issues or shorter battery life.
Tip: Always check your device’s manual or the battery compartment label. Manufacturers often list the recommended battery type, such as SR44, LR44, or 357. Following these guidelines helps you avoid compatibility problems.
Here is a quick guide to help you decide:
| Device Type | Recommended Battery | Reason for Recommendation |
|---|---|---|
| Precision instruments | SR44 / 357 | Needs stable voltage and longer life |
| Medical devices | SR44 / 357 | Requires reliability and steady output |
| High-end watches | SR44 / 357 | Demands consistent performance |
| Toys, remotes, LED lights | LR44 or SR44 / 357 | Less sensitive to voltage changes |
| Basic calculators | LR44 or SR44 / 357 | Can use either, but SR44 lasts longer |
You can use an SR44 as a replacement battery for an LR44 in most cases. The reverse is not always true. Some devices will not work properly if you use an LR44 instead of an SR44, especially if they need a constant voltage.
Risks
Swapping batteries without checking compatibility can cause several problems. Using the wrong battery type, such as putting an LR44 in a device that needs an SR44, can lead to:
Poor device performance or erratic behavior
Shorter battery life, especially in high-drain devices
Increased risk of leakage or corrosion, which can damage your device
Connectivity issues if the voltage or chemistry does not match
Voltage instability, which affects precision instruments and medical devices
You may also face problems if you use low-quality or counterfeit batteries. These can leak, rupture, or damage the internal parts of your device. Always buy batteries from trusted brands and check for the correct type, such as SR44, LR44, or 357.
Note: Using mismatched batteries, like substituting an LR44 for an SR44, increases the risk of leakage or rupture. This can harm your device and create safety hazards. Always make sure you use the correct battery type, brand, and polarity.
SR44 batteries provide a stable voltage and higher capacity, making them the best choice for devices that need reliable power. LR44 batteries work in less demanding devices but may cause voltage drops and reduced reliability in sensitive electronics. Substituting an SR44 for an LR44 is usually safe, but it may not be optimal for every device.
You should always follow the manufacturer’s recommendations for battery compatibility. This helps you avoid malfunctions and keeps your devices working their best. If you are unsure, choose the battery type listed in your device’s instructions or look for the 357 battery equivalent that matches your device’s needs.
Choosing the Right Battery
Device Needs
When you choose a replacement battery, you should always look at your device’s needs first. Some devices need a stable voltage, while others work well with a simple power source. If you use a 357 battery in a medical device, a luxury watch, or a scientific calculator, you want steady power. The sr44 battery gives you a stable 1.55V output, which helps these devices run smoothly. The lr44 battery works best in toys, basic calculators, and remote controls. These devices do not need a constant voltage, so the lr44 is a good fit.
You should also think about how often you use your device. If you use it every day, a longer-lasting replacement like the sr44 will save you time and money. If you only use your device sometimes, the lr44 can be a cost-effective replacement. Always check the size and fit to make sure the 357 battery or its equivalents match your device. Using the wrong size can cause poor connectivity or even damage.
Tip: Always use trusted brands for your replacement battery. This helps your device last longer and keeps it safe.
Quick Reference Table
You can use the table below to help you pick the right replacement for your device. It shows the main differences between lr44 and sr44 batteries, so you can see which one fits your needs.
| Criteria | LR44 (Alkaline) | SR44 (Silver Oxide) |
|---|---|---|
| Voltage | 1.5V, drops over time | 1.55V, stays stable |
| Lifespan | Shorter, 3-5 years shelf life | Longer, 5-10 years shelf life |
| Cost | Lower, good for low-drain devices | Higher, best for demanding devices |
| Performance | Good for toys, remotes, basic calculators | Best for watches, medical tools, precision devices |
| Replacement | Use for non-critical devices | Use for critical or high-drain devices |
| Compatibility | Check device manual for 357 or LR44 | Check device manual for 357 or SR44 |
Recommended Battery Choices by Device
Precision devices (watches, medical instruments, hearing aids, cameras): Choose sr44 or a silver oxide 357 battery for stable power.
General use (toys, basic calculators, remotes): Use lr44 or an alkaline 357 as a replacement battery.
Devices with frequent use: Pick sr44 for longer life.
Devices with occasional use: Lr44 can be a good replacement.
Note: Always check your device’s manual for compatibility before choosing a replacement battery. Using the correct 357 battery or its equivalent helps your device work its best.
LR44 and SR44 Equivalent Batteries
Other Names
You may notice that lr44 and sr44 batteries have many equivalent names. Manufacturers and retailers often use different codes for the same size and chemistry. This can make cross-referencing battery equivalents confusing if you do not know what to look for. The lr44 battery is an alkaline type, and you will see it listed as ag13, a76, 76A, LR1154, or L1154. These equivalents all share the same size and voltage output. The sr44 battery, which uses silver oxide chemistry, also goes by names like 357, 303, 157, and SR44SW. These silver oxide batteries match the lr44 in size but provide a more stable voltage output.
Here is a table to help you with cross-referencing:
| Battery Type | Chemistry | Nominal Voltage | Common Equivalent Names |
|---|---|---|---|
| LR44 | Alkaline | 1.5V | 76A, AG13, LR1154, A76, L1154 |
| SR44 / SR44SW | Silver Oxide | ~1.55V | 303, 357, 157 |
You will often see ag13 and a76 used for lr44 batteries in toys and remotes. The 357 and 303 codes appear on silver oxide batteries for watches and medical devices. Always check the packaging or your device manual for these equivalents before buying a replacement.
Tip: Cross-referencing battery equivalents helps you find the right replacement even if the code on your old battery looks different.
Chemistry Differences
You should understand the chemistry differences between lr44 and sr44 equivalents. The lr44 battery uses alkaline chemistry, which gives you a 1.5V voltage output that drops as the battery drains. Silver oxide batteries like sr44, 357, or 303 provide a steady 1.55V voltage output for most of their life. This makes silver oxide batteries better for devices that need constant power, such as watches or medical tools.
Here are some key points about chemistry and equivalents:
lr44, ag13, and a76 are all alkaline equivalents with the same size and voltage output.
sr44, 357, and 303 are silver oxide batteries. These equivalents offer more stable voltage output and longer life.
You can use lr44 equivalents in low-drain devices. For high-drain or precision devices, choose sr44 or other silver oxide equivalents.
Cross-referencing helps you avoid mistakes when buying replacements. Always match both the size and chemistry.
| Battery | Diameter | Thickness | Chemistry | Equivalent Names |
|---|---|---|---|---|
| LR44 | 11.6 mm | 5.4 mm | Alkaline | AG13, A76, 357, G13, LR1154 |
| SR44 | 11.6 mm | 5.4 mm | Silver Oxide | 303, 357, 157, SR44SW |
You can see that both lr44 and sr44 equivalents fit the same devices. The main difference comes from the chemistry and voltage output. If you want the best performance, use silver oxide batteries like sr44 or 357. For less demanding devices, lr44, ag13, or a76 equivalents work well.
Note: Cross-referencing battery equivalents is important. Always check both the code and chemistry to get the right replacement for your device.
You should choose SR44 batteries for devices that need steady power, like watches or medical tools. LR44 batteries work well in toys or remotes. Always check your device manual for the recommended battery type and use trusted brands for safety and performance.
Tip:
Store your batteries in a cool, dry place and keep them away from children. Remove batteries from unused devices to prevent leaks or damage.
FAQ
Can you use an LR44 battery instead of an SR44 battery?
You can use an LR44 battery in place of an SR44 battery for many devices. However, the SR44 battery gives you more stable voltage output and longer life. Always check your device’s manual for compatibility before making a replacement.
What are the main applications of SR44 batteries?
You will find SR44 batteries in watches, medical devices, cameras, and calculators. These devices need steady voltage output. The SR44 battery works well in precision electronics because it uses silver oxide chemistry.
Are LR44, AG13, and A76 batteries equivalent?
Yes, LR44, AG13, and A76 batteries are equivalent. They share the same size and voltage. You can use them as a replacement battery in many button cell devices. Always check for cross-referencing battery equivalents before buying.
How do you cross-reference button cell battery equivalents?
You should look at the battery code, chemistry, and voltage output. Cross-referencing battery equivalents helps you find the right replacement. For example, a 357 battery is a silver oxide equivalent to the SR44 battery.
What risks come with using the wrong button cell battery?
Using the wrong button cell battery can cause poor performance, short battery life, or even damage. Always check compatibility and use the correct replacement battery. Following cross-referencing guides helps you avoid mistakes.
Power Converter with Inbuilt Charging technology using WBG DevicesSaumitra Jagdale18 January 20242224Although plug-in electric vehicles (PEVs) have gained traction globally, reducing cost, weight, and volume, while enhancing power conversion efficiency in chargers remains crucial. PEVs, recognized by governments for curbing fossil fuel consumption and emissions, rely on sizable battery packs for substantial all-electric range coverage.
Read More
How to Choose the Best Deep Cycle Battery in 2024 | Reviews and Buying GuideUTMEL21 July 20252483You will learn about deep-cycle batteries in this post, including their main characteristics, things to think about while selecting one, and more.
Read More
CR123A vs 123A Batteries Explained for 2025UTMEL27 May 20252901CR123A and 123A batteries differ in capacity, lifespan, and compatibility. Learn how these differences affect your device's performance and safety.
Read More
A Guide to the Best AG13 Battery SubstitutesUTMEL27 May 20251792Discover the top AG13 battery equivalents for 2025, including LR44, SR44, 357, and A76. Compare performance, compatibility, and cost for your devices.
Read More
CR2450 vs CR2032 BatteriesUTMEL18 June 20252003CR2450 vs CR2032: CR2450 offers higher capacity and is larger, ideal for high-drain devices, while CR2032 suits compact, low-power gadgets. Learn more.
Read More
Subscribe to Utmel !
MS27484E16B8PCCorsair
934815330TE Connectivity
098371-0000ITT
D38999/24JC8PB-LCTE Connectivity
881545-1TE Connectivity AMP Connectors
5745781-4TE Connectivity AMP Connectors
65474-001LFAmphenol ICC (FCI)
![8225-6000]()
SNT-100-BK-T-HSamtec Inc.
S1731-46RHarwin Inc.


Product
Brand
Articles
Tools