web counter

Detailed Analysis of Analog IC

Published: 22 November 2021 | Last Updated: 22 November 20214209
This article introduces the main features of analog ICs, their working principle, product classification, market analysis, and the difference with digital ICs.
What Is the difference between analog and digital, and how do they work together to make modern life possible?

Analog vs. Digital As Fast As Possible

Catalog

Ⅰ What is an analog IC?

Ⅱ Working Principle of Analog IC

Ⅲ Types of analog IC products

Ⅳ Analog IC vs digital IC

Ⅴ Analog IC market analysis

 

Ⅰ What is an analog IC?

Analog signals are the source of all information. The physical environment in which we live is characterized by analog quantities, i.e., quantities that vary in a continuous manner rather than in a discrete way, such as temperature, position, light intensity, sound waves, color, texture, etc. These physical quantities are measured asymptotically without limits (e.g. "on and off", "small and large", "black"). When we use graphs to visually represent the values of these analog quantities, the curves become smooth (the most representative is the sine curve). These continuously varying analog quantities constitute the real world and transmit information to the outside world in the form of analog signals, and the integrated circuits used to process them are analog ICs.

Digital signals are the key to the electronic revolution. Although the real world is composed of colorful analog signals, experience has proven that in electrical systems, binary signals bring great convenience and extensibility to the storage, transmission, and processing of information. Therefore, in modern electronic systems, engineers use logic high voltage and logic low voltage (ground) to represent signals 1 and 0, thus converting the mathematical structure of binary into electronic systems, which is the digital signal. Digital signals are widely used in computing, storage, and other fields, and the integrated circuits used to process digital signals are digital ICs.

Interconversion of analog and digital signals.jpg

Interconversion of analog and digital signals

Ⅱ Working Principle of Analog IC

ICs are composed of transistors (including diodes and transistors) and other passive components, which compress complex functions into a small physical area through miniaturization, and communicate between micro devices and the macro world by means of integration, greatly enriching the portability and extensibility of electronic systems. The difference between analog and digital circuits is mainly reflected in the internal electronic devices, that is, the difference between analog and digital ICs in terms of transistors.

analog circuit and digital circuit.jpg

analog circuit and digital circuit

In analog IC, transistors are used to amplify or generate continuously changing signals (bias). When we bias a transistor, we create circuit conditions that allow it to respond correctly to small changes in voltage. Being able to continuously and accurately respond to and amplify analog signals is the main concern of analog ICs. The transistor in an analog IC can be a BJT (bipolar junction diode) or a MOSFET (metal-oxide-semiconductor field-effect transistor).

In digital ICs, the input signal is required to fully turn the transistor on and off, requiring only two values of external output logic high and low. Because of the need for frequent opening and closing, only MOSFETs can meet such performance, so BJTs are generally not applicable in digital ICs. Through complex MOSFET interconnections, Boolean logic-based gate circuits can form complex microprocessors or even general-purpose computing processor units.

Signals go through a process from analog to digital and back again in electronic systems, corresponding to the three stages of information input, processing and storage, and output. The signals from nature are transformed into electrical signals (analog) by sensors and discrete devices. The intermediary of the signal from input to processing to output is done by various analog devices (including digital-analog hybrid circuits). Finally, the analog chip processes the converted digital signal, and the digital IC (processor and memory, etc.) completes the final logic calculation, storage, and other functions.

Electronic systems consisting of semiconductor devices.jpg

Electronic systems consisting of semiconductor devices

Ⅲ Types of analog IC products

In the semiconductor industry, downstream products can be divided into OSDs (including sensors, discrete devices, optoelectronic devices, etc.) and integrated circuit ICs. Digital ICs mainly process digital signals, while discrete devices such as analog ICs and sensors process analog signals and convert them with digital signals.

Semiconductor Product Categories.jpg

Semiconductor Product Categories

According to the different functions (transmission of weak signals/strong electrical energy), we can generally divide analog IC devices into two categories: signal chain and power chain. The Signal chain mainly refers to the IC used to process signals, while the power chain is mainly used to manage the battery and electrical energy. The signal chain mainly includes comparators, operational amplifiers OPA, AD\DA, interface chips, etc.; the power chain mainly includes PMIC, ADC, DAC, PWM, LDO regulators, and driver ICs, etc. In the high-frequency signal part, RF devices are often discussed in a separate category due to the rapid technology iteration and high shipment volume.

Analog IC Product Categories.jpg

Analog IC Product Categories

Divided according to the application areas of downstream products, we can also divide analog IC products into System-Level IC SLIC and application-specific standard product ASSP. SLIC is used in different scenarios, the design performance parameters will not be specifically adapted to a certain type of application. By product type, SLIC generally includes five major categories, amplifier Amp in the signal link, signal converter ADC/DAC, general-purpose interface chip, comparators, and voltage regulators in the power supply chain.

ASSPs, on the other hand, are standardized according to dedicated application scenarios and generally integrate digital as well as analog ICs with a higher degree of complexity and integration, sometimes called mixed-signal ICs. Typical ASSP products include RF devices in cell phones, physical layer interface chips in switches, battery management chips and industrial power control chips, etc. ASSPs are generally divided into five categories according to downstream application scenarios, including automotive electronics, consumer electronics, computer, communication, and industrial markets.

Ⅳ Analog IC vs digital IC

Digital ICs are the core of the semiconductor industry, while analog ICs are the cornerstone of the semiconductor industry and the link between the real world and electronic systems. Due to the different types of signals that need to be processed, we can see that there are major differences between analog ICs and digital ICs in terms of the product life cycle, production process, design threshold, and related auxiliary tools.

Long product life cycle and slow iteration. Digital ICs emphasize the ratio of computing speed to cost. The core of Moore's Law is that designers pursue a more cost-effective computing rate, so new processes and new algorithms are emerging, and the life cycle is only 1-2 years. Analog ICs, on the contrary, emphasize a high signal-to-noise ratio, low distortion, low power consumption, and stability, so once the product is launched, it often has a longer life cycle, and the iteration cycle is longer, and the price will be reduced year by year.

The CMOS process has become the mainstream of digital ICs due to its complete development and shrinking process. However, analog ICs often require high voltage, low distortion, and high signal-to-noise ratio, and the CMOS process has poor drive capability, making it difficult to meet the needs of analog circuits.

Analog ICs early use Bipolar process, but the Bipolar process power consumption is high, so there is BiCMOS process, combining the advantages of both Bipolar process and CMOS process. There is also the CD process, which combines the CMOS process with the DMOS process. The BCD process combines the advantages of Bipolar, CMOS, and DMOS processes. In the high frequency field there are also SiGe and GaAS processes. These special processes need the cooperation of foundries and also need designers to be familiar with them, so most of the general analog IC factories still use the IDM model.

Close relationship with electronic components, design matching layout complex. Analog IC's low noise, low distortion needs in the design layout to consider the structure and components parameters match each other mode. Common resistive and capacitive sensing components can produce distortion, while in the digital IC design process, due to the binary characteristics, there is no need to consider the related impact. In the high-frequency range, the performance of certain RF ICs is also closely related to the wiring, so the designer of analog ICs needs to be familiar with most of the electronic component characteristics, and the design threshold is high.

Few auxiliary tools and high experience knowledge requirements. Since analog IC design requires familiarity with most of the component characteristics and different manufacturing packaging processes, which makes analog IC practitioners have a higher barrier to entry, and the accumulation of experience time is often more than 10 years. Analog ICs are often not very versatile in different scenarios. More performance indicators are involved, and the stability and certification cycle is more factory, which leads to a smaller number of EDA tools that can be used, and higher requirements for the designer's own experience. Therefore, in the analog IC industry, rich design experience (or also called Know-how) is more important.

Ⅴ Analog IC market analysis

Reviewing the market size and growth rate of each segment of the semiconductor industry in the past 15 years, we find that the analog IC market is stable in size and is not affected by short-term fluctuations in certain downstream markets, and the market fluctuations are small. Analog chips are also the barometer of the global semiconductor industry, closely related to macroeconomic changes, and relatively weak cyclical changes.

After continuous development since the 1950s, analog ICs have become a global industry of nearly $60 billion. According to WSTS and Statista data statistics and forecasts, the global analog IC market size reached $55.7 billion in 2020, an increase of 3.3% compared to 2019, the annual semiconductor industry size of $440.4 billion, analog IC market share of 12.6%.

With the global epidemic gradually under control, the semiconductor industry has also ushered in a recovery, in which 5G communications, automotive electronics and other application scenarios will accelerate the development of the analog IC market. It is expected that the analog chip market size can reach $64 billion in 2021, an increase of 15.1% year-on-year, higher than the overall growth rate of the semiconductor industry. Considering the stable development of analog chip track, less affected by the downstream boom, the future will become a segment of the semiconductor industry gold track.

Semiconductor market segment size and growth rate.jpg

Semiconductor market segment size and growth rate

According to ICInsights forecast, the next five years (20-25 years) the growth rate of the entire IC industry is driven by downstream automotive electronics, 5G communication applications. Sales compound growth rate will reach 8.0%, higher than the overall growth rate of the semiconductor industry. Among them analog, logic and storage IC market growth rate will reach 8.2%, 9.1% and 9.9%, respectively. These are three tracks with the fastest compound growth rates in the IC sub-markets.

Analog IC downstream application scenarios include communications, industrial control, automotive electronics, consumer and government military uses, where the largest downstream application is the communications market, typical products such as base station signal chain, RF IC and so on, accounting for a share of 36.5% in 2020. Automotive electronics in the past five years (16-20 years) benefit from the development of downstream demand for new energy vehicles, the most rapid growth, has become the second largest downstream application scenario, the market share of 24.0%.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1. What is analog IC and digital IC?

Analog integrated circuits work on continuous varying (with respect to time) signals. Digital circuits are non-linear because they work on binary or discontinuous signals. The input and output voltages of digital circuits have two possible values (binary high or low) there are no intermediate levels.

2. What are analog IC used for?

Analog integrated circuit design is used for designing operational amplifiers, linear regulators, oscillators, active filters, and phase locked loops. The semiconductor parameters such as power dissipation, gain, and resistance are more concerned in the designing of analog integrated circuit.

3. Is IC 555 analog or digital?

This 555 timer based circuit is a kind of voltmeter, also an analog to digital converter, that converts the analog input voltage to digital output pulses. The output pulse width is proportional to the difference between the analog input voltage and the voltage across the 4.7 uF capacitor namely 2.5V.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242876

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20255581

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 20261860

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More
  • AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    UTMEL15 May 20261003

    The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.

    Read More
  • The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    UTMEL29 May 2026799

    This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.

    Read More

Subscribe to Utmel !

Featured Parts More