Power Management Integrated Circuit (PMIC) Guide

Published: 10 February 2022 | Last Updated: 10 February 202213695
Power Management Integrated Circuits (PMIC) is a chip that is responsible for the conversion, distribution, detection and other power management of electrical energy in electronic equipment systems.
Selecting the right component for your power management application can be a challenge. This video will help you to get familiar with different power management components and describes the selection criteria for finding the optimal component.

How to Select a Power Management Component for Your Application


Catalog

I Basic definition

II PMIC Types

III Application scope

IV Future trends


I Basic definition

Power Management Integrated Circuits (PMIC) is a chip that is responsible for the conversion, distribution, detection, and other power management of electrical energy in electronic equipment systems. It is mainly responsible for converting the source voltage and current into power that can be used by microprocessors, sensors, and other loads.

II PMIC Types

The relatively wide range of power management includes power conversion (DC-DC, AC-DC, and  DC -AC), power distribution and detection, and systems that combine power conversion and power management. Accordingly, the classification of power management integrated circuits includes these aspects, such as linear power supply chipsvoltage reference chips, switching power supply chips.  LCD driver chipsLED driver chips, voltage detection chips, battery charging management chips, gate drivers, load switches, wide bandgap switches, etc.

(1) Voltage regulator chips 

1) Linear regulator chips

(I) Traditional linear regulator chip

Linear regulators convert the input voltage (VI) to different output voltages (VO) using a linear component (i.e. resistive component) to regulate the output voltage VO. Below are the application circuits for linear regulators.

 Figure 1. application circuits for linear regulators.jpg

Figure 1. application circuits for linear regulators

(II) low dropout linear regulator chip

For linear regulators, an important type is a low dropout (LDO) linear regulator. It can continuously output a stable voltage when the difference between the input voltage (VIN) and the output voltage (VOUT) is very small.

The four key elements of  LDO  are:

- Dropout

- Noise

- Power Supply Rejection Ratio (PSRR)

- Static current Iq

(III) Advantages and disadvantages of linear regulator chips

Linear regulators are called "linear regulators" because the relationship between input and output is linear during operation. Because the input and output are connected in series with the control element, sometimes also called "series regulator".

Figure 2. Linear Regulator Circuit.jpg

Figure 2. Linear Regulator Circuit

Linear regulator chips are generally bucked by the control element, so the greater the voltage difference between input and output (the degree of bucking), the greater the losses and the lower the efficiency. Therefore, it is suitable for low-power power supplies.

Advantages

Disadvantages

Simple circuit

Low efficiency

Few external components

High heat generation

Low noise level

Buck converter only

 

2) Switching regulator

 

Switching regulators convert VIN to a different VOUT through a switching element and use an external inductor and capacitor to stabilize the output voltage VOUT. Switching regulators are generally more efficient and support higher output currents than linear regulators. However, there is still ripple or switching noise after the output has been regulated, which remains even after filtering.

I) Types of switching regulator chips

Power supply device to lower the voltage

Buck converter, Buck converter, Step-down converter

Power supply device to increase voltage

Boost converter, Boost converter, Step-up converter

Power supply devices that increase or decrease voltage

Buck-up converters, Buck-boost converters

Power supply device that generates negative voltage

Negative voltage converter, Inverting converter, Inverting converter

 

a) Buck converter chips

 

Buck type step-down switching regulator is the one whose input voltage is higher than the output voltage, and the conversion principle is shown in the following figure.

Figure 3. Buck-type step-down switching regulator conversion principle.jpg

Figure 3. Buck-type step-down switching regulator conversion principle

Figure 4.jpg

Figure 4

①Detect the output voltage and compare it with the reference voltage.

②When it is lower than the set output voltage, the switch is ON and the current direction flows according to the red arrow.

③The inductor stores magnetic energy.

④When the output voltage is higher than the set voltage, the switch is turned OFF and the current direction flows according to the green arrow.

The inductor converts the stored magnetic energy into the current for the load output and then returns it to the inductor.

⑥When the magnetic energy of the inductor disappears and the output voltage starts to drop, the switch turns ON again.

By controlling the turn-off and turn-on time of the switch, a stable output voltage can be obtained.

Example of buck converter circuit application:

 Figure 5. Buck Converter Circuit Application Examples.jpg

Figure 5. Buck Converter Circuit Application Examples

 b) Boost converter chip

The boost circuit is one of the six basic chopper circuits, a switching  DC boost circuit, which can make the output voltage higher than the input voltage. It is mainly used in DC motor drives, single-phase power factor correction (PFC) circuits, and other AC/DC power supplies.

 Figure 6. boost converter circuit.jpg

Figure 6. boost converter circuit

Boost converter circuit application examples:

 Figure 7. Boost Converter Circuit Application Example.jpg

Figure 7. Boost Converter Circuit Application Example

 

c) Buck-boost converter  chip

Buck-boost converter is a DC-DC  converter whose output voltage magnitude can be greater than the input voltage or less than the input voltage. Buck-boost converters are equivalent to revertant converters, but with a single inductor instead of a transformer.

 Figure 8. buck–boost converter.jpg

Figure 8. buck–boost converter 2.jpg

Figure 8. buck-boost converter

Examples of buck-boost converter circuit applications.

 Figure 9. Buck-Boost Converter Circuit Application Example.jpg

Figure 9. Buck-Boost Converter Circuit Application Example

d) Negative voltage converter chips

 Figure 10. Negative Voltage Converter Circuit.jpg

Figure 10. Negative Voltage Converter Circuit

Negative voltage converter circuit application examples.

 Figure 11. Negative Voltage Converter Circuit Application Example.jpg

Figure 11. Negative Voltage Converter Circuit Application Example

II) Advantages and disadvantages of switching regulator chips

The switching regulator chip turns on the switching element (MOSFET) and supplies power from the input to the output until the output voltage reaches the desired voltage. Once the output voltage reaches the specified value, the switching element is turned off and no more input power is consumed. By repeating this action at high speed, the switching element regulates the output voltage to the specified value.

Figure 12. switching regulator circuit.jpg

Figure 12. switching regulator circuit

Advantages

Disadvantages

High efficiency

Many external components

Low heat generation

Difficult to design

Boost/buck/negative voltage conversion

High noise level


(2) Voltage reference chip

Within the rated operating current range, the accuracy of the reference voltage source device (voltage value deviation, drift, current regulation rate, and other indicator parameters) is much better than the ordinary  Zener regulator diode or three-terminal regulator, so it is used in the need for high-precision reference voltage as a reference voltage. It is generally used for A/D, D / A, and high-precision voltage sources. Some voltage monitoring circuits also use the reference voltage source.

Commonly used TL431 voltage reference chip application examples.

Figure 13. TL431 voltage reference chip application example.jpg

Figure 13. TL431 voltage reference chip application example 

(3) Voltage detection chip

Voltage detection chip circuit application examples.

 Figure 14. Application example of voltage detection chip circuit.jpg

Figure 14. Application example of voltage detection chip circuit

(4) Driver chips

Commonly used LED driver chip circuit application examples.

 Figure 15. Application example of LED driver chip circuit.jpg

Figure 15. Application example of LED driver chip circuit

Commonly used digital display driver chip circuit application examples.

 Figure 16. Digital display driver chip circuit application example.jpg

Figure 16. Digital display driver chip circuit application example

Commonly used gate driver chip circuit application examples.

 Figure 17. Application example of gate driver chip circuit.jpg

Figure 17. Application example of gate driver chip circuit

III Application scope

The application range of power management integrated circuits is very wide. The development of power management integrated circuits is important to improve the performance of the whole machine. The choice of a power management integrated circuit is directly related to the needs of the system, and the development of digital power management integrated circuit still needs to cross the cost barrier.

In today's world, people's life is a moment that can not be separated from electronic equipment. Power management integrated circuit in the electronic equipment system is responsible for the transformation of electrical energy, distribution, detection, and other electrical energy management responsibilities. Power management integrated circuit is indispensable to the electronic system, and their performance has a direct impact on the performance of the machine.

IV Future trends

Power management integrated circuit has a bright future. Through the development of new processes, packaging and circuit design technologies, there will be more outstanding performance of the device is born, they can improve power density, extend battery life, reduce electromagnetic interference, enhance power and signal integrity and improve system security, to help engineers around the world to achieve innovation.


UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is PMIC used for?

A power management integrated circuit (PMIC) is used to manage power on an electronic devices or in modules on devices that may have a range of voltages. The PMIC manages battery power charging and sleep modes, DC-to-DC conversion, scaling of voltages down or up, among others.

2.What does PMIC mean in electronics?

Power management ICs (PMICs) are integrated circuits that include multiple power rails and power management functions within a single chip.

3.What is PMIC voltage regulator?

Products in the DC-DC switching regulator PMIC (Power Management Integrated Circuit) family are component-level devices used in applications requiring stabilization of a DC input voltage and/or transformation thereof to an output voltage of different magnitude.

4.What is meant by power management?

Power management is a feature of some electrical appliances, especially copiers, computers, computer CPUs, computer GPUs and computer peripherals such as monitors and printers, that turns off the power or switches the system to a low-power state when inactive.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242455

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • A Comprehensive Guide to FPGA Development Boards
    A Comprehensive Guide to FPGA Development Boards
    UTMEL11 September 202514005

    This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20253473

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • 800G Optical Transceivers: The Guide for AI Data Centers
    800G Optical Transceivers: The Guide for AI Data Centers
    UTMEL24 December 20253491

    The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.

    Read More
  • Xilinx FPGAs: From Getting Started to Advanced Application Development
    Xilinx FPGAs: From Getting Started to Advanced Application Development
    UTMEL09 September 20254193

    This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.

    Read More