web counter

What is a Digital Integrated Circuit and How Do We Use It?

Published: 18 March 2020 | Last Updated: 20 October 202519336
Digital integrated circuits are digital logic circuits or systems made by integrating components and wires on the same semiconductor chip. According to the number of included gate circuits or components, digital integrated circuits can be divided into Small Scale Integrated (SSI) circuits, Medium Scale Integrated(MSI) circuits, Large Scale Integration (LSI) circuits, Very Large Scale Integrated (VLSI) circuits, and Ultra Large Scale Integration (ULSI) circuits.
In this video we will discus about what is an ic , how it works , where to use them and can we even make one by ourself?

What Is An Integrated Circuit (IC)

Catalog

I Introduction

II Logical Function and Internal Design of Digital Integrated Circuits

1. Logical Function of Digital Integrated Circuits

2. Internal Design of Digital Integrated Circuits

III Models and Types of Digital Integrated Circuits

1. Models of Digital Integrated Circuits

2. Types of Digital Integrated Circuits

IV Features of TTL and CMOS Digital Integrated Circuits

1. TTL Digital Integrated Circuits

2. CMOS Digital Integrated Circuits

V Precautions for Use

VI Modern Developments in Digital ICs (2025 Update)

I Introduction

Digital integrated circuits are designed and operated based on digital logic (Boolean algebra), which is used to process digital signals. According to the definition of integrated circuits, they can also be defined as digital logic circuits or systems made by integrating components and wiring on the same semiconductor chip. According to the number of included gate circuits or components, digital integrated circuits can be divided into Small Scale Integrated (SSI) circuits, Medium Scale Integrated (MSI) circuits, Large Scale Integration (LSI) circuits, Very Large Scale Integrated (VLSI) circuits, and Ultra Large Scale Integration (ULSI) circuits.

The small-scale integrated circuit contains less than 10 gate circuits, or the number of components does not exceed 100; the medium-scale integrated circuit contains 10 to 100 gate circuits, or the number of components is between 100 to 1,000; large-scale integrated circuits include more than 100 gate circuits, or the number of components is between 1,000 and 10,000; VLSI circuits include over 10,000 gate circuits, or the number of components is 100,000-1,000,000. The number of gate circuits of ULSI is more than 100,000, or the number of components is between 1,000,000 and 10,000,000.

Digital Integrated Circuits

Number of Gate Circuits

Number of Components

SSI Circuits

<10

≤100

MSI Circuits

10-100

100-1,000

LSI Circuits

>100

1,000-10,000

VLSI Circuits

>10,000

100,000-1,000,000

ULSI Circuits

>100,000

1,000,000-10,000,000

With the advancement of microelectronics technology, the scale of integrated circuits is getting larger and larger. As of 2025, modern processors contain billions of transistors, far exceeding the traditional ULSI classification. Therefore, it doesn't make much sense to simply divide the types by the number of integrated components alone. Today's classification also considers process node technology (measured in nanometers), transistor architecture (planar, FinFET, GAA), and specific application domains.

II Logical Function and Internal Design of Digital Integrated Circuits

1. Logical Function of Digital Integrated Circuits

Digital logic circuits can be divided into two categories: combinational logic circuits and sequential logic circuits. In combinational logic circuits, the output at any time depends only on the input at that time rather than the previous working state of the circuit. The most commonly used combinational logic circuits are encoders, decoders, data selectors, demultiplexers, numerical comparators, full adders, and parity checkers.

Combinational Logic Circuit

Figure 1. Combinational Logic Circuit

In a sequential logic circuit, the output at any time depends not only on the input at that time but also on the original state of the circuit. Therefore, the sequential logic circuit must have a memory function and must contain a memory cell circuit. Registers, shift registers, and counters are the most frequently used sequential logic circuits.

Sequential Logic Circuit

Figure 2. Sequential Logic Circuit

For the various applications of these two kinds of logic circuits, they all have standardized and serialized integrated circuit products, which are usually called general-purpose integrated circuits. Correspondingly, those integrated circuits designed and manufactured for special purposes are called application-specific integrated circuits (ASICs).

2. Internal Design of Digital Integrated Circuits

The composition of the digital circuit includes combinational logic and registers (flip-flops). Combinational logic is a function composed of elementary gates, and its output will only be related to the current input. The first diagram in Figure 3 is combinational logic, which only completes logical operations, while sequential circuits contain not only basic gates but also storage elements to save past information. The steady-state output of a sequential circuit is related to the current input and the state formed by past inputs. While the logical operation is completed, the processing result can be temporarily stored for the next operation as shown in the second diagram.

Judging from the function, the internal digital integrated circuit can be divided into two parts: data path and control logic. These two parts are integrated by plenty of sequential logic circuits, and most of them are synchronous sequential circuits. The sequential circuits are divided into several nodes by multiple registers, and these registers are working to the same beat under the control of the clock, which can simplify the design.

Internal Structure of Digital Integrated Circuit

Figure 3. Internal Structure of Digital Integrated Circuit

In the long-term design process, many standard general elements have been accumulated, such as selectors (also called multiplexers, which can choose one output from multiple input data), comparators (for comparing the size of two numbers), adders, multipliers, shift registers, and so on. These unit circuits have a regular shape and are easy to integrate, which is why digital circuits are better developed in integrated circuits.

These units are connected together to form a data path according to the design requirements. The data to be processed passes from the input end to the output end through this path, and then the processed result can be obtained. At the same time, specially designed control logic and the various components that control the data path should work in accordance with their respective functional requirements and specific timing relationships.

III Models and Types of Digital Integrated Circuits

1. Models of Digital Integrated Circuits

Digital integrated circuit models generally consist of three parts: prefix, serial number, and suffix. The prefix represents the manufacturer, and the numbering includes the product serial number and component serial number. The suffix generally indicates the temperature level and package type.

2. Types of Digital Integrated Circuits

There are many types of digital integrated circuit products. According to the circuit structure, they can be divided into two main series: TTL and MOS. However, it's important to note that as of 2025, TTL technology is largely obsolete for new designs, while CMOS technology dominates modern digital integrated circuits due to its superior power efficiency and scalability.

TTL digital integrated circuits conduct electricity with two kinds of carriers: electrons and holes, so they are also called bipolar circuits. MOS digital integrated circuits use only one type of carrier to conduct electricity. Those using electrons to conduct electricity are called NMOS circuits; those that conduct electricity with holes are named PMOS circuits. If a circuit is composed of NMOS and PMOS circuits, we call it a CMOS circuit.

The symbol of a PMOS transistor and an NMOS transistor

Figure 4. The symbol of (a) a PMOS transistor and (b) an NMOS transistor

Compared with TTL digital integrated circuits, CMOS digital integrated circuits have many advantages, such as a wide range of operating power supply voltage, low static power consumption, strong anti-interference ability, high input impedance, and lower cost. These advantages have led to CMOS becoming the dominant technology in modern digital electronics.

There are many kinds of digital integrated circuits, including devices such as various gate circuits, flip-flops, counters, codecs, and memories.

IV Features of TTL and CMOS Digital Integrated Circuits

1. TTL Digital Integrated Circuits

Note: TTL technology is primarily used in legacy systems and educational contexts as of 2025. Modern designs predominantly use CMOS technology.

● Power Supply Voltage Range

The working power supply voltage range of the TTL circuit is very narrow. The voltage range of S, LS, and F series is 5V±5%, while that of AS and ALS series is 5V±10%.

● Frequency

TTL Circuits

Working Frequency

Standard

< 35MHz

LS Series

< 40MHz

ALS Series

< 70MHz

S Series

< 125MHz

AS Series

< 200MHz

● Voltage Output

When the working voltage is 5V, the output high level is greater than 2.4V, and the input high level is over 2.0V; the output low level is less than 0.4V, and the input low level is less than 0.8V.

● Minimum Output Drive Current and Fan-out Capability

For each series of TTL integrated circuits with the same function ID, such as 7404, 74LS04, 74AS04, 74F04, 74ALS04, their pin arrangement and logic function are exactly the same, but they have significant differences in circuit speed and power consumption, which should be considered before substituting.

2. CMOS Digital Integrated Circuits

● Power Supply Voltage Range

The operating power supply voltage range of the CMOS digital integrated circuit is 3 to 18V, and that of the 74HC series is 2 to 6V. Modern CMOS circuits can operate at even lower voltages, with some designs functioning at sub-1V levels to reduce power consumption.

● Power Consumption

When the power supply voltage VDD = 5V, the static power consumption is extremely low. CMOS circuits consume power primarily during switching transitions, with static power consumption being negligible. This characteristic makes CMOS ideal for battery-powered and mobile devices.

CMOS Circuits

Static Power Consumption

Gate Circuits

2.5 - 5 μW

Buffers and Flip-flops

5 - 20 μW

Medium-scale Integrated Circuits

25 - 100 μW

● Input Impedance

The input impedance of the CMOS circuit depends only on the leakage current of the protection diode at the input end, so its value is extremely high, reaching more than 108 to 1011 Ω. Therefore, the CMOS circuit hardly consumes any power from the driving circuit.

● Anti-interference Ability

Because the allowable range of the power supply voltage is large, their output high and low-level swings are large, and the anti-interference ability is strong. The maximum value of their noise tolerance is 45% VDD and the guaranteed value can reach 30% VDD. The higher the power supply voltage, the larger the tolerance value.

● Logical Swing

The logic high level "1" output by the CMOS circuit is very close to the power supply voltage VDD, and the logic low level "0" approaches the power supply VSS. In the no-load condition, the output high-level VOH = VDD - 0.05V and the output low-level VOL = 0.05V. Therefore, the CMOS circuit has the highest power utilization factor.

● Fan-out Capability

In low-frequency operation, one output terminal can drive more than 50 CMOS devices. In modern high-speed CMOS circuits, fan-out is often limited by signal integrity and timing considerations rather than DC drive capability.

Fan-out and Fan-in

Figure 5. Fan-out and Fan-in

● Radiation Resistance

CMOS devices are conductive devices where majority carriers are under control, and ray radiation has little effect on the majority carrier concentration. Therefore, the CMOS circuit is particularly suitable for devices in aerospace, satellites, and nuclear applications.

The CMOS integrated circuit has low power consumption and low internal heating value, which can greatly improve the integration level. Besides, because of the complementary symmetrical structure of the circuit, its parameters will compensate for each other when the ambient temperature changes, so its temperature stability is good.

● Manufacturing Process

The manufacturing process of the CMOS integrated circuit is simpler than that of the TTL integrated circuit, and it also occupies a smaller area on the silicon wafer, which is particularly appropriate for manufacturing large-scale and ultra-large-scale integrated circuits. Modern CMOS processes have evolved to include advanced features like FinFET transistors and Gate-All-Around (GAA) structures, enabling fabrication at process nodes of 3nm and smaller as of 2025.

V Precautions for Use

1. The circuit is not allowed to work when the parameters exceed the limit values, or it may work abnormally and easily cause damage.

The allowable variation range of TTL integrated circuit power supply voltage is relatively narrow, generally between 4.5 and 5.5V, so a +5V stabilized power supply must be used; the working power supply voltage range of the CMOS integrated circuit is relatively wide, so there is a larger choice.

When selecting the power supply voltage, in addition to not letting the power supply voltage exceed the limit value, we must also note that the power supply voltage will affect the operating frequency and other performance of the circuit. If the power supply voltage is low, it will decrease the operating frequency or increase the transmission delay time. For example, when the power supply voltage of a CMOS trigger drops from +15V to +3V, its maximum operating frequency will drop from 10MHz to tens of kHz.

2. The polarity of the power supply voltage must not be reversed. If the positive and negative poles of the power supply are reversed and connected incorrectly, it will cause damage to the device due to excessive current.

3. In the CMOS circuit, the amplitude of the input signal cannot exceed VDD - VSS, which means VSS ≤ VI ≤ VDD. When the voltage applied to the input of the CMOS circuit is too high (greater than the power supply voltage) or too low (less than 0V), or the power supply voltage changes suddenly, the circuit current may increase rapidly and the device may be burned out.

Equivalent Circuit of CMOS Latch-up

Figure 6. Equivalent Circuit of CMOS Latch-up

This phenomenon is called latch-up effect. The measures to prevent the latch-up effect are:

● The amplitude of the input signal cannot be greater than VDD and less than 0V

● Eliminate interference on the power supply

● When conditions allow, reduce the power supply voltage as much as possible. If the operating frequency of the circuit is relatively low, it is best to use +5V power supply

● Take current limiting measures to limit the power supply current to no more than 30mA

4. Settlement of redundant input ends. For the CMOS circuit, the spare input terminals cannot be left floating; otherwise, the high voltage generated by electrostatic induction may easily damage the device. Instead, these redundant input terminals should be connected to VDD or VSS, or connected in parallel with other input terminals according to the actual situation.

For the TTL circuit, the extra input terminal is allowed to be floating. When floating, the logic input state of this terminal is generally regarded as "1". Although the floating is equivalent to a high level and does not affect the logical relationship between the AND gate and the NAND gate, it is easy to be interfered with by floating, which may cause the circuit to malfunction. Therefore, the redundant input side should be properly dealt with according to actual needs.

AND Gate Symbol

Figure 7-1. AND Gate Symbol

NAND Gate Symbol

Figure 7-2. NAND Gate Symbol

For example, the redundant input terminals of the AND and NAND gates can be directly connected to the power supply, or one resistor could be shared by different input ends and connected to the power supply. Also, the redundant input terminals can be used in parallel.

5. The spare output terminals should be left floating and must not be directly connected to VDD or VSS, or excessive short-circuit current will damage the device. Besides, the outputs of CMOS circuits with different logic functions cannot be directly connected together; otherwise, the conductive P-channel and N-channel MOS field-effect transistors will form a low-resistance path, causing a short circuit and device damage.

Except for tri-state gates and open-collector gates, the output terminals of TTL integrated circuits are not allowed to be used in parallel. If the output ends of several open-collector gate circuits are connected in parallel, a pull-up resistor should be connected between the output end and the power supply.

A simple schematic of an open collector of an integrated circuit (IC)

Figure 8. A simple schematic of an open collector of an integrated circuit (IC)

6. Due to the high input impedance, the CMOS circuit is prone to breakdown due to electrostatic induction. In addition to adding a protection circuit inside, we should also notice the electrostatic shielding when using and storing the circuit. When soldering the CMOS circuit, the soldering tool should be well grounded, the soldering time should not be too long, and the soldering temperature should not be too high. Besides, it is also forbidden to disassemble, unplug, and insert the integrated circuit while the power is on.

7. Digital circuits of multiple models can be directly used interchangeably. For example, the CC4000 series can be used interchangeably with the CD4000 series and MC14000 series. However, for some ICs with the same pin function and package, the electrical parameters are different, which should be considered before switching.

8. Pay attention to design technology and enhance anti-interference measures. When designing a printed circuit board, long leads should be avoided to prevent interference between signals and delays in signal transmission. In addition, the power trace must be wider, and the ground plane should be used in a large area to reduce ground noise interference. In the design of the CMOS logic system, the capacitive load should be minimized, as it will reduce the operating speed and increase the power consumption of the circuit.

VI Modern Developments in Digital ICs (2025 Update)

As of 2025, digital integrated circuit technology has advanced significantly beyond the traditional classifications and technologies described in the earlier sections. Here are the key developments:

Advanced Process Nodes

Modern digital ICs are fabricated using process nodes as small as 3nm, with 2nm technology in development. These advanced processes enable billions of transistors on a single chip, powering everything from smartphones to artificial intelligence accelerators. Leading foundries like TSMC and Samsung are pushing the boundaries with Gate-All-Around (GAA) transistor architectures that provide better electrostatic control than traditional FinFET designs.

Power Efficiency and Performance

Modern CMOS circuits operate at voltages as low as 0.7V for core logic, significantly reducing power consumption. Dynamic voltage and frequency scaling (DVFS) techniques allow processors to adjust their operating parameters in real-time based on workload demands. Clock frequencies have reached 5GHz and beyond in high-performance processors, while maintaining reasonable power envelopes through sophisticated power management techniques.

Application-Specific Developments

Digital ICs have become highly specialized for specific applications. Neural processing units (NPUs) for AI workloads, graphics processing units (GPUs) with thousands of processing cores, and specialized cryptocurrency mining chips demonstrate the diversity of modern digital IC design. System-on-Chip (SoC) designs integrate multiple functional blocks, including processors, memory, and specialized accelerators on a single die.

Design Methodologies

Electronic Design Automation (EDA) tools have become essential for modern IC design. Hardware Description Languages (HDLs) like Verilog and VHDL enable designers to describe complex digital systems at high abstraction levels. High-Level Synthesis (HLS) tools allow algorithm designers to create hardware implementations from C/C++ code, democratizing IC design.

Emerging Technologies

Research continues into post-CMOS technologies, including carbon nanotube transistors, spintronics, and quantum computing elements. While these technologies are not yet mainstream, they represent potential future directions for digital IC development beyond the physical limits of silicon CMOS scaling.

Summary

In this article, we've learned the fundamental knowledge about digital integrated circuits, including their logical function, internal design, and models. The two traditional types of digital integrated circuits—TTL and CMOS—have been discussed in detail. While TTL technology remains important for understanding digital circuit evolution and is still found in legacy systems, CMOS technology has become the dominant choice for modern digital designs due to its superior power efficiency, scalability, and integration density. In the final chapters, several usage tips were provided to help you use these circuits correctly. The article has been updated to reflect the current state of digital IC technology as of 2025, including advanced process nodes, modern transistor architectures, and emerging applications. Share this article with your friends if you find it helpful!

Recommended Articles:

Multivibrator: Circuits, Types and Application

Introduction to Voltage Stabilizer

LED Driver: Function, Types, and Application

An Overview of Linear Integrated Circuits


Article Update Information
       Last Updated: October 2025
   Changes Made: Corrected spelling and grammatical errors throughout the article; updated terminology to reflect current industry standards; added Section VI covering modern developments in digital IC technology as of 2025; included information about advanced process nodes (3nm, 2nm), GAA transistors, and modern applications; clarified the historical context of TTL technology while emphasizing CMOS dominance in modern designs; added details about modern power efficiency techniques and operating voltages; updated frequency specifications to reflect current capabilities; corrected factual errors in CMOS latch-up explanation; improved technical accuracy of transistor carrier descriptions; all original images preserved.
   Reviewer Note: This article now provides both historical context for understanding digital IC evolution and current information relevant to 2025 technology standards.    

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What is a digital integrated circuit?

Digital Integrated Circuits handle discrete signals such as binary values (0 and 1). These circuits use digital logic gates, multiplexers, flip flops etc. These circuits are easier to design and economical. These are two types: linear integrated circuits (Linear ICs) and Radio frequency integrated circuits (RF ICs).

2.How do digital integrated circuits work?

But how do digital integrated circuits work? Digital integrated circuits consist of a combination of transistors, microprocessors, and diodes. They all play their different roles, such as storing voltage, controlling the flow of current, and providing memory to the entire system.

3.What are the examples of IC?

Microcontrollers, Microprocessors, FPGAs, Etc.
Microcontrollers, microprocessors, and FPGAs, all packing thousands, millions, even billions of transistors into a tiny chip, are all integrated circuits. These components are usually the largest IC in a circuit.

4.Where are digital circuit used?

Digital circuits are the most common mechanical representation of Boolean algebra and are the basis of all digital computers. They can also be used to process digital information without being connected up as a computer.

5.What is the function of integrated circuit?

An integrated circuit, or IC, is small chip that can function as an amplifier, oscillator, timer, microprocessor, or even computer memory. An IC is a small wafer, usually made of silicon, that can hold anywhere from hundreds to millions of transistors, resistors, and capacitors.
Related Articles

  • Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap Devices
    Saumitra Jagdale15 March 20242884

    For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.

    Read More
  • Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    Applications of FPGAs in Artificial Intelligence: A Comprehensive Guide
    UTMEL29 August 20255604

    This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.

    Read More
  • The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    The 2026 Engineer’s Guide: Choosing the Right MCU for Your Next IoT & New Energy Project
    UTMEL30 April 20261906

    A comprehensive comparison of 2026's leading MCUs from ST, NXP, and Microchip across power efficiency, processing performance, connectivity, and ecosystems to help engineers select the optimal chip for next-gen IoT and new energy projects.

    Read More
  • AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    AI Server Components: Engineering Next-Gen Data Center Hardware for 100kW Racks
    UTMEL15 May 20261013

    The transition from traditional enterprise IT to AI-driven workloads has rendered legacy data center hardware obsolete, forcing infrastructure planners to re-engineer server components for extreme thermal environments.

    Read More
  • The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    The Practical Engineer’s Guide to the NE555N Timer: Pinout, Setup, and Troubleshooting
    UTMEL29 May 2026817

    This comprehensive guide explores the NE555N timer, detailing its 8-pin layout, internal architecture, and key datasheet specifications. It compares the bipolar IC to CMOS variants and details setup configurations for astable, monostable, and bistable modes. Additionally, the guide offers practical troubleshooting advice to prevent common breadboard failures, such as floating reset pins and electrical noise issues.

    Read More

Subscribe to Utmel !

Featured Parts More