How to Properly Install TVS Diodes in Your PCB Design

Published: 11 July 2025 | Last Updated: 11 July 20254183
Install TVS diodes by placing them near ESD entry points, checking polarity, and using short traces for optimal circuit protection on your PCB.

How    

Image Source: pexels        

You can install TVS diodes for circuit protection by first identifying where ESD may enter your PCB. Choose the right diode for your signal polarity, then place it as close as possible to connectors or exposed conductors. Keep traces short and ensure correct polarity for reliable ESD defense.

Protection Points

ESD Entry Locations

You need to identify where voltage spikes can enter your PCB. These entry points often include places where users connect cables or touch the board. When you find these spots, you can place esd protection diodes to guard against sudden voltage spikes. This step helps you protect sensitive components from damage.

  • Strategic placement of esd protection diodes at these points prevents failure of sensitive components exposed to voltage spikes.

  • You can add suppression circuits to keep voltage spikes within safe limits.

  • Proper esd protection diodes placement supports compliance with certifications like FCC and CE.

  • Devices become more reliable in environments with frequent voltage spikes.

  • Fast-response esd protection diodes at entry locations help stop voltage spikes, surges, and switching transients.

  • Identifying these points also helps you balance noise prevention and esd shielding for your device.

Tip: Always check for any exposed metal or connectors, as these are common paths for voltage spikes.

Board Edge and Connectors

Board edges and connectors face a high risk from voltage spikes. When you handle the board or connect cables, you can introduce static electricity. This static can cause voltage spikes that harm your circuit. Esd protection diodes placed near these areas can stop voltage spikes before they reach sensitive components.

  • Sensitive device junctions on the board become easy targets for voltage spikes.

  • Real-world cases show that touching board edges during assembly increases the risk of voltage spikes.

  • Packaging materials and dry air can make voltage spikes more likely.

  • Lab tests show that voltage spikes can damage devices even without direct contact.

  • Adding esd protection diodes and redesigning circuits can lower failure rates.

  • Using conductive shunts or extra esd protection diodes at board edges and connectors can reduce failures from 30% to about 2%.

You should always place esd protection diodes close to board edges and connectors. This step gives your design the best chance to survive voltage spikes and keeps your sensitive components safe.

TVS Diodes Selection

Voltage Ratings

You need to select tvs diodes with the right voltage ratings to protect your circuit from voltage spikes. If you choose a diode with a clamping voltage that is too high, your sensitive parts may still get damaged. If the clamping voltage is too low, the diode may trigger during normal operation. Always check the stand-off voltage and breakdown voltage. For example, a 24V system often uses a stand-off voltage of 17V and a breakdown voltage of 19V. The clamping voltage should not go above the maximum voltage rating of your downstream components.

Here is a table showing ESD protection voltage thresholds for different device classes:

ESD ModelClassificationVoltage Threshold Range (Volts)Notes
Human Body Model (HBM)0ZLess than 50 VHighest sensitivity
HBM0A50 to less than 125 VSensitive devices
HBM0B125 to less than 250 VModerate sensitivity
HBM1A250 to less than 500 VLower sensitivity
Charged Device Model (CDM)C0ALess than 125 VHigh sensitivity
CDMC0B125 to less than 250 VModerate sensitivity
CDMC1250 to less than 500 VLower sensitivity

Tip: Always use the worst-case clamping voltage when you design your over-voltage protection circuit. This helps you protect your devices from unexpected voltage spikes.

Application Matching

You must match tvs diodes to your specific application. Unidirectional diodes work well for DC circuits, while bidirectional diodes protect AC or data lines from voltage spikes in both directions. In RF circuits, pick diodes with low capacitance to avoid signal loss. Make sure the peak pulse current rating can handle the largest expected surge. For example, large surge events need careful fuse selection, since polyfuses may not work well above 30V and several amps.

  • Choose the right type:

    • Unidirectional: For one-way voltage spikes.

    • Bidirectional: For two-way voltage spikes.

  • Check the placement. Place tvs diodes close to connectors or board edges to stop voltage spikes before they reach sensitive parts.

  • Use wide traces and ground pours to help the diode handle high currents.

  • Always test the diode before installation. Use a multimeter to check for shorts or open circuits.

TVS diodes act fast to shunt excess current and reset after the event. They work better than varistors or polymer devices for most ESD events. When you select and test the right diode, you improve your circuit’s safety and reliability.

Preparation

Tools Needed

Before you install a new diode, gather the right tools. You want to make sure your work is safe and accurate. Here is a list of tools you should have ready:

  • ESD-safe work mat and wrist strap

  • Soldering iron with adjustable temperature

  • Solder wire and flux

  • Fine-tip tweezers

  • Multimeter (with diode test mode)

  • Magnifying glass or inspection microscope

  • Solder sucker or desoldering braid

You can check the performance of your tools using simple tests. For example, a multimeter in diode test mode should show a forward voltage drop between 0.5V and 0.7V for a good diode. If you see an open circuit or a very high voltage drop, the diode may be faulty. When you use a curve tracer or a transient voltage suppressor tester, you can measure clamping voltage and response time. These tests help you confirm that your tools and diodes work as expected.

Test TypeTool/Method UsedPerformance Data / Expected Result
Forward Bias TestingMultimeter (diode test mode)Forward voltage drop between 0.5V and 0.7V; open circuit or high voltage drop indicates fault
Reverse Bias TestingMultimeterOpen circuit or very high resistance (OL) expected; low resistance or short indicates failure
Dynamic TestingCurve tracer or transient voltage suppressor testerMeasures clamping voltage, peak pulse current, and response time under surge conditions; critical for confirming diode effectiveness
In-Circuit TestingMultimeter (with power off)Resistance measurement; very low reading suggests short circuit; readings may vary due to parallel components

Safety Steps

You need to follow safety steps to protect yourself and your circuit. Always wear an ESD wrist strap and work on an ESD-safe mat. This prevents static electricity from damaging sensitive parts. Set your soldering iron to the correct temperature. IPC-J-STD-001 recommends using the right solder alloy and keeping the iron at the right heat level for clean joints. Keep your workspace clean and free of clutter.

Here is a table showing important IPC standards that guide safe and reliable PCB work:

IPC StandardFocus AreaNumerical Data / Tool Specifications Supported
IPC-2221PCB design rulesTrace widths, spacing, annular ring sizes, conductor thickness, voltage-based clearance tables, CAD tool DRC settings
IPC-J-STD-001Soldering process requirementsSoldering iron temperature settings, solder alloy compositions, flux types, solder joint quality criteria, ESD prevention
IPC-6012PCB qualification and performancePlating thickness, laminate materials, copper foil quality, dimensional tolerances, electrical testing criteria
IPC-A-610Assembly acceptability and inspectionVisual acceptance criteria for solder joints, component placement tolerances, cleanliness standards
IPC-7711/7721Rework, modification, and repair proceduresTemperature and handling guidelines for soldering/desoldering, tool specifications for rework stations
IPC-7351Surface mount design and land pattern standardsPad dimensions, spacing, footprint density levels, solder fillet geometry

Tip: Always check your tools and workspace before you install. This helps you avoid mistakes and keeps your circuit safe.

TVS Diodes Placement

TVS    

Image Source: pexels        

Proximity to ESD Points

You need to place esd protection diodes as close as possible to where voltage spikes can enter your circuit. These entry points often include connectors, switches, and board edges. When you position tvs diodes near these locations, you give your circuit the best chance to stop voltage spikes before they reach sensitive components.

Placing tvs diodes close to ESD entry points lowers the clamp voltage during an ESD event. This means the diode reacts faster and more effectively, protecting your circuit. Technical studies show that when you reduce the distance between the diode and the entry point, you also reduce the inductance in the trace. Lower inductance helps the diode clamp voltage spikes more efficiently. You can see this improvement in real-world tests, where circuits with nearby diodes show fewer failures and better ESD protection.

Tip: Always check your PCB layout to make sure esd protection diodes sit right next to connectors or exposed metal parts. This simple step can make a big difference in how well your board survives voltage spikes.

Trace Minimization

Short traces matter a lot when you install esd protection diodes. Long traces add unwanted inductance and resistance. These extra elements slow down the response of tvs diodes and can let voltage spikes slip past, putting sensitive components at risk.

When you keep traces short, you improve signal integrity. For example, if you work with a 100MHz signal that has a 3ns rise time, the trace should not be longer than 21cm. If your signal is faster, like 500MHz with a 0.6ns rise time, the trace should be even shorter—about 4cm. Staying within these limits helps you avoid problems like reflections, ringing, and distortion. Your signals stay clean, and your esd protection diodes can react quickly to voltage spikes.

You can follow these best practices to minimize trace length and improve protection:

  • Place components close together to reduce trace length and lower the risk of EMI.

  • Use wide traces and ground pours to help esd protection diodes handle high currents from voltage spikes.

  • Maintain continuous ground planes under signal traces. This gives a stable return path and reduces noise.

  • Route traces orthogonally and maximize spacing to cut down on crosstalk and coupling.

  • Choose impedance-controlled tracks for high-frequency signals. This keeps signal quality high and helps tvs diodes work better.

Best PracticeBenefit
Short tracesFaster diode response, less voltage drop
Wide tracesHandles higher surge currents
Ground pours/planesReduces noise, improves ESD shunting
Impedance controlMaintains signal integrity
Close placement to entryLowers clamp voltage, protects components

Remember: Every millimeter counts. Even a small increase in trace length can weaken your ESD protection and let voltage spikes reach sensitive components.

By following these placement and routing tips, you make sure your esd protection diodes and tvs diodes work at their best. Your circuit will stand up better to voltage spikes and keep sensitive components safe.

Orientation and Soldering

Orientation    

Image Source: pexels        

Polarity Check

You must always check the polarity before you install tvs diodes. Most tvs diodes have a marking, such as a line or a dot, that shows the cathode side. If you install the diode backward, it will not protect your circuit. In some cases, it may even damage your board. For unidirectional tvs diodes, connect the cathode to the voltage line and the anode to ground. For bidirectional types, you can install them either way, but you should still follow the datasheet.

Tip: Always double-check the symbol on the PCB and the marking on the diode. Mistakes in polarity are a common cause of ESD protection failure.

Here is a quick reference table:

Diode TypeCathode ConnectionAnode Connection
UnidirectionalVoltage lineGround
BidirectionalEither sideEither side

Soldering Methods

You need to use the right soldering method to ensure a strong and reliable connection. Start by cleaning the pads and the leads of the tvs diodes. Use a small amount of flux to help the solder flow. Heat the pad and the lead at the same time, then apply solder until it forms a shiny joint. Avoid using too much solder, as this can cause bridges. If you use surface-mount tvs diodes, tweezers help you hold the part in place. For through-hole types, trim the leads after soldering.

  • Use a soldering iron set to the correct temperature (usually 320–350°C).

  • Hold the iron on the joint for 1–2 seconds only.

  • Inspect each joint with a magnifying glass to check for cold solder or bridges.

🔍 Note: Good soldering keeps your ESD protection working. Poor joints can cause your tvs diodes to fail during a voltage spike.

ESD Protection Diodes Testing

Visual Inspection

You should always start by checking your esd protection diodes with a careful visual inspection. This step helps you catch problems before they affect your circuit. Look for any signs of physical damage, such as cracks, chips, or burn marks on the diodes. Check the solder joints to make sure they are shiny and smooth, not dull or cracked. Examine the PCB layers for correct thickness and structure. Make sure the esd protection diodes match the placement and orientation shown in your design.

Follow these steps for a good visual inspection:

  1. Verify that each esd protection diode sits in the correct spot and faces the right direction.

  2. Look for corrosion or dirt on the diode and nearby pads.

  3. Check for missing or extra solder that could cause shorts or open circuits.

  4. Compare your board to industry standards for quality and reliability.

Tip: Automated visual inspection tools can help you find tiny defects that are hard to see with your eyes.

Electrical Testing

After you finish the visual check, you need to test the tvs diode with electrical tools. Use a multimeter to measure voltage and resistance across each esd protection diode. This helps you find open circuits or shorts. For deeper analysis, use an oscilloscope and a signal generator to check how the esd protection diodes respond to voltage spikes.

Key performance metrics show if your esd protection diodes work as expected:

MetricDescription
Breakdown Voltage (VBR)The voltage where the diode starts to conduct and clamp spikes.
Clamping Voltage (Vc)The voltage the diode holds during a surge to protect your circuit.
Peak Current (Ipp)The highest current the diode can handle during a spike.
Reverse Leakage Current (IR)The small current that flows when the diode is reverse-biased.
CapacitanceThe stored charge, which can affect high-speed signals.

You should also check that the response time is fast enough to protect your board. Standards like IEC 61000-4-2 help you know what to expect from your esd protection diodes. Careful testing ensures your circuit stays safe from voltage spikes.

Common Mistakes

Wrong Orientation

You might install tvs diodes in the wrong direction if you do not check the markings. This mistake can stop the diode from protecting your circuit. Always look for the line or dot on the diode. Match it with the symbol on your PCB. If you find a diode facing the wrong way, you should remove it and install it correctly. Wrong orientation often leads to failed ESD protection and can damage your board.

Poor Placement

Placing tvs diodes far from ESD entry points weakens their effect. You should keep these diodes close to connectors or exposed metal. Long traces between the entry point and the diode add resistance and slow down the response. If you spot a poorly placed diode, remove the broken diode and place a new one near the entry point. Good placement helps your circuit survive voltage spikes.

Soldering Issues

Bad soldering can cause tvs diodes to fail. Cold joints, too much solder, or bridges between pads create problems. You need to inspect each joint after soldering. If you see a bad joint, remove the diode, clean the pads, and solder again. Good soldering keeps your ESD protection strong and reliable.

Tip: Careful work during installation helps you avoid these common mistakes and keeps your circuit safe.


You can protect your circuit from voltage spikes by following these steps:

  • Place tvs diodes close to entry points.

  • Check orientation before soldering.

  • Test each diode after installation.

Follow these guidelines to avoid mistakes and keep your PCB safe.

FAQ

How do you know if a TVS diode is working?

Use a multimeter in diode mode. You should see a small voltage drop in one direction. If you see a short or open, replace the diode.

Can you use any TVS diode for any voltage?

No. You must match the TVS diode’s voltage rating to your circuit. Using the wrong rating can cause poor protection or damage.

Where should you place TVS diodes on a PCB?

  • Place TVS diodes close to connectors or board edges.

  • Keep traces short.

  • This helps the diode react quickly to voltage spikes.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

  • HF PCB Circuit Design 10 Questions
    HF PCB Circuit Design 10 Questions
    UTMEL16 March 20224979

    Hello everyone, I am Rose. Today I want to give you a full explanation about PCB design. I Hope the following ten questions will give you a satisfied answer.

    Read More
  • How Many do You Know About the 12 Components Included in the Circuit Board?
    How Many do You Know About the 12 Components Included in the Circuit Board?
    UTMEL12 February 20228103

    We are lucky to live in an era where electronic devices are readily available. These electronic devices, on the other hand, come to us thanks to the incredible components on the circuit board, and we frequently wonder what makes electronic devices operate, how they achieve such massive success, and how they accomplish it. Electronic devices are incredible things; you can't see what's going on within them, but you can see what they're capable of. We'll talk about the wonders of PCBs and how to get past them to construct the circuit board in this article.

    Read More
  • 50 Frequently Asked Questions about PCB Layout [Q&A]
    50 Frequently Asked Questions about PCB Layout [Q&A]
    UTMEL16 November 20216748

    In the design of electronic products, PCB layout and routing is an important step, and the quality of PCB layout and routing will directly affect the performance of the circuit.

    Read More
  • An Overview of Development Board
    An Overview of Development Board
    UTMEL18 December 202514528

    The development board is a circuit board used for embedded system development. Development boards are generally customized by embedded system developers according to development needs.

    Read More
  •  PCB Design Guidelines
    PCB Design Guidelines
    UTMEL21 December 20216984

    Hello everyone, I am Rose. Today I will provide you a comprehensive guideline of PCB design.

    Read More