2N2218 Bipolar NPN Transistor: 2N2218 40V 0.8A Transistor, Datasheet and Pinout
Trans GP BJT NPN 30V 0.8A 3-Pin TO-39
The 2N2218 is a silicon NPN transistor manufactured by the epitaxial planar process and designed for small signal general purpose and switching applications. This article is going to introduce details about the 2N2218 bipolar transistor.

Transmissor fm com transistor 2N2218
What is 2N2218?
The 2N2218 is silicon planar epitaxial NPN transistor s in Jedec TO-39 metal cases. It is designed for high-speed switching applications at collector currents up to 500 mA, and features useful current gain over a wide range of collector current, low leakage currents, and low saturation voltages.
2N2218 Pinout

2N2218 Pinout
| Pin No | Pin Name |
| 1 | Emitter |
| 2 | Base |
| 3 | Collector |
2N2218 CAD Model

2N2218 Footprint

2N2218 3D Model
Specifications
- TypeParameter
- Lifecycle Status
Lifecycle Status refers to the current stage of an electronic component in its product life cycle, indicating whether it is active, obsolete, or transitioning between these states. An active status means the component is in production and available for purchase. An obsolete status indicates that the component is no longer being manufactured or supported, and manufacturers typically provide a limited time frame for support. Understanding the lifecycle status is crucial for design engineers to ensure continuity and reliability in their projects.
IN PRODUCTION (Last Updated: 1 month ago) - Factory Lead Time22 Weeks
- Mount
In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.
Through Hole - Mounting Type
The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.
Through Hole - Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
TO-205AD, TO-39-3 Metal Can - Number of Pins3
- Supplier Device Package
The parameter "Supplier Device Package" in electronic components refers to the physical packaging or housing of the component as provided by the supplier. It specifies the form factor, dimensions, and layout of the component, which are crucial for compatibility and integration into electronic circuits and systems. The supplier device package information typically includes details such as the package type (e.g., DIP, SOP, QFN), number of pins, pitch, and overall size, allowing engineers and designers to select the appropriate component for their specific application requirements. Understanding the supplier device package is essential for proper component selection, placement, and soldering during the manufacturing process to ensure optimal performance and reliability of the electronic system.
TO-39 (TO-205AD) - Current-Collector (Ic) (Max)800mA
- Number of Elements1
- Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
-55°C~200°C TJ - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Bulk - Published2007
- Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Discontinued - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Max Operating Temperature
The Maximum Operating Temperature is the maximum body temperature at which the thermistor is designed to operate for extended periods of time with acceptable stability of its electrical characteristics.
200°C - Min Operating Temperature
The "Min Operating Temperature" parameter in electronic components refers to the lowest temperature at which the component is designed to operate effectively and reliably. This parameter is crucial for ensuring the proper functioning and longevity of the component, as operating below this temperature may lead to performance issues or even damage. Manufacturers specify the minimum operating temperature to provide guidance to users on the environmental conditions in which the component can safely operate. It is important to adhere to this parameter to prevent malfunctions and ensure the overall reliability of the electronic system.
-55°C - Max Power Dissipation
The maximum power that the MOSFET can dissipate continuously under the specified thermal conditions.
800mW - Polarity
In electronic components, polarity refers to the orientation or direction in which the component must be connected in a circuit to function properly. Components such as diodes, capacitors, and LEDs have polarity markings to indicate which terminal should be connected to the positive or negative side of the circuit. Connecting a component with incorrect polarity can lead to malfunction or damage. It is important to pay attention to polarity markings and follow the manufacturer's instructions to ensure proper operation of electronic components.
NPN - Power Dissipation
the process by which an electronic or electrical device produces heat (energy loss or waste) as an undesirable derivative of its primary action.
800mW - Power - Max
Power - Max is a parameter that specifies the maximum amount of power that an electronic component can handle without being damaged. It is typically measured in watts and indicates the upper limit of power that can be safely supplied to the component. Exceeding the maximum power rating can lead to overheating, malfunction, or permanent damage to the component. It is important to consider the power-max rating when designing circuits or systems to ensure proper operation and longevity of the electronic components.
800mW - Transistor Type
Transistor type refers to the classification of transistors based on their operation and construction. The two primary types are bipolar junction transistors (BJTs) and field-effect transistors (FETs). BJTs use current to control the flow of current, while FETs utilize voltage to control current flow. Each type has its own subtypes, such as NPN and PNP for BJTs, and MOSFETs and JFETs for FETs, impacting their applications and characteristics in electronic circuits.
NPN - Collector Emitter Voltage (VCEO)
Collector-Emitter Voltage (VCEO) is a key parameter in electronic components, particularly in transistors. It refers to the maximum voltage that can be applied between the collector and emitter terminals of a transistor while the base terminal is open or not conducting. Exceeding this voltage limit can lead to breakdown and potential damage to the transistor. VCEO is crucial for ensuring the safe and reliable operation of the transistor within its specified limits. Designers must carefully consider VCEO when selecting transistors for a circuit to prevent overvoltage conditions that could compromise the performance and longevity of the component.
30V - Max Collector Current
Max Collector Current is a parameter used to specify the maximum amount of current that can safely flow through the collector terminal of a transistor or other electronic component without causing damage. It is typically expressed in units of amperes (A) and is an important consideration when designing circuits to ensure that the component operates within its safe operating limits. Exceeding the specified max collector current can lead to overheating, degradation of performance, or even permanent damage to the component. Designers must carefully consider this parameter when selecting components and designing circuits to ensure reliable and safe operation.
800mA - DC Current Gain (hFE) (Min) @ Ic, Vce
The parameter "DC Current Gain (hFE) (Min) @ Ic, Vce" in electronic components refers to the minimum value of the DC current gain, denoted as hFE, under specific operating conditions of collector current (Ic) and collector-emitter voltage (Vce). The DC current gain hFE represents the ratio of the collector current to the base current in a bipolar junction transistor (BJT), indicating the amplification capability of the transistor. The minimum hFE value at a given Ic and Vce helps determine the transistor's performance and efficiency in amplifying signals within a circuit. Designers use this parameter to ensure proper transistor selection and performance in various electronic applications.
40 @ 150mA 10V - Current - Collector Cutoff (Max)
The parameter "Current - Collector Cutoff (Max)" refers to the maximum current at which a transistor or other electronic component will cease to conduct current between the collector and emitter terminals. This parameter is important in determining the maximum current that can flow through the component when it is in the cutoff state. Exceeding this maximum cutoff current can lead to malfunction or damage of the component. It is typically specified in the component's datasheet and is crucial for proper circuit design and operation.
10nA - Vce Saturation (Max) @ Ib, Ic
The parameter "Vce Saturation (Max) @ Ib, Ic" in electronic components refers to the maximum voltage drop across the collector-emitter junction when the transistor is in saturation mode. This parameter is specified at a certain base current (Ib) and collector current (Ic) levels. It indicates the minimum voltage required to keep the transistor fully conducting in saturation mode, ensuring that the transistor operates efficiently and does not enter the cutoff region. Designers use this parameter to ensure proper transistor operation and to prevent overheating or damage to the component.
1.6V @ 50mA, 500mA - Voltage - Collector Emitter Breakdown (Max)
Voltage - Collector Emitter Breakdown (Max) is a parameter that specifies the maximum voltage that can be applied between the collector and emitter terminals of a transistor or other semiconductor device before it breaks down and allows excessive current to flow. This parameter is crucial for ensuring the safe and reliable operation of the component within its specified limits. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the device. Designers and engineers must carefully consider this parameter when selecting components for their circuits to prevent potential issues and ensure proper functionality.
30V - Collector Base Voltage (VCBO)
Collector Base Voltage (VCBO) is the maximum allowable voltage that can be applied between the collector and base terminals of a bipolar junction transistor when the emitter is open. It is a critical parameter that determines the voltage rating of the transistor and helps prevent breakdown in the collector-base junction. Exceeding this voltage can lead to permanent damage or failure of the component.
60V - Emitter Base Voltage (VEBO)
Emitter Base Voltage (VEBO) is a parameter used in electronic components, particularly in transistors. It refers to the maximum voltage that can be applied between the emitter and base terminals of a transistor without causing damage to the device. Exceeding this voltage limit can lead to breakdown of the transistor and potential failure. VEBO is an important specification to consider when designing circuits to ensure the proper operation and reliability of the components. It is typically provided in the datasheet of the transistor and should be carefully observed to prevent any potential damage during operation.
5V - Radiation Hardening
Radiation hardening is the process of making electronic components and circuits resistant to damage or malfunction caused by high levels of ionizing radiation, especially for environments in outer space (especially beyond the low Earth orbit), around nuclear reactors and particle accelerators, or during nuclear accidents or nuclear warfare.
No - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
Non-RoHS Compliant
2N2218 Features
Type: NPN
Collector-Emitter Voltage: 30 V
Collector-Base Voltage: 60 V
Emitter-Base Voltage: 5 V
Collector Current: 0.8 A
Collector Dissipation: 0.8 W
DC Current Gain (hfe): 40 to 120
Transition Frequency: 250 MHz
Operating and Storage Junction Temperature Range: -65 to +200 °C
Package: TO-39
2N2218 Complementary PNP transistor
The 2N2102 is a complementary PNP transistor for the 2N2218.
Equivalents for 2N2218
2N2219, 2N4237, NTE123, 2N3108, 2N4030, 2N4238, ECG123, 2N2219A, 2N3252, 2N3110
2N2218 Applications
General and High Speed Switching
Audio Amplifiers
Signal Amplifiers
RF Circuits
Darlington Pairs
Variety of General Purpose Applications
Parts with Similar Specs
Where an how to use 2N2218
The 2N2218 transistor is suitable for any general-purpose application that comes within its specifications. It can, for example, be used as a switch to drive loads of up to 800mA; with an 800mA collector current, it can power high-power LEDs, motors, relays, and transistors, among other things. It can also be used as a stand-alone audio amplifier to drive a speaker or in the stages of an audio amplifier. Aside from that, it can be utilized in RF circuits such as FM radios and FM transmitters, as well as other RF circuits below 250MHz.
How does 2N2218 work in a circuit safely?
The 2N2218 transistor is suitable for any general-purpose application that comes within its specifications. It can, for example, be used as a switch to drive loads of up to 800mA; with an 800mA collector current, it can power high-power LEDs, motors, relays, and transistors, among other things. It can also be used as a stand-alone audio amplifier to drive a speaker or in the stages of an audio amplifier. Aside from that, it can be utilized in RF circuits such as FM radios and FM transmitters, as well as other RF circuits below 250MHz.
2N2218 Package Dimensions

2N2218 Package Dimensions
2N2218 Manufacturer
Microsemi Corporation (Nasdaq: MSCC) offers a comprehensive portfolio of semiconductor and system solutions for aerospace & defense, communications, data center, and industrial markets. Products include high-performance and radiation-hardened analog mixed-signal integrated circuits, FPGAs, SoCs, and ASICs; power management products; timing and synchronization devices and precise time solutions, setting the world's standard for time; voice processing devices; RF solutions; discrete components; enterprise storage and communication solutions, security technologies, and scalable anti-tamper products; Ethernet solutions; Power-over-Ethernet ICs and midspans; as well as custom design capabilities and services.
Datasheet PDF
- Datasheets :
What is the use of 2N2218?
2N2218 is designed for high-speed switching applications at collector currents up to 500 mm and features useful current gain over a wide range of collector current, low leakage currents, and low saturation voltages.
What is the voltage of 2N2218?
1.6V
A General Introduction to BMX055 [Faq]20 April 20221575
STM32F302RCT6 Microcontroller: 32-Bit, 64-LQFP, Pinout and Datasheet17 January 2022710
M6060P-E3/45 Schottky Rectifier: Datasheet, Pinout, Specifications18 August 2021414
CR123A VS. RCR123A: Are They Interchangeable? [FAQ & Video]24 August 20229780
H11L1 Trigger Photocoupler: Pinout, Datasheet and Circuit14 July 20218553
Introduction to NXP KL28Z Microcontroller28 February 2024177
AD7768 Analog-to-Digital Converter (ADC): AD7768 Arduino, Datasheet, Pinout18 January 20226041
LNK304PN integrated circuit: Features, Applications and datasheet13 October 20233191
How to Select Stepper Motor Controllers for Precision19 July 2025582
Automatic Voltage Regulator: Ultimate Guide to Stable Power and Equipment Protection06 May 20256012
What is a Memory Controller?12 August 202032666
Chip Packaging Lead Time Has Grown to 50 Weeks07 April 20224201
What is a SAW Sensor? Types, Working and Applications29 March 202118989
What is a Microcontroller?30 October 2025114738
Challenges in Enhancing Power Electronic Systems with Artificial Intelligence26 December 20232636
What is ISP (Image Signal Processor)?15 September 202135212
Microsemi Corporation
In Stock: 5470