A76 Battery VS 357: Which battery to choose?

UTMEL

Published: 24 March 2022 | Last Updated: 24 March 2022

27779

A76

A76

Energizer Battery Company

BATTERY ALKA 1.5V BUTTON 11.6MM

Purchase Guide

BATTERY ALKA 1.5V BUTTON 11.6MM

Size 357 batteries are silver oxide batteries, while A76 batteries are alkaline batteries. Check with this article if uncertain on which battery to choose.

This video demonstrates details about a76 battery.

Button Battery LR44 = AG13 = L1154 = 357 = SR44 = A76

Introduction

Size 357 batteries are silver oxide batteries, while A76 batteries are alkaline batteries. The Energizer 357  and A76  batteries are small batteries with a wide range of applications. Watches, medical devices, laser pointers, and other items require these 1.5 volts 357 batteries.

 a76 vs 357.jpg

A76 VS 357


What is A76  battery?

The Energizer A76 Miniature Alkaline Cell 1.5-Volt Battery gives your button-battery-operated products, such as medical devicescalculatorstoys, and watches, long-lasting, consistent power. When stored properly, button batteries can last up to 5 years, ensuring that you have them on hand when you need them.

a76 battery.jpg

A76 Battery

What is 357 battery?

The Energizer 357 battery is a 1.55V silver oxide battery. Small deviceswatches, gadgets, and toys frequently use these batteries. The following batteries are compatible with the 357 battery:

LR1154, L1154, LR44, SR44SW/W, 303, A76, AG13, EPX76, LR1154, L1154, LR44SW/W


A76 VS 357 Battery: Specifications

Battery No.A76357
Chemical System Manganese Dioxide (MnO2) Silver Oxide (Zn/Ag2O)
Designation ANSI/NEDA 1166A, IEC-LR44 ANSI-1131SO, IEC-SR44
Nominal Voltage 1.5 Volts 1.55 Volts
Typical Capacity 175 mAh* (to 0.9 volts) 150 mAh* (to 1.2 volts)
Capacity Test 6.8K ohm continuous drain   at 21°C (70°F) 6.8K ohm continuous drain   at 21°C
Typical Weight 1.85 grams (0.07 oz.) 2.3 grams (0.08 oz.)
Typical Volume 0.57 cubic centimeters   (0.035 cubic inch) 0.57 cubic centimeters   (0.035 cubic inch)
Impedance (40 Hz) 5 to 15 ohms 5 to 15 ohms


A76 VS 357 Battery: Where to use

A76 is designed to power your small gadgets, most commonly used in watches, thermometers, calculators, key fobs, garage door openers, electronic toys, and more.

These 1.5-volt size 357 batteries are used in watches, medical equipment, laser pointers, and more.


A76 VS 357 Battery: Internal Diagram

A76 internal diagram.jpg

A76 Internal Diagram

357 internal diagram.jpg

357 Internal Diagram

A76 VS 357 Battery: Discharge Characteristics

a76 discharge characteristics.jpg

A76 Discharge Characteristics

357 discharge characterstics.jpg

357 Discharge Characteristics

A76 VS 357 Battery: Dimensions

A76 dimensions.jpg

A76 Dimensions

357 dimensions.jpg

357 Dimensions

A76 VS 357 Battery: Manufacturer

With global headquarters in St. Louis and widely recognized the world over, Energizer® and Eveready® branded products are marketed and sold in more than 150 countries around the globe. Energizer's battery business delivers the industry's most comprehensive portfolio of products. This extensive portfolio includes Carbon Zinc; Industrial Alkaline; Lithium AA Super-Premium; Photo Lithium; Coin cells; Flashlights and Lanterns.  Energizer Holdings, Inc. became an independent, publicly held company in 2000 and is traded on the New York Stock Exchange under the symbol ENR.

Are A76 and LR44 the same?

The LR44 designation is an international standard (IEC 60086-3) that specifies the battery size and chemistry. The power is provided by alkaline chemistry in L batteries; in the case of the LR44, it is zinc-manganese dioxide. Both the manufacturer's part numbers AG13 and A76 are for batteries that can be used instead of LR44 batteries. Despite the fact that they are the same size as the LR44, the internal chemistry employed can differ, affecting battery life.

The Differences between silver oxide and alkaline batteries

The Silver Oxide batteries are primary cells with very high energy to weight ratio. Its energy capacity is roughly twice that of button-type alkaline batteries. Compared with alkaline batteries, silver oxide batteries offer a flatter discharge curve than alkaline batteries and a longer operating time than lithium-ion batteries.

Frequently Asked Questions

Are A76 and 357 batteries interchangeable?

Yes. The 357 is compatible in size with the A76. The A76 uses an alkaline manganese dioxide construction and will have a shorter service life than the 357 which has silver oxide chemistry.

Is a Duracell 76 the same as a 76A?

This Duracell 76 Alkaline battery is equivalent to LR44, A76, PX76A, V136A, AG13, and L1154.

Is A76 same as LR1130?

A6 battery is not a replacement for the LR1130.

What battery is equivalent to A76?

LR44 battery equivalents are also referred to as A76, AG13, L1154, LR1154, 157. These sizes are possible LR44 battery replacements. Other batteries are similar to the LR44 battery but are different in composition chemistry.

What battery can replace 357?

LR44 Alkaline Battery replaces 357 SG13 303 A76 EXP76 SR44 AG13 LR1154 SR44SW/W, Pack of 4 batteries.
A76

Energizer Battery Company

In Stock
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
Related Parts More