Everything You Need to Know About TL494 Current-Mode PWM Controller
16 Terminals TL494 DC to DC converter IC SWITCHING CONTROLLER 2 Outputs 200kHz Transistor Driver









16 Terminals TL494 DC to DC converter IC SWITCHING CONTROLLER 2 Outputs 200kHz Transistor Driver
The TL494 IC is a fixed frequency current-mode PWM controller IC with all the functions that are required in the construction of the pulse-width modulation (PWM) control circuit on a single chip. This article will introduce TL494 systematically from its features, pinout to its specifications, applications, and so much more.

Difference between sg3525 and TL494 (Who is Winner Lts Find Out).???
TL494 Description
The TL494 device incorporates all the functions required in the construction of a pulse-width-modulation (PWM) control circuit on a single chip. Designed primarily for power-supply control, this device offers the flexibility to tailor the power-supply control circuitry to a specific application.
The TL494 device contains two error amplifiers, an on-chip adjustable oscillator, a dead-time control (DTC) comparator, a pulse-steering control flip-flop, a 5-V, 5%-precision regulator, and output-control circuits.
The error amplifiers exhibit a common-mode voltage range from –0.3 V to VCC – 2 V. The dead-time control comparator has a fixed offset that provides approximately 5% dead time. The on-chip oscillator can be bypassed by terminating RT to the reference output and providing a sawtooth input to CT, or it can drive the common circuits in synchronous multiple-rail power supplies.
The uncommitted output transistors provide either common-emitter or emitter-follower output capability. The TL494 device provides for push-pull or single-ended output operation, which can be selected through the output-control function. The architecture of this device prohibits the possibility of either output being pulsed twice during push-pull operation.
The TL494C device is characterized for operation from 0°C to 70°C. The TL494I device is characterized for operation from –40°C to 85°C.
TL494 Features
Complete PWM Power-Control Circuitry
Uncommitted Outputs for 200-mA Sink or Source Current
Output Control Selects Single-Ended or Push-Pull Operation
Internal Circuitry Prohibits Double Pulse at Either Output
Variable Dead Time Provides Control Over Total Range
Internal Regulator Provides a Stable 5-V Reference Supply With 5% Tolerance
Circuit Architecture Allows Easy Synchronization
TL494 Applications
Desktop PCs
Microwave Ovens
Power Supplies: AC/DC, Isolated, With PFC, > 90 W
Server PSUs
Solar Micro-Inverters
Washing Machines: Low-End and High-End
E-Bikes
Power Supplies: AC/DC, Isolated, No PFC, < 90 W
Power: Telecom/Server AC/DC Supplies: Dual Controller: Analog
Smoke Detectors
Solar Power Inverters
TL494 Application Examples
As we mentioned earlier, the TL494 is a PWM controller circuit. Hence, most of its applications are PWM-based circuits. Here are a few examples:
TL494 Solar Charger
You can easily configure this design by building a 5v/10A switching power supply buck. For this configuration, you can get your output in parallel modes. While you’re at it, connect the output-control pin 13 to the ground.
This application also uses two error amps efficiently (one controls voltage feedback and maintains a constant output while the other controls the maximum current).
TL494 Classic Inverter Circuit
In this application, you can configure the output to work in the push-pull mode. Hence, it would help connect the out-put control pin with the +5 V reference to pin 14. The other nails have the same configuration as the pinout datasheet above.
TL494 Pinout and Configurations

| Name | NO. | Description |
| 1IN+ | 1 | Noninverting input to error amplifier 1 |
| 1IN | 2 | Inverting input to error amplifier 1 |
| 2IN+ | 16 | Noninverting input to error amplifier 2 |
| 2IN- | 15 | Inverting input to error amplifier 2 |
| C1 | 8 | The collector terminal of BJT output 1 |
| C2 | 11 | The collector terminal of BJT output 2 |
| CT | 5 | The capacitor terminal used to set the oscillator frequency |
| DTC | 4 | Dead-time control comparator input |
| E1 | 9 | The emitter terminal of BJT output 1 |
| E2 | 10 | The emitter terminal of BJT output 2 |
| FEEDBACK | 3 | Input pin for feedback |
| GND | 7 | Ground |
| OUTPUT CTRL | 13 | Selects single-ended/parallel output or push-pull operation |
| REF | 14 | The 5-V reference regulator output |
| RT | 6 | The resistor terminal used to set the oscillator frequency |
| VCC | 12 | Positive Supply |
How to use TL494?
A test circuit from the TL494 datasheet is shown below.

Non-inverting pins are connected to the Ref pin while inverting pins are connected to the ground. Test inputs are given to DTC and FEEDBACK pins. The external capacitor and resistor are connected to pins 5 & 6 to control the oscillator frequency. The error amplifier compares a sample of the 5-V output to the reference and adjusts the PWM to maintain a constant output current
Where to use TL494 ?
The TL494 fixed frequency PWM Controller can be used for DC to DC conversion regardless of buck or boost topology. TL494 can be used to provide a constant current by varying the output voltage to the load. This IC feature an output control circuit, a flip flop, a dead time comparator, two different error amplifiers, a 5V reference voltage, an oscillator, and a PWM comparator.
So if you are looking for an IC to produce PWM signals for controlling a power switch based on the current flowing through the circuit, then this IC might be the right choice for you.
TL494 Package
| Package | Pins | Size |
| PDIP (N) | 16 | 181 mm² 19.3 x 9.4 |
| SOIC (D) | 16 | 59 mm² 9.9 x 6 |
| SOP (NS) | 16 | 80 mm² 10.2 x 7.8 |
| TSSOP (PW) | 16 | 22 mm² 4.4 x 5 |
Datasheet PDF
- PCN Obsolescence/ EOL :
- Datasheets :
Parts with Similar Specs
What is PWM IC?
The TL494 fixed frequency PWM Controller can be used for DC to DC conversion regardless of buck or boost topology. ... This IC feature an output control circuit, a flip flop, a dead time comparator, two different error amplifiers, a 5V reference voltage, an oscillator, and a PWM comparator.
How does PWM IC work?
As its name suggests, pulse width modulation speed control works by driving the motor with a series of “ON-OFF” pulses and varying the duty cycle, the fraction of time that the output voltage is “ON” compared to when it is “OFF”, of the pulses while keeping the frequency constant.
What is TL494?
TL494 is a PWM controller IC used for power electronics circuits. It comprises on-chip two error amplifiers an oscillator with adjustable frequency feature, an output flip-flop having pulse steering control, and an output control circuit with feedback.
What is the use of TL494?
TL494 is a PWM controller IC used for power electronics circuits. It comprises on-chip two error amplifiers an oscillator with adjustable frequency feature, an output flip-flop having pulse steering control, and an output control circuit with feedback.
Is PWM AC or DC?
It's neither, really. AC means that the voltage/current changes polarity. A PWM signal typically is a logic signal that turns on and off. So, a PWM signal is more accurately described as a pulsed DC signal.
1N4728A Zener Diode: Datasheet, Voltage and Specifications30 September 20215506
Understanding STM32G0B0RET6 Troubleshooting Techniques09 July 2025504
2N3906 PNP Transistor: Pinout, Datasheet and Circuit13 July 202116267
Comprehensive Guide to STM32L431CBT6 for Developers24 July 20253033
BC558 Transistor: Pinout, Alternatives and Datasheet06 August 20219873
TDA2050 Amplifier: Datasheet, Circuit, Replacement29 October 202126890
A Comprehensive Guide to LTC6801HG#3ZZTRPBF Battery Management PMIC06 March 2024272
74HC259 8-Bit Addressable Latch : Pinout, Application and Datasheet08 July 20213640
Chiplet Brings Change to the Business Model of IP Design Companies05 September 20224624
MCU with Built-in NPU: How to Pick an Edge AI Microcontroller in 202630 July 20261992
What is Solenoid Valve? How to Choose a Solenoid Valve?06 January 20224560
Msemitek Authorized Distributor | UTMEL Electronics21 November 20234103
Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators19 November 20243372
Getting Started with Arduino: What is Arduino and How to Use Arduino Boards28 September 20237382
What is a Synchronous Motor?16 March 20217490
Trusted Vibration Sensors for Homeowners and Industry Professionals17 July 20251648
ON Semiconductor
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools