Is LM317 better than LM7805?[video+FAQ]

Sophie

Published: 27 April 2022 | Last Updated: 27 April 2022

8691

LM7805CT

LM7805CT

ON Semiconductor

Fixed 2.54mm LM7805 PMIC TO-220-3

Purchase Guide

Fixed 2.54mm LM7805 PMIC TO-220-3

Here is a comparison article about LM317 and LM7805, which introduces their datasheets, features, applications, pinouts, and advantages respectively.

This is a introduction video about LM317.

LM317 VOLTAGE REGULATOR Tutorial | How to use? | Pinout

LM317 Basics

LM317 is an adjustable three-terminal regulator. The world's major IC manufacturers have similar products to choose from. Therefore, LM317 is a widely used series of integrated voltage regulators and can be used as a voltage regulator circuit in a DC-regulated power supply.

lm317 pinout.jpg

lm317 pinout

Pin NumberPin NameDescription
1AdjustThese pins adjust the output voltage
2Output Voltage (Vout)The regulated output voltage set by the adjusted pin can be obtained from this pin
3Input Voltage (Vin)The input voltage which has to be regulated is given to this pin


LM7805 Basics

LM7805 is a 5V output positive voltage regulator IC. It is the IC of the LM78xx positive voltage regulator series. It is manufactured in TO-220 and other packages. This IC is quite reliable and it is widely used in commercial equipment and educational project.

lm7805 pinout.jpg

lm7805 pinout

Pin NumberPin NameDescription
1Input (V+)Unregulated Input Voltage
2Ground (GND)Connected to Ground
3Output (Vo)Outputs Regulated +5V


What is LM in LM7805?

A prefix is given by the manufacturer to identify the version. The prefix LM stands for linear monolithic. LM series was firstly manufactured by National Semiconductor & the first time prefix LM was given for linear ICs.


What does 7805 stand for?

7805 in LM7805 signifies two meanings-

78” means that it is a positive voltage regulator. It produces a voltage that has a positive magnitude with respect to the ground.

05” represents its output voltage value.


LM317 VS LM7805: Datasheet

LM317 VS LM7805: Features

LM317 Features

  • Output voltage range adjustable from 1.25V to 37V

  • Output current greater than 1.5A

  • Internal short-circuit current limiting

  • Thermal overload protection

  • Output safe-area compensation

LM7805 Features

  • 5V Positive Voltage Regulator

  • The minimum Input Voltage is 7V

  • The maximum Input Voltage is 25V

  • Operating current(IQ) is 5mA     

  • Internal Thermal Overload and Short circuit current limiting protection are available.

  • Junction Temperature maximum 125 degrees Celsius

  • Available in TO-220 and KTE package


LM317 VS LM7805: Applications

LM317 Applications

  • Used for Positive voltage regulations

  • Variable power supply

  • Current limiting circuits

  • Reverse polarity circuits

  • Commonly used in Desktop PC, DVDs, and other consumer products

  • Used in motor control circuits

 

LM7805 Applications

  • Constant +5V output regulator to power microcontrollers and sensors in most of the projects

  • Adjustable Output Regulator

  • Current Limiter for certain applications

  • Regulated Dual Supply

  • Output Polarity-Reversal-Protection Circuit


LM317 VS LM7805: Equivalents

LM317 Equivalents

LT1086, LM1117 (SMD), PB137, LM337 (Negative Variable Voltage regulator)

LM7805 Equivalents

LM317, L78M05(0.5 A), LM117V33


Is LM7805 better than LM317?

  1. The ability for adjustable voltage:

LM317 can give an adjustable output voltage in the range of 1.5V to 37V, whereas LM7805 can only give an output voltage of 5V

  2. Output Current Capabilities:

LM317 has the capability to give an output current of more than 1.5A whereas LM7805 can only give an output current only up to 1.5A

  3. Components needed:

LM317 requires more external components (adjustment pot or precision resistors to set the voltage divider etc.) as compared to the LM7805


LM317 VS LM7805: Conclusion

  1. LM317 is an adjustable voltage regulator, while LM7805 is the constant voltage regulator.

  2. LM317 can give an adjustable output voltage in the range of 1.5V to 37V, whereas LM7805 can only give an output voltage of 5V.

  3. What’s more, LM317 has the capability to give an output current of more than 1.5A whereas LM7805 can only give an output current only up to 1.5A.

  4. LM317 requires more external components (adjustment pot or precision resistors to set the voltage divider etc.) as compared to the LM7805.


Frequently Asked Questions

What is the max input voltage for LM7805?

35V

How to Safely Long Run LM7805 in a Circuit?

For stable and long term performance consideration,  LM7805 is suggested to not operate load more than 1.5A, and make sure always use a suitable heatsink with it, always check pinout before using in your application, and do not operate in temperature below 0 degree Celsius and above +125 degree Celsius, what's more,  always store it in temperature above -65 degree Celsius and below +150 degree Celsius.

What is the maximum input voltage of a LM317?

The maximum input voltage of LM317 is 40 V. The LM317 can operate as long as the difference between its input voltage and the desired output voltage is in the range of 3-40 V.

What is a LM317 used for?

The LM317 is commonly used as:
1. A voltage regulator in electronic devices to provide a stable output voltage.
2. A precision current regulator to provide constant current.
3. In designing battery charger circuits and variable power supplies.

How does LM317 work?

An LM317 is a voltage regulator that can supply variable output voltage. The working principle of the LM317 is very simple. It uses a voltage divider, formed by using two external resistors connected in series. The output voltage is adjusted by varying the resistor values.
LM7805CT

ON Semiconductor

In Stock: 1
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
Related Parts More