LP5569RTWR 9 CHANNEL RGB DRIVER

Sophie

Published: 24 March 2022 | Last Updated: 24 March 2022

856

LP5569RTWR

LP5569RTWR

Texas Instruments

0.5mm PMIC LP5569 24 Pin 3.6V 24-WFQFN Exposed Pad

Purchase Guide

0.5mm PMIC LP5569 24 Pin 3.6V 24-WFQFN Exposed Pad

Texas Instruments LP5569RTWR I2C RGB LED Driver is a programmable, easy-to-use 9-channel I2C LED driver designed to produce lighting effects for various applications. This passage is going to introduce LP5569RTWR from the perspectives of the datasheet, pinout, and other ways.

LP5569RTWR Description

The LP5569RTWR  is a programmable, easy-to-use 9  -channel I2C  LED driver that may be used to create various lighting effects. The LED driver includes an internal SRAM memory for user-programmed sequences as well as three programmable LED engines for operation without the usage of a processor. When the processor is put into sleep mode, autonomous functioning minimizes system power usage.

Even with a 2.5  -V input voltage, a high-efficiency charge pump can drive LEDs with high VF. By autonomously selecting the appropriate charge-pump gain depending on LED forward voltage needs, the LP5569RTWR   LED driver maintains good efficiency throughout a wide operating voltage range. When LEDs are not active, the LP5569RTWR  gadget enters power-saving mode, significantly reducing idle-current usage.


LP5569RTWR Pins and Pins Functions

QQ截图20220324112150.jpg

PINTYPEDESCRIPTION
NAMENO.
ADDR20II2C slave-address selection pin.
AGND4GAnalog and digital ground. Connect to PGND, exposed thermal pad, and common ground plane.
C1-24ANegative pin of charge-pump flying capacitor 1. If a charge pump is not used, this pin must be left floating.
C1+2APositive pin of charge-pump flying capacitor 1. If a charge pump is not used, this pin must
be left floating.
C2-23ANegative pin of charge-pump flying capacitor 2. If a charge pump is not used, this pin must
be left floating.
C2+1APositive pin of charge-pump flying capacitor 2. If a charge pump is not used, this pin must
be left floating.
CLK6I, ODClock input/output. By default, this pin is a clock input. If not used, this pin must be
connected to GND or VIN.
EN/PWM5IChip enable and PWM input pin.
GPIO/TRIG/INT7I, ODGeneral-purpose input or open-drain output, trigger input or open-drain output, or interrupt open-drain output. This pin function is configured in the I2C registers. By default, this pin is a general-purpose output (open-drain) and can be left floating if not used.
LED019ALED current sink 0. If not used, this pin can be left floating.
LED118ALED current sink 1. If not used, this pin can be left floating.
LED217ALED current sink 2. If not used, this pin can be left floating.
LED316ALED current sink 3. If not used, this pin can be left floating.
LED415ALED current sink 4. If not used, this pin can be left floating.
LED514ALED current sink 5. If not used, this pin can be left floating.
LED613ALED current sink 6. If not used, this pin can be left floating.
LED712ALED current sink 7. If not used, this pin can be left floating.
LED811ALED current sink 8. If not used, this pin can be left floating.
PGND21GCharge-pump power ground. Connect to AGND, exposed thermal pad, and common
ground plane.
SCL9II2C bus clock line. If not used, this pin must be connected to GND or VIN.
SDA8I, ODI2C bus data line. If not used, this pin must be connected to GND or VIN.
V1P810PInput power for digital circuitry.
VIN3PInput power, a 1-µF capacitor must be connected between PGND and this pin.
VOUT22ACharge-pump output voltage. If a charge pump is used, a 1-µF capacitor must be
connected between PGND and this pin. If charge pump is not used or is used in 1×
the mode only, the capacitor can be omitted.


LP5569RTWR Feature

  • Supply Voltage Range: 2.5 V–5.5 V • Nine High-Accuracy Current Sinks

– 25.5 mA Maximum per Channel 

– 8-Bit Individual Current Control

– 12-Bit 20-kHz Internal Individual PWM Control Without Audio Noise

  • Three Programmable LED Engines

– Independent Illumination Control Without Active Microcontroller Control

– Synchronization Among Multiple Devices 

– Up to 256 Instructions in SRAM Memory  for Storing Sequences of Lighting Patterns 

– LP5523  - and LP5523  1-Device-Compatible Command Set

  • Flexible Dimming Control

– I2C Dimming Control

– PWM Direct-Input Dimming 

– PWM Input Frequency: 100-Hz to 20-kHz

  • Adaptive High-Efficiency Charge-Pump Control for driving High  -VF LEDs  With Low Battery Voltage

  • Master Fader Control Allows Dimming of MultipleLEDs by Writing to Only One Register to Reduce the I2C Bus Traffic

  • 2-µA Low Standby Current  and 10-µA in automatic Power-Save Mode When LEDs  AreInactive

  • POR, UVLO, and TSD Protections 


LP5569RTWR CAD Models

Symbol

symbol.jpg

Footprint

footprint.jpg

3D Models

3d.jpg

Specifications

Texas Instruments LP5569RTWR technical specifications, attributes, parameters and parts with similar specifications to Texas Instruments LP5569RTWR.
  • Type
    Parameter
  • Lifecycle Status

    Lifecycle Status refers to the current stage of an electronic component in its product life cycle, indicating whether it is active, obsolete, or transitioning between these states. An active status means the component is in production and available for purchase. An obsolete status indicates that the component is no longer being manufactured or supported, and manufacturers typically provide a limited time frame for support. Understanding the lifecycle status is crucial for design engineers to ensure continuity and reliability in their projects.

    ACTIVE (Last Updated: 2 days ago)
  • Factory Lead Time
    6 Weeks
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    24-WFQFN Exposed Pad
  • Surface Mount

    having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.

    YES
  • Number of Pins
    24
  • SwitchingFrequency
    1.25MHz
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -40°C~85°C
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e4
  • Pbfree Code

    The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.

    yes
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    2 (1 Year)
  • Number of Terminations
    24
  • Type
    Linear
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Nickel/Palladium/Gold (Ni/Pd/Au)
  • Applications

    The parameter "Applications" in electronic components refers to the specific uses or functions for which a component is designed. It encompasses various fields such as consumer electronics, industrial automation, telecommunications, automotive, and medical devices. Understanding the applications helps in selecting the right components for a particular design based on performance, reliability, and compatibility requirements. This parameter also guides manufacturers in targeting their products to relevant markets and customer needs.

    General Purpose
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    QUAD
  • Number of Functions
    1
  • Supply Voltage

    Supply voltage refers to the electrical potential difference provided to an electronic component or circuit. It is crucial for the proper operation of devices, as it powers their functions and determines performance characteristics. The supply voltage must be within specified limits to ensure reliability and prevent damage to components. Different electronic devices have specific supply voltage requirements, which can vary widely depending on their design and intended application.

    3.6V
  • Terminal Pitch

    The center distance from one pole to the next.

    0.5mm
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    LP5569
  • Number of Outputs
    9
  • Output Voltage

    Output voltage is a crucial parameter in electronic components that refers to the voltage level produced by the component as a result of its operation. It represents the electrical potential difference between the output terminal of the component and a reference point, typically ground. The output voltage is a key factor in determining the performance and functionality of the component, as it dictates the level of voltage that will be delivered to the connected circuit or load. It is often specified in datasheets and technical specifications to ensure compatibility and proper functioning within a given system.

    5.5V
  • Max Supply Voltage

    In general, the absolute maximum common-mode voltage is VEE-0.3V and VCC+0.3V, but for products without a protection element at the VCC side, voltages up to the absolute maximum rated supply voltage (i.e. VEE+36V) can be supplied, regardless of supply voltage.

    5.5V
  • Min Supply Voltage

    The minimum supply voltage (V min ) is explored for sequential logic circuits by statistically simulating the impact of within-die process variations and gate-dielectric soft breakdown on data retention and hold time.

    2.5V
  • Output Current

    The rated output current is the maximum load current that a power supply can provide at a specified ambient temperature. A power supply can never provide more current that it's rated output current unless there is a fault, such as short circuit at the load.

    160mA
  • Topology

    In the context of electronic components, "topology" refers to the arrangement or configuration of the components within a circuit or system. It defines how the components are connected to each other and how signals flow between them. The choice of topology can significantly impact the performance, efficiency, and functionality of the electronic system. Common topologies include series, parallel, star, mesh, and hybrid configurations, each with its own advantages and limitations. Designers carefully select the appropriate topology based on the specific requirements of the circuit to achieve the desired performance and functionality.

    Switched Capacitor (Charge Pump)
  • Internal Switch(s)

    The term "Internal Switch(s)" in electronic components typically refers to a built-in mechanism within a device that allows for the control of electrical current flow. These internal switches can be used to turn circuits on or off, change the direction of current, or regulate the flow of electricity within the component. They are often designed to be controlled externally, either manually or automatically, to enable various functions or operations within the electronic device. Internal switches play a crucial role in the overall functionality and performance of electronic components by providing a means to manage and manipulate electrical signals effectively.

    No
  • fmax-Min

    fmax-Min refers to the frequency range that an electronic component or system can operate within. It represents the difference between the maximum frequency (fmax) and the minimum frequency (Min) limits of operation. This parameter is crucial in defining the bandwidth of the component, indicating how effectively it can transmit or receive signals over that range. A wider fmax-Min value typically signifies better performance for applications that require broad frequency response.

    0.4 MHz
  • Dimming

    Dimming is a feature in electronic components, such as LED lights or display screens, that allows the user to adjust the brightness level of the device. It is a method of controlling the amount of light output by the component, typically by varying the voltage or current supplied to it. Dimming can be achieved through various techniques, such as pulse-width modulation (PWM) or analog dimming. This feature is commonly used to save energy, create ambiance, or enhance visual comfort in different applications.

    I2C, PWM
  • Number of Segments
    9
  • Max Junction Temperature (Tj)

    Max Junction Temperature (Tj) refers to the maximum allowable temperature at the junction of a semiconductor device, such as a transistor or integrated circuit. It is a critical parameter that influences the performance, reliability, and lifespan of the component. Exceeding this temperature can lead to thermal runaway, breakdown, or permanent damage to the device. Proper thermal management is essential to ensure the junction temperature remains within safe operating limits during device operation.

    125°C
  • Voltage - Supply (Min)

    Voltage - Supply (Min) is a parameter in electronic components that specifies the minimum voltage required for the component to operate within its specified performance range. This parameter indicates the lowest voltage level that can be safely applied to the component without causing malfunctions or damage. It is crucial to ensure that the supply voltage provided to the component is equal to or higher than the specified minimum voltage to guarantee proper functionality and reliability. Failure to meet this requirement may result in erratic behavior, reduced performance, or even permanent damage to the component.

    2.5V
  • Multiplexed Display Capability

    Multiplexed Display Capability refers to the ability of an electronic component or system to control multiple display elements using fewer input/output lines. This is achieved by rapidly switching between different displays or segments, allowing for efficient communication and reduced wiring complexity. In multiplexed systems, each display is activated sequentially, creating the illusion of simultaneous display to the user. This capability is commonly utilized in devices like LED matrices and LCD screens to enhance functionality while conserving space and resources.

    NO
  • Ambient Temperature Range High

    This varies from person to person, but it is somewhere between 68 and 77 degrees F on average. The temperature setting that is comfortable for an individual may fluctuate with humidity and outside temperature as well. The temperature of an air conditioned room can also be considered ambient temperature.

    85°C
  • Data Input Mode

    Data Input Mode in electronic components refers to the specific method or protocol used to input data into the component. This parameter determines how data is received and processed by the component, whether it be through serial communication, parallel communication, or other interfaces. The data input mode is crucial for ensuring compatibility and proper functioning of the component within a larger electronic system. Understanding and configuring the data input mode correctly is essential for effective data transfer and communication between different components in a circuit or system.

    SERIAL
  • Height
    800μm
  • Length
    4mm
  • Width
    4mm
  • Thickness

    Thickness in electronic components refers to the measurement of how thick a particular material or layer is within the component structure. It can pertain to various aspects, such as the thickness of a substrate, a dielectric layer, or conductive traces. This parameter is crucial as it impacts the electrical, mechanical, and thermal properties of the component, influencing its performance and reliability in electronic circuits.

    750μm
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
0 Similar Products Remaining

LP5569RTWR Applications

LED Lighting, Indicator Lights, and Fun Lights for:

• Smart Speaker

• Smart Home Appliance

• Doorbell

• Electric Lock

• Smoke Detector

• Thermostat

• Set-Top Box

• Smart Router

• Bluetooth® Headset

• Cell Phone


LP5569RTWR Applications Circuit

QQ截图20220324111959.jpg

LP5569RTWR Functional Block Diagram

functional block diagram.jpg

LP5569RTWR Manufacturer

Texas Instruments Incorporated (TI) is an American technology company based in Dallas, Texas, that designs and manufactures semiconductors and integrated circuits for electronic designers and manufacturers around the world. Based on sales volume, it is one of the top ten semiconductor companies in the world. Analog chips and embedded processors, which account for more than 80  % of the company's revenue, are the company's main focus. TI also makes calculators, microcontrollers, and multi-core processors, as well as TI digital light processing technology and education technology,  As of 2016, the company had 45,000  patents worldwide.

LP5569RTWR Package

LP5569RTWR Advantages

  1. Current Sinks

The LP5569RTWR   LED drivers are constant-current sources. Maximum output-current scale can be programmed by control registers up to 25.5 mA.

  1. Charge Pump

The LP5569RTWR  device includes a pre-regulated switched-capacitor charge pump with a programmable voltage multiplication of 1× or 1.5×.

  1. Energy Efficiency

The red LED  (R) element of an RGB LED  typically has a forward voltage of about 2 V. these LED s can be powered directly from the input voltage because battery voltage is typically high enough to drive red LED  s over the whole operating voltage range.

  1. Automatic Power-Save Mode

When the LED  outputs are not active, the LP5569RTWR  device is able to enter power-save mode automatically, thus lowering idle-current consumption down to TBD μA (typical). Automatic power-save mode is enabled when the MISC register (address 2Fh) POWERSAVE_EN bit = 1.

  1. Protection Features

It has four protection features, including Thermal Shutdown, Undervoltage Lockout  (UVLO), Power-On Reset  (POR), LED  Fault Detection

  1. Clock Generation and Synchronization 

The LP5569RTWR  device can generate a 32-kHz clock signal and use it for synchronizing multiple devices. The CLK pin is configured as an input by default 


P5569RTWR Dimensions

Height800μm
Length4mm
Thickness750μm
Width4mm


Trend Analysis

Datasheet PDF

Download datasheets and manufacturer documentation for Texas Instruments LP5569RTWR.

Parts with Similar Specs

Frequently Asked Questions

What is LP5569RTWR?

The LP5569RTWR device is a fully integrated lighting management unit for producing lighting effects for various LED applications. The LP5569RTWR device includes all necessary power management, low-side current sinks, a two-wire serial I2C-compatible interface, and programmable LED engines.

Does LP5569RTWR have protection features?

Yes, its protection features include power-on reset, charge-pump, input-current limiter, thermal shutdown(TSD), and under-voltage lockout(UVLO).

Can LP5569RTWR be operated in 100℃?

No, its operating temperature is between -40 and 85℃.

Where is LP5569RTWR made from?

It is made by an American company-Texas Instruments Incorporated.

What’s the main parameters of LP5569RTWR?

the main parameters of this part are: Nine-channel I2C RGB LED driver with engine control and charge pump 24-WQFN -40 to 85.
LP5569RTWR

Texas Instruments

In Stock: 10000

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More