The World's Top 10 Innovative LED Drivers

How To Choose The Correct LED Driver For Your LED Lights
Catalog |
As the core component of LED lighting products, the technical content of the LED driver is directly related to the quality of light brought by the LED lighting source. With the global lighting industry showing the trend of multi-discipline application expansion in recent years, the industry chain "source" attribute of the LED driver has become more and more prominent, and a number of strong upstream and midstream lighting companies around the world have been through the technical innovation in this core lighting component to bring a surge of power for the diversified development of the lighting industry.
To this end, Utmel.com brings important scientific and technological references for LED driver manufacturing enterprises by showing the top ten innovative LED driver parts in the world in the past three years.
1 Three channel linear LED driver
Application areas: automotive lighting

AL5873Q
In June 2021, the United States Diodes Incorporated launched a three-channel linear LED driver AL5873Q, designed to simplify the design of tail light sets and expand its portfolio of devices to support automotive exterior lighting.
The device is automotive-compatible and AEC-Q100 Level 1 compliant to meet the needs of next-generation automotive designs. It saves both energy and space, thereby reducing overall system cost.
The AL5873Q can drive up to 250mA per channel. It is set via two reference resistors connected to the REF1 and REF2 pins of the driver IC. Two different levels of LED current are supported, allowing for a more streamlined lighting system.
The AL5873Q features analog and master PWM dimming control and supports pulse width modulation (PWM) frequencies of up to 1 kHz. The PWM dimming function is important for improving current accuracy when driving LED s at low currents. The current on each channel of the device can be accurate to within ±4% tolerance so that the rear combination of lights to achieve better channel-channel matching.
2 Multi-mode intelligent dimming LED driver
Application areas: Indoor space lighting

NCL31000
In June 2021, ON Semiconductor introduced two new devices to improve the performance of interconnected lighting systems NCL31000 and NCL31001 LED driver, allowing manufacturers to develop LED luminaires with light-based positioning technology and visible light communication. These solutions add data intelligence and accurate positioning (up to 30 cm) that will revolutionize lighting in many spaces including supermarkets, warehouses, hospitals, and airports.
Designed for luminaire applications, the NCL31000 supports high-bandwidth analog dimming and PWM dimming down to zero current. The driver device contains an integrated 3V3 fixed DC-DC converter and a further adjustable DC-DC (2.5 to 24V) for powering system components such as sensing and microcontrollers and greatly simplifies system design while improving energy efficiency by integrating multiple power schemes into the driver.
More importantly, the NCL31000's precise linear dimming enables visible light communication (VLC) and supports the development of light-based indoor positioning systems for many places where RF-based solutions cannot be used (e.g., hazardous spaces such as mines, or RF-sensitive areas such as hospitals or aircraft).
The NCL31001, as a companion driver to the NCL31000, can provide the same features as the NCL31000 while creating a solution that supports multi-string lighting applications in combination with the NCL31000, opening up more new business opportunities for intelligent lighting systems.
3 Solderability side DFN package LED driver
Application areas: general lighting, automotive lighting, etc.

DFN2020D-6
In June 2020, NEXPERIA announced a series of new LED drivers in the space-saving DFN2020D-6 (SOT1118D) package. This is one of the first LED drivers in the global lighting industry to use this beneficial package.
The new DFN2020D-6 LED driver pin size is only 2x2mm, thickness is only 0.65mm and supports NPN and PNP technology. Its output current is up to 250mA (NCR32x type) and the maximum supply voltage is 75V with powerful high thermal power.
For automotive lighting products, the solderability side of the DFN2020D-6 LED driver enables the use of AOI technology while also improving reliability. The solderable sides also exhibit greater shear resistance, and the DFN2020D-6 LED driver is more bendable and less prone to breakage than devices without solderable sides.
4 Embedded UVC LED driver module
Application area: UVC sterilization
In July 2020, ZETTLER Magnetics developed a complete UVC LED embedded solution for home appliance manufacturers. The solution includes the necessary driver/controller circuitry, transformer, and housing to allow the module to be easily embedded in any device.
The module is a UVC 275nm type with 2mW-20mW optical power with embedded MCU, capable of providing multiple I / O and A/D ports and flexible design from driver components to complete module design with the ability to withstand 1.6MPa water pressure.
With this solution, relevant UVC sterilization product developers have the necessary functional requirements along with cost advantages, helping to bring more UVC sterilization solutions to the end of the product application.
5 Compact High Output Linear LED Driver ICs
Application areas: automotive lighting

BD18336NUF-M
In June 2020, Japan's ROHM announced the development of an ultra-compact, high-output, linear LED driver IC (BD18336NUF-M) that provides stable lighting even when the battery voltage drops on a single chip, making it particularly suitable for various socket-type LED lights in vehicle systems, such as DRLs (daytime running lights), navigation lights, taillights, etc.
The BD18336NUF-M incorporates a current bypass function that prevents LED lights from turning off and always maintains at least 30% brightness by switching the LED light current path even if the battery voltage drops from 13V to 9V. The IC is packaged in a very compact package, as small as 3.0 square millimeters, yet can efficiently input 600mA of current. Compared to conventional solutions (including external circuitry), the IC reduces the mounting area by approximately 30% and thus can be mounted on a 10 mm2 substrate for mounting small socket LED lamps.
In addition, the BD18336NUF-M has a built-in function to suppress heat generated by LEDs, providing support for white LEDs that would normally generate heat during operation, and can be used in DRLs and other vehicle lighting systems that use white LEDs.
6 Programmable 12-channel RGB-LED driver
Application areas: Home smart lighting, indication lighting for wearable devices, etc.

LED1202
In April 2019, STMicroelectronics, a merger of Italy's SGS Microelectronics and France's Thomson Semiconductor, released the LED1202, a 12-channel LED driver that prevents scattering in "running lights" LED animation effects in the distraction of the flash phenomenon, so that smart home device, wearable devices, and small appliances, human-computer interaction is more smooth and natural.
The LED1202 stores eight programmable lighting patterns and sequences and operates independently of the host controller, enabling the host system to save power while continuously running complex lighting effects. The device's internal 12-bit PWM dimming enables precise control of programmed sequences, and the host controller can set 8-bit values to enable analog dimming via the driver's I2C interface.
The LED1202 has 12 output channels, and a single device can drive up to four RGB LED beads with a maximum output current of 20mA per channel. Up to eight LED1202 drivers can be connected together to control larger LED lighting arrays through an innovative synchronization feature. In addition, the LED1202 low-current channel matching is less than 2% (typical) at 2.5mA, which enhances light color uniformity with excellent matching. Inter-channel phase shift technology minimizes current ripple, and the device also prevents excessive peak current demand.
7 PWX UNV LED driver
Application areas: street lighting, etc.

PWX UNV LED DRIVER
In December 2019, Universal Lighting Technologies, a member of the Panasonic Group in Japan, introduced the 180W PWX UNV LED driver. The device is available with 12Vdc or 24Vdc auxiliary power and is suitable for outdoor lighting applications with on-board sensors or radios, such as streets, roads, and construction sites.
The PWX UNV LED driver operates at 120-277 VAC and provides 0-10V dimming in the dimming-to-off state with low standby power consumption (<0.5W). The driver offers a wide operating range in all three models and provides 180W of full power over the output current range of 640mA to 2000mA. The driver is UL Class P listed and offers advanced programming features, including programmable thermal overload without external NTC.
In addition, the device has only three SKUs and can be programmed wirelessly using the EVERset™ GUI and LDPC000A tuner bar, allowing OEM partners to control output current, dimming level, dimming curve, dimming setpoint, and lumen maintenance.
8 12-bit Integrated PWM RGB LED Driver
Application area: building landscape lighting

LP5036
In December 2018, Texas Instruments introduced the LP5018, LP5024, LP5030, and LP5036 LED family of drivers that integrate independent color mixing, brightness control, and power-saving modes. The devices support smooth, realistic colors and also help lighting products to reduce power consumption.
All four drivers can provide a dimming frequency that is higher than the human ear hearing range of 29-kHz. Therefore, it helps designers design portable electronic devices, building automation and equipment, such as the use of human-machine interface applications, to eliminate dimming when the ear can usually hear the noise.
In addition, compared to standard pulse-width modulation (PWM) solutions, designers can add more innovative lighting features to their lighting systems with the 12-bit PWM generator integrated into these four drivers, which allows for smoother adjustment of color and brightness levels.
9 Headlight troubleshooting LED driver
Application area: automotive lighting

LITIX™ Basic+
In November 2018, Infineon introduced its new LED driver LITIX™ Basic+, which allows car drivers to avoid frequent trips to the mechanic's store with flexible individual LED short-circuit diagnostics and Active Retry function mode.
The LITIX Basic+ family includes three devices with this feature: the TLD2132-1EP with one input and one output channel (1 in/1 out), the TLD2132-1EP (1 in/3 out), and the TLD2331-3EP (3 in/3 out). This LED driver reports faults to the microcontroller in the event of a fault. Depending on the system's diagnostic request, the driver will either deactivate the affected channel or keep it active.
LITIX Basic+ devices have the option to select the Active Retry option when a channel is disabled. Active Retry briefly reactivates the channel, scans the LEDs cyclically, and can automatically restart if the fault is no longer present. In addition to diagnosing individual LED shorts, LITIX Basic + products can also detect open load faults and short-circuit ground faults.
The LITIX Basic+ LED driver family consists of six devices (single and three-channel versions) supporting LED currents in the range of 5 mA to 360 mA. In addition to devices with individual LED short-circuit detection, the family also offers two devices with integrated PWM timers (pulse width modulation): TLD2141- 3EP (1 in/3 out) and TLD2142-1EP (1 in/1 out) for a cost-effective combination of taillight functions (e.g. brake light and taillight). Thanks to pulse width modulation, it is also possible to achieve precise light intensity. With the TLD1114-1EP (1-in/1-out) device, this integrated power conversion function allows power to be dissipated externally.
10 High-frequency regulator LED driver
Application area: Automotive lighting

ALT80802
In October 2018, Allegro MicroSystems, LLC introduced the ALT80802, the latest member of the 62xx/808xx family of lighting LED driver products, to meet the needs of applications such as fog lights, reverse lights, daytime running lights (DRLs), mirror sidelights and other automotive lighting.
The ALT80802 is a high-frequency switching regulator that provides a constant output current to drive high-power LEDs. This device can improve EMC/EMI design through frequency jitter, soft continuity diode shutdown, and well-controlled switching node conversion rate. Its built-in programmable oscillator allows the ALT80802 to switch frequencies up to 2.5 MHz, thus being outside the EMI-sensitive frequency band (such as AM band).
The ALT80802 integrates a power MOSFET for a buck or inverting buck-boost conversion, and its 50V rated voltage enable pin can be connected to Vin for auto-start to support battery-level PWM dimming common in traditional body controllers, resulting in a very high flexibility.
With current mode control and external compensation, the ALT80802 device achieves fast transient response, short dimming turn-on time, low on-off impulse, accurate PWM duty cycle, and wide dimming range. In addition, the ALT80802 device also has a wide range of protection functions, including pulse-by-pulse current limit, hiccup mode short-circuits protection, open/short continuity diode protection, BOOT open/short protection, VIN under-voltage lockout, and thermal shutdown function.
1.What does the LED driver do?
An LED driver is an electrical device that regulates power to an LED or a string of LEDs. Forward Voltage is the amount of volts the light emitting diode requires to conduct electricity and light up. As temperature increases, the forward voltage of the LED decreases, causing the LED to draw more current.
2.How do I choose an LED driver for my LED?
Use an LED driver with at least the same value as your LED(s). The driver must have a higher output power than your LEDs require for extra safety. If the output is equivalent to the LED power requirements, it is running at full power. Running at full power may cause the driver to have a shorter life span.
3.Is a LED driver the same as a transformer?
A transformer converts AC to AC; e.g., 240V AC to 12V AC. An LED driver typically supplies a constant current (e.g, 150mA DC) to a fairly-low voltage load (e.g., 36V DC; 12x 3V series LEDs, probably paralleled), while being powered by a high-voltage (e.g., 240V AC) input.
4.Are LED drivers AC or DC?
LED drivers are devices which regulate and supply the power used to 'drive' runs of LED strip lighting. Similar to traditional transformers, they transform mains voltage alternating current (240v AC) to a lower voltage.
5.How long do LED drivers last?
The driver is the heart of the LED light, and driver life can range from 10,000 to over 50,000 hours, depending on the design features, heat sink efficiency, capacitor construction, and overall quality. The above graph compares the lifespans of various types of lighting.
Discovering New and Advanced Methodology for Determining the Dynamic Characterization of Wide Bandgap DevicesSaumitra Jagdale15 March 20242452For a long era, silicon has stood out as the primary material for fabricating electronic devices due to its affordability, moderate efficiency, and performance capabilities. Despite its widespread use, silicon faces several limitations that render it unsuitable for applications involving high power and elevated temperatures. As technological advancements continue and the industry demands enhanced efficiency from devices, these limitations become increasingly vivid. In the quest for electronic devices that are more potent, efficient, and compact, wide bandgap materials are emerging as a dominant player. Their superiority over silicon in crucial aspects such as efficiency, higher junction temperatures, power density, thinner drift regions, and faster switching speeds positions them as the preferred materials for the future of power electronics.
Read More
A Comprehensive Guide to FPGA Development BoardsUTMEL11 September 202513914This comprehensive guide will take you on a journey through the fascinating world of FPGA development boards. We’ll explore what they are, how they differ from microcontrollers, and most importantly, how to choose the perfect board for your needs. Whether you’re a seasoned engineer or a curious hobbyist, prepare to unlock new possibilities in hardware design and accelerate your projects. We’ll cover everything from budget-friendly options to specialized boards for image processing, delve into popular learning paths, and even provide insights into essential software like Vivado. By the end of this article, you’ll have a clear roadmap to navigate the FPGA landscape and make informed decisions for your next groundbreaking endeavor.
Read More
Applications of FPGAs in Artificial Intelligence: A Comprehensive GuideUTMEL29 August 20253462This comprehensive guide explores FPGAs as powerful AI accelerators that offer distinct advantages over traditional GPUs and CPUs. FPGAs provide reconfigurable hardware that can be customized for specific AI workloads, delivering superior energy efficiency, ultra-low latency, and deterministic performance—particularly valuable for edge AI applications. While GPUs excel at parallel processing for training, FPGAs shine in inference tasks through their adaptability and power optimization. The document covers practical implementation challenges, including development complexity and resource constraints, while highlighting solutions like High-Level Synthesis tools and vendor-specific AI development suites from Intel and AMD/Xilinx. Real-world applications span telecommunications, healthcare, autonomous vehicles, and financial services, demonstrating FPGAs' versatility in mission-critical systems requiring real-time processing and minimal power consumption.
Read More
800G Optical Transceivers: The Guide for AI Data CentersUTMEL24 December 20253439The complete guide to 800G Optical Transceiver standards (QSFP-DD vs. OSFP). Overcome supply shortages and scale your AI data center with Utmel Electronic.
Read More
Xilinx FPGAs: From Getting Started to Advanced Application DevelopmentUTMEL09 September 20254184This guide is your comprehensive roadmap to understanding and mastering the world of Xilinx FPGA technology. From selecting your first board to deploying advanced AI applications, we'll cover everything you need to know to unlock the potential of these remarkable devices. The global FPGA market is on a significant growth trajectory, expected to expand from USD 8.37 billion in 2025 to USD 17.53 billion by 2035. This surge is fueled by the relentless demand for high-performance, adaptable computing in everything from 5G networks and data centers to autonomous vehicles and the Internet of Things (IoT). This guide will walk you through the key concepts, tools, and products in the Xilinx ecosystem, ensuring you're well-equipped to be a part of this technological revolution.
Read More
Subscribe to Utmel !
80HCPS1432CRMRenesas Electronics America Inc.
SI8261BBD-C-ISSilicon Labs
SI8261BAD-C-ISSilicon Labs
FOD8333ON Semiconductor
FOD8332R2ON Semiconductor
ACPL-302J-500EBroadcom Limited
SI8275GB-IS1Silicon Labs
SI8238AD-D-IS3Silicon Labs
FOD3120SDON Semiconductor
ADUM3223BRZAnalog Devices Inc.


Product
Brand
Articles
Tools