web counter

Hybrid Sources Powered Electric Vehicles - Part 2

Published: 20 March 2023 | Last Updated: 20 March 20233383
Hello everyone, welcome to the new post today. Concern over the rising cost of fossil fuels and the depletion of their resources is growing. New green automobile technologies are being created, including hybrid electric vehicles and fully electric vehicles. The fully electric vehicles are discussed in this article.


Topics covered in this article:
Ⅰ. Recent Trends in Battery Electric Vehicles
Ⅱ. Full Electric Vehicle
Ⅲ. Summarizing with Key Points



Overview: Concern over the rising cost of fossil fuels and the depletion of their resources is growing. New green automobile technologies are being created, including hybrid electric vehicles and fully electric vehicles. The fully electric vehicles are discussed in this article.

Click here to access the previous part of this article.

People all over the world are worried about how hydrocarbon-based transportation pollutes the air. The International Energy Agency (IEA) states that by 2030, transportation will use 298 Mtoe of biofuel. This sector uses 49% of the world's oil, and it looks like the world's oil will run out by 2038. According to the U.S. Environmental Protection Agency, 29% of greenhouse gas emissions (CO2, NO2, CO, NO) come from burning fossil fuels in transportation.

Studies by the European Union and other groups show that the transportation industry is responsible for about 28% of all carbon dioxide (CO2) emissions. More than 70% of these emissions come from road transport. Light commercial vehicles makeup 59%, medium and heavy commercial trucks 23%, planes and helicopters 9%, ships and boats 3%, trains 2%, and others 4%.


Ⅰ. Recent Trends in Battery Electric Vehicles

Many automakers are hard at work making new electric vehicles (EVs):

l General Motors plans to switch to an all-electric vehicle by the year 2023.

l In the future, Ford will offer seven plug-in hybrids that are electric and can be customized.

l Mazda, Denso, and Toyota are all working together to create technologies for electric vehicles (EVs).

l Renault, Nissan, and Mitsubishi are all working on electric vehicles, and they hope to have 12 of them on the market by 2023.

l By 2030, electric and hybrid versions of 300 vehicles from the Volkswagen group, which also owns the Audi and Porsche brands, will be available.

Over the past few decades, a lot of research has been done on energy management strategies, both for hybrid electric vehicles (HEVs) and for full electric vehicles (FEVs). But because automotive technology is getting better and new ideas are being added, the energy management system (EMS) for HEV and FEV is an area that is always changing and will continue to get new ideas for many years to come.

Yet, recent rapid advancements in the use of autonomous vehicles, emerging advances in powertrain components, and computational approaches have greatly increased the prospects for EMS performance improvement. Vehicle-to-vehicle, vehicle-to-infrastructure, and automated linked vehicles are some of the new communication technologies that are now being evaluated for use in renewable energy charging systems. To further improve driving efficiency and fuel economy, the promising potential must be explored.


Ⅱ. Full Electric Vehicle

At the moment, FEV possesses seven distinct types of power transfer topologies, each of which is illustrated in Fig. 1. Nevertheless, only three of these topologies are commonly used in the auto-industrial sector. Table 1 displays, for convenience, the relative configurations of the various hybrid energy storage systems (HESS).

Fig. 1. Various possible configurations of the Ultra Capacitor (UC) and battery Source IEEE Access.png

Fig. 1. Various possible configurations of the Ultra Capacitor (UC) and battery Source: IEEE Access

Table 1: Comparison of Various Configurations of Hybrid Energy Storage System

Table 1 Comparison of Various Configurations of Hybrid Energy Storage System.png

 

Fully electric vehicles fall into one of two groups, depending on the type of energy source they use, which can be either a fuel cell or a battery. Thirdly, PV-based vehicles have recently attracted a significant amount of interest from researchers who are looking for ways to improve the efficiency with which renewable resources, which are found in nature in abundant supply, are utilized.

1) Battery-Based FEVs

In this fuel-efficient vehicle, the high-energy content of the primary source is provided by the battery. To create the hybrid energy storage system, the battery is paired with another high-density power device, such as a supercapacitor, which is also referred to as an ultra capacitor (UC). In some circles, it is also referred to as a double-layer electric capacitor. The energy density of batteries is much higher than that of supercapacitors, but the power density of batteries is much lower. Hence, HESS stores sufficient energy to meet sudden demands for power in order to reach the desired level of vehicle performance.

2) Fuel Cell-Based FEVs

The production of electricity from H2 and O2 was accomplished with the use of FC as the principal source in this FEV. The specific energy and power of the FC are comparable to those of gasoline, but they are not the same. Because of the chemical reactions that take place, fuel cells have a delayed response, which means that it is not ideal for them to handle the frequently changing load. As a solution to this issue, it has hybridized with UC and battery technology. The configuration of the FC-based FEVs is depicted in Fig. 2.

 

Fig. 2. FC-based FEVs. Source IEEE Access.png

Fig. 2. FC-based FEVs. Source: IEEE Access

3) A PV-Based Fuel Economy Vehicle

A solar power-based FEV, also known as a PV-FEV, has an architecture that is very similar to that of a plug-in hybrid electric vehicle (HEV), with the exception of an additional photovoltaic (PV) panel that supplies the current for battery charging during the day. In addition, the maximum power point tracking control algorithms are utilized so as to extract the maximum amount of power from the PV panels. The configuration of the PV-based FEV can be seen in Fig. 3.

Fig. 3. PV-based FEV structure. Source IEEE Access.png

Fig. 3. PV-based FEV structure. Source: IEEE Access

 

Existing electric vehicles with more than one source of power and hybrid powertrains give the system a lot of room to be designed and make the control algorithm more complicated. The objective function of the EMS optimization problem is usually tied to the collection of powertrain topologies, while technology and the size of components are treated as optimization constraints. The growth of the new generation of green vehicles will depend on how well they manage power. 


Ⅲ. Summarizing with Key Points

Some of the takeaways from the article are as follows:

l As automobile technology improves and new concepts are incorporated, the energy management system for hybrid electric vehicles and full electric vehicles will continue to change for years to come.

l Full electric vehicle currently has seven different types of power transmission topologies. Only three of these topologies are, however, frequently utilized in the auto-industrial sector.

l Depending on the sort of power source they use, a fuel cell or battery-based electric vehicles are the two categories. Recently solar, powered photovoltaic-based automobiles that use renewable resources have been developed.

l The energy density of batteries is substantially higher than that of supercapacitors in battery-based full electric vehicles, storing enough energy to fulfill unexpected demands for power to achieve the appropriate level of vehicle performance.

l In fuel cell-based full electric vehicles, H2 and O2 were used to make electricity. Because of the chemical reactions that happen, fuel cells take a while to respond. This means that they are not the best choice for a load that changes often.

l An additional photovoltaic panel that provides the current for battery charging during the day distinguishes a solar power-based full electric vehicle from plug-in hybrid electric vehicles.

This blog post is part of a full research article from IEEE Access.

The featured image is used courtesy of OPEN AI.

 

 


Rakesh Kumar, Ph.D.

Rakesh Kumar holds a Ph.D. in electrical engineering with a specialization in power electronics. He is a Senior member of the IEEE Power Electronics Society, Class of 2021. He is currently associated with the KPR Institute of Engineering and Technology, India. He writes high-quality, long-form technical articles on power electronics for B2B electronics platforms. Feel free to reach out to him at rakesh.a@ieee.org!

Related Articles

  • Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators
    Improving the Energy Conversion Efficiency of Triboelectric Nanogenerators
    Saumitra Jagdale19 November 20243398

    There is a huge growth in demand for self-sustaining electronic devices, as the traditional power-generating devices fail in remote and harsh environments due to the periodic requirement of battery changes. Also, these devices are frequency specific; some work only in high frequency and some in low frequency. Triboelectric nanogenerators (TENGs) provide a promising solution by efficiently converting mechanical energy into electricity as they are versatile, compact, and cheap, making them a popular choice.

    Read More
  • Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy Generation
    Methodologies for Increasing Efficiency of Fuel Stack Technology for Energy Generation
    Saumitra Jagdale19 November 20243230

    Presently, power companies are moving towards renewable energy systems. Conventional energy sources are more expensive because they require a vast network to be maintained and huge human resources. Also, they harm the environment by releasing several harmful gases. As the industry’s focus shifts toward renewable energy sources, energy systems powered by Proton Exchange Membrane Fuel Stacks (PEMFS) are gaining traction.

    Read More
  • VSC Light Meaning, Causes, and Step-by-Step Diagnostics
    VSC Light Meaning, Causes, and Step-by-Step Diagnostics
    UTMEL19 May 20265476

    A VSC (Vehicle Stability Control) light indicates the system is disabled, often as a fail-safe triggered by unrelated engine faults like a loose gas cap. While the stability system prevents lateral skidding, it shuts down when sensor data is unreliable. Proper diagnosis requires an ABS-capable OBD2 scanner. Resolving the root engine code, checking wheel speed sensors, or performing a zero-point calibration usually restores system function.

    Read More
  • What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component Buyers
    What JEDEC JEP203 and JEP204 Actually Change for SiC Qualification Engineers and Component Buyers
    UTMEL29 July 2026739

    ​Summary: When JEDEC published JEP203 and JEP204 on June 3, 2026[1], most coverage treated them as an announcement. They are better understood as the first shared language the silicon carbide industry has had for two problems that have quietly consumed engineering hours since the first commercial SiC MOSFETs shipped: short-circuit evaluation that produces numbers you can compare across suppliers, and a consolidated reference of stress procedures so qualification engineers stop reinventing test plans from scratch. This article explains what changes on Monday morning and what to ask suppliers for now.

    Read More
  • 2nm vs 3nm Chips: What the Latest Process Nodes Mean for Performance
    2nm vs 3nm Chips: What the Latest Process Nodes Mean for Performance
    UTMEL19 August 20262830

    The shift from 3nm to 2nm process nodes marks a fundamental change in transistor architecture, moving from FinFET to Gate-All-Around (GAA) nanosheets. This transition delivers meaningful improvements in performance, power, and density, but also introduces new challenges like SRAM scaling limits, thermal density, and backside power delivery. The article compares TSMC, Samsung, and Intel approaches, offering a practical decision framework for engineering teams.

    Read More

Subscribe to Utmel !