web counter

Kyoto University Successfully Demonstrates That SiC Can Also Work at 350°C

Published: 26 March 2022 | Last Updated: 26 March 2022943
Kyoto University (KU) recently announced that it has successfully demonstrated basic operation at high temperatures of 350°C, where Si semiconductor integrated circuits cannot operate, using SiC semiconductor integrated circuits.
SiC is as important as battery technologies. It enables huge reductions in power loss for example, in a MOSFET diode, SiC makes it easier to achieve a thinner drift layer because of its critical breaking strength that can be a much as 10x higher than that of silicon. This results in less electrical resistance, culminating in up to 70% reduction in conduction and switching losses at high voltages.

Silicon Carbide - The subtle REVOLUTION

Kyoto University (KU) recently announced that it has successfully demonstrated basic operation at high temperatures of 350°C, where Si semiconductor integrated circuits cannot operate, using SiC semiconductor integrated circuits.

 

The result is based on the research team of Assistant Professor Bright Kaneko and Professor Tsunobu Kimoto at the Graduate School of Engineering, Kyoto University. Details were presented on March 25 at the "69th Japan Society of Applied Physics Spring Lecture Meeting" held online from March 22 to 26 at Aoyama Gakuin University Sagamihara Campus.

 

It is said that Si semiconductors fail at about 250°C and cannot operate in higher temperatures. Therefore, it is expected to use SiC integrated circuits that have better heat resistance and can operate even at about 800°C. However, if structures similar to transistors in Si integrated circuits are fabricated from SiC, the characteristics will be difficult to control reliability in high-temperature environments due to SiC-specific defects, and there are problems of high power consumption.

 

To solve these problems, transistors for SiC integrated circuits with structures different from MOSFETs in Si integrated circuits are being developed, in which JFETs do not have physical interface defects in the current flow region as MOSFETs do. Therefore, it is promising as a transistor that constitutes a SiC integrated circuit with high-temperature action.

 

However, JFETs fabricated by the general method require large standby power and low power consumption because they cannot form a complementary circuit with a combination of n-type and p-type on the same substrate as MOSFETs, and conversion is required.

 

Kyoto University Successfully Demonstrates That SiC Can Also Work at 350°C(1).jpg


Schematic diagram of an n-type JFET fabricated by the general method (crystal growth)

(Source: Kyoto University Press Release PDF)

 

In this context, the research team has proposed a unique transistor structure and circuit configuration. It is said to have successfully demonstrated the operation of SiC logic gates from room temperature to 350°C with low power consumption.

 

There are two points of implementation. The first is the realization of a technique to fabricate both n-type and p-type on the same substrate, which is not possible with conventional general-purpose JFET fabrication methods. It is said to have succeeded in producing both n-type and p-type JFETs on the same substrate by performing ion implantation for local conductivity type control of the entire device structure.

 

Kyoto University Successfully Demonstrates That SiC Can Also Work at 350°C(2).jpg


Schematic diagram of n-type and p-type JFETs produced by the proposed method (ion implantation) (Source: Kyoto University Press Release PDF)

 

The second is that the JFET achieves a normally-off type characteristic, i.e., a characteristic that does not allow current to flow as a transistor when no voltage is applied to the gate terminal. This characteristic is also said to be difficult to achieve by the general JFET fabrication method, but by using a dual-gate structure, which constitutes the gate region by clamping the channel region from both sides, a normally off-type JFET can be fabricated. is said to have been accomplished.

 

It has been confirmed that the fabricated complementary JFETs operate normally in the temperature range from room temperature to 350°C, and that the power consumption in the standby state can be suppressed to a maximum of a few tens of nW or less.

 

The research team explained that the advantage of this research is that the circuit presented here can be fabricated using standard processes for SiC semiconductors as power semiconductors, but we will continue with MOSFETs, and further fundamental research is needed to determine if JFETs can be made smaller, faster, and more precise by miniaturization, and continued research is needed.

 

Related News

1、MediaTek, Qualcomm announce joining Russia sanctions

2、Automotive chips rose across the board!

3、Apple M1 Ultra -- The Technology Behind the Chip Interconnection

4、Foxconn Announces Investment of $9 Billion to Build A Chip Factory in Saudi Arabia

5、Japanese Companies Increase Investment in Power Semiconductors



UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

Subscribe to Utmel !

Featured Parts More