web counter

74LS107 Dual JK Flip-Flops: Flip-Flops Datasheet pdf, Pinout and Diagram

UTMEL

Published: 20 December 2021 | Last Updated: 20 December 2021

6555

74LS107A

74LS107A

SIGNETICS CORP

74LS107A datasheet pdf and Unclassified product details from SIGNETICS CORP stock available at Utmel

Purchase Guide

The 74LS107 is a JK Flip-Flop with individual J, K, Direct Clear, and Clock Pulse inputs. This article is going to explain datasheet, pinout, equivalent, applications, and other details about 74LS107 flip-flops.

This video demonstrates introduction to JK flip flop.

Introduction to JK flip flop

What is 74LS107?

The 74LS107  is a JK  Flip-Flop with individual J, K, Direct Clear, and  Clock Pulse inputs. The clock's HIGH-to-LOW transition is what triggers output adjustments. For predictable functioning, the J and K inputs must be steady one setup time before the high-to-low clock change. The 74LS107  IC offers a large operating voltage range, a wide operating temperature range, and directly interfaces with CMOS, NMOS, and TTL.

74LS107 logic diagram.jpg

Logic Diagram

74LS107 Pinout

74LS107 pin .jpg

74LS107 pin.jpg

74LS107 Pinout

Pin NoPin NameDescription
1J1Input Pin J1
2Q1Active high Output   pin 1
3Q1′Active low output pin   1
4K1Input Pin K1
5Q2Active high Output   pin 2
6Q2′Active low output pin   2
7GNDGround Pin
8J2Input Pin J2
9CP2Clock Pulse Input Pin   2
10CD2Reset Pin 2
11K2Input Pin K2
12CP1Clock Pulse Input Pin   1
13CD1Reset Pin 1
14VCCSupply Voltage


Product details of 74LS107

  • Technology Family: LS

  • Dual JK   Flip Flop  Package IC

  • -ve edge-triggered

  • VCC (Min): 4.75V

  • VCC (Max): 5.25

  • Bits (#): 2

  • Operating Voltage (Nom): 5V

  • Frequency at normal voltage (Max): 35MHz

  • Propagation delay (Max): 20ns

  • IOL (Max): 8mA

  • IOH (Max):-0.4mA

  • Rating: Catalog

  • Available in 14-pin PDIP, GDIP, PDSO packages


Specifications

SIGNETICS CORP 74LS107A technical specifications, attributes, parameters and parts with similar specifications to SIGNETICS CORP 74LS107A.
  • Type
    Parameter
  • Surface Mount

    having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.

    NO
  • Number of Terminals
    14
  • Operating Temperature (Max.)
    70°C
  • HTS Code

    HTS (Harmonized Tariff Schedule) codes are product classification codes between 8-1 digits. The first six digits are an HS code, and the countries of import assign the subsequent digits to provide additional classification. U.S. HTS codes are 1 digits and are administered by the U.S. International Trade Commission.

    8542.39.00.01
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    DUAL
  • Terminal Form

    Occurring at or forming the end of a series, succession, or the like; closing; concluding.

    THROUGH-HOLE
  • Number of Functions
    2
  • Supply Voltage

    Supply voltage refers to the electrical potential difference provided to an electronic component or circuit. It is crucial for the proper operation of devices, as it powers their functions and determines performance characteristics. The supply voltage must be within specified limits to ensure reliability and prevent damage to components. Different electronic devices have specific supply voltage requirements, which can vary widely depending on their design and intended application.

    5V
  • JESD-30 Code

    JESD-30 Code refers to a standardized descriptive designation system established by JEDEC for semiconductor-device packages. This system provides a systematic method for generating designators that convey essential information about the package's physical characteristics, such as size and shape, which aids in component identification and selection. By using JESD-30 codes, manufacturers and engineers can ensure consistency and clarity in the specification of semiconductor packages across various applications and industries.

    R-PDIP-T14
  • Qualification Status

    An indicator of formal certification of qualifications.

    Not Qualified
  • Temperature Grade

    Temperature grades represent a tire's resistance to heat and its ability to dissipate heat when tested under controlled laboratory test conditions.

    COMMERCIAL
  • Load Capacitance

    the amount of capacitance measured or computed across the crystal terminals on the PCB. Frequency Tolerance. Frequency tolerance refers to the allowable deviation from nominal, in parts per million (PPM), at a specific temperature, usually +25°C.

    15pF
  • Number of Bits
    2
  • Family

    In electronic components, the parameter "Family" typically refers to a categorization or classification system used to group similar components together based on their characteristics, functions, or applications. This classification helps users easily identify and select components that meet their specific requirements. The "Family" parameter can include various subcategories such as resistors, capacitors, diodes, transistors, integrated circuits, and more. Understanding the "Family" of an electronic component can provide valuable information about its compatibility, performance specifications, and potential uses within a circuit or system. It is important to consider the "Family" parameter when designing or troubleshooting electronic circuits to ensure proper functionality and compatibility with other components.

    LS
  • Output Polarity

    Output polarity in electronic components refers to the orientation of the output signal in relation to the ground or reference voltage. It indicates whether the output voltage is positive or negative with respect to the ground. Positive output polarity means the signal is higher than the ground potential, while negative output polarity signifies that the signal is lower than the ground. This characteristic is crucial for determining compatibility with other components in a circuit and ensuring proper signal processing.

    COMPLEMENTARY
  • Logic IC Type

    Logic IC Type refers to the type of integrated circuit (IC) that is specifically designed to perform logical operations. These ICs are commonly used in digital electronic devices to process and manipulate binary data according to predefined logic functions. The Logic IC Type parameter typically specifies the specific logic family or technology used in the IC, such as TTL (Transistor-Transistor Logic), CMOS (Complementary Metal-Oxide-Semiconductor), or ECL (Emitter-Coupled Logic). Understanding the Logic IC Type is important for selecting the appropriate IC for a given application, as different logic families have varying characteristics in terms of speed, power consumption, and noise immunity.

    J-K FLIP-FLOP
  • Trigger Type

    Trigger Type in electronic components refers to the mechanism or method by which a device, such as a flip-flop or timer, responds to an input signal. It defines how the device transitions between states based on specific conditions, such as rising or falling edges of a signal, levels, or pulses. Different trigger types such as edge-triggered, level-triggered, or pulse-triggered influence the timing and behavior of the circuit, thereby determining how input signals affect the output in various applications.

    NEGATIVE EDGE
  • Propagation Delay (tpd)

    Propagation delay (tpd) is a crucial parameter in electronic components, especially in digital circuits. It refers to the time taken for a signal to travel from the input of a component to its output. This delay is caused by various factors such as the internal circuitry, interconnections, and the physical properties of the component. Propagation delay is essential to consider in designing circuits to ensure proper timing and functionality. It is typically measured in nanoseconds or picoseconds and plays a significant role in determining the overall performance and speed of electronic systems.

    30 ns
  • Power Supply Current-Max (ICC)

    The parameter "Power Supply Current-Max (ICC)" in electronic components refers to the maximum amount of current that the component will draw from the power supply under specified operating conditions. It is an important specification as it helps determine the power consumption of the component and ensures that the power supply can provide enough current to meet the component's requirements without being overloaded. Exceeding the maximum power supply current can lead to overheating, component damage, or system failure. Designers use this parameter to select an appropriate power supply and ensure the reliable operation of the electronic system.

    8mA
  • fmax-Min

    fmax-Min refers to the frequency range that an electronic component or system can operate within. It represents the difference between the maximum frequency (fmax) and the minimum frequency (Min) limits of operation. This parameter is crucial in defining the bandwidth of the component, indicating how effectively it can transmit or receive signals over that range. A wider fmax-Min value typically signifies better performance for applications that require broad frequency response.

    30 MHz
0 Similar Products Remaining

74LS107 Features

  • Two Independent JK  Flip-Flops with Clock and Clear Inputs

  • Standard Pin Arrangement

  • Fast Switching Times

  • Operating Temperature up to 70°C

  • Standard TTL Switching Voltages


Where to use 74LS107?

They are used in digital clocks, electronic meters, and other electronic devices that display numerical information.

74LS107 Equivalent

SN7476, 74HC76, 74HC73a, 4027B

Advantage and Disadvantages of Flip-Flops

  • Advantages

The timing difficulty known as "RACE" is a downside of the JK  flip-flop. RACE occurs when the output Q changes state before the clock input's timing pulse has a chance to move into the OFF state. To avoid timing issues, the timing pulse time (T) should be kept as short as possible.

  • Disadvantage

When both the inputs and clock pulse signal are at level 1 after the output is complemented once, output transmission will start getting repeated and continuous.


74LS107 Package Dimensions

74LS107 outline.jpg

74LS107 Package Dimensions

74LS107 Manufacturer

Signetics was an American electronics manufacturer specifically established to make integrated circuits. Founded in 1961, they went on to develop several early microprocessors and support chips, as well as the widely used 555 timer chip. They were bought by Philips in 1975 and incorporated in Philips Semiconductors (now NXP).

Frequently Asked Questions

What is the use of 74LS107?

The 74LS107 is used in digital clocks, electronic meters, and other electronic devices that display numerical information.

How does Flip-flop work?

The JK flip flop work in the same way as the SR flip flop work. The JK Flip Flop is a gated SR flip-flop having the addition of a clock input circuitry.

What is disadvantage of JK flip flop?

JK flip-flop has a drawback of timing problem known as “RACE”. The condition of RACE arises if the output Q changes its state before the timing pulse of the clock input has time to go in the OFF state. The timing pulse period (T) should be kept as short as possible to avoid the problem of timing.
74LS107A

SIGNETICS CORP

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe