web counter

Difference between RS232 RS422 and RS485

Sophie

Published: 08 March 2022 | Last Updated: 08 March 2022

4592

RS232

RS232

Greenlee Communications

PUNCH UNIT-CONNECTOR 25 PIN

Purchase Guide

PUNCH UNIT-CONNECTOR 25 PIN

In telecommunications, RS-232 or Recommended Standard 232 is a standard originally introduced in 1960 for serial communication transmission of data. RS-422, also known as TIA/EIA-422, is a technical standard originated by the Electronic Industries Alliance that specifies the electrical characteristics of a digital signaling circuit. RS-485, also known as TIA-485(-A) or EIA-485, is a standard defining the electrical characteristics of drivers and receivers for use in serial communications systems. This article is going to cover the differences between RS232, RS422, and RS485 from the perspective of description, specifications, related standards, and more details.

This video introduces the differences between RS 232, RS 422 and RS 485.

Difference between RS 232 RS 422 and RS 485 communication

RS232 Description

RS-232 was first introduced in 1960  by the Electronic Industries Association (EIA) as a Recommended Standard. The original DTEs were electromechanical teletypewriters, and the original DCEs were (usually) modems. When electronic terminals  (smart and dumb) began to be used, they were often designed to be interchangeable with teletypewriters, and so supported RS-232.

RS422 Description

RS-422 is the common short form title of American National Standards Institute  (ANSI) standard ANSI/TIA/EIA-422-B Electrical Characteristics of Balanced Voltage Differential Interface Circuits and its international equivalent ITU-T   Recommendation T-REC-V.11, also known as X.27.

RS485 Description

RS-485 supports inexpensive local networks and multidrop communications links, using the same differential signaling over twisted pair as RS-422. It is generally accepted that RS-485  can be used with data rates up to 10 Mbit/s or, at lower speeds, distances up to 1,200 m (4,000 ft). As a rule of thumb, the speed in bit/s multiplied by the length in meters should not exceed 108. Thus a 50-meter cable should not signal faster than 2 Mbit/s.

The Interfaces for RS232, RS422, and RS485


Port nameRS-232RS-422RS-485
Transfer typeFull duplexFull duplexHalf duplex (2 wires), full duplex (4 wires)
Maximum distance15 meters at 9600 bps1200 meters at 9600 bps1200 meters at 9600 bps
Contacts in useTxD, RxD, RTS, CTS, DTR, DSR,
DCD.GND*
TxA.TxB, RxA, RxB, GNDDataA, DataB, GND
TopologyPoint-to-PointPoint-to-PointMulti-point
Max. Number of connected devices11 (10 devices in receive mode)32 (with repeaters larger, usually up to 256)

The Protocols for RS232, RS422, and RS485



RS-232RS-485RS-422
Network TopologyPoint-to-PointPoint-to-Point or MultidropPoint-to-Point or Multidrop
Duplex TypeFull DuplexFull Duplex Half DuplexFull Duplex Half Duplex
Number of Devices1 controller32 unit loads (controllers or receivers)1 controller
1 receiver10 receivers
SignalingUnbalancedBalanced (differential signaling)Balanced (differential signaling)
Max Distance50 feet at 19.2 Kbps4000 feet at 100 Kbps4000 feet at 100 Kbps
Mark (data 1)•15 to -3 V1.5Vto5 V(B> A)2 Vto6 V(B > A)
Space (data 0)+3 to +15V1.5Vto5 V(A>B)2 Vto6 V(A>B)


The Specifications for RS232, RS422, and RS485


SPECIFICATIONSRS232RS422RS485
Mode of OperationSINGLE -ENDEDDIFFERENTIALDIFFERENTIAL
Total Number of Drivers and Receivers on One Line (One driver active at a time for RS485 networks)1 DRIVER1 DRIVER32 DRIVER
1 RECVR10 RECVR32 RECVR
Maximum Cable Length50 FT.4000 FT.4000 FT.
Maximum Data Rate (40ft. - 4000ft. for RS422/RS485)20 kb/slOMb/s-lOOKb/slOMb/s-lOOKb/s
Maximum Driver Output Voltage+/-25V-0.25V to +6V-7V to +12V
Driver Output Signal Level (Loaded Min.)Loaded+/-5V to +/-15V+/-2.0V+/-1.5V
Driver Output Signal Level (Unloaded Max)Unloaded+/-25V+/-6V+/-6V
Driver Load Impedance (Ohms)3k to 7k10054
Max. Driver Current in High Z StatePower OnN/AN/A+/-100UA
Max. Driver Current in High Z StatePower Off+/-6mA @ +/-2v+/-100UA+/-100UA
Slew Rate (Max.)30V/USN/AN/A
Receiver Input Voltage Range+/-15V-10V to +10V-7V to +12V
Receiver Input Sensitivity+/-3V+/-200mV+/-200mV
Receiver Input Resistance (Ohms), (1 Standard Load for RS485)3k to 7k4k min.> = 12k


Specifications

Greenlee Communications RS232 technical specifications, attributes, parameters and parts with similar specifications to Greenlee Communications RS232.
  • Type
    Parameter
  • Factory Lead Time
    4 Weeks
  • Number of Pins
    25
  • Weight
    272.15545g
  • Published
    2009
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    Not Applicable
  • Tool Type

    Tool Type in electronic components refers to the classification of tools used for designing, testing, assembling, or modifying electronic circuits and systems. It encompasses a variety of instruments such as simulators, PCB design software, soldering equipment, and diagnostic tools. Each Tool Type serves specific functions in the development and maintenance of electronic products, facilitating tasks like circuit design, performance analysis, and troubleshooting.

    Punch
  • Height
    11.9mm
  • Length
    88.9mm
  • Width
    42mm
  • REACH SVHC

    The parameter "REACH SVHC" in electronic components refers to the compliance with the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation regarding Substances of Very High Concern (SVHC). SVHCs are substances that may have serious effects on human health or the environment, and their use is regulated under REACH to ensure their safe handling and minimize their impact.Manufacturers of electronic components need to declare if their products contain any SVHCs above a certain threshold concentration and provide information on the safe use of these substances. This information allows customers to make informed decisions about the potential risks associated with using the components and take appropriate measures to mitigate any hazards.Ensuring compliance with REACH SVHC requirements is essential for electronics manufacturers to meet regulatory standards, protect human health and the environment, and maintain transparency in their supply chain. It also demonstrates a commitment to sustainability and responsible manufacturing practices in the electronics industry.

    Unknown
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    Non-RoHS Compliant
0 Similar Products Remaining

Related standards between RS232, RS422, and RS485

Other serial signaling standards may not interoperate with standard-compliant RS-232  ports. For example, using the TTL levels of near +5 and 0 V puts the mark level in the undefined area of the standard. Such levels are sometimes used with  NMEA 0183 -compliant GPS receivers and depth finders.


A 20 mA current loop uses the absence of 20 mA current for high, and the presence of current in the loop for low; this signaling method is often used for long-distance and optically isolated links. Connection of a current-loop device to a compliant RS-232  port requires a level translator. Current-loop devices can supply voltages in excess of the withstand voltage limits of a compliant device. The original IBM  PC  serial port card implemented a 20 mA current-loop interface, which was never emulated by other suppliers of plug-compatible equipment.


Other serial interfaces similar to RS-232  :

RS-422 – a high-speed system similar to RS-232  but with differential signaling 

RS-485 – a descendant of RS-422  that can be used as a bus in multidrop configurations


Parts with Similar Specs

Trend Analysis

Datasheet PDF

Download datasheets and manufacturer documentation for Greenlee Communications RS232.

Conclusion

RS232, RS422, and RS485  are all essentially physical layer protocols. They are all serial communication protocols and are ubiquitous device interfaces. Serial interfaces are widely used in electronics and embedded systems, often for remote acquisition of device data or remote control. They change the way the signal is transmitted, whether it is a PC, microcontroller, or serial communication using serial communication protocols or TTL level transmission. They all need to be converted to RS232RS422.  or RS485  signals by a communication converter chip.

RS232

Greenlee Communications

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More