ESP32 vs. STM32: Which one is better?

Sophie

Published: 22 February 2022 | Last Updated: 22 February 2022

63557

ESP-32

ESP-32

RF Solutions

2.4GHz~2.5GHz Bluetooth, WiFi -40°C~85°C 2.7V~3.6V ADC, GPIO, I2C, I2S, PWM, SDIO, SPI, UART 150Mbps 20.5dBm 802.11b/g/n, Bluetooth v4.2 + EDR, Class 1, 2 and 3 -97dBm Module

Purchase Guide

2.4GHz~2.5GHz Bluetooth, WiFi -40°C~85°C 2.7V~3.6V ADC, GPIO, I2C, I2S, PWM, SDIO, SPI, UART 150Mbps 20.5dBm 802.11b/g/n, Bluetooth v4.2 + EDR, Class 1, 2 and 3 -97dBm Module

ESP32 is a series of low-cost, low-power systems on a chip microcontroller with integrated Wi-Fi and dual-mode Bluetooth. STM32 is a family of 32-bit microcontroller integrated circuits by STMicroelectronics. This article is going to cover the differences between STM32 and ESP32 from the perspective of description, Arduino, CAD Model, features, and more details.

This video will introduce a comparison of features and performance of the ESP32 vs. STM32.

#345 ESP32 vs STM32: Which one is better (Bluepill)?

ESP32 Description

ESP32 is a series of low-cost, low-power systems on a chip microcontroller with integrated Wi-Fi and dual-mode Bluetooth. The ESP32  series employs either a Tensilica Xtensa LX6  microprocessor in both dual-core and single-core variations, Xtensa LX7  dual-core microprocessor, or a single-core RISC-V  microprocessor and includes built-in antenna switches, RF balun, power amplifier, low-noise receive amplifier, filters, and power management modules. ESP32  is created and developed by Espressif Systems, a Shanghai-based Chinese company, and is manufactured by TSMC  using its 40 nm process. It is a successor to the ESP8266  microcontroller.


STM32 Description

STM32 is a family of microcontroller ICs based on the 32-bit RISC ARM  Cortex-M3 3FCortex-M7FCortex-M4F, Cortex-M3, Cortex-M0+, and Cortex-M0 cores. STMicroelectronics licenses the ARM Processor IP from ARM Holdings. The ARM core designs have numerous configurable options, and ST chooses the individual configuration to use for each design. ST attaches its own peripherals to the core before converting the design into a silicon die. The following tables summarize the STM32  microcontroller families.

Comparison of Arduinos of the ESP8266 vs. ESP32

Comparison of Arduinos of the ESP8266 vs. ESP32.png


Running the Loop a million times and analyzing how many milliseconds each microcontroller took for such actions. The table above shows that the Arduino Uno took 4.920 milliseconds, while the ESP32 needed only 164ms.


Comparison of features of the ESP32 vs. STM32

Features of the ESP32 include the following:

Processors:

CPU: Xtensa dual-core (or single-core) 32-bit LX6 microprocessor, operating at 160 or 240 MHz and performing at up to 600 DMIPS

Ultra-low-power (ULP) co-processor

Memory: 320 KiB RAM, 448 KiB ROM

Wireless connectivity:

Wi-Fi: 802.11 b/g/n

Bluetooth: v4.2 BR/EDR and BLE (shares the radio with Wi-Fi)

Peripheral interfaces:

34 × programmable GPIOs

12-bit SAR ADC up to 18 channels

2 × 8-bit DACs

10 × touch sensors (capacitive sensing GPIOs)

4 × SPI

2 × I²S interfaces

2 × I²C interfaces

3 × UART

SD/SDIO/CE-ATA/MMC/eMMC host controller

SDIO/SPI slave controller

Ethernet MAC interface with dedicated DMA and planned IEEE 1588 Precision Time Protocol support

CAN bus 2.0

Infrared remote controller (TX/RX, up to 8 channels)

Motor PWM

LED PWM (up to 16 channels)

Hall effect sensor

Ultra-low-power analog pre-amplifier

 

Features of the STM32 F4 include the following:

Core:

ARM Cortex-M4F core at a maximum clock rate of 84 / 100 / 168 / 180 MHz.

Memory:

Static RAM consists of up to 192 KB general-purpose, 64 KB core-coupled memory (CCM), 4 KB battery-backed, 80 bytes battery-backed with tamper-detection erase.

Flash consists of 512 / 1024 / 2048 KB general-purpose, 30 KB system boot, 512 bytes one-time programmable (OTP), 16 option bytes.

Each chip has a factory-programmed 96-bit unique device identifier number.

Peripherals:

Common peripherals included in all IC packages are USB 2.0 OTG HS and FS, two CAN 2.0B, one SPI + two SPI or full-duplex I²S, three I²C, four USART, two UART, SDIO for SD/MMC cards, twelve 16-bit timers, two 32-bit timers, two watchdog timers, temperature sensor, 16 or 24 channels into three ADCs, two DACs, 51 to 140 GPIOs, sixteen DMA, improved real-time clock (RTC), cyclic redundancy check (CRC) engine, random number generator (RNG) engine. Larger IC packages add 8/16-bit external memory bus capabilities.

The STM32F4x7 models add Ethernet MAC and camera interface.

The STM32F41x/43x models add a cryptographic processor for DES / TDES / AES and a hash processor for SHA-1 and MD5.

The STM32F4x9 models add an LCD-TFT controller.

Oscillators consist of internal (16 MHz, 32 kHz), optional external (4 to 26 MHz, 32.768 to 1000 kHz).

IC packages: WLCSP64, LQFP64, LQFP100, LQFP144, LQFP176, UFBGA176. STM32F429/439 also offers LQFP208 and UFBGA216.

The operating voltage range is 1.8 to 3.6 volt.


Specifications

RF Solutions ESP-32 technical specifications, attributes, parameters and parts with similar specifications to RF Solutions ESP-32.
  • Type
    Parameter
  • Factory Lead Time
    4 Weeks
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    Module
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -40°C~85°C
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    Not Applicable
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    2.7V~3.6V
  • Frequency

    In electronic components, the parameter "Frequency" refers to the rate at which a signal oscillates or cycles within a given period of time. It is typically measured in Hertz (Hz) and represents how many times a signal completes a full cycle in one second. Frequency is a crucial aspect in electronic components as it determines the behavior and performance of various devices such as oscillators, filters, and communication systems. Understanding the frequency characteristics of components is essential for designing and analyzing electronic circuits to ensure proper functionality and compatibility with other components in a system.

    2.4GHz~2.5GHz
  • Data Rate

    Data Rate is defined as the amount of data transmitted during a specified time period over a network. It is the speed at which data is transferred from one device to another or between a peripheral device and the computer. It is generally measured in Mega bits per second(Mbps) or Mega bytes per second(MBps).

    150Mbps
  • Protocol

    In electronic components, the parameter "Protocol" refers to a set of rules and standards that govern the communication between devices. It defines the format, timing, sequencing, and error checking methods for data exchange between different components or systems. Protocols ensure that devices can understand and interpret data correctly, enabling them to communicate effectively with each other. Common examples of protocols in electronics include USB, Ethernet, SPI, I2C, and Bluetooth, each with its own specifications for data transmission. Understanding and adhering to protocols is essential for ensuring compatibility and reliable communication between electronic devices.

    802.11b/g/n, Bluetooth v4.2 + EDR, Class 1, 2 and 3
  • Power - Output

    Power Output in electronic components refers to the amount of electrical power that a device can deliver to a load. It is typically measured in watts and indicates the effectiveness of the component in converting electrical energy into usable work or signal. Power Output can vary based on the component's design, operating conditions, and intended application, making it a critical factor in the performance of amplifiers, power supplies, and other electronic devices. Understanding the Power Output helps in selecting appropriate components for specific applications to ensure efficiency and reliability.

    20.5dBm
  • RF Family/Standard

    The parameter "RF Family/Standard" in electronic components refers to the specific radio frequency (RF) technology or standard that the component complies with or is designed for. RF technology encompasses a wide range of frequencies used for wireless communication, such as Wi-Fi, Bluetooth, cellular networks, and more. Different RF standards dictate the frequency bands, modulation techniques, data rates, and other specifications for communication systems. Understanding the RF family/standard of a component is crucial for ensuring compatibility and optimal performance in RF applications.

    Bluetooth, WiFi
  • Sensitivity

    Sensitivity in electronic components refers to the degree to which the output of a device responds to changes in input. It indicates how effectively a component translates a specific input signal into an observable output. High sensitivity means that even small variations in input can produce significant changes in output, making the device more responsive to signals. Sensitivity is crucial in applications where precise measurements or signal detection are required.

    -97dBm
  • Serial Interfaces

    A serial interface is a communication interface between two digital systems that transmits data as a series of voltage pulses down a wire. Essentially, the serial interface encodes the bits of a binary number by their "temporal" location on a wire rather than their "spatial" location within a set of wires.

    ADC, GPIO, I2C, I2S, PWM, SDIO, SPI, UART
  • Modulation

    In electronic components, modulation refers to the process of varying one or more properties of a periodic waveform, known as the carrier signal, in order to encode information. This modulation technique is commonly used in communication systems to transmit data efficiently over long distances. By modulating the carrier signal, information such as audio, video, or data can be embedded onto the signal for transmission and then demodulated at the receiving end to retrieve the original information. There are various types of modulation techniques, including amplitude modulation (AM), frequency modulation (FM), and phase modulation (PM), each with its own advantages and applications in different communication systems.

    CCK, DSSS, OFDM
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

Parts with Similar Specs

Trend Analysis

Datasheet PDF

Download datasheets and manufacturer documentation for RF Solutions ESP-32.
ESP-32

RF Solutions

In Stock: 138

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More