TDA7377 Amplifier vs TDA7388 Amplifier

Sophie

Published: 18 August 2022 | Last Updated: 05 November 2024

18718

TDA7388

TDA7388

STMicroelectronics

350mA mA 20 kHz kHz 41W W Audio Amplifiers 80W W 25 pins 25-Flexiwatt (Formed Leads)

Purchase Guide

350mA mA 20 kHz kHz 41W W Audio Amplifiers 80W W 25 pins 25-Flexiwatt (Formed Leads)

TDA7377 and TDA7388 are two Class AB power audio amplifier ICs. This article will introduce TDA7377 and TDA7388 systematically from their features, pinout to their specifications, applications, and so much more.

In this video you will be able to learn about the TDA series audio amplifier ICs which are TDA7377, TDA7388, TDA1514a.

Best TDA series amplifier ICs | TDA7377 , TDA7388, TDA1514A

TDA7377 VS TDA7388 Description

TDA7377 Description


The TDA7377 is a new technology class AB car radio amplifier, and it is able to work either in DUAL bridge or quad single-ended configuration. The exclusive fully complementary structure of the output stage and the internally fixed gain guarantees the highest possible power performances with few external components. The onboard clip detector simplifies gain compression operation. The fault diagnostics make it possible to detect mistakes during car radio set assembly and wiring in the car.

 

TDA7388 Description


TDA7388 is a class AB radio amplifier designed for car radio applications. It allows the rail-to-rail output swing for an entirely complementary PNP/NPN output configuration. And it does not require any bootstrap capacitors. Hence, it is a significantly reduced boundary component that makes a compact set.

TDA7388 belongs to package Flexiwatt25 and is a quad bridge amplifier. Therefore, it has four output channels where four speakers can be connected. It has a high output capability with low noise and is a 4-channel amplifier with 25 pins.


TDA7377 VS TDA7388 Features

TDA7377 Features


  • High Output Power@VCC=14.4V, f=1KHz,RL=4Ω:

      – 2 x 35W Max.

      – 2 x 20W@THD= 10%

      – 4 x 6 W @10%

      – 4 x 10W / 2Ω@10%

      – 2 x 30W / EIAJ@ VCC =13.7V,RL=4Ω

  • CMOS Compatible Stand-by Function (Low ICC)

  • No Audible pop During st-by Operations

  • Internally Fixed Gain (26dB BTL and 20dB single-ended)

  • No Bootstrap Capacitors and boucherot Cells

  • Diagnostics Facility on pin10 when output Clipping, shorted to

  • Vcc or GND, thermal shutdown, and soft short at turn on.

  • Rail to rail output swing

  • Absolute Stability Without Any External Compensation.

 

TDA7388 Features


  • High output power (4x45 W / 4 Ω max and 4x26 W / 4 Ω @14.4 V, 1 kHz, 10%)

  • Low output noise

  • Standby function

  • Mute function

  • Low distortion

  • Automate at minimum supply voltage detection

  • Low external component count

  • Operating supply voltage VS: 18 V

  • DC supply voltage VS(DC): 28 V

  • Peak supply voltage (t=50 ms) VPK: 50 V

  • Output peak current IO:

                Repetitive (duty cycle 10% @ f=10 Hz): 4.5 A

                Non-repetitive (t=100 μs): 5.5 A

  • Power dissipation Pd: 80 W

  • Quiescent current IQ: 190 mA (typ)

  • Output power PO: 26 W (typ) (VS = 14.4 V THD = 10%)

  • Maximum power output Pmax:

                41 W (@ VS = 14.4 V)

                45W (@ VS = 15.2 V)

  • THD: 0.04% (@PO = 4 W)


TDA7377 VS TDA7388 Applications

TDA7377 Applications

1. Connect to speakers

Connect the two wires of the speakers to the audio output port of the power amplifier, the left channel speaker is connected to the LOUT port of the amplifier and the right channel speaker is connected to the ROUT port, the positive connects to "+", the negative connects to "-".

 

2. Connect to sound source

Use an audio cable with an end of 3.5mm stereo headphone plug and plug in the 3.5 stereo headphone jack of the amplifier.

The other end of the audio cable is connected to the audio source (such as computers, mobile phones, MP3, DVD).

 

3. Connecting to the power supply

1) Connect to the adapter of the power supply

Use the power supply in which the output is above DC12V3A.

Connect the adapter's output cable to the 12V port of the power amplifier board.

The positive connects to the "+" of the port while the negative connects to "-".

2) Connect voltage converter

Use the voltage converter in which the output is above AC12V3A.

Connect the two output cables of the converter to the 12V port of the power amplifier board.

Because the converter's output is alternating current, it is not positive or negative.

 

4. Play music

Plugin the power, and the blue power indicator will light up which means that the power amplifier board starts working.

You can adjust the volume knob according to their preferences.

 

 

TDA7388 Applications

  • In-Car Radios

  • It can be used for Portable Speakers, Portable DVD Players, Game Machines

  • Any possible Quad Bridge amplifier-based project.


TDA7377 VS TDA7388 Pinout

7377 pinout.jpg

TDA7377 pinout


Pin NoPin NameDescription
1OUT 1Output 1
2OUT 2Output 2
3VCCCollector Supply   Voltage
4IN 1Input 1
5IN 2Input 2
6SVRSupply Voltage Rejection
7ST-BYStand By
8PW-GNDPower Ground
9S-GNDSignal Ground
10DIAG:Diagnostics
11IN 4Input 4
12IN 3Input 3
13VCCCollector Supply   Voltage
14OUT 4Output 4
15OUT 3Output 3


7388 pinout.jpg

TDA7388 pinout

Pin NoPin NamePin Function
1TABConnect to ground
2P-GND2Power ground of Channel 2
3OUT2-Inverting Output of Channel 2
4ST-BYStand-by
5OUT2+Non-Inverting Output of Channel 2
6VCCSupply Voltage
7OUT1-Inverting Output of Channel 1
8P-GND1Power ground of Channel 1
9OUT1+Non-Inverting Output of Channel 1
10SVRSupply Voltage Rejection
11IN1The input of Channel 1
12IN2The input of Channel 2
13S-GNDSignal ground
14IN4The input of Channel 4
15IN3The input of Channel 3
16AC-GNDAC ground
17OUT3+Non-Inverting Output of Channel 3
18P-GND3Power ground of Channel 3
19OUT3-Inverting Output of Channel 3
20VCCSupply Voltage
21OUT4+Non-Inverting Output of Channel 4
22MUTEMute
23OUT4-Inverting Output of Channel 4
24P-GND4Power GND of Channel 4
25HSDNo Connection


Parts with Similar Specs

The three parts on the right have similar specifications to STMicroelectronics & TDA7388.

TDA7377 VS TDA7388 Equivalents

TDA7377 Equivalents

TDA7377 and TDA7379 are class AB audio processor amplifiers that can operate in dual bridge or quad single-ended mode. The TDA 7377 has an operating supply voltage of 18v, whereas the TDA7379 has a 20v operating supply voltage. They are both equivalents to one another.

 

TDA7388 Equivalents

The equivalent amplifier ICs for TDA7388 is TDA7851F, TDA7561, TDA7387EP, and TB2941HQ .


TDA7377 VS TDA7388 Protection Systems

TDA7377 Protection Systems

  • Load Dump Voltages surge

  • Reversed Battery

  • Output DC Short Circuit protection with the low current when shorted to GND or VCC.

  • Output AC short circuit protection: across the load

  • Silent Turn On/Off

  • thermal shutdown

  • Load very Inductive speakers

  • Fortuitous Open GND

  • ESD

 

 

TDA7388 Protection Systems

  • Output short circuit to GND, to Vs across the load

  • Very inductive loads

  • Overrating chip temperature with thermal limiter

  • Load dump voltage

  • Fortuitous open GND

  • Reversal battery

  • ESD


TDA7377 VS TDA7388: Datasheet

Frequently Asked Questions

What is the difference between TDA7377 vs TDA7297?

TDA7377 has less distortion than TDA7297. TDA7297 is a plain stereo amplifier IC while TDA7377 offers 4 channels that may in used in stereo BTL coupling. Sound-wise, TDA7377 should be best. Both are cheap.

How do amplifiers work?

An amplifier takes an input signal from a source, such as a laptop, turntable, or CD player, and creates a larger copy of the original signal before it's sent to the speakers. It gets the power to do this from your mains electricity, which is sent directly to the power supply within the amplifier.

What is TDA7388?

The TDA7388 is an AB class audio power amplifier, packaged in Flexiwatt 25 and designed for high-end car radio applications. Based on a fully complementary PNP/NPN configuration, the TDA7388 allows a rail-to-rail output voltage swing with no need for bootstrap capacitors.

Can a TDA7377 be replaced by a JRC4558?

Everyone works in a similar way and many are compatible. The TL072 contains two amplifiers. So it’s used in stereo preamps. It can be replaced by JRC4558, TL082, or NE5532. Each one has its characteristic sound, without demeriting one from the other.

What kind of radio amplifier is a TDA7377?

This is one of the Power Amplifier types. The TDA7377 is a new technology class AB car radio amplifier able to work either in DUAL BRIDGE or QUAD SINGLE ENDED configuration.
TDA7388

STMicroelectronics

In Stock: 42840

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More