Sort by
Development Board vs Single-Board Computer (SBC): Differences, History, and How to Choose14 July 2026
If you have ever scoped a prototype, you have probably hit the same fork in the road: do you reach for a development board built around a specific chip, or a single-board computer that boots a full operating system? The two look similar on a bench, both arrive as a populated PCB with connectors along the edges, yet they belong to different design philosophies and solve different problems. This guide draws a clean line between them, sketches how each category grew up, lays out the real technical differences in side-by-side tables, and ends with a practical framework for picking the right one.
Tantalum Capacitors Explained: How They Work, Where They Fit, and How to Use Them Safely14 July 2026
Tantalum capacitors sit in an interesting spot in the design engineer's parts bin. They pack a large amount of capacitance into a small, stable, board-friendly package, yet they carry a reputation for failing dramatically when mistreated. Both halves of that reputation are true, and neither tells the whole story. Used within their ratings, tantalum capacitors are dependable workhorses; used carelessly, they can short and overheat. This guide walks through what they actually are, how the two main families differ, how they compare with aluminum electrolytic and ceramic parts, and the engineering discipline that keeps them reliable.
Commonly Used Circuit Protection Components: How to Match the Right Device to Each Threat14 July 2026
This guide organizes the commonly used components by threat and lays out a selection path for your own input stage. Exact numbers such as clamping voltage, interrupting current, and trip points always belong to the manufacturer datasheet, and each section points you there.
What Is a Safety Capacitor? Class X vs Class Y on the AC Line14 July 2026
A safety capacitor looks ordinary, but it does a job that an ordinary capacitor is not allowed to do: it connects directly to the AC mains and is built so that when it eventually fails, it fails in a way that does not put a person or the rest of the equipment at risk. That single difference, designed-in failure behavior backed by a certification standard, is what separates a "safety capacitor" from any other film or ceramic part with a high voltage rating printed on it.
What Is a Decoupling Capacitor? Function, Placement, and Selection Guide14 July 2026
In electronic circuits, it is often seen that there is an electrolytic capacitor near the power supply pins of the integrated circuit. This capacitor is a decoupling capacitor. Decoupling capacitors usually have two functions: one is energy storage, and the other is to remove high-frequency noise.
Film Capacitors Explained: Types, Characteristics, and How to Choose14 July 2026
This guide walks through what makes the family distinct, the plastic dielectrics that distinguish each variant, the two main ways the parts are built, the characteristics worth weighing, and a practical way to decide which film wins for a given design.
Ceramic Capacitor Dielectrics Explained: C0G, X7R, Y5V and How to Choose14 July 2026
A ceramic capacitor is also called a monolithic capacitor, whose dielectric material is ceramic. According to the different ceramic materials, it can be divided into two types: low-frequency ceramic capacitors and high-frequency ceramic capacitors. According to the structure, it can be divided into wafer capacitor, tubular capacitor, rectangular capacitor, a chip capacitor, feedthrough ceramic capacitor and so on.
How Electric Fuses Work: Types, Ratings, and Selection Guide14 July 2026
This guide walks through how a fuse actually interrupts a fault, the difference between fast and slow elements, the main fuse families and where each one belongs, the ratings that genuinely matter, and a repeatable method for choosing a fuse for your own circuit. It closes with the mistakes that most often cause either nuisance opening or unsafe under-protection, a clear comparison with circuit breakers, and a frequently asked questions section.
What Is an Electrical Connector? Types and Selection Checklist14 July 2026
This guide walks through the parts that actually matter, the main connector families and how to tell them apart, the locking methods that keep a mate secure, the role of contact plating, and a practical checklist you can apply when selecting one. It closes with the failure modes worth knowing and a short set of frequently asked questions.
Fiber Optic Connectors Explained: LC, SC, ST, FC and How to Choose14 July 2026
This guide walks through what the connector actually does, the families you will meet in the field, the difference between UPC and APC endfaces, how to tell similar plugs apart, and a practical way to choose for your own link.
Smartphone RF Chips Availability Forecast 2026: Lead-Time Risks and Alternatives14 July 2026
In 2026, the smartphone supply chain faces intense pressure as generative AI chips monopolize wafer and packaging capacity. Consequently, mobile manufacturers endure rising BOM costs and a projected 13.9% drop in shipments. While RF front-end lead times hover at 16 to 26 weeks, procurement teams must adopt multi-sourcing strategies, leverage specialized nodes like RF-SOI, and transition to "Just-in-Case" inventory models to survive.
Thermal Management in AI Servers: Specifying Class 2 MLCCs (X7R/X7S) for Liquid Cooling Environments13 July 2026
Explore how the transition from traditional air-cooling to liquid cooling (direct-to-chip and immersion) in high-density AI server racks alters component thermal profiles. Focus on why design engineers are increasingly specifying Class 2 MLCCs (X7R and X7S dielectrics) over standard X5R variants to prevent thermal degradation near the liquid cooling microchannels. Explain how these capacitors mitigate acoustic noise and voltage bias degradation under heavy workloads. Provide sourcing advice for high-reliability passives via UTMEL during this high-demand memory and passive component super-cycle.


Product
Brand
Articles
Tools