web counter

What is a Printed Circuit Board?

Published: 22 April 2021 | Last Updated: 22 April 20218087
A printed circuit board(PCB) is the provider of electrical connections for electronic components. Printed circuit boards are often represented by "PCB", but cannot be called "PCB boards".
This video tells you how are PCBs made and how do they make modern electronics possible.

How Do PCBs Work?

Catalog

Ⅰ Introduction
Ⅱ Printed circuit board history
Ⅲ Printed circuit board classification
Ⅳ Printed circuit board composition


Ⅰ Introduction

The printed circuit board has a history of more than 100 years. Its design is mainly layout design. The main advantage of using circuit boards is to greatly reduce wiring and assembly errors, and improve the level of automation and production labor rate.

According to the number of circuit boards, it can be divided into single-sided boards, single-sided boards, four-layer boards, six-layer boards, and other multilayer circuit boards.

PCB.jpg

PCB

Since the printed circuit board is not a general terminal product, the definition of the name is a little confusing. For example, the motherboard used in personal computers is called the mainboard, and cannot be directly called the circuit board. Although there are circuit boards on the mainboard, they are not the same. So when evaluating the industry, the two are related but cannot be said to be the same. Another example: because there are integrated circuit parts mounted on the circuit board, the news media call it an IC board, but in fact, it is not the same as a printed circuit board. We usually say that the printed circuit board refers to the bare board-that is, the circuit board without components.

The bare board (no parts on it) is also often referred to as "Printed Wiring Board (PWB)". The base plate of the board itself is made of materials that are insulated and heat-insulated, and not easy to bend. The small circuit material that can be seen on the surface is copper foil. The copper foil was originally covered on the entire board, but part of it was etched away during the manufacturing process, and the remaining part became a network of small lines. These lines are called conductor patterns or wiring and are used to provide circuit connections for parts on the PCB.

Usually, the color of PCB is green or brown, which is the color of the solder mask. It is an insulating protective layer that can protect the copper wire, prevent short circuits caused by wave soldering, and save the amount of solder. A silkscreen is also printed on the solder mask. Usually, words and symbols (mostly white) are printed on this to mark the position of each part on the board. The screen printing surface is also called the legend surface.

When the final product is made, integrated circuits, transistors, diodes, passive components (such as resistors, capacitors, connectors, etc.), and various other electronic parts will be installed on it. Through the wire connection, the electronic signal connection can be formed and the application function can be formed.

Ⅱ Printed circuit board history

Before the advent of printed circuit boards, the interconnection between electronic components relied on the direct connection of wires to form a complete circuit. In modern times, the circuit panel only exists as an effective experimental tool, and the printed circuit board has become an absolutely dominant position in the electronics industry.

At the beginning of the 20th century, in order to simplify the production of electronic equipment, reduce the wiring between electronic parts, and reduce production costs, people began to delve into the method of replacing wiring with printing. Over the past 30 years, engineers have repeatedly proposed to use metal conductors for wiring on insulated substrates. The most successful was in 1925, Charles Ducas of the United States printed circuit patterns on an insulating substrate, and then used electroplating to successfully establish conductors for wiring.

Until 1936, Austrian Paul Eisler published the foil technology in the United Kingdom. He used a printed circuit board in a radio device. In Japan, Miyamoto Kinosuke used the spray-attached wiring method "メタリコンMethod of Wiring (Patent No. 119384)" successfully applied for a patent. Among the two, Paul Eisler’s method is the most similar to today’s printed circuit boards. This type of method is called subtraction, which removes unnecessary metal. While Charles Ducas and Miyamoto Kinosuke’s method is to add only what is needed. The wiring is called the additive method. Even so, because the electronic components at that time generated a lot of heat, the substrates of the two were difficult to use together. 

Ⅲ Printed circuit board classification 

Single-sided PCB

On the most basic PCB, the parts are on one side, and the wires are on the other side. Because the wires only appear on one side, this kind of PCB is called single-sided. Because single-sided boards have many strict restrictions on the design of the circuit, only early circuits use this type of board. (because there is only one side, the wiring cannot cross and must be around a separate path.)

Double-sided PCB

This kind of circuit board has wiring on both sides, but to use wires on both sides, there must be a proper circuit connection between the two sides. The "bridge" between such circuits is called a via. A via is a small hole filled or coated with metal on the PCB, which can be connected with the wires on both sides. Because the area of the double-sided is twice as large as the single-sided, the double-sided solves the difficulty of the single-sided due to the interlacing of wiring (it can be passed to the other side through via holes), and it is more suitable for use in more complicated circuits than the single-sided.

Multilayer PCB

Multilayer PCB structure.jpg

Multilayer PCB structure

In order to increase the area that can be wired, multi-layer boards use more single or double-sided wiring boards. Use one double-sided as the inner layer, two single-sided as the outer layer, or two double-sided as the inner layer and two single-sided as the outer layer of the printed circuit board. Through the positioning system and the insulating bonding material alternately together. The printed circuit board with the conductive pattern interconnected according to the design requirements becomes a four-layer or six-layer printed circuit board, also known as a multilayer printed circuit board. The number of layers of the board does not mean that there are several independent wiring layers. In special cases, empty layers are added to control the thickness of the board. Usually, the number of layers is even and includes the two outermost layers. Most motherboards have a 4 to 8 layer structure, but technically, it can be a PCB of nearly 100 layers in theory. Most large supercomputers use fairly multi-layered motherboards, but because these types of computers can already be replaced by clusters of many ordinary computers, super-multilayered boards have gradually ceased to be used. Because the various layers in the PCB are tightly integrated, it is generally not easy to see the actual number, but if you look closely at the motherboard, you can still see it.

Ⅳ Printed circuit board composition

The current circuit board mainly consists of the following:

Circuit and pattern: The circuit is used as a tool for conduction between the originals. In the design, a large copper surface will be additionally designed as a grounding and power layer. The circuit and pattern are made at the same time.

Dielectric: It is used to maintain the insulation between the circuit and each layer, commonly known as the substrate.

Through hole / via: The through hole can make the lines of more than two levels connect to each other, the larger through hole is used as a part plug-in, and the non-through hole (nPTH) is usually used as a surface mount.

Solder resistant /Solder Mask: Not all copper surfaces need to be tin-on parts. The non-tin area will be printed with a layer of material (usually epoxy resin) that insulates the copper surface from eating tin. There is a short circuit between non-tinned lines. According to different processes, it is divided into green oil, red oil, and blue oil.

Legend /Marking/Silk screen: This is a non-essential composition. The main function is to mark the name and position frame of each part on the circuit board, which is convenient for maintenance and identification after assembly.

Surface Finish: Since the copper surface is easily oxidized in the general environment, it can not be tinned (poor soldering properties). It will be protected on the copper surface that needs to be tinned. The protection methods include HASL, ENIG, Immersion Silver, Immersion Tin, and Organic Solder Preservative (OSP). Each method has its advantages and disadvantages, which are collectively referred to as surface treatment.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Frequently Asked Questions

1.What does a printed circuit board do?

A printed circuit board, or PCB, is used to mechanically support and electrically connect electronic components using conductive pathways, tracks or signal traces etched from copper sheets laminated onto a non-conductive substrate.

2.What is a printed circuit board called?

The PCB revolutionized electrical engineering when it was invented back in 1936. To put it simply, the PCB made it possible to mass-produce electronic devices for the first time. The printed circuit board is the most common name but may also be called "printed wiring boards" or "printed wiring cards".

3.What is the difference between PCB and PWB?

When comparing PWB vs PCB, one difference that comes out is that PCB refers to a board with a complete circuit while PWB focuses on the board rather than the course. The use of the two terms varies from one place to the other. For example, in the manufacturing industry in the US, the two terms are used interchangeably.

4.What is a printed circuit board made of?

Printed circuit boards (PCBs) are usually flat laminated composite made from non-conductive substrate materials with layers of copper circuitry buried internally or on external surfaces. They can be as simple as one or two layers of copper, or in high-density applications, they can have fifty layers or more.

5.Why are PCBs green?

It is due to the solder mask, which protects the copper circuits printed on the fibre glass core to prevent short circuits, soldering errors, etc. The colour of the solder mask gives the board its appearance.
Related Articles

  • Pull-Down Circuit Guide: Working Principle, Resistor Value, Circuit Design, and Applications
    Pull-Down Circuit Guide: Working Principle, Resistor Value, Circuit Design, and Applications
    UTMEL26 June 2026566

    Learn how pull-down circuits work, how to choose a pull-down resistor value, and how to design reliable microcontroller inputs, MOSFET gates, reset pins, and sensor interfaces.

    Read More
  • Smd Components Outlook 2026: Supply, Lead Times, and Sourcing Options
    Smd Components Outlook 2026: Supply, Lead Times, and Sourcing Options
    UTMEL21 July 20261089

    The 2026 electronic component market faces a selective shortage driven by AI infrastructure and electric vehicles. While active ICs face lead times up to 55 weeks, commodity SMD passives remain stable at 12–20 weeks. This procurement guide details key trends in MLCCs and circuit protection, outlining actionable strategy solutions like dual-sourcing and flexible footprints to mitigate supply chain risks.

    Read More
  • Decoupling Capacitor Placement Guide: Maximizing Power Integrity in High-Speed Digital PCBs
    Decoupling Capacitor Placement Guide: Maximizing Power Integrity in High-Speed Digital PCBs
    UTMEL12 August 2026556

    This technical guide details how to optimize decoupling capacitor layout to maximize Power Integrity (PI) in high-speed digital PCBs. It explains how switching ICs induce power rail noise, the physics of parasitic loop inductance, and the impact of stackup plane separation. Layout engineers will find practical strategies for via placement, anti-resonance mitigation across multi-value capacitor networks, and sourcing reliable low-ESR MLCCs.

    Read More
  • sar-adc-reference-driver-selection-managing-dynamic-kickback-noise-loop-stability
    sar-adc-reference-driver-selection-managing-dynamic-kickback-noise-loop-stability
    UTMEL17 September 2026307

    Precision SAR ADCs present high-speed dynamic switched-capacitor loads that demand instantaneous transient currents during bit trials. This guide details how to size local decoupling capacitors accounting for MLCC DC bias derating, stabilize reference buffers using dual-loop in-loop compensation, and minimize multiplicative noise degradation. It also provides layout directives and dynamic bench verification protocols across sampling rate sweeps and burst modes.

    Read More
  • HF PCB Circuit Design 10 Questions
    HF PCB Circuit Design 10 Questions
    UTMEL16 March 20225552

    Hello everyone, I am Rose. Today I want to give you a full explanation about PCB design. I Hope the following ten questions will give you a satisfied answer.

    Read More

Subscribe to Utmel !

Featured Parts More