web counter

74LS86 Quad 2-Input XOR Gate IC: Pin, Datasheet pdf and Circuit Using 7486 Gate [FAQ]

UTMEL

Published: 08 December 2021 | Last Updated: 08 December 2021

17733

74LS86

74LS86

HIT(Hitachi)

74LS86 datasheet pdf and Unclassified product details from HIT(Hitachi) stock available at Utmel

Unit Price: $0.347175

Ext Price: $0.35

Purchase Guide

74LS86 is a quadruple XOR gate digital IC. XOR gates are logic gates with the combination of two NOT, two AND & one OR gates. This article is going to explain pin configuration, datasheet pdf, a circuit using gate IC, and other details about the 74LS86 XOR gate.

In this video, I've explained how to use xor gate IC 7486 and also explained its truth table on the breadboard.

SN74LS86 | XOR logic gate IC 7486 explained | Truth table explained

What is 74LS86?

74LS86 is a quadruple XOR gate IC. There are three types of gates AND, NOT, and NAND gates but with these gates, we can make multiple gates according to the requirement. Four independent positive logic 2-input exclusive OR (XOR) Gates are included in the 74LS86 IC package. It belongs to the 74XXYY IC family.

The 74LS86 IC supports a wide range of operating conditions and interfaces directly with CMOS, NMOS, and TTL devices. The IC's output is always in TTL, making it simple to interface with other TTL devices and microcontrollers.


74LS86 Pin Configuration

74LS86 pinout.jpg

74LS86 Pin

Pin NoPin NameDescription
11AINPUT 1 of GATE 1
21BINPUT 2 of GATE 1
31YOUTPUT of GATE 1
42AINPUT 1 of GATE 2
52BINPUT 2 of GATE 2
62YOUTPUT of GATE 2
7GNDGround pin
83YOUTPUT of GATE 3
93BINPUT 2 of GATE 3
103AINPUT 1 of GATE 3
114YOUTPUT of GATE 4
124BINPUT 2 of GATE 4
134AINPUT 1 of GATE 4
14VCCSupply Voltage


74LS86 CAD Model

74ls86.jpg

74LS86 Footprint

74ls86 3d model.jpg

74LS86 3D Model

Specifications

HIT(Hitachi) 74LS86 technical specifications, attributes, parameters and parts with similar specifications to HIT(Hitachi) 74LS86.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    DIP-14
  • Series

    In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.

    74LS
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube-packed
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    4.75V~5.25V
  • Logic Type

    Logic Type in electronic components refers to the classification of circuits based on the logical operations they perform. It includes types such as AND, OR, NOT, NAND, NOR, XOR, and XNOR, each defining the relationship between binary inputs and outputs. The logic type determines how the inputs affect the output state based on specific rules of Boolean algebra. This classification is crucial for designing digital circuits and systems, enabling engineers to select appropriate components for desired functionalities.

    XOR
  • Number of Circuits/Elements
    4
  • Number of Inputs/Bits per Element
    2
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

74LS86 Features

  • IOL (Max): 16mA

  • IOH (Max) -0.8mA

  • Technology Family: LS

  • VCC (Min): 4.75V

  • VCC (Max): 5.25V

  • No. of Channels: 4

  • Inputs per channel: 2

  • Input type: TTL-Compatible CMOS

  • Output type: Push-Pull

  • Features: High Speed (TPD 10-50ns)

  • Data rate (Max): 35Mbps

  • Rating: Catalog

  • Operating temperature range: 0°C to 70°C


74LS86 Applications

  • XOR gates are used to implement binary addition in computers.

  • Also used in Network equipment

  • Televisions & Home entertainment systems

 


How to Use 74LS86

The 74LS86 is based on the basic three gates' simple logic. The 7486 is a logical circuit with two AND gates, two NOT gates, and one OR gate. At input pins, the NOT gate will be employed, and the input will be passed to the AND gates without being inverted. The output from both AND gates will then be fed into the OR gate, which will then get the final output. The following is a circuit diagram.

74LS86 use.jpg

The OR gate only delivers a LOW output when both inputs are LOW; in this case, the NOT and AND gates are filtering the HIGH states before they reach the OR gates. The XOR gate circuit is created using this simple filtering method. Other combinations can be used to create the XOR gate, but each XOR gate will produce a different output depending on the inputs. A truth table can be used to represent the inputs and outcomes.


74LS86 Truth Table

TRUTH TABLE
INPUTS
OUTPUTS
ABOUTPUTS
000
011
101
110

When any one of the two inputs in the matching gate is high, the output of each gate in the chip should be high, as shown in the truth table. If both inputs are high or LOW, the output of an EX-OR gate will be low.


Circuit Using 74LS86 Gate IC

We're going to use a 1K resistor to draw both gate inputs to the ground in this XOR gate design. The inputs are then connected to electricity through a button.

As a result, when the button is pressed, the gate's corresponding pin becomes high. So the truth table of the EX-OR gate may be realized with just two buttons. When one of the buttons is pressed, one of the gate's inputs will be high and the other will be low; the output should be high at this moment.

74LS86 circuit.jpg

74LS86 Circuit

 

Because the chosen CHIP is a positive edge triggering one, these pull-down resistors are required. The circuit may produce unforeseen effects if the resistors are neglected.

The capacitors in this circuit are used to counteract the bouncing effect of buttons. Although the capacitors are not required, they may help the gate work more smoothly.


74LS86 Package Dimensions

74ls86 dimensions1.jpg

74ls86 dimensions2.jpg

74ls86 dimensions3.jpg

74LS86 Package Dimensions

74LS86 Manufacturer

On Semiconductor is driving energy-efficient innovations, empowering customers to reduce global energy use. The company offers a comprehensive portfolio of energy-efficient power and signal management, logic, discrete and custom solutions to help design engineers solve their unique design challenges in automotive, communications, computing, consumer, industrial, LED lighting, medical, military/aerospace, and power supply applications. On Semiconductor operates a responsive, reliable, world-class supply chain and quality program, and a network of manufacturing facilities, sales offices, and design centers in key markets throughout North America, Europe, and the Asia Pacific regions.


74LS86 Datasheet pdf

Frequently Asked Questions

What is 74LS86?

74LS86 is a quadruple XOR gate digital IC. XOR gates are logic gates with the combination of two NOT, two AND & one OR gates. The output state gets LOW only at the same inputs.

How many logic gates does 74LS86 have?

The 74LS86 IC package contains four independent positive logic 2-input exclusive OR (XOR) Gates.

How does 74ls86 work?

74LS86 is a quadruple XOR gate digital IC. When we combine these gates then we come up with multiple gates and XOR is one of them. XOR gates are logic gates with the combination of two NOT, two AND & one OR gates. The output state gets LOW only at the same inputs.

How many XOR gates does the 7486 have?

7486 has 4 EX-OR gates of 2 inputs in 1 package. The internal gates in the ICs are made of Schottky Transistor of low power. Another name of this IC is 'quadruple 2 inputs EXOR gate'.

What is the structure of 74LS86?

The 74LS86 follows the simple logic of the main basic three gates. The 7486 consists of a logical circuit using two AND, two NOT, and one OR gate. The NOT gate will be used at input pins and at the same time the input will be given to the AND gates without inverting.