web counter

AO4466 30V N-Channel MOSFET, 10A 8SOIC, AO4466 Datasheet pdf

UTMEL

Published: 11 February 2022 | Last Updated: 11 February 2022

4930

AO4466

AO4466

Alpha & Omega Semiconductor Inc.

N-Channel Tape & Reel (TR) 23m Ω @ 10A, 10V ±20V 448pF @ 15V 8.6nC @ 10V 30V 8-SOIC (0.154, 3.90mm Width)

Purchase Guide

N-Channel Tape & Reel (TR) 23m Ω @ 10A, 10V ±20V 448pF @ 15V 8.6nC @ 10V 30V 8-SOIC (0.154, 3.90mm Width)

AO4466 is a 30V N-Channel MOSFET packaged in 8-Pin SOIC. This article is going to cover AO4466 datasheet pdf, equivalents, pinout, features, and other details about AO4466 MOSFET.

This video demonstrates MOSFET Push Pull Amplifier Visual Demo.

MOSFET Push Pull Amplifier Visual Demo

What is AO4466?

The AO4466 employs innovative trench technology for high RDS  (ON) and low gate charge. This device can be used as a load switch or as part of a PWM  system. The source leads are separated to enable a Kelvin connection to the source, which can be utilized to bypass the inductance of the source.

AO4466 Pinout

ao4466 pinout.jpg

AO4466 Pinout

AO4466 CAD Model

AO4466 symbol.jpg

AO4466 Symbol

AO4466 footprint.jpg

AO4466 Footprint

AO4466 3d model1.jpg

AO4466 3D Model


Specifications

Alpha & Omega Semiconductor Inc. AO4466 technical specifications, attributes, parameters and parts with similar specifications to Alpha & Omega Semiconductor Inc. AO4466.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    8-SOIC (0.154, 3.90mm Width)
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    Surface Mount
  • Number of Pins
    8
  • Transistor Element Material

    The "Transistor Element Material" parameter in electronic components refers to the material used to construct the transistor within the component. Transistors are semiconductor devices that amplify or switch electronic signals and are a fundamental building block in electronic circuits. The material used for the transistor element can significantly impact the performance and characteristics of the component. Common materials used for transistor elements include silicon, germanium, and gallium arsenide, each with its own unique properties and suitability for different applications. The choice of transistor element material is crucial in designing electronic components to meet specific performance requirements such as speed, power efficiency, and temperature tolerance.

    SILICON
  • Voltage - Gate Threshold (Vgs(th)) (Max) @ Id
    2.6V @ 250μA
  • Power Dissipation (Max)
    3.1W Ta
  • Number of Elements
    1
  • Drive Voltage (Max Rds On, Min Rds On)
    4.5V 10V
  • Current - Continuous Drain (Id) @ 25℃
    10A Ta
  • Published
    2013
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -55°C~150°C TJ
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Not For New Designs
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    8
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    DUAL
  • Terminal Form

    Occurring at or forming the end of a series, succession, or the like; closing; concluding.

    GULL WING
  • Qualification Status

    An indicator of formal certification of qualifications.

    Not Qualified
  • Configuration

    The parameter "Configuration" in electronic components refers to the specific arrangement or setup of the components within a circuit or system. It encompasses how individual elements are interconnected and their physical layout. Configuration can affect the functionality, performance, and efficiency of the electronic system, and may influence factors such as signal flow, impedance, and power distribution. Understanding the configuration is essential for design, troubleshooting, and optimizing electronic devices.

    SINGLE WITH BUILT-IN DIODE
  • Operating Mode

    A phase of operation during the operation and maintenance stages of the life cycle of a facility.

    ENHANCEMENT MODE
  • Power Dissipation

    the process by which an electronic or electrical device produces heat (energy loss or waste) as an undesirable derivative of its primary action.

    3.1W
  • FET Type

    "FET Type" refers to the type of Field-Effect Transistor (FET) being used in an electronic component. FETs are three-terminal semiconductor devices that can be classified into different types based on their construction and operation. The main types of FETs include Metal-Oxide-Semiconductor FETs (MOSFETs), Junction FETs (JFETs), and Insulated-Gate Bipolar Transistors (IGBTs).Each type of FET has its own unique characteristics and applications. MOSFETs are commonly used in digital circuits due to their high input impedance and low power consumption. JFETs are often used in low-noise amplifiers and switching circuits. IGBTs combine the high input impedance of MOSFETs with the high current-carrying capability of bipolar transistors, making them suitable for high-power applications like motor control and power inverters.When selecting an electronic component, understanding the FET type is crucial as it determines the device's performance and suitability for a specific application. It is important to consider factors such as voltage ratings, current handling capabilities, switching speeds, and power dissipation when choosing the right FET type for a particular circuit design.

    N-Channel
  • Transistor Application

    In the context of electronic components, the parameter "Transistor Application" refers to the specific purpose or function for which a transistor is designed and used. Transistors are semiconductor devices that can amplify or switch electronic signals and are commonly used in various electronic circuits. The application of a transistor can vary widely depending on its design and characteristics, such as whether it is intended for audio amplification, digital logic, power control, or radio frequency applications. Understanding the transistor application is important for selecting the right type of transistor for a particular circuit or system to ensure optimal performance and functionality.

    SWITCHING
  • Rds On (Max) @ Id, Vgs

    Rds On (Max) @ Id, Vgs refers to the maximum on-resistance of a MOSFET or similar transistor when it is fully turned on or in the saturation region. It is specified at a given drain current (Id) and gate-source voltage (Vgs). This parameter indicates how much resistance the component will offer when conducting, impacting power loss and efficiency in a circuit. Lower Rds On values are preferred for better performance in switching applications.

    23m Ω @ 10A, 10V
  • Input Capacitance (Ciss) (Max) @ Vds

    The parameter "Input Capacitance (Ciss) (Max) @ Vds" in electronic components refers to the maximum input capacitance measured at a specific drain-source voltage (Vds). Input capacitance is a crucial parameter in field-effect transistors (FETs) and power MOSFETs, as it represents the total capacitance at the input terminal of the device. This capacitance affects the device's switching speed and overall performance, as it influences the time required for charging and discharging during operation. Manufacturers provide this parameter to help designers understand the device's input characteristics and make informed decisions when integrating it into a circuit.

    448pF @ 15V
  • Gate Charge (Qg) (Max) @ Vgs

    Gate Charge (Qg) (Max) @ Vgs refers to the maximum amount of charge that must be supplied to the gate of a MOSFET or similar device to fully turn it on, measured at a specific gate-source voltage (Vgs). This parameter is crucial for understanding the switching characteristics of the device, as it influences the speed at which the gate can charge and discharge. A higher gate charge value often implies slower switching speeds, which can impact the efficiency of high-frequency applications. This parameter is typically specified in nanocoulombs (nC) in the component's datasheet.

    8.6nC @ 10V
  • Drain to Source Voltage (Vdss)

    The Drain to Source Voltage (Vdss) is a key parameter in electronic components, particularly in field-effect transistors (FETs) such as MOSFETs. It refers to the maximum voltage that can be applied between the drain and source terminals of the FET without causing damage to the component. Exceeding this voltage limit can lead to breakdown and potentially permanent damage to the device.Vdss is an important specification to consider when designing or selecting components for a circuit, as it determines the operating range and reliability of the FET. It is crucial to ensure that the Vdss rating of the component is higher than the maximum voltage expected in the circuit to prevent failures and ensure proper functionality.In summary, the Drain to Source Voltage (Vdss) is a critical parameter that defines the maximum voltage tolerance of a FET component and plays a significant role in determining the overall performance and reliability of electronic circuits.

    30V
  • Vgs (Max)

    Vgs (Max) refers to the maximum gate-source voltage that can be applied to a field-effect transistor (FET) without causing damage to the component. This parameter is crucial in determining the safe operating limits of the FET and helps prevent overvoltage conditions that could lead to device failure. Exceeding the specified Vgs (Max) rating can result in breakdown of the gate oxide layer, leading to permanent damage to the FET. Designers must ensure that the applied gate-source voltage does not exceed the maximum rating to ensure reliable and long-term operation of the electronic component.

    ±20V
  • Continuous Drain Current (ID)

    Continuous Drain Current (ID) is a key parameter in electronic components, particularly in field-effect transistors (FETs) such as MOSFETs. It refers to the maximum current that can flow continuously through the drain terminal of the FET without causing damage to the component. This parameter is crucial for determining the power handling capability of the FET and is specified by the manufacturer in the component's datasheet. Designers must ensure that the actual operating current does not exceed the specified Continuous Drain Current to prevent overheating and potential failure of the component.

    10A
  • Gate to Source Voltage (Vgs)

    The Gate to Source Voltage (Vgs) is a crucial parameter in electronic components, particularly in field-effect transistors (FETs) such as MOSFETs. It refers to the voltage difference between the gate and source terminals of the FET. This voltage determines the conductivity of the FET and controls the flow of current through the device. By varying the Vgs, the FET can be switched on or off, allowing for precise control of electronic circuits. Understanding and properly managing the Vgs is essential for ensuring the reliable and efficient operation of FET-based circuits.

    20V
  • Drain-source On Resistance-Max

    Drain-source On Resistance-Max, commonly referred to as RDS(on) max, is a specification for MOSFETs that indicates the maximum resistance between the drain and source terminals when the device is turned on. This parameter is critical for assessing the efficiency of a MOSFET in a circuit, as lower values result in reduced power loss and heat generation during operation. It is measured in ohms and is influenced by factors such as temperature and gate-to-source voltage. Understanding RDS(on) max is essential for optimizing performance in power management and switching applications.

    0.023Ohm
  • Pulsed Drain Current-Max (IDM)

    The parameter "Pulsed Drain Current-Max (IDM)" in electronic components refers to the maximum current that the device can handle when operated under pulsed conditions. This specification is important for understanding the device's capability to handle short bursts of high current without causing damage. It is typically measured in amperes and is specified for a specific pulse width and duty cycle. Designers use this parameter to ensure that the component can withstand transient current spikes without failing, making it crucial for applications where pulsed operation is common, such as in power electronics and RF circuits.

    50A
  • DS Breakdown Voltage-Min

    The parameter "DS Breakdown Voltage-Min" in electronic components refers to the minimum voltage at which the device will experience a breakdown in its Drain-Source (DS) junction. This voltage represents the point at which the component can no longer effectively regulate or control the flow of current, leading to potential damage or failure. It is an important specification to consider when designing or selecting components for a circuit, as exceeding this breakdown voltage can result in permanent damage to the device. Manufacturers provide this specification to ensure proper usage and to help engineers determine the appropriate operating conditions for the component.

    30V
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
0 Similar Products Remaining

Features of AO4466

  • Type of TransistorMOSFET 

  • Type of Control Channel: N -Channel 

  • Maximum Power Dissipation  (Pd): 3.1 W

  • Maximum Drain-Source Voltage |Vds|: 30 V

  • Maximum Gate-Source Voltage |Vgs|: 20 V

  • Maximum Gate-Threshold Voltage |Vgs(th)|: 2.6 V

  • Maximum Drain Current |Id|: 10 A

  • Maximum Junction Temperature  (Tj): 150 °C

  • Rise Time (tr): 2.8 nS

  • Drain-Source Capacitance (Cd): 67 pF

  • Maximum Drain-Source On-State Resistance (Rds): 0.023 Ohm

  • Package: SO-8


AO4466 Product Summary

  • VDS (V) = 30V 

  • ID = 10A (VGS = 10V)

  • RDS(ON) < 23mΩ (VGS = 10V)

  • RDS(ON) < 35mΩ (VGS = 4.5V)

  • 100% UIS Tested

  • 100% Rg Tested


AO4466 Equivalents

AO4459, AO4459, AO4466, AO4466AO4466, AO4468, AO4468, AO4468, AO4474

Parts with Similar Specs

The three parts on the right have similar specifications to Alpha & Omega Semiconductor Inc. & AO4466.

AO4466 Package Dimensions

ao4466 dimensions1.jpg

ao4466 dimensions2.jpg

ao4466 dimensions3.jpg

AO4466 Package Dimensions

AO4466 Manufacturer

Alpha and Omega Semiconductor, Inc., or AOS, is a designer, developer, and global supplier of a broad range of power semiconductors, including a wide portfolio of Power MOSFET and Power IC products. AOS seeks to differentiate itself by integrating its expertise in device physics, process technology, design, and advanced packaging to optimize product performance and cost, and its product portfolio is designed to meet the ever-increasing power efficiency requirements in high volume applications, including portable computers, flat-panel TVs, battery packs, portable media players and power supplies.


Popularity by Region

Datasheet PDF

Download datasheets and manufacturer documentation for Alpha & Omega Semiconductor Inc. AO4466.
Frequently Asked Questions

What can be the AO4466 used as?

The load switch

What is the maximum voltage of the AO4466 Type of Transistor?

2.6 V

What is AO4466 used for?

The AO4466 is a 30V N-Channel MOSFET using advanced trench technology to provide excellent RDS(ON) and low gate charge. This device is suitable for use as a load switch or in PWM applications. The source leads are separated to allow a Kelvin connection to the source, which may be used to bypass the source inductance.
AO4466

Alpha & Omega Semiconductor Inc.

In Stock: 30

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More
  • AON6562
    AON6562

    Alpha & Omega Semiconductor Inc.

  • AOL1428
    AOL1428

    Alpha & Omega Semiconductor Inc.

  • AON6912ALS
    AON6912ALS

    Alpha & Omega Semiconductor Inc.

  • AO4722
    AO4722

    Alpha & Omega Semiconductor Inc.

  • AO3422
    AO3422

    Alpha & Omega Semiconductor Inc.

  • AO3419
    AO3419

    Alpha & Omega Semiconductor Inc.

  • AOD458
    AOD458

    Alpha & Omega Semiconductor Inc.

  • AO4459
    AO4459

    Alpha & Omega Semiconductor Inc.

  • AO3401A
    AO3401A

    Alpha & Omega Semiconductor Inc.

  • AO3400A
    AO3400A

    Alpha & Omega Semiconductor Inc.