ESP32S2 WiFi 802.11b/g/n Transceiver Module: Datasheet, Pinout, and Application

UTMEL

Published: 13 January 2022 | Last Updated: 13 January 2022

2910

ESP32-S2

ESP32-S2

Espressif Systems

2.4GHz WiFi -40°C~125°C 2.8V~3.6V ADC, I2C, I2S, SPI, PWM, UART Antenna Not Included 150Mbps 19.5dBm 802.11b/g/n -97dBm 56-VFQFN Exposed Pad

Purchase Guide

2.4GHz WiFi -40°C~125°C 2.8V~3.6V ADC, I2C, I2S, SPI, PWM, UART Antenna Not Included 150Mbps 19.5dBm 802.11b/g/n -97dBm 56-VFQFN Exposed Pad

ESP32S2 is WiFi Transceiver Module. This article is going to introduce pinout, applications, features, and more details about ESP32S2.

This video demonstrates how relevant is ESP32-S2 for the makers and show more detailed information about ESP32-S2.

The new ESP32-S2: How relevant is it for the Makers?

Overview of ESP32S2

ESP32-S2 family is a highly-integrated, low-power, 2.4 GHz Wi-Fi System-on-Chip (SoC) solution. With its state-of-the-art power and RF performance, this SoC is an ideal choice for a wide variety of application scenarios relating to the Internet of Things (IoT), wearable electronics, and smart homes. ESP32-S2 family includes a Wi-Fi subsystem that integrates a Wi-Fi MAC, Wi-Fi radio and baseband, RF switch, RF balun, power amplifier, low noise amplifier (LNA), etc. The chip is fully compliant with the IEEE 802.11b/g/n protocol and offers a complete Wi-Fi solution. At the core of this chip is an Xtensa® 32-bit LX7 CPU that operates at up to 240 MHz. The chip supports application development, without the need for a host MCU. The on-chip memory includes 320 KB SRAM and 128 KB ROM. It also supports multiple external SPI/QSPI/OSPI flash and external RAM chips for more memory space.

ESP32S2 Features

  • ESP32-S2-WROOM or ESP32-S2-WROVER module with Xtensa® 32-bit LX7 CPU 240 MHz

  • 320 KB SRAM, 128KB ROM, 16 KB SRAM in RTC

  • 4MB Flash

  • 2MB PSRAM in ESP32-S2-WROVER-DevKit-Lipo

  • WiFi 1T1R 150Mbps

  • LiPo battery charger

  • Battery monitoring

  • External power sense

  • Low consumption

  • RGB LED

  • CH340T programmer works with Espressif SDK, Arduino, Platform IO

  • Reset button

  • User button

  • Pin-to-pin compatible with ESP32-S2-SAOLA-1


Specifications

Espressif Systems ESP32-S2 technical specifications, attributes, parameters and parts with similar specifications to Espressif Systems ESP32-S2.
  • Type
    Parameter
  • Factory Lead Time
    8 Weeks
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    56-VFQFN Exposed Pad
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    -40°C~125°C
  • Series

    In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.

    ESP32
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Active
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    3 (168 Hours)
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    2.8V~3.6V
  • Frequency

    In electronic components, the parameter "Frequency" refers to the rate at which a signal oscillates or cycles within a given period of time. It is typically measured in Hertz (Hz) and represents how many times a signal completes a full cycle in one second. Frequency is a crucial aspect in electronic components as it determines the behavior and performance of various devices such as oscillators, filters, and communication systems. Understanding the frequency characteristics of components is essential for designing and analyzing electronic circuits to ensure proper functionality and compatibility with other components in a system.

    2.4GHz
  • Memory Size

    The memory capacity is the amount of data a device can store at any given time in its memory.

    128kB ROM 320kB SRAM
  • Data Rate

    Data Rate is defined as the amount of data transmitted during a specified time period over a network. It is the speed at which data is transferred from one device to another or between a peripheral device and the computer. It is generally measured in Mega bits per second(Mbps) or Mega bytes per second(MBps).

    150Mbps
  • Utilized IC / Part

    Utilized IC / Part is a parameter that refers to the extent to which an integrated circuit (IC) or electronic component is being used or consumed within a system or application. It typically indicates the percentage or ratio of the component's capabilities that are being utilized in a given scenario. This parameter is important for assessing the efficiency and performance of the component, as well as for determining if the component is being underutilized or overburdened in a particular application. Monitoring and optimizing the utilization of ICs and electronic parts can help improve overall system reliability, efficiency, and cost-effectiveness.

    ESP32-S2
  • Protocol

    In electronic components, the parameter "Protocol" refers to a set of rules and standards that govern the communication between devices. It defines the format, timing, sequencing, and error checking methods for data exchange between different components or systems. Protocols ensure that devices can understand and interpret data correctly, enabling them to communicate effectively with each other. Common examples of protocols in electronics include USB, Ethernet, SPI, I2C, and Bluetooth, each with its own specifications for data transmission. Understanding and adhering to protocols is essential for ensuring compatibility and reliable communication between electronic devices.

    802.11b/g/n
  • Power - Output

    Power Output in electronic components refers to the amount of electrical power that a device can deliver to a load. It is typically measured in watts and indicates the effectiveness of the component in converting electrical energy into usable work or signal. Power Output can vary based on the component's design, operating conditions, and intended application, making it a critical factor in the performance of amplifiers, power supplies, and other electronic devices. Understanding the Power Output helps in selecting appropriate components for specific applications to ensure efficiency and reliability.

    19.5dBm
  • RF Family/Standard

    The parameter "RF Family/Standard" in electronic components refers to the specific radio frequency (RF) technology or standard that the component complies with or is designed for. RF technology encompasses a wide range of frequencies used for wireless communication, such as Wi-Fi, Bluetooth, cellular networks, and more. Different RF standards dictate the frequency bands, modulation techniques, data rates, and other specifications for communication systems. Understanding the RF family/standard of a component is crucial for ensuring compatibility and optimal performance in RF applications.

    WiFi
  • Antenna Type

    There are several different types of antennas in three broad categories: omni-directional, directional, and semi-directional.

    Antenna Not Included
  • Sensitivity

    Sensitivity in electronic components refers to the degree to which the output of a device responds to changes in input. It indicates how effectively a component translates a specific input signal into an observable output. High sensitivity means that even small variations in input can produce significant changes in output, making the device more responsive to signals. Sensitivity is crucial in applications where precise measurements or signal detection are required.

    -97dBm
  • Serial Interfaces

    A serial interface is a communication interface between two digital systems that transmits data as a series of voltage pulses down a wire. Essentially, the serial interface encodes the bits of a binary number by their "temporal" location on a wire rather than their "spatial" location within a set of wires.

    ADC, I2C, I2S, SPI, PWM, UART
  • Current - Receiving

    Current - Receiving refers to the amount of electrical current that an electronic component or device is capable of accepting from a power source or another component in a circuit. It indicates the maximum current that can be safely received without causing damage or malfunction. This parameter is crucial for ensuring compatibility and reliability in electronic designs, as exceeding the rated receiving current can lead to overheating or failure of the component.

    63mA~68mA
  • Current - Transmitting

    Current - Transmitting is a parameter used to describe the maximum amount of electrical current that an electronic component can handle while in the transmitting mode. This parameter is crucial for components such as transistors, diodes, and integrated circuits that are involved in transmitting signals or power within a circuit. Exceeding the specified current transmitting rating can lead to overheating, component failure, or even damage to the entire circuit. Designers and engineers must carefully consider this parameter when selecting components to ensure the reliability and performance of the electronic system.

    160mA~310mA
0 Similar Products Remaining

ESP32S2 Pinout

ESP32S2 Pinout.png

ESP32S2 Pinout


ESP32S2 Block Diagram

ESP32S2 Block Diagram.png

ESP32S2 Block Diagram


ESP32S2 Applications

• Generic Low-power IoT Sensor Hubs

• Generic Low-power IoT Data Loggers

• Cameras for Video Streaming

• Over-the-top (OTT) Devices

• USB Devices

• Speech Recognition

• Image Recognition

• Mesh Networks

• Home Automation

– Light control

– Smart plugs

– Smart door locks

• Smart Buildings

– Smart lighting

– Energy monitoring

• Industrial Automation

– Industrial wireless control

– Industrial robotics

• Smart Agriculture

– Smart greenhouses

– Smart irrigation

– Agriculture robotics

• Audio Applications

– Internet music players

– Live streaming devices

– Internet radio players

– Audio headsets

• Health Care Applications

– Health monitoring

– Baby monitors

• Wi-Fi-enabled Toys

– Remote control toys

– Proximity sensing toys

– Educational toys

• Wearable Electronics

– Smart watches

– Smart bracelets

• Retail & Catering Applications

– POS machines

– Service robots

• Touch Sensing Applications

– Waterproof design

– Distance sensing applications

– Linear slider, wheel slider designs


ESP32S2 Package information

ESP32S2 Package information.png

ESP32S2 Package information


ESP32S2 Manufacturer

Espressif Systems is a world-leading Internet-of-Things (IoT) company. They are an innovative team of chip-design specialists, software/firmware developers, and marketers. They are committed to providing some of the best IoT devices and software platforms in the industry. They also help their customers build their own solutions and connect with other partners in the IoT ecosystem. Their passion lies in creating state-of-the-art chipsets and enabling their partners to deliver great products. Espressif’s products are widely deployed in the tablet, OTT boxes, cameras, and IoT markets.


Datasheet PDF

Download datasheets and manufacturer documentation for Espressif Systems ESP32-S2.

Popularity by Region

Parts with Similar Specs

Frequently Asked Questions

How many pins of ESP32S2 ?

56 pins.

What’s the operating temperature of the ESP32S2?

-40°C~125°C
ESP32-S2

Espressif Systems

In Stock: 25
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
Related Parts More