web counter

Exploring the Cypress MB91520 Series: 32-bit FR81S Microcontroller for Automotive Devices

UTMEL

Published: 29 February 2024 | Last Updated: 29 February 2024

256

MB91F522BSCPMC1-GSE1

MB91F522BSCPMC1-GSE1

Cypress Semiconductor

Microcontroller 80MHz LQFP

Purchase Guide

Microcontroller 80MHz LQFP

This article delves into the features, functions, and applications of the Cypress MB91520 series, a 32-bit FR81S microcontroller tailored for automotive devices. The detailed overview covers the FR81S CPU core, peripheral functions, memory configurations, built-in interfaces, unique features, and applications in automotive systems.

Product Introduction

Description
The Cypress MB91520 series comprises the FR81S CPU, featuring a 32-bit RISC load/store architecture pipeline with a maximum operating frequency of 80 MHz. The microcontroller offers exceptional support for embedded applications, with a rich set of built-in peripherals, and is designed to meet the stringent requirements of automotive systems.

Features
The MB91520 series presents a wide array of features including:
- 32-bit RISC load/store architecture pipeline with 5-stage structure
- Maximum operating frequency of 80 MHz
- General-purpose register: 32 bits × 16 sets
- High-level language support instructions
- Built-in memory protection function (MPU)
- Built-in FPU (floating point arithmetic)
- Clock generation with SSCG function
- Built-in flash memory capacity ranging from 256+64KB to 1024+64KB
- Built-in RAM capacity up to 128KB
- General-purpose ports with various configurations
- External bus interface
- DMA controller, A/D converter, and D/A converter
- Multi-function serial communication with UART, CSIO, LIN, I2C, and CAN support
- PPG, Input capture, Output compare, Real-time clock, and Base timer functions

Applications
The MB91520 series is specifically designed for various automotive applications including, but not limited to:
- Engine control systems
- Transmission control units
- Body control modules
- Automotive infotainment and telematics
- Advanced driver-assistance systems (ADAS)
- Automotive gateway and networking systems
- Electric vehicle (EV) and hybrid electric vehicle (HEV) control units
- Automotive lighting and climate control

FAQs
Q: What is the maximum operating frequency of the FR81S CPU in the MB91520 series?
A: The FR81S CPU has a maximum operating frequency of 80 MHz, providing high performance for automotive applications.

Q: Are there specific development tools and software available for programming the MB91520 series microcontrollers?
A: Cypress provides a range of development tools, including integrated development environments (IDEs) and programming tools, to support the programming and debugging of the MB91520 series for automotive applications.

Q: Can the MB91520 series microcontrollers be used in safety-critical systems within automotive environments?
A: Yes, the MB91520 series microcontrollers feature a built-in memory protection function (MPU) and comply with relevant automotive industry standards, making them suitable for use in safety-critical automotive systems.

Q: What are the key features that make the MB91520 series well-suited for electric vehicle (EV) and hybrid electric vehicle (HEV) control units?
A: The MB91520 series offers a comprehensive set of built-in peripherals, including advanced A/D converters, D/A converters, and multi-function serial communication, making them well-suited for EV and HEV control units.

Specifications

Cypress Semiconductor MB91F522BSCPMC1-GSE1 technical specifications, attributes, parameters and parts with similar specifications to Cypress Semiconductor MB91F522BSCPMC1-GSE1.
  • Type
    Parameter
  • Factory Lead Time
    21 Weeks
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    LQFP
  • Operating Temperature (Max)

    The parameter "Operating Temperature (Max)" in electronic components refers to the maximum temperature at which the component can safely operate without experiencing damage or performance degradation. This specification is crucial for ensuring the reliability and longevity of the component in various operating conditions. Exceeding the maximum operating temperature can lead to thermal stress, reduced efficiency, and ultimately failure of the component. It is important for designers and engineers to consider this parameter when selecting and using electronic components to ensure proper functionality and prevent potential issues related to overheating.

    105°C
  • Memory Types
    FLASH
  • Operating Temperature (Min)

    The parameter "Operating Temperature (Min)" in electronic components refers to the minimum temperature at which the component is designed to operate effectively and reliably. This specification indicates the lowest temperature at which the component can function within its specified performance limits. Operating below this minimum temperature may result in reduced efficiency, slower response times, or even complete failure of the component. It is important to consider the operating temperature range of electronic components to ensure proper functionality and longevity in various environmental conditions.

    -40°C
  • Number of I/Os
    44
  • Published
    2017
  • Frequency

    In electronic components, the parameter "Frequency" refers to the rate at which a signal oscillates or cycles within a given period of time. It is typically measured in Hertz (Hz) and represents how many times a signal completes a full cycle in one second. Frequency is a crucial aspect in electronic components as it determines the behavior and performance of various devices such as oscillators, filters, and communication systems. Understanding the frequency characteristics of components is essential for designing and analyzing electronic circuits to ensure proper functionality and compatibility with other components in a system.

    80MHz
  • Interface

    In electronic components, the term "Interface" refers to the point at which two different systems, devices, or components connect and interact with each other. It can involve physical connections such as ports, connectors, or cables, as well as communication protocols and standards that facilitate the exchange of data or signals between the connected entities. The interface serves as a bridge that enables seamless communication and interoperability between different parts of a system or between different systems altogether. Designing a reliable and efficient interface is crucial in ensuring proper functionality and performance of electronic components and systems.

    CAN, I2C, LIN, SPI, UART, USART
  • Memory Size

    The memory capacity is the amount of data a device can store at any given time in its memory.

    320kB
  • Oscillator Type

    Wien Bridge Oscillator; RC Phase Shift Oscillator; Hartley Oscillator; Voltage Controlled Oscillator; Colpitts Oscillator; Clapp Oscillators; Crystal Oscillators; Armstrong Oscillator.

    External
  • Peripherals

    In the context of electronic components, "Peripherals" refer to devices or components that are connected to a main system or device to enhance its functionality or provide additional features. These peripherals can include input devices such as keyboards, mice, and touchscreens, as well as output devices like monitors, printers, and speakers. Other examples of peripherals include external storage devices, network adapters, and cameras. Essentially, peripherals are external devices that expand the capabilities of a main electronic system or device.

    DMA, LVD, POR, PWM, WDT
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

Parts with Similar Specs

Datasheet PDF

Download datasheets and manufacturer documentation for Cypress Semiconductor MB91F522BSCPMC1-GSE1.
MB91F522BSCPMC1-GSE1

Cypress Semiconductor

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More