web counter

KA7500B Controller: Features, Pinout, and Datasheet [Video&FAQ]

Sophie

Published: 21 October 2021 | Last Updated: 21 October 2021

61510

KA7500B

KA7500B

ON Semiconductor

16 Terminals 16-Pin KA7500 DC to DC converter IC SWITCHING CONTROLLER 1 Outputs 1kHz~300kHz Transistor Driver

Purchase Guide

16 Terminals 16-Pin KA7500 DC to DC converter IC SWITCHING CONTROLLER 1 Outputs 1kHz~300kHz Transistor Driver

Hello guys. The KA7500B is used for the control circuit of the PWM switching regulator. This article mainly introduces features, pinout, datasheet and other detailed information about ON Semiconductor KA7500B.

This video will show you how to test TL494 and KA7500B.

How to test TL494 / KA7500 PWM Controller IC

KA7500B Description

The KA7500B is used for the control circuit of the  PWM  switching regulator. The KA7500B consists of a 5V reference voltage circuit, two error amplifiers, a flip flop, an output control circuit, a  PWM comparator, a dead time comparator and an oscillator. This device can be operated in the switching frequency of 1kHz to 300kHz.

 

KA7500B Pinout

pinout.jpg

Pinout

Pin NumberPin NameDescription
11IN+The non-inverting input terminal of error amplifier 1. In the closed-loop system, the given signal of the controlled quantity will be input to the error amplifier through this pin, while in the open-loop system, the pin needs to be grounded or left floating.
21IN-The inverting input terminal of the error amplifier 1. In the closed-loop system, the feedback signal of the controlled quantity will be input into the error amplifier through this pin. At this time, it is also necessary to connect the feedback network between this pin and pin 3. In the open-loop system, this pin is grounded or left floating.
3FEEDBACKFeedback/PWM comparator input terminal. In a closed-loop system, different types of feedback networks can be connected between this pin and pin 2 as required to form various types of regulators such as proportional, proportional-integral, and integral to meet different user needs.
4DTCThe dead time controls the output of the comparator. This terminal is used to set the value of TL494 dead time. When this pin is grounded, the dead time is the smallest, and the maximum station-to-empty ratio can be obtained.
5CTOscillator timing capacitor access terminal. The value range of CT is usually between 0.001 and 0.1yF.
6RTOscillator timing resistor access terminal. The value range of the foot is usually between 5 to 100kQ.
7GNDSignal ground (reference ground for chip work).
8C1The collector terminal of the output transistor VT1, which is the positive pulse output terminal. In push-pull working mode, this terminal outputs a positive pulse signal, and pin 11 outputs a negative pulse signal. The phase difference between the two is 1800. After isolation and amplification, the switching tube is driven separately. In single-ended working mode, this terminal can be connected in parallel with pin 11 to improve the output capability of the pulse width modulation controller TL494.
9E1The emitter terminal of the output transistor VT1, this terminal is the reference ground terminal of the pin 8 output pulse signal and is generally directly connected to pin 7.
10E2The emitter terminal of the output transistor VT2, this terminal is the reference ground terminal of the pin 11 output pulse signal and is generally directly connected to pin 7.
11C2The collector terminal of the output transistor VT2, which is the reverse pulse output terminal. In the push-pull working mode, this terminal outputs a reverse pulse signal, and pin 8 outputs a forward pulse signal. The phase difference between the two is 1800. After isolation and amplification, they drive the switch tubes respectively. In single-ended working mode, this terminal can be connected in parallel with pin 8 to improve the output capability of the pulse width modulation controller TL494.
12VccBias power (chip working power) access terminal. In application, a filter capacitor with a capacity of 0.1UF or more must be connected to the common ground terminal.
13OUTPUT CTRLOutput working mode control terminal. Push-pull or single-ended output mode can be selected through this pin. When the terminal is connected to a high level, TL494 will work in push-pull mode, and the maximum duty cycle can reach 48% at this time. When the terminal is connected to a low level, the two output pulses are exactly the same, and the maximum duty cycle can reach 96%.
14REFThe input current of the reference power supply output can reach 10mA.
152IN-The inverted input terminal of the error amplifier 2. This terminal can be connected to the feedback signal of the protection circuit to realize fault protection such as over-current and over-voltage.
162IN+The non-inverting input terminal of error amplifier 2. This terminal is the protection threshold voltage (current) setting terminal, which is used to realize fault protection such as overcurrent and overvoltage.


KA7500B CAD Model

The followings are the Symbol, Footprint, 3D Model of KA7500B.

symbol.png

Symbol

footprint.png

Footprint

3D Model.jpg

3D Model


KA7500B Features

• Internal Regulator Provides a Stable 5V Reference Supply Trimmed to 5%

• Uncommitted Output TR for 200mA Sink or Source Current

• Output Control For Push-Pull or Single Ended Operation

• Variable Duty Cycle By Dead Time Control Complete PWM Control Circuit

• On-Chip Oscillator With Master or Slave Operation

• Internal Circuit Prohibits Double Pulse at Either Output


Specifications

ON Semiconductor KA7500B technical specifications, attributes, parameters and parts with similar specifications to ON Semiconductor KA7500B.
  • Type
    Parameter
  • Lifecycle Status

    Lifecycle Status refers to the current stage of an electronic component in its product life cycle, indicating whether it is active, obsolete, or transitioning between these states. An active status means the component is in production and available for purchase. An obsolete status indicates that the component is no longer being manufactured or supported, and manufacturers typically provide a limited time frame for support. Understanding the lifecycle status is crucial for design engineers to ensure continuity and reliability in their projects.

    ACTIVE, NOT REC (Last Updated: 2 days ago)
  • Factory Lead Time
    19 Weeks
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    Through Hole
  • Mounting Type

    The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.

    Through Hole
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    16-DIP (0.300, 7.62mm)
  • Number of Pins
    16
  • Weight
    1.627826g
  • Voltage - Input (Nom)
    20V
  • Operating Temperature

    The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.

    0°C~70°C TA
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube
  • Published
    2002
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e3
  • Pbfree Code

    The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.

    yes
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Not For New Designs
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Number of Terminations
    16
  • ECCN Code

    An ECCN (Export Control Classification Number) is an alphanumeric code used by the U.S. Bureau of Industry and Security to identify and categorize electronic components and other dual-use items that may require an export license based on their technical characteristics and potential for military use.

    EAR99
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Tin (Sn)
  • Voltage - Supply

    Voltage - Supply refers to the range of voltage levels that an electronic component or circuit is designed to operate with. It indicates the minimum and maximum supply voltage that can be applied for the device to function properly. Providing supply voltages outside this range can lead to malfunction, damage, or reduced performance. This parameter is critical for ensuring compatibility between different components in a circuit.

    7V~42V
  • Terminal Position

    In electronic components, the term "Terminal Position" refers to the physical location of the connection points on the component where external electrical connections can be made. These connection points, known as terminals, are typically used to attach wires, leads, or other components to the main body of the electronic component. The terminal position is important for ensuring proper connectivity and functionality of the component within a circuit. It is often specified in technical datasheets or component specifications to help designers and engineers understand how to properly integrate the component into their circuit designs.

    DUAL
  • Terminal Pitch

    The center distance from one pole to the next.

    2.54mm
  • Base Part Number

    The "Base Part Number" (BPN) in electronic components serves a similar purpose to the "Base Product Number." It refers to the primary identifier for a component that captures the essential characteristics shared by a group of similar components. The BPN provides a fundamental way to reference a family or series of components without specifying all the variations and specific details.

    KA7500
  • Function

    The parameter "Function" in electronic components refers to the specific role or purpose that the component serves within an electronic circuit. It defines how the component interacts with other elements, influences the flow of electrical signals, and contributes to the overall behavior of the system. Functions can include amplification, signal processing, switching, filtering, and energy storage, among others. Understanding the function of each component is essential for designing effective and efficient electronic systems.

    Step-Down
  • Number of Outputs
    1
  • Output Type

    The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.

    Transistor Driver
  • Operating Supply Voltage

    The voltage level by which an electrical system is designated and to which certain operating characteristics of the system are related.

    42V
  • Analog IC - Other Type

    Analog IC - Other Type is a parameter used to categorize electronic components that are integrated circuits (ICs) designed for analog signal processing but do not fall into more specific subcategories such as amplifiers, comparators, or voltage regulators. These ICs may include specialized analog functions such as analog-to-digital converters (ADCs), digital-to-analog converters (DACs), voltage references, or signal conditioning circuits. They are typically used in various applications where precise analog signal processing is required, such as in audio equipment, instrumentation, communication systems, and industrial control systems. Manufacturers provide detailed specifications for these components to help engineers select the most suitable IC for their specific design requirements.

    SWITCHING CONTROLLER
  • Output Configuration

    Output Configuration in electronic components refers to the arrangement or setup of the output pins or terminals of a device. It defines how the output signals are structured and how they interact with external circuits or devices. The output configuration can determine the functionality and compatibility of the component in a circuit design. Common types of output configurations include single-ended, differential, open-drain, and push-pull configurations, each serving different purposes and applications in electronic systems. Understanding the output configuration of a component is crucial for proper integration and operation within a circuit.

    Positive
  • Current - Output

    Current - Output is a parameter in electronic components that refers to the maximum amount of current that can be delivered by the output of the component. It is a crucial specification as it determines the capability of the component to supply power to connected devices or circuits. The current output rating is typically specified in amperes (A) and is important for ensuring that the component can safely and effectively power the load it is connected to without overheating or failing. Designers and engineers must consider the current output rating when selecting components to ensure compatibility and reliable operation of the overall system.

    250mA
  • Control Features

    Control features in electronic components refer to specific functionalities or characteristics that allow users to manage and regulate the operation of the component. These features are designed to provide users with control over various aspects of the component's performance, such as adjusting settings, monitoring parameters, or enabling specific modes of operation. Control features can include options for input/output configurations, power management, communication protocols, and other settings that help users customize and optimize the component's behavior according to their requirements. Overall, control features play a crucial role in enhancing the flexibility, usability, and performance of electronic components in various applications.

    Dead Time Control
  • Input Voltage (Min)

    Input Voltage (Min) is a parameter in electronic components that specifies the minimum voltage level required for the component to operate properly. It indicates the lowest voltage that can be safely applied to the component without causing damage or malfunction. This parameter is crucial for ensuring the reliable and safe operation of the component within its specified operating range. It is important for designers and engineers to consider the minimum input voltage requirement when selecting and using electronic components in their circuits to prevent potential issues such as underperformance or failure.

    7V
  • Topology

    In the context of electronic components, "topology" refers to the arrangement or configuration of the components within a circuit or system. It defines how the components are connected to each other and how signals flow between them. The choice of topology can significantly impact the performance, efficiency, and functionality of the electronic system. Common topologies include series, parallel, star, mesh, and hybrid configurations, each with its own advantages and limitations. Designers carefully select the appropriate topology based on the specific requirements of the circuit to achieve the desired performance and functionality.

    Buck
  • Control Mode

    In electronic components, "Control Mode" refers to the method or mode of operation used to regulate or control the behavior of the component. This parameter determines how the component responds to input signals or commands to achieve the desired output. The control mode can vary depending on the specific component and its intended function, such as voltage regulation, current limiting, or frequency modulation. Understanding the control mode of an electronic component is crucial for proper integration and operation within a circuit or system.

    VOLTAGE-MODE
  • Frequency - Switching

    "Frequency - Switching" in electronic components refers to the rate at which a device, such as a transistor or switching regulator, turns on and off during operation. This parameter is crucial in determining the efficiency and performance of power converters, oscillators, and other circuits that rely on rapid switching. Higher switching frequencies typically allow for smaller component sizes but may require more advanced design considerations to manage heat and electromagnetic interference.

    1kHz~300kHz
  • Input Voltage (Max)

    Input Voltage (Max) refers to the maximum voltage that an electronic component can safely handle without getting damaged. This parameter is crucial for ensuring the proper functioning and longevity of the component. Exceeding the maximum input voltage can lead to overheating, electrical breakdown, or even permanent damage to the component. It is important to carefully consider and adhere to the specified maximum input voltage when designing or using electronic circuits to prevent any potential issues or failures.

    40V
  • Control Technique

    In electronic components, "Control Technique" refers to the method or approach used to regulate and manage the operation of the component. This parameter is crucial in determining how the component functions within a circuit or system. Different control techniques can include analog control, digital control, pulse-width modulation (PWM), and various feedback mechanisms. The choice of control technique can impact the performance, efficiency, and overall functionality of the electronic component. It is important to select the appropriate control technique based on the specific requirements and characteristics of the application in which the component will be used.

    PULSE WIDTH MODULATION
  • Synchronous Rectifier

    Synchronous rectification is a technique for improving the efficiency of rectification by replacing diodes with actively controlled switches, usually power MOSFETs or power bipolar junction transistors (BJT).

    Yes
  • Switcher Configuration

    Switcher Configuration in electronic components refers to the arrangement or setup of a switcher circuit, which is a type of power supply that converts one form of electrical energy into another. The configuration of a switcher circuit includes the specific components used, such as transistors, diodes, capacitors, and inductors, as well as their interconnections and control mechanisms. The switcher configuration determines the efficiency, voltage regulation, and other performance characteristics of the power supply. Different switcher configurations, such as buck, boost, buck-boost, and flyback, are used for various applications depending on the desired output voltage and current requirements. Understanding and selecting the appropriate switcher configuration is crucial in designing reliable and efficient power supply systems for electronic devices.

    SINGLE
  • Max Frequency

    Max Frequency refers to the highest frequency at which an electronic component can operate effectively without degradation of performance. It is a critical parameter for devices such as transistors, capacitors, and oscillators, indicating their limitations in speed and response time. Exceeding the max frequency can lead to issues like signal distortion, heat generation, and potential failure of the component. Understanding this parameter is essential for designing circuits to ensure reliable and efficient operation.

    300kHz
  • Duty Cycle (Max)

    The "Duty Cycle (Max)" parameter in electronic components refers to the maximum percentage of time that a signal is active or on within a specific period. It is commonly used in components such as pulse-width modulation (PWM) controllers, oscillators, and timers. A duty cycle of 100% means the signal is always on, while a duty cycle of 0% means the signal is always off. Understanding the maximum duty cycle is important for ensuring proper operation and performance of the electronic component within its specified limits. It is typically expressed as a percentage and helps determine the amount of power or energy being delivered by the signal.

    45%
  • Clock Sync

    Clock synchronization is a topic in computer science and engineering that aims to coordinate otherwise independent clocks. Even when initially set accurately, real clocks will differ after some amount of time due to clock drift, caused by clocks counting time at slightly different rates.

    No
  • Height Seated (Max)

    Height Seated (Max) is a parameter in electronic components that refers to the maximum allowable height of the component when it is properly seated or installed on a circuit board or within an enclosure. This specification is crucial for ensuring proper fit and alignment within the overall system design. Exceeding the maximum seated height can lead to mechanical interference, electrical shorts, or other issues that may impact the performance and reliability of the electronic device. Manufacturers provide this information to help designers and engineers select components that will fit within the designated space and function correctly in the intended application.

    5.08mm
  • Width
    7.62mm
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    ROHS3 Compliant
0 Similar Products Remaining

Parts with Similar Specs

The three parts on the right have similar specifications to ON Semiconductor & KA7500B.

KA7500B Internal Block Diagram

The following figure shows the Internal Block Diagram of KA7500B.

Internal Block Diagram.png

Internal Block Diagram


KA7500B Typical Application

The following figure is the KA7500B Typical Application.

Typical Application.png

Typical Application


KA7500B Alternatives

Part NumberDescriptionManufacturer
LM78S40CJPOWER CIRCUITS1.5A SWITCHING REGULATOR, 100kHz SWITCHING FREQ-MAX, CDIP16, CERAMIC, DIP-16Texas Instruments
CS5150HGDR16POWER CIRCUITSSwitching Controller, Voltage-mode, 1.5A, PDSO16, 0.150 INCH, SO-16Cherry Semiconductor Corporation
SG2526JPOWER CIRCUITSSwitching Controller, Voltage-mode, 0.2A, 350kHz Switching Freq-Max, BIPolar, CDIP16, HERMETIC SEALED, CERAMIC, DIP-16Microsemi Corporation
SG1526JPOWER CIRCUITSSwitching Controller, Voltage-mode, 0.2A, 400kHz Switching Freq-Max, CDIP18, CERAMIC, DIP-18Motorola Semiconductor Products
CS-5151D16POWER CIRCUITSSwitching Controller, Voltage-mode, 1.5A, 1000kHz Switching Freq-Max, BIPolar, PDSO16,Cherry Semiconductor Corporation
TL494CNPOWER CIRCUITS0.5A SWITCHING CONTROLLER, 200kHz SWITCHING FREQ-MAX, PDIP16, 648-08Motorola Mobility LLC
UPC494C-APOWER CIRCUITSSwitching Controller, 0.25A, 300kHz Switching Freq-Max, BIPolar, PDIP16, 0.300 INCH, PLASTIC, DIP-16NEC Electronics America Inc
CS5157GD16POWER CIRCUITSCPU 5-Bit Synchronous Buck Controller, SOIC 16 LEAD, 48-TUBEonsemi
5962-8876101EAPOWER CIRCUITSIC 1.5 A SWITCHING REGULATOR, CDIP16, CERAMIC, DIP-16, Switching Regulator or ControllerDefense Supply Center Columbus
L6910GPOWER CIRCUITSAdjustable step down controller with synchronous rectificationSTMicroelectronics


KA7500B Applications

• 5V Reference Source

• Sawtooth Oscillator

• Operational Amplifier

• Comparators

• Pulse Trigger

• Quiet Time Comparator


KA7500B Package

The following figure shows you the Package of KA7500B.

Package.png

Package


KA7500B Manufacturer

ON Semiconductor is a manufacturer dedicated to reducing energy use. It has a comprehensive combination of power, signal management and logic, energy-saving customized solutions. As a world-class high-reliability supply chain, it has a network of manufacturing facilities, sales, offices and design centers in major markets in North America, Europe and the Asia-Pacific region.


Trend Analysis

Datasheet PDF

Download datasheets and manufacturer documentation for ON Semiconductor KA7500B.
Frequently Asked Questions

1.Is it normal that the input voltage of the KA7500B chip is only 6 volts?

The pin definition and function of KA7500B are the same as TL494, PWM controller, mostly used for switching power supply of half-bridge structure. To determine whether it is normal, first explain which pin is being tested. If it is a power supply pin, 6v cannot start the chip.

2.What model is used to replace the KA7500B manifold?

The same as TL494.

3.Can the original EST7502B of computer switching power supply control be replaced with KA7500B?

There may be a problem with the main control chip of the switching power supply. This chip is rarely used in the power supply. It is not clear whether it can be replaced with the KA7500B, but it is obvious that your power supply is malfunctioning.

4. What is the KA7500B used for?

PWM switching regulator.

5. What is the switching frequency of the KA7500B?

1kHz to 300kHz.
KA7500B

ON Semiconductor

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe

Related Parts More