web counter

JRC4558 Dual Operational Amplifier: Equivalent, Datasheet and Pinout

UTMEL

Published: 15 October 2021 | Last Updated: 15 October 2021

34198

JRC4558

JRC4558

Gcore

JRC4558 datasheet pdf and Unclassified product details from Gcore stock available at Utmel

Purchase Guide

The JRC4558 is a high-performance monolithic dual operational amplifier. This article enforces pinout, datasheet, equivalent, circuit diagram, and other details about JRC4558 op-amp. Furthermore, there is a huge range of semiconductors, capacitors, resistors, and Ics in stock. Welcome your RFQ!

This preamp uses IC JRC 4558. This preamp consists of a non-inverting buffer and amplifier circuit. So the incoming input signal is stabilized using a buffer circuit and then amplified by a non-inverting amplifier circuit.

The Best Preamplifier JRC4558

JRC4558 Pinout

JRC4558 pinout.jpg

JRC4558 Pinout

Pin   NumberPin NameDescription
1OUT (A)The output pin of the   Op-amp A
2Inverting Input (A)The Inverting input   pin of the Op-Amp A
3Non- Inverting Input   (A)The Non - Inverting   Input Pin of Amplifier A
4Power (-Vs)Negative supply   terminal
5ReferenceThe Non - Inverting   Input Pin of Amplifier B
6OutputThe Inverting input   pin of the Op-Amp B
7Power (+Vs)The output pin of the   Op-amp B
8'+V SPositive supply   terminal


Overview of JRC4558

The JRC4558 is a monolithic dual operational amplifier with exceptional performance. Internally adjusted and built on a single silicon chip, the JRC4558 It's ideal for pedal circuit designs because of its high voltage gain (100 dB typ. ), good input impedance (5 M typ. ), and adaptable power supply (4 to 18 Volts).


JRC4558 CAD Model

Symbol

JRC4558 symbol.jpg

JRC4558 Symbol

Footprint

JRC4558 footprint.jpg

JRC4558 Footprint


JRC4558 Features

  • No frequency compensation required

  • No latch-up

  • Large common mode and differential voltage range

  • Parameter tracking over the temperature range

  • Gain and phase match between amplifiers

  • Internally frequency compensated

  • Low noise input transistors

  • Pinto pin-compatible with MC1458/LM358


JRC4558 Block Diagram

JRC4558 block diagram.jpg

JRC4558 Block Diagram

Specifications

Gcore JRC4558 technical specifications, attributes, parameters and parts with similar specifications to Gcore JRC4558.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    DIP-8
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

JRC4558 Applications

  • Comparators

  • Function Generators

  • Instrumentation Amplifiers

  • Ground Referenced Single Amplifiers in Automobile and

  • Portable Instrumentation

  • Sample and Hold Amplifiers

  • Photocurrent Instrumentation

  • Intrusion Alarm System

  • Long Duration Timers/Multivibrators (Microseconds Minutes-Hours)


JRC4558 Alternatives

LM747,LM158, LM158A, LM358, LM358A, LM2904, LM2904Q, LM4558


Where to Use JRC4558

The JRC4558 IC is a general-purpose op-amp that can be utilized in circuits such as comparator, differential amplification, and mathematical computations. Furthermore, the device is developed specifically for applications such as transducer amplifiers and dc amplification blocks, making it easier to install in single-supply-voltage systems. These devices, for example, can be powered directly from the normal 5V supply used in digital electronics without the need for a separate -5V supply. Because the gadget has two of such op-amps on board, it may execute two separate functions at the same time, which is useful in applications. Because of its inexpensive cost and high performance, the device is popular among hobbyists and engineers.


JRC4558 Input Stage

A Long-Tailed Pair (LTP) differential amplifier with a current mirror forms the input stage. Q1, Q2, Q3, Q4, Q5, R1, R2, R3, and C1 make up this stage, which is outlined in red.

JRC4558 input stage.jpg

JRC4558 Input Stage


JRC4558 Output Stage

The Vbe Multiplier sets the bias current for the Output Stage (OPS), which is a Class AB push-pull emitter follower amplifier. Q11, Q12, R6, R7, and R8 make up this block, which is outlined in blue:

 JRC4558 output stage.jpg

JRC4558 Output Stage

The Output Stage's job is to produce enough current gain for the VAS voltage potential to exist across the low load output impedance.

The VAS efficiently drives this stage. Crossover distortion and quiescent current may be prone to significant variance due to variations in bias with temperature or amongst parts with the same type number. Because of the Vbe of the output transistors, Q11 and Q12, the JRC4558's output range is around 1.5 volts less than the supply voltage.

 JRC4558 output stage2.jpg

JRC4558 Output Stage


The output resistors R6, R7, and R8, which are inserted between output pair emitters and are also known as ballast resistors, are used to smooth out discrepancies in internal emitter resistances of transistors, allowing for better current sharing. The resistor values are typically low, which improves thermal stability, prevents complementary transistors from loading each other directly, and keeps quiescent current steady.


JRC4558 Dimension

JRC4558 dimension.jpg

JRC4558 Dimension

JRC4558 Manufacturer

GCORE provides a platform for connection, collaboration, education, and risk management for students, fieldworkers, and universities. We bring everything our members need into one place, connect peers and businesses in a new way, and maximize the impact of research by keeping researchers, journalists, and aid workers safe, effective, and efficient in the field.


Frequently Asked Questions

What is a JRC4558 IC used in?

This general-purpose dual op-amp is used to perform general-purpose op-amp operation circuits like comparator, mathematical operations, or differential amplification. The high common-mode i/p voltage range & the lack of latch-up will make these ICs perfect for the applications of voltage-follower.

What is the difference between JRC4558D, YG4558, F4558, 4558D four operational amplifiers?

F4558 is domestically produced, 4558D is imported, the internal structure and parameters are the same, but the quality is different.

Can jrc4558 and rc4558p be directly replaced?

The two 4558s are just different products, but they can be replaced.

Can jrc4558 be replaced by ne5532?

Yes, it can.
JRC4558

Gcore

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe