SS54 DIODE SCHOTTKY 5A 40V SMA[Video+FAQ]
SS54 datasheet pdf and Unclassified product details from MDD(Microdiode Electronics) stock available at Utmel









With a low voltage drop of 0.55V and a high forward current of 5A, the SS54 is a high-power surface-mount Schottky Rectifier. This article is going to talk about the features, applications, and equivalents of SS54.

How to check smd Diode with Multimeter
Overview of SS54
The SS54 is a high-power surface-mount Schottky Rectifier with a low voltage drop of 0.55V and a high forward current of 5A. This diode has high efficiency and can handle a 150A surge current. It's typically found in low-voltage, high-frequency inverters, freewheeling, and polarity protection systems. For low voltage/high-frequency inverters, freewheeling, and polarity protection applications, the SS54 Schottky Barrier Rectifier Diode is used.
SS54 Features
Metal-semiconductor junction with guarding
Epitaxial construction
Low forward voltage drop
High current capability
Plastic material has UL flammability classification 94V-0
For use in low voltage, high-frequency inverters, freewheeling, and polarity protection applications
SS54 Dimensions

SS54 Dimensions
SS54 Pinout

SS54 Pinout
Pin Descriptions
| Pin No. | Pin Name | Description |
| 1 | Anode | Current always Enters through Anode |
| 2 | Cathode | Current always Exits through Cathode |
SS54 CAD Model

SS54 Symbol

SS54 Footprint
Specifications
- TypeParameter
- Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
SMC(DO-214AB) - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tape & Reel (TR) - Voltage - Forward (Vf) (Max) @ If
The parameter "Voltage - Forward (Vf) (Max) @ If" refers to the maximum voltage drop across a diode when it is forward-biased and conducting a specified forward current (If). It indicates the maximum potential difference the diode can withstand while allowing current to flow in the forward direction without breaking down. This value is crucial for designing circuits as it helps determine how much voltage will be lost across the diode during operation. Higher Vf values can lead to reduced efficiency in power applications, making this parameter essential for optimizing circuit performance.
550mV @ 5A - Voltage - DC Reverse (Vr) (Max)
Voltage - DC Reverse (Vr) (Max) is a parameter in electronic components that specifies the maximum reverse voltage that the component can withstand without breaking down. This parameter is crucial for components like diodes and transistors that are often subjected to reverse voltage during operation. Exceeding the maximum reverse voltage can lead to the component failing or getting damaged. Designers need to consider this parameter when selecting components to ensure the reliability and longevity of their circuits.
40V - Current - Average Rectified (Io)
The parameter "Current - Average Rectified (Io)" in electronic components refers to the average value of the rectified current flowing through the component. This parameter is important in determining the average power dissipation and thermal considerations of the component. It is typically specified in datasheets for diodes, rectifiers, and other components that handle alternating current (AC) and convert it to direct current (DC). Understanding the average rectified current helps in selecting the appropriate component for a given application to ensure reliable operation and prevent overheating.
5A - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
SS54 Rating and Characteristics Curve

SS54 Maximum Ratings and Electrical Characteristics
| Characteristics | Symbol | Values | |
| Max. Recurrent Peak Reverse Voltage | Vrrm | 40 | V |
| Max. RMS Voltage | Vrms | 28 | |
| Max. DC Blocking Voltage | V DC | 40 | |
| Maximum Average Forward Rectified Current 0.375″ (9.5mm) Lead Lengths at Tl = 95°C | I (AV) | 5 | A |
| Peak Forward Surge Current A 8.3 ms Single Half Sine-wave Super Imposed on Rated Load (JEDEC Method) | Ifsm | 150 | |
| Max. Forward Voltage at 5A DC | Vf | 0.55 | V |
| Max. DC Reverse Current at Tj = 25°C Rated DC Blocking Voltage at Tj = 100°C | Ir | 1 50 | mA |
| Typical Junction Capacitance (Note 1) | Cj | 500 | pF |
| Typical Thermal Resistance (Note 2) | RθJA | 15 | °C / W |
| Operating Temperature Range | Tj | -55 to +125 | °C |
| Storage Temperature Range | Tstg | -55 to +150 |
SS54 Datasheet
SS54 Package information

SS54 Package information
Popularity by Region
What is SS54?
The SS54 is a high-power surface-mount Schottky Rectifier with a low voltage drop of 0.55V and a high forward current of 5A. This diode has high efficiency and can handle a 150A surge current. It's typically found in low-voltage, high-frequency inverters, freewheeling, and polarity protection systems.
What is a Schottky barrier rectifier diode?
The symbol for electronic devices. The Schottky diode, also known as the Schottky barrier diode or hot-carrier diode, is a semiconductor diode formed by the junction of a semiconductor and a metal. It is named after German physicist Walter H. Schottky. It has a low forward voltage drop and switches very quickly.
What is Schottky diode used for?
Schottky diodes are utilized in high-frequency applications because of their low turn-on voltage, quick recovery time, and low energy loss. Schottky diodes can correct a current because of these features, which allow for a fast change from conducting to blocking states.
What is the difference between diode and Schottky diode?
A 2V DC source is used to power both. The standard diode consumes 0.7 volts, leaving just 1.3 volts to power the load. The Schottky diode consumes only 0.3V due to its smaller forward voltage drop, allowing 1.7V to power the load. The Schottky diode would be the sole option if our load demanded 1.5V.
What’s the voltage of SS54?
40V.
Arduino Micro microcontroller:Datasheet, Features, Applications[FAQs]06 October 20233937
AT24C08D I²C-Compatible Serial EEPROM: Pinout, Features and Datasheet02 April 20221491
SST25VF040B 4-Mbit SPI Serial Flash: Pinout, Equivalent and Datasheet31 March 20221300
LM338 Regulator: Circuit, Price and Pinout31 August 20215471
INA219 Current/Power Monitor: Features, Speicifications and Applications24 May 20212873
CCS811 Digital Gas Sensors: Datasheet, Pinout and Applications27 July 20216233
MSP430 Mixed-Signal Microcontroller: MSP430 Features, Pinout and Datasheet [FAQ]13 January 20224509
How to Access the STM32G071RBT6 Datasheet from STMicroelectronics16 June 2025496
BSNPC Inverters in Photovoltaic Applications Using SiC and GaN04 January 20234424
Introduction to Optical Zoom and Digital Zoom19 June 20219161
Si vs SiC Diodes: A Performance Study of Interleaved Boost Converters for PV Applications14 March 20233154
Will AI Eventually Compete With Humans for Energy Resources?14 February 20234374
RTD Sensors: Working Principle, Features and Applications22 May 202513654
Working and Types of Touch Screen20 March 20216336
General PCB Layout Design Guidelines for RF and Digital-to-Analog Circuits20 January 202214471
What is Color Ring Inductor? How to Read Inductor Color Code?01 April 202516199
MDD(Microdiode Electronics)
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools