RS232 Connector: Pinout, Circuit and Datasheet
PUNCH UNIT-CONNECTOR 25 PIN
RS232 connector is a port used for data exchange between equipment designed for data exchange between DTE or PC and DCE or MODEM. This article will explain pinout, circuit, applications, schematics, and other details about the RS232 connector. Furthermore, there is a huge range of semiconductors, capacitors, resistors, and ICs in stock. Welcome your RFQ!

What is RS232 and What is it used for?
What is RS232?
The RS232 connector is a port that allows data to be exchanged between devices. It was created to transfer data between DTE (Data Terminal Equipment) or a computer and DCE (Data Communication Equipment) or a modem. Parallel data exchange posed constraints, which necessitated the use of RS232. RS232 is a serial communication standard that allows data to be sent bit by bit. Although speedier USB (Universal Serial Bus) eventually superseded RS232, it remains popular in some areas. RS232 used to be a 25-pin connector. However, it has since been reduced to merely 9 pins.
RS232 Pinout


RS232 Pinout
| Pin Number | Pin Name | Description |
| DATA pins (Data flow takes through these pins) | ||
| 2 | RXD | Receive Data (Data is received through this pin) |
| 3 | TXD | Transmit Data (Data is transmitted through this pin) |
| CONTROL pins (These pins are for establishing interface and to avoid data loss) | ||
| 1 | CD | Carrier Detect(Set by MODEM when the answer is received by remote MODEM ) |
| 4 | DTR | Data Terminal Ready(Set by PC to prepare MODEM to be connected to telephone circuit) |
| 6 | DSR | Data Set Ready(Set by MODEM to tell PC it is ready to receive and send data) |
| 7 | RTS | Request To Send(Set by PC to tell MODEM that MODEM can begin sending data) |
| 8 | CTS | Clear To Send(Set by MODEM to tell PC that it is ready to receive data) |
| 9 | RI | Set by MODEM to tell PC a ringing condition has been detected. |
| REFERENCE | ||
| 5 | GND | Ground (Used as reference for all pin voltage pulses) |
RS232 Specifications
Voltage Levels: RS232 is also used as ground & 5V level. Binary 0 works with voltages up to +5V to +15Vdc. It is called ‘ON’ or spacing (high voltage level) whereas Binary 1 works with voltages up to -5V to -15Vdc. It is called ‘OFF’ or marking (low voltage level).
Received signal voltage level: Binary 0 works on the received signal voltages up to +3V to +13 Vdc & Binary 1 works with voltages up to -3V to -13 Vdc.
Line Impedance: The impedance of wires is up to 3 ohms to 7 ohms & the maximum cable length is 15 meters, but the new maximum length is in terms of capacitance per unit length.
Operation Voltage: The operation voltage will be 250v AC max.
Current Rating: The current rating will be 3 Amps max.
Dielectric withstanding voltage: 1000 VAC min.
Slew Rate: The rate of change of signal levels is termed as Slew Rate. Its slew rate is up to 30 V/microsecond and the maximum bitrate will be 20 kbps.
RS232 Features
Easy to use
Stable, high speed
High-cost performance
±15-kV ESD Protection
Low power consumption
Two Drivers and Two Receivers
Female DB9 Header
Advantages of RS232
Low cost
Widely available and applicable due to its long presence in the telecommunications industry
Many manufacturers still use RS232 to connect PLCs to devices like HMIs, input and output modules, motor drives, etc.
Simple wiring and connectors will only max support for 1 driver and 1 receiver
Suitable for long-distance transmissions
Similar to microcontroller serial signals; transmit bits one at a time, at specific baud rates, with/without parity and/or stop bits
Still requires max232 to avoid voltages to destroy microcontroller serial pins
RS232 Applications
Personal Computers
Modems
Servers
Memory devices
Motor control units
Printers and Scanners
Telephone lines
Used basically where serial data transfer is required
Where to Use RS232
RS232 is a serial communication standard that is used to connect a computer and its peripheral devices so that serial data can be sent between them. It obtains the voltage for the data transmission route between the devices. It has a 1.492kbps rate and is utilized in serial communication up to 50 feet. The RS232 is used to connect Data Transmission Equipment (DTE) and Data Communication Equipment (DCE), as defined by the EIA (DCE).
How to Use RS232
We need a MAX232 IC to convert high voltage signals to TTL and vice versa because we can't connect RS232 directly to the controller. The circuit diagram for it is provided below.

RS232 Circuit
We're using a MAX232 converter chip to link the controller to a female RS232 port. In RS232, the communication voltages can be as high as +15V and as low as -15V. Because voltage levels can't be used in delicate devices, we employ MAX232 as a mediator.
The chip converts controller TTL logic pulses to RS232 voltage level pulses and back. You could permanently damage something if you don't have this chip.
Interfacing RS232 to Microcontrollers using Max232
Max 232 serves as the processor's buffer driver. It accepts 0 and 5 volts of digital logic and converts them to the RS232 standard of +10 and -10 volts. Only a few microcontrollers have built-in serial connectors that can connect directly to the PC's RS232 serial port. Many microcontrollers, on the other hand, produce a 0 to 5V output, which necessitates the use of an intermediate buffer circuit to convert the 0 to 5V to the +10 and -10V required by the RS232 connection.
The Max 232 IC has two transmitters and receivers, allowing two serial ports to be linked on the same chip. To generate the needed RS232 standard voltage from the TTL/CMOS voltage, 5 capacitors of 1microFarad each are employed. The transmitters convert TTL/CMOS voltage to RS232 voltage, while the receiver receives RS232 input and transforms it to TTL voltage.
The transmitter pins are linked to the microcontroller and the port so that the input transmitter pin receives TTL input from the microcontroller and the output transmitter pin supplies output to the RS232 port. The receiver pins are linked to the RS232 port in such a way that the input receiver pin gets RS232 standard input from the PC port and the output receiver pin supplies the Microcontroller with TTL input. The transmitter receives data from the Microcontroller and sends it to the RS232 port, while the receiver receives data from the RS232 port and sends it to the Microcontroller.
RS232 Dimensions

RS232 Dimensions
RS232 Manufacturer
After more than 140 years of development, Greenlee has become a supplier of quality tools for the woodworking industry. During these more than 70 years, Greenlee has also been a supplier of quality tools in the electrical industry. More than 20 years ago, Greenlee made a sincere promise to customers. We must use high technology to meet the ever-changing needs of our customers. We have achieved this promise through modern facilities, state-of-the-art production equipment, and enhanced quality assurance programs. The way Greenlee operates today is made up of our plans. To ensure the convenient, fast, and accurate exchange of information between Greenlee and its suppliers and customers, we continue to research and successfully expand the EDI (Electronic Data Interchange) function.
Is RS232 the same as USB?
Although RS232 and USB (universal serial bus) are both serial communication standards to connect peripherals to computers, they are different in design. There are however converter modules and cables that can be successfully used to connect RS232 devices to computers via a USB port.
What are the advantages of USB over RS232?
USB allows data to travel at an average of ten times the speed of the normal parallel port. It is also faster than a serial port. The average serial port transfer rate is 150 kbps; the USB port is up to 12 Mbps. USB 2 is forty times faster, with a maximum transfer rate of 480 Mbps.
What is RS232 used for?
RS232 is a standard protocol used for serial communication, it is used for connecting computers and their peripheral devices to allow serial data exchange between them. As it obtains the voltage for the path used for the data exchange between the devices.
How does RS232 communication work?
RS232 works on the two-way communication that exchanges data to one another. There are two devices connected, (DTE) Data Transmission Equipment& (DCE) Data Communication Equipment which has the pins like TXD, RDX, and RTS& CTS. Now, from the DTE source, the RTS generates the request to send the data.
dsPIC30F Acoustic Echo Cancellation (AEC) Library: Comprehensive Analysis29 February 2024468
ADM232LJN IC RS: Pinout, Specification, Datasheet14 August 20241469
LM2576 vs LM2596: How to differentiate?28 April 202218751
LTC6950IUHH#TRPBF Clock Generator: A Comprehensive Overview06 March 2024314
1N5822 Schottky Diode: Pinout, Datasheet, and Applications06 August 20268143
AD9516-1 14-Output Clock Generator: Features, Equivalent and Datasheet17 December 20211996
Everything You Need to Know About TL494 Current-Mode PWM Controller19 April 202212548
HMC344LC3TR-R5 RF Switch: Pinout, Feature, Datasheet14 August 2024579
What is Field Programmable Gate Array?29 September 20204419
Introduction to Servo System08 September 202115627
Lattice FPGA: The Ultimate Guide to Low-Power, Small Form Factor Solutions19 September 20257234
Introduction to Inductive Reactance16 April 202115395
Characteristics, Types, and Functions of Electrolytic Capacitors17 October 202511192
What is a variable capacitor?16 April 202568049
Exploring the Strengths and Hurdles of Wide Bandgap Devices in Alternating Current Electric Drives19 January 20243811
All You Need to Know About Rectifier Circuit24 April 202518373
Greenlee Communications
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools