TLP521-2XGB Optocoupler: TLP521 Series, Datasheet, Pinout [FAQ]
OPTOISO 5.3KV 2CH TRANS 8DIP
This post will unlock its datasheet, pinout, applications and more details about TLP521-2XGB.
TLP521-2XGB Pinout

TLP521-2XGB Pinout
TLP521-2XGB CAD Model
Symbol

TLP521-2XGB Symbol
Footprint

TLP521-2XGB Footprint
3D Model

TLP521-2XGB 3D Model
TLP521-2XGB Brief Introduction
The ISOCOM TLP521-2XGB consists of infrared light-emitting diodes and NPN silicon phototransistors in space-efficient dual-in-line plastic packages.
TLP521-2XGB Applications
Computer terminals
Industrial systems controllers
Measuring instruments
Signal transmission between systems of different potentials and impedances
Different Version of TLP521 Optocoupler
The TLP521 is a very versatile IC that can be used for many different applications, so there are many different versions of this IC available, including the TLP521-1, TLP521-2, and TLP521-3, which are 4-pin, 8-pin, and 16-pin devices that contain one, two, and four optocouplers in a single package, respectively.
TLP521-2XGB Package

TLP521-2XGB Package
TLP521-2XGB Manufacturer
Isocom Components is a leader in high-performance infrared optoelectronic devices among global manufacturers. We are focused on providing optocouplers and optoswitches. During its 25-year development, Isocom insists on delivering in excess of its customer's expectations. Therefore, we have become one of the most respected brands in the optoelectronic industry worldwide. Due to our high-quality products and superior customer service, we win the praise of our long-term customers. Isocom Components provides a natural alternative to the industry standard type of commercial optocouplers. At the same time, in order to meet the customer's specific circuit design requirements, we have carried out a unique parameter selection. Our products are in compliance with leading recognized industry standards.
Specifications
- TypeParameter
- Factory Lead Time2 Weeks
- Mounting Type
The "Mounting Type" in electronic components refers to the method used to attach or connect a component to a circuit board or other substrate, such as through-hole, surface-mount, or panel mount.
Through Hole - Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
8-DIP (0.300, 7.62mm) - Current Transfer Ratio-Min100% @ 5mA
- Number of Elements2
- Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
-30°C~100°C - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Tube - Pbfree Code
The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.
yes - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Additional Feature
Any Feature, including a modified Existing Feature, that is not an Existing Feature.
UL RECOGNIZED, VDE APPROVED - HTS Code
HTS (Harmonized Tariff Schedule) codes are product classification codes between 8-1 digits. The first six digits are an HS code, and the countries of import assign the subsequent digits to provide additional classification. U.S. HTS codes are 1 digits and are administered by the U.S. International Trade Commission.
8541.40.80.00 - Voltage - Isolation
Voltage - Isolation is a parameter in electronic components that refers to the maximum voltage that can be safely applied between two isolated points without causing electrical breakdown or leakage. It is a crucial specification for components such as transformers, optocouplers, and capacitors that require isolation to prevent electrical interference or safety hazards. The voltage isolation rating ensures that the component can withstand the specified voltage without compromising its performance or safety. It is typically measured in volts and is an important consideration when designing circuits that require isolation between different parts of the system.
5300Vrms - Output Type
The "Output Type" parameter in electronic components refers to the type of signal or data that is produced by the component as an output. This parameter specifies the nature of the output signal, such as analog or digital, and can also include details about the voltage levels, current levels, frequency, and other characteristics of the output signal. Understanding the output type of a component is crucial for ensuring compatibility with other components in a circuit or system, as well as for determining how the output signal can be utilized or processed further. In summary, the output type parameter provides essential information about the nature of the signal that is generated by the electronic component as its output.
Transistor - Number of Channels2
- Voltage - Forward (Vf) (Typ)
The parameter "Voltage - Forward (Vf) (Typ)" in electronic components refers to the typical forward voltage drop across the component when it is conducting current in the forward direction. It is a crucial characteristic of components like diodes and LEDs, indicating the minimum voltage required for the component to start conducting current. The forward voltage drop is typically specified as a typical value because it can vary slightly based on factors such as temperature and manufacturing tolerances. Designers use this parameter to ensure that the component operates within its specified voltage range and to calculate power dissipation in the component.
1.15V - Input Type
Input type in electronic components refers to the classification of the signal or data that a component can accept for processing or conversion. It indicates whether the input is analog, digital, or a specific format such as TTL or CMOS. Understanding input type is crucial for ensuring compatibility between different electronic devices and circuits, as it determines how signals are interpreted and interacted with.
DC - Rise / Fall Time (Typ)
The parameter "Rise / Fall Time (Typ)" in electronic components refers to the time it takes for a signal to transition from a specified low level to a specified high level (rise time) or from a high level to a low level (fall time). It is typically measured in nanoseconds or picoseconds and is an important characteristic in determining the speed and performance of a component, such as a transistor or integrated circuit. A shorter rise/fall time indicates faster signal switching and can impact the overall speed and efficiency of a circuit. Designers often consider this parameter when selecting components for high-speed applications to ensure proper signal integrity and timing.
4μs 3μs - Forward Current-Max
Forward Current-Max is a parameter used to specify the maximum amount of current that an electronic component, such as a diode or LED, can safely handle when it is forward-biased. This parameter is crucial for determining the operating limits of the component to prevent damage or failure due to excessive current flow. Exceeding the specified Forward Current-Max can lead to overheating, degradation of the component, or even permanent damage. It is important to carefully consider this parameter when designing circuits to ensure the component operates within its safe limits.
0.05A - Current - DC Forward (If) (Max)
The parameter "Current - DC Forward (If) (Max)" in electronic components refers to the maximum forward current that can safely pass through the component without causing damage. This parameter is typically specified in datasheets for diodes and LEDs, indicating the maximum current that can flow through the component in the forward direction. Exceeding this maximum current rating can lead to overheating and potentially permanent damage to the component. It is important to ensure that the current flowing through the component does not exceed this specified maximum to maintain proper functionality and reliability.
50mA - Current Transfer Ratio (Max)
The "Current Transfer Ratio (Max)" is a parameter used to describe the efficiency of a specific type of electronic component known as an optocoupler or optoisolator. This parameter indicates the maximum ratio of output current to input current that can be achieved under ideal conditions. In simpler terms, it quantifies how effectively the optocoupler can transfer an electrical signal from its input side to its output side. A higher Current Transfer Ratio (Max) value typically indicates better performance and stronger signal transmission capabilities for the optocoupler. It is an important specification to consider when designing circuits that require isolation between different electrical systems or components.
600% @ 5mA - Vce Saturation (Max)
Vce Saturation (Max) is a parameter commonly found in datasheets of bipolar junction transistors (BJTs) and refers to the maximum voltage drop across the collector-emitter junction when the transistor is fully saturated. When a BJT is in saturation mode, it is fully turned on and acts like a closed switch, allowing maximum current to flow through it. The Vce Saturation (Max) value indicates the maximum voltage that can be dropped across the collector-emitter junction in this state without affecting the transistor's performance. It is an important parameter to consider when designing circuits to ensure proper operation and efficiency of the transistor.
400mV - Dark Current-Max
Dark Current-Max refers to the maximum amount of current that flows through a photodetector or similar electronic component in the absence of incident light. It is an important parameter that indicates the level of noise in a sensor and is typically measured in terms of amperes or milliamperes. High dark current values can lead to decreased signal-to-noise ratio, affecting the overall sensitivity and performance of the device in low-light conditions. Understanding this parameter is crucial for applications that require precise light detection and measurement.
100nA - Coll-Emtr Bkdn Voltage-Min
Coll-Emtr Bkdn Voltage-Min refers to the minimum voltage required for the breakdown of a collector-emitter junction in bipolar transistors. It indicates the threshold at which the transistor can no longer effectively block current flow in the off state. Exceeding this voltage can lead to unwanted conduction and potential damage to the device. This parameter is essential for ensuring reliable operation in electronic circuits, especially in high-voltage applications. Manufacturers specify this value to help designers select appropriate components for their specific needs.
55V - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
ROHS3 Compliant - Lead Free
Lead Free is a term used to describe electronic components that do not contain lead as part of their composition. Lead is a toxic material that can have harmful effects on human health and the environment, so the electronics industry has been moving towards lead-free components to reduce these risks. Lead-free components are typically made using alternative materials such as silver, copper, and tin. Manufacturers must comply with regulations such as the Restriction of Hazardous Substances (RoHS) directive to ensure that their products are lead-free and environmentally friendly.
Lead Free
Datasheet PDF
- Datasheets :
What is the TLP521 series?
The TLP521 Series optocoupler has a phototransistor that is controlled by light (photon). It also has an IR (infrared) LED on the opposite side. When the IR LED is turned on, the light from the LED is collected by the transistor's receiver, which conducts.
How to use TLP521 series?
Using the TLP521 IC is fairly simple; we simply connect the device's anode pin to VCC and its cathode pin to ground.
CD4017 CMOS Counter IC: Equivalent, Price and Datasheet09 September 20217075
ESP8266EX SMD IC QFN32-pin: Features, Datasheet,Pinout, and Application08 January 20222051
ADXL345 Accelerometer: Datasheet, Pinout and Alternatives09 September 20218578
What is TDA2009A 10 +10W STEREO AMPLIFIER? [FAQ&Video]25 April 202211345
In-Depth Analysis of the Microchip PIC16F873/874/876/877 Microcontrollers29 February 2024385
2SC2240 Transistor: 2SC2240, Pinout, Equivalents05 September 20224164
OP27G OP-AMP: Application, Pinout and Datasheet07 July 20218164
LM723 Voltage Regulator: Datasheet, Schematic, Circuit23 July 20219998
Step-by-Step Guide to 2.2 k Ohm Resistor Color Code in 202520 August 20252175
Shift Registers Made Simple for New Learners15 July 20251464
7 Promising Semiconductor Stocks Amid U.S.-China Chip War18 September 20234191
What is Comparator?11 April 20226080
Optimizing Energy Exchange with Vehicle-to-Grid Technology25 April 20232873
What is Band Pass Filter?17 November 20216692
Opportunities and Challenges for 2D Materials22 March 20225053
Introduction to TTL and CMOS Logic Gate Circuits24 November 202520405
Isocom Components 2004 LTD
In Stock: 19200