web counter

How to make an Obstacle Avoiding Robot?

Published: 24 March 2023 | Last Updated: 29 August 202316199
The article will tell you How to make an Obstacle Avoiding Robot.
This video will show you the rotating obstacle avoiding robot.

ROTATING OBSTACLE AVOIDING ROBOT

Introduction

A robot that is capable of avoiding obstacles is known as an obstacle avoidance robot, and it operates autonomously. This means that when it encounters an obstacle while moving forward, it will automatically halt and take a step back. The robot then scans its surroundings to the left and right to determine the best possible route to take, either in the left direction if there is an obstacle on the right, or in the right direction if there is an obstacle on the left. To create an obstacle-avoidance robot, we will use an Arduino and an ultrasonic sensor, which will calculate the distance between the robot and any obstacles in its path. If the robot detects an obstacle, it will change its direction and continue to move.

Building obstacle avoiding robot using Ultrasonic Sensor

Prior to constructing the robot, it is crucial to comprehend the operational mechanism of the ultrasonic sensor, as it plays a vital role in detecting obstacles. The fundamental principle behind the functioning of the ultrasonic sensor involves measuring the time taken by the sensor to emit ultrasonic waves, which bounce off surfaces and are subsequently received by the sensor. Distance is then calculated by employing a formula. In this endeavor, we will be employing the HC-SR04 Ultrasonic Sensor, which is widely accessible. To use this sensor, the same methodology as explained above will be applied.

图片1.png

The Trig pin of the HC-SR04 is set to a high state for a minimum of 10 microseconds. This initiates the transmission of an ultrasonic wave consisting of eight pulses, each having a frequency of 40 kilohertz


图片2.png


The wave is then emitted and strikes a surface before being reflected back to the Echo pin of the HC-SR04, which had already been set to a high state.

图片3.png


The time elapsed between the transmission and reception of the signal is recorded and stored in a variable. Appropriate calculations are then employed to convert this time interval into distance. The necessary components for constructing this obstacle avoidance robot are readily available. Any toy chassis can be employed, or a custom-built one can be utilized

Components and Materials Required:

1. Arduino Uno

2. Smart robot car chassis with 2 x toy car wheels and 1 x Universal wheel (or ball casters)

3. HC-SR04 Ultrasonic Sensor

4. LM298N Motor Driver Module

5. Two DC motors

6. servo motor 9g

7. 7805 and 7812 IC

8. 7.4V 1300mah Lipo battery

9. Mounting bracket of Ultrasonic Sensor

10. Arduino Jumper wires

11. Screws and Nuts

As the official partner of Arduino, Utmel provides you with official original Arduino products. Welcome to shop at the Arduino product page.

Software Required:

· Arduino IDE

Hardware:

image.png

Once the circuit is ready we have to build our obstacle-avoiding car by assembling the circuit on top of a robotic chassis as shown below. 

Connections

Power Supply

To operate the circuit, the Arduino UNO, servo motor, and ultrasonic sensor necessitate a regulated DC power supply of 5V, whereas the motor driver IC requires a 12V DC supply. To fulfill this requirement, a 12V NIMH battery is employed as the primary source of power. The battery's supply is controlled to produce 5V and 12V outputs utilizing 7805 and 7812 ICs, respectively. Pin 1 of both voltage regulator ICs is connected to the battery's anode, and pin 2 of both ICs is linked to the ground. The voltage outputs are then drawn from pin 3 of their corresponding regulator ICs. Furthermore, an LED connected to a 10K Ω pull-up resistor is joined between the common ground and the output pin to indicate the continuity of the supply. Despite the use of a 12V battery, the 7812 regulator IC is employed to produce a steady and regulated supply to the motor driver IC.

Ultrasonic Sensor

The ultrasonic sensor, which is situated at the front, is linked to pins A0 and A1 on the Arduino board. The sensor consists of four pins - Ground (Pin 1), Echo (Pin 2), Trigger (Pin 3), and VCC (Pin 4). The VCC and Ground pins are connected to common VCC and Ground respectively. The Echo pin of the sensor is joined to pin A1, while the Trigger pin is linked to pin A0 of the Arduino board.

Servo Motor SG-9:

The SG-9 servo motor is utilized in the project to move the ultrasonic sensor back and forth from the front to the left side, then to the right side, and finally back to the front. The servo motor comprises three terminals: VCC, Ground, and Control, with VCC and Ground being linked to a common VCC and Ground, respectively. The Control terminal of the servo motor is connected to pin 11 of the Arduino board. To shift the servo motor within the range of 0 to 180 degrees, a pulse width modulated signal is necessary. This is why the SG-9 servo motor, which can rotate within that range, is chosen for the project.

DC Motor:

There are two DC motors used for making the robotic car. The DC motors are interfaced between pins 3 and 6 and pins 14 and 11 of the motor driver IC. 

The L293D motor driver IC has its pins 4, 5, 13, and 12 grounded, whereas pins 1, 16 and 9 are connected to 5V DC and pin 8 is connected to 12V DC. The pins 15, 2, 7, and 10 of the motor driver IC are connected to pins 5, 2, 3 and 4 of the Arduino board, respectively. The right wheel's DC motor is connected to pins 11 and 14 of the motor driver IC, while the left wheel's DC motor is connected to pins 3 and 6. The enable pins 1 and 9 of the motor driver IC are connected to pins 9 and 10 of the Arduino UNO.

Assembling the Chassis

 

图片5.png

图片6.png

图片7.png

图片8.png

Place the Arduino UNO, L298n motor driver, and servo motor on the chassis. It is essential to take note that while mounting the Arduino board, adequate space should be left to connect the USB cable, as it will be required to program the board later by linking it to the computer via USB.

If you do not understand how to build the robot on chassis you can watch YouTube videos of how to build an Arduino Chassis robot

Working

This self-governing robot operates very simply. Once the battery is attached, the robot powers on and checks for obstacles in front of it. If there are no obstacles, the robot moves forward. However, if it detects an obstacle, it stops and the servo motor rotates the ultrasonic sensor to the left (at 0 degrees) to measure the distance on the left side. Then the servo rotates the ultrasonic sensor to the right (at 180 degrees) to measure the distance on the right side. The program on the Arduino board compares the distances on the left and right sides and directs the robot to turn in the direction with the greater distance to avoid the obstacle. The robot then turns back in the opposite direction to continue moving forward.

Software

To begin, download the NewPing library file (which is a function library for the ultrasonic sensor) and paste it into the Arduino libraries folder.

Download the NewPing.rar file and extract it to the following path: C:\Arduino\libraries.

Afterward, download and open the obstacle_avoiding.ino file. Finally, connect the USB cable to the Arduino board and upload the code to the board.

图片9.png

Code

 

###

 

//Program to

 

#include <Servo.h>

 

#include <NewPing.h>      

 

Servo myservo;

 

//define the pins to be connected to ultrasonic sensor

 

#define trigPin A0

 

#define echoPin A1

 

//define the pins to be connected to ultrasonic sensor

 

#define LeftMotor1  4

 

#define LeftMotor2  5

 

#define RightMotor1 2

 

#define RightMotor2 3

 

#define maxdist 300

 

#define objdist 23

 

NewPing sonar(trigPin, echoPin, maxdist);

 

int leftDistance, rightDistance;

 

//setup function to define the pinmodes

 

void setup()

 

{

 

  pinMode(LeftMotor1,  OUTPUT);

 

  pinMode(LeftMotor2,  OUTPUT);

 

  pinMode(RightMotor1, OUTPUT);

 

  pinMode(RightMotor2, OUTPUT);

 

 

  pinMode(trigPin, OUTPUT);

 

  pinMode(echoPin, INPUT);

 

  myservo.attach(11);   

 

  myservo.write(90);

 

 

  delay(1000);

 

}

 

//Loop infinite function

 

void loop()

 

{

 

   int read_dist;

 

  //Make servo to turn 90 degree

 

   myservo.write(90);

 

  

 

   delay(90);

 

   //calling read sensor function to read the sensor data

 

   read_dist = readsensors();

 

   //checking the distance that is measured with the predefined value

 

    if(read_dist < objdist)

 

   {

 

    //if low calling the decide path function

 

    decide_path();

 

   }

 

   //calling the move forward function to move the robot forward

 

   moveforward();

 

 

   delay(500);

 

}

 

//Function to read the sensor value

 

int readsensors()

 

{

 

  int distance;

 

 

  delay(70);   

 

  //using the newping.h library function to measure the distance

 

  unsigned int uS = sonar.ping();

 

  distance = uS/US_ROUNDTRIP_CM;

 

  return distance;

 

}

 

void decide_path()

 

{

 

  robostop();

 

  //rotating the servo to 3 degree to right side

 

  myservo.write(3);  

 

  delay(500);

 

  //calling read sensor function to measure the distance on right side

 

  rightDistance = readsensors();

 

  delay(500);

 

  myservo.write(180);  

 

  delay(700);

 

  leftDistance = readsensors();

 

  delay(500);

 

  myservo.write(90);

 

  delay(100);

 

  check_distance();

 

}

 

//function to compare the distances

 

void check_distance()

 

{

 

  //checking whether left measured distance is lesser that right

 

  if (leftDistance < rightDistance)

 

  {

 

    turnright();

 

  }

 

  //checking whether left measured distance is greater that right

 

  else if (leftDistance > rightDistance)

 

  {

 

    turnleft();

 

  }

 

  else

 

  {

 

    turnaround();

 

  }

 

}

 

void moveforward()

 

{

 

  digitalWrite(LeftMotor1, HIGH);

 

  digitalWrite(LeftMotor2, LOW);

 

  digitalWrite(RightMotor1, HIGH);

 

  digitalWrite(RightMotor2, LOW);

 

}

 

void turnleft()

 

{

 

  digitalWrite(LeftMotor1, LOW);

 

  digitalWrite(LeftMotor2, LOW);

 

  digitalWrite(RightMotor1, HIGH);

 

  digitalWrite(RightMotor2, LOW);

 

  delay(350);

 

  moveforward();

 

}

 

void turnright()

 

{

 

  digitalWrite(LeftMotor1, HIGH);

 

  digitalWrite(LeftMotor2, LOW);

 

  digitalWrite(RightMotor1, LOW);

 

  digitalWrite(RightMotor2, LOW);

 

  delay(350);

 

  moveforward();

 

}

 

void turnaround()

 

{

 

  digitalWrite(LeftMotor1, LOW);

 

  digitalWrite(LeftMotor2, HIGH);

 

  digitalWrite(RightMotor1, HIGH);

 

  digitalWrite(RightMotor2, LOW);

 

  delay(700);

 

  moveforward();

 

}

 

void robostop()

 

{

 

  digitalWrite(LeftMotor1, LOW);

 

  digitalWrite(LeftMotor2, LOW);

 

  digitalWrite(RightMotor1, LOW);

 

  digitalWrite(RightMotor2, LOW);

 

}

 

###

 

Conclusion

The obstacle avoidance robot is an extremely beneficial creation that serves as a foundation for numerous large-scale projects. It is utilized in various applications such as automated cars, robots deployed in manufacturing facilities, and even in spacecraft.

UTMEL

We are the professional distributor of electronic components, providing a large variety of products to save you a lot of time, effort, and cost with our efficient self-customized service. careful order preparation fast delivery service

Related Articles

Subscribe to Utmel !

Featured Parts More