2CR5 Lithium battery[FAQ+Video]: Equivalents, Datasheet, and 2CR5 vs CR123A
BATTERY LITHIUM 6V 2CR5
The lithium 2CR5 battery is a very popular 6V non-rechargeable lithium battery. This passage provides you with a basic overview of the 2CR5, including its descriptions, applications and specifications, equivalent products, etc., to help you quickly understand what 2CR5 is.

PROJECT: Make 2CR5 Batteries Rechargeable on the cheapest way!
2CR5 Description
Lithium 2CR5 battery is a very popular 6V rechargeable lithium battery commonly used not only in cameras and other photo equipment, but also in some flashlights, security systems, toys, and similar. The 2CR5 Lithium Photo Battery is a high-voltage battery specifically designed for today's 35mm, APS, and digital cameras. These impressive cells deliver superior performance, producing up to 6 Volts of power and holding a charge of 1400 mAh. The battery's Lithium/Manganese Dioxide chemistry (Li/MnO2) allows it to function in extreme temperatures and gives it extensive 10-year-long shelf life, so your camera will always be at full power. Best of all, they deliver a quicker recovery time between flashes, letting you snap more photos in a shorter span of time.
2CR5 Features
Energizer 2CR5 Lithium Photo Batteries, deliver long-lasting performance for your camera, shot after shot
Compatible with today’s high-tech, power-hungry devices: perfect for film and digital cameras
Type: Lithium; Volt: 6
Replacement for: DL245, KL2CR5
Powerful: Energizer Photo Batteries are built to meet the requirements of today’s high-powered devices
Specifications
- TypeParameter
- Weight38g
- Voltage Rated
RATED voltage is the voltage on the nameplate - the "design point" for maximum power throughput and safe thermal operation.
6V - Size / Dimension
In electronic components, the parameter "Size / Dimension" refers to the physical dimensions of the component, such as its length, width, and height. These dimensions are crucial for determining how the component will fit into a circuit or system, as well as for ensuring compatibility with other components and the overall design requirements. The size of a component can also impact its performance characteristics, thermal properties, and overall functionality within a given application. Engineers and designers must carefully consider the size and dimensions of electronic components to ensure proper integration and functionality within their designs.
1.34Lx0.67W x 1.77 H 34.0mmx17.0mmx45.0mm - Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Obsolete - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
Not Applicable - Termination
Termination in electronic components refers to the practice of matching the impedance of a circuit to prevent signal reflections and ensure maximum power transfer. It involves the use of resistors or other components at the end of transmission lines or connections. Proper termination is crucial in high-frequency applications to maintain signal integrity and reduce noise.
Flat - Termination Style
"Termination style" in electronic components refers to the method used to connect the component to a circuit board or other electronic devices. It determines how the component's leads or terminals are designed for soldering or mounting onto the circuit board. Common termination styles include through-hole, surface mount, and wire lead terminations.Through-hole components have leads that are inserted through holes in the circuit board and soldered on the other side. Surface mount components have flat terminals that are soldered directly onto the surface of the circuit board. Wire lead terminations involve attaching wires to the component for connection.The choice of termination style depends on factors such as the type of component, the manufacturing process, and the space available on the circuit board. Different termination styles offer various advantages in terms of ease of assembly, reliability, and space efficiency in electronic designs.
Flat Top (Side Contacts) - Battery Chemistry
A battery is a device that stores chemical energy, and converts it to electricity. This is known as electrochemistry and the system that underpins a battery is called an electrochemical cell. A battery can be made up of one or several (like in Volta's original pile) electrochemical cells.
Lithium Manganese Dioxide - Battery Cell Size
The most common lithium-ion cell is the 18650 (the numbers define the physical dimensions and shape as follows: 18mm in diameter, 65mm long and the 0 means it has a round cross-section) which is due to its widespread use in laptop battery packs.
2CR5 - Capacity
In electronic components, "Capacity" typically refers to the maximum amount of electrical charge that a component can store. It is measured in units called farads (F). Capacitors are the most common components that have a capacity rating. The capacity of a capacitor determines how much energy it can store and release when connected in a circuit. Higher capacity capacitors can store more charge and are often used in applications requiring larger energy storage or filtering capabilities. It is important to select a capacitor with the appropriate capacity to ensure proper functioning of the circuit.
1.4Ah - Discharge Rate
The "Discharge Rate" in electronic components refers to the rate at which a component can release stored energy or power. This parameter is particularly important in devices that use batteries or capacitors, as it determines how quickly these components can discharge their stored energy. A high discharge rate means that the component can release energy quickly, while a low discharge rate indicates a slower release of energy. Understanding the discharge rate of electronic components is crucial for designing circuits and systems that require specific power delivery characteristics.
10mA - Height44.958mm
- Length34.036mm
- Width17.018mm
- RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
Non-RoHS Compliant
2CR5 Applications
All these features make the LITHIUM 2CR5 battery the right choice for e.g. cameras and smoke detectors and security equipment. In the LITHIUM 2CR5, there are 2 parallel cells with each 3V that together make up 6V, which makes them especially adequate for cameras.
2CR5 Manufacturer
Fujitsu Limited (富士通株式会社, Fujitsū Kabushiki-Kaisha) is a Japanese multinational information and communications technology equipment and services corporation, established in 1935 and headquartered in Tokyo. Fujitsu is the world's sixth-largest IT services provider by annual revenue, and the largest in Japan, in 2021. The hardware offerings from Fujitsu are mainly personal and enterprise computing products, including x86, SPARC, and mainframe compatible server products, although the corporation and its subsidiaries also offer a diversity of products and services in the areas of data storage, telecommunications, advanced microelectronics, and air conditioning. It has approximately 126,400 employees and its products and services are available in approximately 180 countries.
2CR5 Equivalents
DL245, KL2CR5, 5032LC and EL2CR5 are equivalents to 2CR5.
2CR5 Dimensions

2CR5 Battery vs CR123A Battery

The CR123A battery is a non-rechargeable 3V lithium battery with physical dimensions of 34.5 x 17 mm (H x D). The average CR123A battery has a 1500 mAh capacity, a nominal voltage of 3.0 volts, and a cutoff voltage of 2.0 volts.
Because the dimensions of a 2CR5 battery are somewhat larger than two CR123A cells stacked side by side, certain gadgets have a specific battery holder that allows the user to power the device with either one 2CR5 battery or two CR123A batteries.
Because the CR123A battery is also available as a rechargeable CR123A battery (also known as RCR123A battery), two RCR123A batteries might theoretically be used to power devices that need 2CR5 batteries.
In real life, two RCR123A batteries feature a nominal voltage of 7.2 - 7.4 volts and this voltage difference between 2CR5 and two RCR123A batteries of 1.2 - 1.4 volts can damage or even destroy some sensitive devices.
Trend Analysis
Datasheet PDF
- Datasheets :
Parts with Similar Specs
What is a 2CR5 battery used for?
The 2CR5 245 Lithium battery is a powerful battery that allows for the high-functioning needs of today's cameras. Offering a stable voltage and long shelf life, it is perfect to power your medical instruments, flashlights, night vision devices, and electronic locks.
How long do 2CR5 batteries last?
The lithium 2CR5 battery lasts for up to 40 hours of camera use.
What’s 2CR5 Dimensions?
Length - 1.77" (45.0 mm)/Width - 1.34" (34.0 mm)/Height - 0.67" (17.0 mm)
What’s 2CR5 Operating Temperature?
-4°F to 140°F (-20°C to 60°C)
What is a CR2 battery?
The CR2 battery is a lithium cell classified by its 27mm x 15.6mm dimensions. They're typically used in older film cameras, shutter remotes, compact flashlights, and other small devices. Most CR2 cells are primary single-use and are not rechargeable.
BCM857BS Transistor: SOT363 Package, BCM857BS Datasheet, Pinout21 February 20223788
BC327 PNP Transistor: Equivalents, Uses, and Pinout12 August 202114622
LM337 Voltage Regulator: Pinout, Feature and Datasheet23 October 202114073
1N5408 Power Diode : Pinout, Price, Datasheet27 July 202110227
74HC86 Exculsive or Gates : Pinout, Application and Datasheet13 July 20216728
DA221TL Diode: Datasheet, Pinout, Inner Circuit22 September 2021623
PC817 optocoupler: Datasheet, Circuit and Equivalents29 December 202238333
TCRT5000 IR Sensor: Datasheet, Pinout and Circuit19 October 202139315
Samsung: 3nm Yield Rate of 20%19 April 20225515
What is an Electromagnetic Relay?13 October 202012216
What is Smoke Detector?26 October 20213877
What is a Synchronous Motor?16 March 20217213
Top Chinese Photoresist Manufacturers Guide07 January 202210357
Buffer Amplifier Guide: How It Works, Key Specifications, Applications and Selection16 June 2026800
Semiconductor R&D Spending: Top 12 Countries20 September 20233852
Introduction to MD8002A Audio Amplifier27 March 20259528
FDK America, Inc., a member of Fujitsu Group
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools