web counter

A733 PNP Tip Power Transistor: 60V 100mA, TO-92 Plastic A733 Equivalent and Pinout

UTMEL

Published: 18 January 2022 | Last Updated: 18 January 2022

13258

A733

A733

Changjiang Electronics Tech (CJ)

A733 datasheet pdf and Unclassified product details from Changjiang Electronics Tech (CJ) stock available at Utmel

Purchase Guide

A733 is a widely used TO-92 size BJT transistor designed to use for amplification and switching purposes. This article is going to explain pinout, equivalents, applications, and other details about the A733 transistor.

In this video I make a simple short circuit protection circuit using c945 & A733 transistor.

12V short circuit protection circuit homemade using c945 & A733 transistor

What is A733?

The A733 is a TO-92 size BJT transistor that can be used for both amplification and switching. It's found in a wide range of commercial products, educational devices, and toys, among other things. It's also utilized in instructional electronic circuits and projects made by students.

The transistor can drive a load with a voltage of -50V and a current of 150mA. The transistor's highest emitter-base voltage is 5V, and its minimum saturation voltage is merely 0.3V. It's perfect for use as an amplifier in a variety of applications due to its maximum collector dissipation of 250mW and DC gain of up to 600.


A733 Pinout

a733 pinout.jpg

A733 Pinout

Pin NoPin Name
1Emitter
2Collector
3Base


Specifications

Changjiang Electronics Tech (CJ) A733 technical specifications, attributes, parameters and parts with similar specifications to Changjiang Electronics Tech (CJ) A733.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    SOT-23(SOT-23-3)
  • Current-Collector (Ic) (Max)
    150mA
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tape & Reel (TR)
  • Power - Max

    Power - Max is a parameter that specifies the maximum amount of power that an electronic component can handle without being damaged. It is typically measured in watts and indicates the upper limit of power that can be safely supplied to the component. Exceeding the maximum power rating can lead to overheating, malfunction, or permanent damage to the component. It is important to consider the power-max rating when designing circuits or systems to ensure proper operation and longevity of the electronic components.

    200mW
  • Transistor Type

    Transistor type refers to the classification of transistors based on their operation and construction. The two primary types are bipolar junction transistors (BJTs) and field-effect transistors (FETs). BJTs use current to control the flow of current, while FETs utilize voltage to control current flow. Each type has its own subtypes, such as NPN and PNP for BJTs, and MOSFETs and JFETs for FETs, impacting their applications and characteristics in electronic circuits.

    PNP
  • Voltage - Collector Emitter Breakdown (Max)

    Voltage - Collector Emitter Breakdown (Max) is a parameter that specifies the maximum voltage that can be applied between the collector and emitter terminals of a transistor or other semiconductor device before it breaks down and allows excessive current to flow. This parameter is crucial for ensuring the safe and reliable operation of the component within its specified limits. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the device. Designers and engineers must carefully consider this parameter when selecting components for their circuits to prevent potential issues and ensure proper functionality.

    50V
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

A733 Features

  • Type: PNP

  • Collector-Emitter Voltage: -50 V

  • Collector-Base Voltage: -60 V

  • Emitter-Base Voltage: -5 V

  • Collector Current: -0.15 A

  • Collector Dissipation: 0.25 W

  • DC Current Gain (hfe): 90 to 600

  • Transition Frequency: 180 MHz

  • Operating and Storage Junction Temperature Range: -55 to +150 °C

  • Package: TO-92


A733 Applications

  •  Darlington Pairs  

  •  RF Circuits

  •  Audio Preamplifiers

  •  Audio Amplifier

  • Sensor Circuits

  •  Audio Amplifier Stages

  •  Signal Amplification

  • Switching Loads under 150mA 


Equivalents for A733

C945, 2N2907, 2N3906, 2SA1015, 2SA1266

Where to use A733?

This A733 transistor can be used for a variety of amplification and switching applications. When used as a switch, it can drive loads of up to 150mA.  which is sufficient to power relays, LEDs, high-power transistors, and integrated circuits, among other things. It can be utilized in low voltage circuits because it only requires a 0.3V base voltage for saturation. It can, however, be utilized in audio amplification stages as well as an amplifier to amplify a variety of signals.

How to run A733 safely?

It is recommended that you keep these items in mind when using this gadget in your circuits if you want it to last a long time. Do not drive a load that is higher than 50 volts and 150 milliamps. It is usually preferable to drive at a lower load than the maximum capacity. Always use a proper base resistor, and do not use or store this transistor between -55 and +150 degrees Celsius.

 


A733 Dimensions

A733 dimensions.jpg

A733 Dimensions

A733 Manufacturer

Changjiang Electronics has become the No. 1 and No. 3 integrated circuit packaging and testing enterprise in China. Changjiang Technologies provides packaging design, product development, and certification, as well as a full range of professional manufacturing services ranging from chip testing, packaging to finished product testing and shipping.

Frequently Asked Questions

What is the use of A733?

A733 PNP General Purpose Transistor is designed for the driver stage of the AF amplifier.2SA733 is Complimentary to C945.

What is the voltage of A733?

50V

What can I use to replace A733?

2SC945, BC177 (4a), BC204 (4), BC513 (21a), 2N2906-07(4a), 3CG120C

Can A733 and A1013 be interchangeable?

No, they are not interchangeable.
A733

Changjiang Electronics Tech (CJ)

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe