A940 PNP Transistor: 2SA940 150V 1.5A Power Transistor, TO-220 and Equivalents

UTMEL

Published: 19 January 2022 | Last Updated: 19 January 2022

7909

A940C

A940C

FeiHong

A940C datasheet pdf and Unclassified product details from FeiHong stock available at Utmel

Purchase Guide

A940 is a TO-220 packaged PNP BJT transistor. This article is going to explain pinout, features, applications, equivalents, and other details about the A940 transistor.

This video is going to show how to make 5watt audio Amplifier loud.

How to make Audio Amplifier Using Transistor A940 BC547 - Audio amplifier circuit diagram

What is A940?

2SA940 is a PNP BJT transistor in a TO-220  package. This transistor is intended for general-purpose amplification and vertical output circuits, although it is not confined to these applications and can be utilized in a wide range of other applications. It also has a fast switching capability, which makes it excellent for applications that require quick switching. It can drive a maximum load of -1.5A and a maximum load voltage of -150V when used as a switch.

A940 Pinout

a940 pinout.jpg

A940 Pinout

Specifications

FeiHong A940C technical specifications, attributes, parameters and parts with similar specifications to FeiHong A940C.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    TO-220
  • Current-Collector (Ic) (Max)
    1.5A
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube-packed
  • Power - Max

    Power - Max is a parameter that specifies the maximum amount of power that an electronic component can handle without being damaged. It is typically measured in watts and indicates the upper limit of power that can be safely supplied to the component. Exceeding the maximum power rating can lead to overheating, malfunction, or permanent damage to the component. It is important to consider the power-max rating when designing circuits or systems to ensure proper operation and longevity of the electronic components.

    25W
  • Voltage - Collector Emitter Breakdown (Max)

    Voltage - Collector Emitter Breakdown (Max) is a parameter that specifies the maximum voltage that can be applied between the collector and emitter terminals of a transistor or other semiconductor device before it breaks down and allows excessive current to flow. This parameter is crucial for ensuring the safe and reliable operation of the component within its specified limits. Exceeding the maximum breakdown voltage can lead to permanent damage or failure of the device. Designers and engineers must carefully consider this parameter when selecting components for their circuits to prevent potential issues and ensure proper functionality.

    150V
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

A940 Features

  • Type: PNP 

  • Collector-Emitter Voltage: -150 V

  • Collector-Base Voltage: -150 V

  • Emitter-Base Voltage: -5 V

  • Collector Current: -1.5 A

  • Collector Dissipation: 25 W

  • DC Current Gain (hfe): 40 to 140

  • Transition Frequency: 4 MHz

  • Operating and Storage Junction Temperature Range: -55 to +150 °C

  • Package: TO-220 


A940 Applications

  • Darlington Pair

  • Audio Amplifiers

  • Vertical Output Circuitry 

  • Switching Loads under -1.5A

  • Many general-purpose applications 


A940 Equivalents

2SC2073, 2SA1304, 2SA740, 2SA940  A, 2SB546, 2SB546A, 2SB547, 2SB630, KSA1304, KSA940, KSB546, MJE15031, MJE15031G, MJE5850, MJE5850G, MJF15031, MJF15031G

Where to use A940?

The A940 is primarily intended for use in vertical output circuitry and general-purpose audio amplification, although it is not confined to these uses and can be utilized for a wide range of other applications. It can also be used as a switch to drive a wide range of loads under -1.5A, such as high-power transistors, high-power LEDs, Relays, ICs, and circuit components. Its general-purpose audio amplification applications include audio amplifiers and high-power audio amplifier stages.

 


How to run A940 in a safe circuit?

It is recommended that you do not utilize a component to its absolute maximum ratings and instead use it 20 percent below those ratings for long-life performance. The same is true for the A940  transistor; the transistor's maximum collector current is -1.5A, therefore do not drive a load of more than 1.2A. Because the maximum collector to emitter voltage is -150V, do not drive loads higher than -120V. Use a proper heat sink with the transistor, and always store or operate it at temperatures between -55 and +150 degrees Celsius.

A940 Package Dimensions

A940 dimensions.jpg

A940 Package Dimensions

A940 Manufacturer

Toshiba is a world leader and innovator in pioneering high technology, a diversified manufacturer and marketer of advanced electronic and electrical products spanning information & communications systems; digital consumer products; electronic devices and components; power systems, including nuclear energy; industrial and social infrastructure systems; and home appliances. Toshiba was founded in 1875, and today operates a global network of more than 740 companies, with 204,000 employees worldwide and annual sales surpassing 6.3 trillion yen (US$68 billion).

Frequently Asked Questions

What is A940 used for?

A940 PNP 1.5A 150V power transistor used for general purpose power amplifier applications.

What is the voltage of A940?

150V

Can A940 be replaced with 2SC5200?

No. The A940 medium power pair tube is 25W, which is commonly used in the booster stage; the 2SC5200 high power pair tube is 150W, which is used in the power output stage.

What is the purpose of the 2SA940 transistor?

The 2SA940 is intended for general-purpose amplification and vertical output circuits.

What does 2SA940 have?

It has a fast switching capability.

What is the maximum load voltage of 2SA940 when used as a switch?

-150V
A940C

FeiHong

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe