ES110-0017 Sensor: Datasheet, Application, Features

Sophie

Published: 01 September 2021 | Last Updated: 01 September 2021

845

ES110-0017

ES110-0017

Honeywell Sensing and Productivity Solutions

Industrial Temperature Sensors AIR SENSOR

Purchase Guide

Industrial Temperature Sensors AIR SENSOR

The ES110-0017 comes from Honeywell’s ES110 Series, which is a modular range of inflow thermistor-based sensor specifically designed for use in the transportation industry.

ES110-0017

ES110-0017-1.jpg

ES110-0017

ES110-0017 Description

The ES110-0017 comes from Honeywell's ES110 Series, which is a modular range of inflow thermistor-based sensors specifically designed for use in the transportation industry.


Specifications

Honeywell Sensing and Productivity Solutions ES110-0017 technical specifications, attributes, parameters and parts with similar specifications to Honeywell Sensing and Productivity Solutions ES110-0017.
  • Type
    Parameter
  • Factory Lead Time
    14 Weeks
  • Number of Pins
    2
  • Housing Material

    The parameter "Housing Material" in electronic components refers to the material used to encase or protect the internal circuitry of the component. The housing material plays a crucial role in providing physical protection, insulation, and environmental resistance to the electronic component. Common housing materials include plastics, metals, ceramics, and composites, each offering different levels of durability, heat resistance, and electrical properties. The choice of housing material is important in determining the overall performance, reliability, and longevity of the electronic component in various operating conditions.

    Brass
  • Series

    In electronic components, the "Series" refers to a group of products that share similar characteristics, designs, or functionalities, often produced by the same manufacturer. These components within a series typically have common specifications but may vary in terms of voltage, power, or packaging to meet different application needs. The series name helps identify and differentiate between various product lines within a manufacturer's catalog.

    ES120
  • Published
    2008
  • Tolerance

    In electronic components, "tolerance" refers to the acceptable deviation or variation from the specified or ideal value of a particular parameter, such as resistance, capacitance, or voltage. It indicates the range within which the actual value of the component can fluctuate while still being considered acceptable for use in a circuit. Tolerance is typically expressed as a percentage or a specific value and is important for ensuring the accuracy and reliability of electronic devices. Components with tighter tolerances are more precise but may also be more expensive. It is crucial to consider tolerance when selecting components to ensure proper functionality and performance of the circuit.

    5%
  • Pbfree Code

    The "Pbfree Code" parameter in electronic components refers to the code or marking used to indicate that the component is lead-free. Lead (Pb) is a toxic substance that has been widely used in electronic components for many years, but due to environmental concerns, there has been a shift towards lead-free alternatives. The Pbfree Code helps manufacturers and users easily identify components that do not contain lead, ensuring compliance with regulations and promoting environmentally friendly practices. It is important to pay attention to the Pbfree Code when selecting electronic components to ensure they meet the necessary requirements for lead-free applications.

    no
  • Part Status

    Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.

    Obsolete
  • Moisture Sensitivity Level (MSL)

    Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures

    1 (Unlimited)
  • Resistance

    Resistance is a fundamental property of electronic components that measures their opposition to the flow of electric current. It is denoted by the symbol "R" and is measured in ohms (Ω). Resistance is caused by the collisions of electrons with atoms in a material, which generates heat and reduces the flow of current. Components with higher resistance will impede the flow of current more than those with lower resistance. Resistance plays a crucial role in determining the behavior and functionality of electronic circuits, such as limiting current flow, voltage division, and controlling power dissipation.

    2kOhm
  • Max Operating Temperature

    The Maximum Operating Temperature is the maximum body temperature at which the thermistor is designed to operate for extended periods of time with acceptable stability of its electrical characteristics.

    150°C
  • Min Operating Temperature

    The "Min Operating Temperature" parameter in electronic components refers to the lowest temperature at which the component is designed to operate effectively and reliably. This parameter is crucial for ensuring the proper functioning and longevity of the component, as operating below this temperature may lead to performance issues or even damage. Manufacturers specify the minimum operating temperature to provide guidance to users on the environmental conditions in which the component can safely operate. It is important to adhere to this parameter to prevent malfunctions and ensure the overall reliability of the electronic system.

    -40°C
  • Reach Compliance Code

    Reach Compliance Code refers to a designation indicating that electronic components meet the requirements set by the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation in the European Union. It signifies that the manufacturer has assessed and managed the chemical substances within the components to ensure safety and environmental protection. This code is vital for compliance with regulations aimed at minimizing risks associated with hazardous substances in electronic products.

    unknown
  • Accuracy

    Accuracy in electronic components refers to the degree to which a measured value agrees with the true or accepted value. It evaluates the precision of a component in providing correct output or measurement under specified conditions. High accuracy indicates minimal deviation from the actual value, while low accuracy shows significant error in measurement. This parameter is crucial in applications where precise data is essential for reliable performance and decision-making.

    5 %
  • Terminal Type

    Terminal type or emulation specifies how your computer and the host computer to which you are connected exchange information.

    Connector
  • Temperature Range

    The difference between the maximum and minimum temperatures or between the highest and lowest mean temperatures during a specified time interval.

    -40°C~150°C
  • Element Type

    describes a class of elements, including their properties and applicable actions.

    Thermistor
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

ES110-0017 Features

• Air/gas or immersion sensing

• NTC (Negative Temperature Coefficient) or KTY (silicon-based positive temperature coefficient) type outputs

• Enhanced sensitivity

• Enhanced accuracy

• Enhanced reliability

• Robust packaging

• Fast response

• Wide operating temperature range

• Easy installation

• Customizable


ES110-0017 Application

• Transportation: engine coolant, oil temperature, air intake, fuel and engine block sensing

• Industrial: compressor, duct, hydraulic oil temperature sensing


ES110-0017 Advantage

The ES110-0017's Robust and easy-to-install threaded packaging often provides reliable operation in harsh application environments. Fast response times over a wide operating temperature range of -40 °C to 150 °C [-40 °F to 302 °F] allow application flexibility.


ES110 vs. ES120

The ES110 Series air/gas sensor has an exposed thermistor element that offers enhanced response for greater levels of control, while the ES120 Series is primarily used for immersion temperature measurements. Its fully enclosed brass body makes it often ideal for applications requiring direct contact with liquids.


ES110-0017 Dimensions

ES110-0017 Dimensions.jpg

Dimensions

ES110-0017 Manufacturer

Honeywell International Inc. is an American publicly traded, multinational conglomerate headquartered in Charlotte, North Carolina. It primarily operates in four areas of business: aerospace, building technologies, performance materials and technologies (PMT), and safety and productivity solutions (SPS).


Datasheet PDF

Download datasheets and manufacturer documentation for Honeywell Sensing and Productivity Solutions ES110-0017.

Popularity by Region

Frequently Asked Questions

What is the ES110-0017?

The ES110-0017 comes from Honeywell’s ES110 Series, which is a modular range of inflow thermistor-based sensors specifically designed for use in the transportation industry.

Is the ES110 Series same as the ES120 Series?

No, The ES110 Series air/gas sensor has an exposed thermistor element that offers enhanced response for greater levels of control, while the ES120 Series is primarily used for immersion temperature measurements. Its fully enclosed brass body makes it often ideal for applications requiring direct contact with liquids.

What is the ES110-0017’s number of pins?

2.
ES110-0017

Honeywell Sensing and Productivity Solutions

In Stock
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
Related Parts More