Hex Inverter 74LS04: Datasheet, Specifications, and Pinout

Sophie

Published: 09 May 2022 | Last Updated: 09 May 2022

13516

74LS04N

74LS04N

RAYTHEON SEMICONDUCTOR

74LS04N datasheet pdf and Unclassified product details from RAYTHEON SEMICONDUCTOR stock available at Utmel

Purchase Guide

74LS04 Hex Inverter is a member of the 74XXYY IC series. In today's article, we'll have a detailed introduction to the 74LS04 Hex Inverter, after reading this article, you will learn what is 74LS04, what's its features, in which country it is the most popular, and what's the difference between 74HC04.

This is an introduction video about 74LS04 Inverter(NOT) Gate IC.

74LS04 Inverter(NOT) Gate IC

74LS04 Description

     74LS04 Hex Inverter is a member of the 74XXYY IC series. The 74-series are digital logic integrated circuits, It includes six independent inverse HEX gates. Each gate consists of an input and an output. The reverse-phase is one of its main functions. The 74LS04 IC has a wide range of working voltage, a wide range of working conditions, and directly interfaces with CMOS, NMOS, and TTL.


74LS04 Pinout and Configurations

pinout.jpg

Pin NumberDescription
INPUT OF INVERTING GATES
11A-INPUT of GATE 1
32A-INPUT of GATE 2
53A-INPUT of GATE 3
94A-INPUT of GATE 4
115A-INPUT of GATE 5
136A-INPUT of GATE 6
SHARED TERMINALS
7GND- Should be connected to ground
14VCC-Should be connected to a positive voltage
OUTPUT OF INVERTING GATES
21Y-OUTPUT of GATE 1
42Y-OUTPUT of GATE 2
63Y-OUTPUT of GATE 3
84Y-OUTPUT of GATE 4
105Y-OUTPUT of GATE 5
126Y-OUTPUT of GATE 6


74LS04 Features

  • Supply voltage range: +4.75V to +5.25V

  • Maximum supply voltage: +7V

  • Maximum current allowed to draw through each gate output: 8mA

  • Totally lead-free

  • TTL outputs

  • Maximum Rise Time: 15ns

  • Maximum Fall Time: 15ns

  • Operating temperature:0°C  to 70 °C


74LS04 CAD Models

Symbol

symbol.jpg

Footprint

footprint.jpg

3D

3d1.jpg

3d2.jpg

Specifications

RAYTHEON SEMICONDUCTOR 74LS04N technical specifications, attributes, parameters and parts with similar specifications to RAYTHEON SEMICONDUCTOR 74LS04N.
  • Type
    Parameter
  • JESD-609 Code

    The "JESD-609 Code" in electronic components refers to a standardized marking code that indicates the lead-free solder composition and finish of electronic components for compliance with environmental regulations.

    e0
  • Terminal Finish

    Terminal Finish refers to the surface treatment applied to the terminals or leads of electronic components to enhance their performance and longevity. It can improve solderability, corrosion resistance, and overall reliability of the connection in electronic assemblies. Common finishes include nickel, gold, and tin, each possessing distinct properties suitable for various applications. The choice of terminal finish can significantly impact the durability and effectiveness of electronic devices.

    Tin/Lead (Sn/Pb)
  • Peak Reflow Temperature (Cel)

    Peak Reflow Temperature (Cel) is a parameter that specifies the maximum temperature at which an electronic component can be exposed during the reflow soldering process. Reflow soldering is a common method used to attach electronic components to a circuit board. The Peak Reflow Temperature is crucial because it ensures that the component is not damaged or degraded during the soldering process. Exceeding the specified Peak Reflow Temperature can lead to issues such as component failure, reduced performance, or even permanent damage to the component. It is important for manufacturers and assemblers to adhere to the recommended Peak Reflow Temperature to ensure the reliability and functionality of the electronic components.

    NOT SPECIFIED
  • Time@Peak Reflow Temperature-Max (s)

    Time@Peak Reflow Temperature-Max (s) refers to the maximum duration that an electronic component can be exposed to the peak reflow temperature during the soldering process, which is crucial for ensuring reliable solder joint formation without damaging the component.

    NOT SPECIFIED
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    Non-RoHS Compliant
0 Similar Products Remaining

74LS04 Applications

There are many applications for this device. It has very important in inversion circuits. A few of its applications are explained here and discussed.

  • It is a Universal use logic instrument used in the different logic circuit.

  • It is used on different servers.

  • It is used in different storage modules to store data.

  • This module is also used in different personal computers and notebooks as a storing device.

  • It is also used in different digital reluctance circuits and instruments.

  • This module is used in different networking systems.

  • It is also used in different Digital instruments and networks.


74LS04 Circuit Diagram

circuit diagram.jpg

74LS04 Equivalents

CD7404, 74LS14, A single transistor can be configured to form a NOT gate.


74LS04 Manufacturer

Raytheon Technologies Corporation is an American multinational aerospace and defense conglomerate headquartered in Waltham, Massachusetts. It is one of the largest aerospace, intelligence services providers, and defense manufacturers in the world by revenue and market capitalization. Raytheon Technologies (RTX) researches, develops and manufactures advanced technology products in the aerospace and defense industry, including aircraft enginesavionicsaerostructurescybersecurityguided missilesair defense systemssatellites, and drones. The company is also a large military contractor, getting a significant portion of its revenue from the U.S. government.


Where to use 74LS04

Here are a few cases where 74LS04 is used.

 

1. The chip is basically used where a logic inverter is needed. Inverter Gates in this chip provides an output that is negated logic input. The chip has six gates that do NOT operate.

2. When you want TTL outputs. The gates in this chip provide TTL logic outputs which are a must in some applications.

3. 74LS04 is a low-cost chip available in the market and so it is used when application cost is low.


How to use 74LS04

As mentioned earlier 74LS04 has six INVERTING GATES which can be used individually. The internal connection of gates can be given as below.

how to use.jpg

Now let us take a single gate of the six and connect it as shown in the circuit diagram.

1.jpg

For understanding the working of NOT gate, let’s redraw it in a more simplified version.

2.jpg

As shown in the diagram, we have a transistor forming a NOT gate. Input here is 1A which is connected to the button. Output 1Y is connected to LED through a resistor. The LED is connected to know the output status.

 

In the circuit,

When the button is not pressed:

The current through the base of the transistor will be zero. Because the base current is zero the transistor will be in an OFF state. Under the OFF state, the total supply voltage appears across the transistor. Under such a case, the output 1Y here will be HIGH, since the output is nothing but voltage across the transistor. Hence when a button is not pressed INPUT 1A = LOW and OUTPUT 1Y = HIGH.

When a button is pressed:

Voltage appears at the base of the transistor and current flows through it. Because the base current is present the transistor will turn ON. Under the ON state, the total supply voltage appears across the resistor and the voltage across the transistor will be zero. Under such a case, the output 1Y here will also be LOW since the output is nothing but voltage across the transistor. Hence when a button is pressed INPUT 1A = HIGH and OUTPUT 1Y = LOW.

 

If we draw a truth table based on the above cases, we will have.

Input 1AOutput 1Y
LOWHIGH
HIGHLOW

By truth table, you can understand that OUTPUT for NOT gate is negation or inversion of INPUT. We can write the output function as, Y = A.

 

We have six of these gates in the 74LS04 chip. We can use one or all six of these gates depending on the requirement.


74LS04 Package

package.jpg

package.jpg1.jpg

74LS04 vs 74HC04

pinout.jpg74HC04 circuit.jpg

                            74LS04 Pinout                                             74HC04 Pinout   


 

74LS04 contains six independent gates each of which performs the logic INVERT function. The output signals of the six inverters are opposite to the input signals. The inverter can reverse the phase of the input signal by 180 degrees. This circuit is used in analog circuits, such as audio amplifiers, clock oscillators, etc.

74HC04 is a hex inverter of a CMOS circuit, and the working voltage is 2V-6V. Both 74LS04 and 74HC04 are inverters, but LS stands for low-power Schottky and HC is high-speed COMS. LS is slightly faster than HC. LS adopts TTL level. HC is CMOS level. 74HC04 is easy to understand. Input low level, output high level. Input high level, output low level.

Trend Analysis

Parts with Similar Specs

Frequently Asked Questions

What is a NOT gate?

A NOT gate is a digital logic gate that inverts the input digital signal.  A NOT gate always has high or logic level 1 output when its input is low or at logic level 0. On the other hand, a logical NOT gate always has low or logic level 0 output when input is high or at logic level 1.

What is the function of ic 74ls04?

74LS04 Hex NOT Gate IC. 74LS04 is a 2-input quadruple 8-bit NOT gate IC. Inverter in logic converters is an electronics device whose basic functions are to invert the incoming logic whether it is HIGH or LOW. They are also known as NOT gates.

What is 74LS04?

74LS04 is a member of the 74XXYY IC series. The 74-series are digital logic integrated circuits. 74LS04 IC has six NOT gates. These NOT gates perform Inverting function. Hence name HEX INVERTING GATES.

What is a hex inverter?

A hex inverter is a type of integrated circuit that contains six inverters. Many sophisticated digital devices use inverters, including multiplexers, decoders, and state machines.  An inverter circuit's main function is to output the voltage representing the opposite level to its input.

Why is NOT gate called an inverter?

A NOT gate often called an inverter, is a nice digital logic gate to start with because it has only a single input with simple behavior. A NOT gate performs logical negation on its input. In other words, if the input is true, then the output will be false.
74LS04N

RAYTHEON SEMICONDUCTOR

In Stock

United States

China

Canada

Japan

Russia

Germany

United Kingdom

Singapore

Italy

Hong Kong(China)

Taiwan(China)

France

Korea

Mexico

Netherlands

Malaysia

Austria

Spain

Switzerland

Poland

Thailand

Vietnam

India

United Arab Emirates

Afghanistan

Åland Islands

Albania

Algeria

American Samoa

Andorra

Angola

Anguilla

Antigua & Barbuda

Argentina

Armenia

Aruba

Australia

Azerbaijan

Bahamas

Bahrain

Bangladesh

Barbados

Belarus

Belgium

Belize

Benin

Bermuda

Bhutan

Bolivia

Bonaire, Sint Eustatius and Saba

Bosnia & Herzegovina

Botswana

Brazil

British Indian Ocean Territory

British Virgin Islands

Brunei

Bulgaria

Burkina Faso

Burundi

Cabo Verde

Cambodia

Cameroon

Cayman Islands

Central African Republic

Chad

Chile

Christmas Island

Cocos (Keeling) Islands

Colombia

Comoros

Congo

Congo (DRC)

Cook Islands

Costa Rica

Côte d’Ivoire

Croatia

Cuba

Curaçao

Cyprus

Czechia

Denmark

Djibouti

Dominica

Dominican Republic

Ecuador

Egypt

El Salvador

Equatorial Guinea

Eritrea

Estonia

Eswatini

Ethiopia

Falkland Islands

Faroe Islands

Fiji

Finland

French Guiana

French Polynesia

Gabon

Gambia

Georgia

Ghana

Gibraltar

Greece

Greenland

Grenada

Guadeloupe

Guam

Guatemala

Guernsey

Guinea

Guinea-Bissau

Guyana

Haiti

Honduras

Hungary

Iceland

Indonesia

Iran

Iraq

Ireland

Isle of Man

Israel

Jamaica

Jersey

Jordan

Kazakhstan

Kenya

Kiribati

Kosovo

Kuwait

Kyrgyzstan

Laos

Latvia

Lebanon

Lesotho

Liberia

Libya

Liechtenstein

Lithuania

Luxembourg

Macao(China)

Madagascar

Malawi

Maldives

Mali

Malta

Marshall Islands

Martinique

Mauritania

Mauritius

Mayotte

Micronesia

Moldova

Monaco

Mongolia

Montenegro

Montserrat

Morocco

Mozambique

Myanmar

Namibia

Nauru

Nepal

New Caledonia

New Zealand

Nicaragua

Niger

Nigeria

Niue

Norfolk Island

North Korea

North Macedonia

Northern Mariana Islands

Norway

Oman

Pakistan

Palau

Palestinian Authority

Panama

Papua New Guinea

Paraguay

Peru

Philippines

Pitcairn Islands

Portugal

Puerto Rico

Qatar

Réunion

Romania

Rwanda

Samoa

San Marino

São Tomé & Príncipe

Saudi Arabia

Senegal

Serbia

Seychelles

Sierra Leone

Sint Maarten

Slovakia

Slovenia

Solomon Islands

Somalia

South Africa

South Sudan

Sri Lanka

St Helena, Ascension, Tristan da Cunha

St. Barthélemy

St. Kitts & Nevis

St. Lucia

St. Martin

St. Pierre & Miquelon

St. Vincent & Grenadines

Sudan

Suriname

Svalbard & Jan Mayen

Sweden

Syria

Tajikistan

Tanzania

Timor-Leste

Togo

Tokelau

Tonga

Trinidad & Tobago

Tunisia

Turkey

Turkmenistan

Turks & Caicos Islands

Tuvalu

U.S. Outlying Islands

U.S. Virgin Islands

Uganda

Ukraine

Uruguay

Uzbekistan

Vanuatu

Vatican City

Venezuela

Wallis & Futuna

Yemen

Zambia

Zimbabwe