LMR240 Times Microwave Coax Cable 50 Ohm 0.240 Diameter: Datasheet, Features, and Application |LMR®-240
COAX ;ROHS COMPLIANT: YES
LMR240 is a coaxial cable. This article is going to introduce applications, features, and more details about LMR240.

LMR240 Making an SMA connection
Overview of LMR240
LMR®-240 coax cable from L-com is only one of a large number of radio frequency coaxial cable types specifically stocked to be ready for quick shipment. L-com Microwave LMR-240 coax cable is manufactured in a flexible design and has a 50 Ohm impedance. This low loss flexible 50 Ohm coax cable LMR-240 is constructed with a 0.24-inch diameter and Black PE jacket.
LMR-240 flexible 50 Ohm coax cable with PE jacket is rated for a 5.8 GHz maximum operating frequency. This 50 Ohm 0.24 inch diameter and low loss flexible coax cable are built with a double shield count and RF shielding of 90 dB. L-com Microwave LMR-240 coax is constructed with PE (F) dielectric and a maximum operating temperature of 85 degrees C. Times Microwave LMR-240 coax cable specs for this wire properties can be found on its RF coax cable LMR-240 datasheet.
LMR-240 cable is part of more than one million RF, microwave parts in stock at L-com. This Times Microwave low loss LMR-240 coax cable is ready to buy and can be shipped worldwide. L-com also maintains a wide selection of other radio frequency coaxial cable types that ship same-day from our warehouse as with the rest of our other RF/microwave components.
LMR240 Features
PE jacket
Max operating temperature 85 °C
Min Install Bend radius of 2.5 inches
Phase Velocity 84%
Max operating Frequency of 5.8 GHz
Specifications
- TypeParameter
- Factory Lead Time8 Weeks
- Dielectric Material
a substance that is a poor conductor of electricity, but an efficient supporter of electrostatic field s.
Foam Polyethylene (FPE) - Conductor Material
A conductor is a material which contains movable electric charges. In metallic conductors, such as copper or aluminum, the movable charged particles are electrons, though in other cases they can be ions or other positively charged species.
Copper, Bare - Jacket (Insulation) Material
The parameter "Jacket (Insulation) Material" in electronic components refers to the material used to cover and protect the internal components of a cable or wire. This material provides insulation to prevent electrical interference, short circuits, and damage from environmental factors such as moisture, heat, and chemicals. Common jacket materials include PVC (polyvinyl chloride), Teflon, rubber, and polyethylene. The choice of jacket material depends on the specific application requirements, such as temperature range, flexibility, and resistance to abrasion. Selecting the appropriate jacket material is crucial for ensuring the reliability and longevity of the electronic component in its intended operating conditions.
Polyethylene (PE) - Shield Material
Shield Material in electronic components refers to the material used to create a shield or barrier that protects the component from electromagnetic interference (EMI) or radio frequency interference (RFI). The shield material is typically a conductive material such as copper or aluminum that is capable of blocking or absorbing unwanted electromagnetic signals. By using the appropriate shield material, electronic components can maintain their performance and reliability in environments where EMI or RFI may be present. The effectiveness of the shield material is crucial in ensuring the proper functioning of electronic devices and preventing interference from external sources.
Aluminum; Copper, Tinned - Cable TypesCoaxial
- Operating Temperature
The operating temperature is the range of ambient temperature within which a power supply, or any other electrical equipment, operate in. This ranges from a minimum operating temperature, to a peak or maximum operating temperature, outside which, the power supply may fail.
-40°C~85°C - Published2009
- Part Status
Parts can have many statuses as they progress through the configuration, analysis, review, and approval stages.
Active - Moisture Sensitivity Level (MSL)
Moisture Sensitivity Level (MSL) is a standardized rating that indicates the susceptibility of electronic components, particularly semiconductors, to moisture-induced damage during storage and the soldering process, defining the allowable exposure time to ambient conditions before they require special handling or baking to prevent failures
1 (Unlimited) - Impedance
In electrical engineering, impedance is the opposition to alternating current presented by the combined effect of resistance and reactance in a circuit.
50Ohms - Jacket Color
The parameter "Jacket Color" in electronic components refers to the color of the protective outer layer that encases wires, cables, or other electronic components. This color can indicate specific attributes such as the type of insulation material, intended use, or compliance with certain standards. Different colors might be used to distinguish between various types of signals, voltage levels, or applications, providing a visual means of identifying components in a system. Additionally, the jacket color can also influence heat dissipation and aesthetic appeal in electronic assemblies.
Black - Conductor Strand
Stranded conductors are composed of uninsulated “strands” of wire twisted together. The advantages of conductor stranding over a single strand of equal cross-section are increased flexibility and flex-fatigue life.
Solid - Jacket (Insulation) Diameter
The "Jacket (Insulation) Diameter" parameter in electronic components refers to the outer diameter of the insulation or protective jacket surrounding a wire or cable. This measurement is important for determining the overall size and compatibility of the component within a system or circuit. A larger jacket diameter may provide better protection against environmental factors and mechanical stress, while a smaller diameter may be more flexible and space-saving. It is crucial to consider the jacket diameter when selecting and installing electronic components to ensure proper fit and functionality.
0.240 (6.10mm) - Shield Type
Shield Type in electronic components refers to the method used to protect sensitive circuits from electromagnetic interference (EMI) and radio frequency interference (RFI). It encompasses the materials and techniques employed to create barriers around wires, circuits, or devices, which may include metallic enclosures, conductive coatings, or grounding practices. The choice of shield type can significantly impact the performance and reliability of electronic systems, especially in environments with high levels of interference.
Braid - Dielectric Diameter
Dielectric diameter is a parameter used in electronic components, particularly in capacitors. It refers to the physical size of the dielectric material within the capacitor. The dielectric material is an insulating substance that separates the two conductive plates of the capacitor. The dielectric diameter is important because it affects the capacitance value and performance of the capacitor. A larger dielectric diameter typically results in a higher capacitance value and better insulation properties. Manufacturers specify the dielectric diameter to ensure proper functioning of the capacitor in electronic circuits.
0.150 (3.81mm) - VoP, Velocity of Propagation
The Velocity of Propagation (VoP) is a parameter used to describe the speed at which an electrical signal travels through a medium, such as a cable or transmission line, in electronic components. It is typically expressed as a percentage of the speed of light in a vacuum. A higher VoP indicates that the signal propagates faster through the medium, which can affect the overall performance of the electronic system. VoP is an important consideration in designing and analyzing high-speed digital communication systems to ensure signal integrity and minimize signal distortion. It is also used in determining the delay characteristics of signals in transmission lines and is a key factor in determining the maximum operating frequency of a system.
83 - Length500.0' 152.40m
- RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
LMR240 CAD Model

LMR240 CAD Model
LMR240 Application
Antenna Installs
RF Test Systems
General Purpose RF Interconnect
Laboratory applications
Comparison between the LMR240 and RG8X
When Comparing RG8x to LMR-240-UF the biggest difference is the cutoff or maximum operating frequency. RG-8x has a maximum operating frequency of 1,000MHz (1GHz), LMR-240 Cable will operate beyond 1,000MHz successfully operating to 5.8GHz.
LMR240 Manufacturer
Times Microwave Systems is a leader in coaxial transmission line technology and production. They provide a broad range of RF and microwave transmission line solutions for military, aerospace, wireless communications, and industrial applications. Their engineering expertise and range of manufacturing capabilities are highly regarded in the industry. With production facilities in the US and China, they can address both specialized applications with extremely demanding performance requirements and high volume commercial applications at frequencies from a few kHz to 110 GHz.
Note: LMR® is a registered trademark of Times Microwave Systems.
Datasheet PDF
- Datasheets :
Popularity by Region
Parts with Similar Specs
What does LMR stand for cable?
Low Loss.
How flexible is LMR 240?
LMR-240-UF flexible 50 Ohm coax cable with TPE jacket is rated for a 5.8 GHz maximum operating frequency. This 50 Ohm 0.24 inch diameter and low loss flexible coax cable are built with a double shield count and RF shielding of 90 dB.
LPS53 Open Frame AC DC Converters Output 12V: Datasheet, Features, and LPS53 VS NPS63-M-00612 April 2022686
STM32F103ZET6 Microcontroller: Specification, Pinout and Datasheet20 October 20217198
ATtiny202 tinyAVR 0-series 20MHz Microcontroller: Datasheet, Pinout, and UPDI Programming Analysis10 March 20261526
2N5457 N-Channel JFET : Pinout, Alternative and Datasheet15 July 20214953
Where & How to Use SN74LS74AN Dual D Flip-Flop IC?14 July 20225015
MAX232ACSE Driver/Receiver: Features, Pinout, and Datasheet17 April 2025929
AD9516-4 Clock Generator: Pinout, Equivalent and Datasheet09 April 2022507
AD708 Dual Precision Op Amp: DC Performance Analysis and Modern Replacement Notes20 May 2026385
Demand for Automotive Chips Will Surge 300%09 April 20225768
Film Capacitors Explained: Types, Characteristics, and How to Choose14 July 202611967
Multiplexers: Types, Functionality, and Applications21 April 20253102
What is a Memory Controller?12 August 202035238
Semiconductor Industry's Water Risk Underpriced, Warn Fund Managers14 September 20234002
Function and Application of Laser Sensors28 October 20258667
How Does the A4988 Stepper Motor Driver Work29 August 20267034
What is a variable capacitor?16 April 202566938
Amphenol Times Microwave Systems
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools