M10385 FM Module:Datasheet, Application, Schematic

Sophie

Published: 01 September 2021 | Last Updated: 01 September 2021

783

M10385

M10385

Antenova

FM MODULE

Purchase Guide

FM MODULE

Antenova’s M10385 is an internal FM antenna module, and this article will unlock more details about M10385.

M10385

M10385.jpg

M10385

M10385 Description

Antenova's M10385 is an internal FM antenna module designed to address the growing market for FM Radio functionality in mobile devices such as mobile phones, PNDs, PMPs, Digital Photo Frames and Media Tablets.

Specifications

Antenova M10385 technical specifications, attributes, parameters and parts with similar specifications to Antenova M10385.
  • Type
    Parameter
  • Mount

    In electronic components, the term "Mount" typically refers to the method or process of physically attaching or fixing a component onto a circuit board or other electronic device. This can involve soldering, adhesive bonding, or other techniques to secure the component in place. The mounting process is crucial for ensuring proper electrical connections and mechanical stability within the electronic system. Different components may have specific mounting requirements based on their size, shape, and function, and manufacturers provide guidelines for proper mounting procedures to ensure optimal performance and reliability of the electronic device.

    PCB, Surface Mount
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    Module
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Bulk
  • Published
    2010
  • Termination

    Termination in electronic components refers to the practice of matching the impedance of a circuit to prevent signal reflections and ensure maximum power transfer. It involves the use of resistors or other components at the end of transmission lines or connections. Proper termination is crucial in high-frequency applications to maintain signal integrity and reduce noise.

    Solder
  • Frequency

    In electronic components, the parameter "Frequency" refers to the rate at which a signal oscillates or cycles within a given period of time. It is typically measured in Hertz (Hz) and represents how many times a signal completes a full cycle in one second. Frequency is a crucial aspect in electronic components as it determines the behavior and performance of various devices such as oscillators, filters, and communication systems. Understanding the frequency characteristics of components is essential for designing and analyzing electronic circuits to ensure proper functionality and compatibility with other components in a system.

    108MHz
  • Gain

    In electronic components, "Gain" refers to the ratio of the output signal amplitude to the input signal amplitude. It is a measure of the amplification provided by the component, such as a transistor or operational amplifier. Gain is typically expressed in decibels (dB) or as a numerical value, indicating how much the signal is amplified by the component.A higher gain value indicates a greater amplification of the input signal, while a lower gain value indicates less amplification. Gain is an important parameter in designing and analyzing electronic circuits, as it determines the overall performance and functionality of the system. Different components have different gain characteristics, and understanding the gain of a component is crucial for achieving the desired signal processing or amplification in electronic systems.

    13.5 dB
  • Number of Bands
    1
  • Height
    1.4986mm
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

M10385 Features

  • Low-cost single package Internal SMD FM

  • Antenna Module

  • Low 1.5mm height for thin devices

  • High performance

  • Easily interfaced to any FM receiver

  • Transmit + Receive through a single line

  • Built-in ESD protection ±20kV (contact)

  • Easy to integrate

  • Intended for SMD mounting


M10385 Block Diagram

M10385 Block Diagram.jpg

Block Diagram

M10385 Application

  • Mobile phones / Smartphones

  • Portable Media Players (PMPs)

  • Portable Navigation Devices (PNDs)

  • Notebooks / Netbooks / Media Tablets

  • Digital Photo/Media Frames

  • FM transmitters for Music Players


M10385 Application Schematic

M10385 Application Schematic.jpg

Application Schematic

M10385 Manufacturer

Antenova is a prominent inventor and provider of high-performance antenna systems for mobile phones, laptop computers, and other portable devices. Antenova's patented High Dielectric Antenna (HDA®) and balanced antenna technology enable integrated antenna solutions and radio antenna modules for mobile handsets, portable devices, laptop applications, and peripheral devices that are smaller, more efficient, operate across multiple bands and offer more robust performance. 

M10385 Package

M10385 Package.jpg

Package

Datasheet PDF

Download datasheets and manufacturer documentation for Antenova M10385.
Frequently Asked Questions

What is the M10385?

Antenova’s M10385 is an internal FM antenna module designed to address the growing market for FM Radio functionality in mobile devices such as mobile phones, PNDs, PMPs, Digital Photo Frames and Media Tablets.

How to use M10385?

A minimum clearance of 2mm between the antenna and the host PCB ground plane is recommended for the best FM signal reception.

What is transmitting/receiving FM frequency of M10385?

The M10385 is capable of transmitting/receiving FM frequencies from 87.5 - 108 MHz and is intended to be planar mounted at the edge of the host PCB for minimum PCB space requirement.
M10385

Antenova

In Stock
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
Related Parts More