SIM800L How to use SIM800L GSM Module with Arduino?[Video]
SIM800L datasheet pdf and Unclassified product details from SIMCom Wireless Solutions stock available at Utmel









SIM800L belongs to the small cellular module that can send and receive GPRS data, send and receive SMS, and make and receive voice calls. This article is going to talk about the pinout, features, application, and more detailed information about SIM800L.

Tutorial: How to use SIM800L GSM Module with Arduino
Overview of SIM800L
The SIM800L module, which supports a quad-band GSM/GPRS network and can deliver GPRS and SMS message data remotely, is used in the Mini GSM / GPRS breakout board. The board is compact and uses very little energy. Because of the power-saving technology, the current consumption in sleep mode is as low as 1mA. It connects to the microcontroller through a UART port and supports instructions such as 3GPP TS 27.007, 27.005, and SIMCOM enhanced AT Commands.
The SIM800L Component allows you to make and receive phone calls as well as send and receive text messages. To connect the device, a UART bus must be used, which must support both receiving and transmitting lines. The UART bus must be set to the module's default speed of 9600bps. The required connecting wires are +VCC, GND, RX, and TX.
SIM800L Features
Supports Quad-band: GSM850, EGSM900, DCS1800 and PCS1900
Connect onto any global GSM network with any 2G SIM
Make and receive voice calls using an external 8Ω speaker & electret microphone
Send and receive SMS messages
Send and receive GPRS data (TCP/IP, HTTP, etc.)
Scan and receive FM radio broadcasts
Transmit Power:
-Class 4 (2W) for GSM850
-Class 1 (1W) for DCS1800
Serial-based AT Command Set
FL connectors for cell antennae
Accepts Micro SIM Card
Specifications
- TypeParameter
- Package / Case
refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.
LGA - Packaging
Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.
Box-packed - Module Type
In electronic components, the parameter "Module Type" refers to the classification or categorization of a particular component based on its functionality, design, or purpose within a larger system. It helps identify the specific role or function that the component serves in a circuit or device. The module type can indicate whether the component is a sensor, actuator, amplifier, processor, memory module, or any other type of electronic module. Understanding the module type is crucial for selecting the right components for a given application and ensuring compatibility and proper functioning within the overall system design.
GSM/GPRS - GNSS Types
GNSS Types refer to the different Global Navigation Satellite System technologies that are used in electronic components for positioning and navigation purposes. GNSS systems include well-known systems such as GPS (Global Positioning System), GLONASS (Global Navigation Satellite System), Galileo, and BeiDou. Each GNSS type has its own network of satellites that provide signals to receivers on Earth, allowing for accurate positioning and timing information. By supporting multiple GNSS types, electronic components can improve accuracy, reliability, and coverage for location-based services and applications.
No - RoHS Status
RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.
RoHS Compliant
SIM800L Pinout

SIM800L Pinout
SIM800L Dimensions

SIM800L Dimensions
How to use SIM800L GSM Module with Arduino?
Because the Arduino Uno (view new Arduino Uno) utilizes 5V GPIO, we can't connect the Rx pin on the module to the Arduino's digital pin because the SIM800L module employs 3.3V level logic and isn't 5V tolerant. This means that the Arduino Uno's Tx signal must be brought down to 3.3V to avoid damaging the SIM800L module. There are a few options, but the simplest is to use a simple resistor divider. A 10K resistor between the SIM800L Rx and the Arduino D2 would suffice, as would a 20K resistor between the SIM800L Rx and GND.

Now we're only dealing with the pins that supply power to the module. We've supplied two example schematics because there are several ways to power up the module. One employs a Li-Po battery with a capacity of 1200mAh, while the other makes use of an LM2596 DC-DC buck converter.
How to use the SIM800L?
The SIM800L is a GSM module with a serial interface. It can send and receive text messages and receive phone calls. It can also connect to the internet and receive FM signals. The SIM800L can be connected to a microcontroller using the serial UART interface, and in the example shown below, connected to an Arduino.
The module recognizes AT commands, which can be used to do things like check signal strength, get the SIM card number, check the network connection and battery state, in addition to reading texts, and making and receiving calls.

SIM800L Applications
Remote System Monitoring
Home Alarm System
Remote Controlling System
Security Access Control
Vehicle tracking
SMS Gateway
Pre-paid Electricity
SIM800L Equivalents
SIM808, SIM900A
SIM800L Datasheet
SIM800L Manufacturer
Chenxun Technology Group's SIMCom Wireless Solutions Co., Ltd. (SIMCom Wireless Solutions) is a wholly-owned subsidiary (HK: 2000). SIMCom Wireless Technology is dedicated to developing wireless module solutions for GSM / GPRS / EDGE / WCDMA / HS * PA, TD-SCDMA, CDMA EVDO, LTE, GPS / GNSS, SRD, and other platforms. SIMCom's wireless module shipments occupied the world's second-largest market position for the first time in 2008, according to the ABI survey report. SIMCom's wireless technology has been used in a variety of industries, including M2M, WLL, Mobile Computing, and GPS. In applications, provide customers with cost-effective customized solutions and ODM services.
Popularity by Region
Parts with Similar Specs
What is a SIM800L?
The SIM800L is a small cellular module that can send and receive GPRS data, send and receive SMS, and make and receive voice calls. This module's low cost, small footprint, and quad-band frequency capabilities make it an ideal choice for any project requiring long-range connectivity.
What are the differences between the SIM800L and SIM900A?
The SIM800L and SIM900A GSM modules are extremely identical, with the exception that the SIM800L model supports Bluetooth and has AT instructions for Bluetooth/FM.
Can SIM800L connect to Internet?
For connecting to the internet through HTTP, the SIM800L supports General Packet Radio Service (GPRS). AT commands can be used to access the module's built-in TCP/IP stack. This is particularly useful for long-term data logging on low-bandwidth networks.
Does SIM800L support 4G SIM?
Only 2G services are supported by the SIM800L. If it's not getting network, try another 2G card, and then connect the GSM antenna. I have both Airtel and Vodafone 4G SIM cards. They function perfectly on the 2G network by default.
Can SIM800L handle 5V?
Because the Arduino Uno utilizes 5V GPIO, we can't connect the Rx pin on the module to the Arduino's digital pin because the SIM800L module employs 3.3V level logic and isn't 5V tolerant.
LM2596 Switching Regulator: 3.0A, DC to DC, LM2596 Datasheet30 December 202210472
LM317 Voltage Regulator[Video+FAQ]: Pinout, Circuit, LM317 VS LM7805 and Datasheet27 April 202214865
TL431 Shunt Regulator: How to Test and Replace?26 April 202221290
STMPE811QTR S-Touch 8-bit GPIO expander QFN16: 3D Model, Datasheet, and Application17 January 2022324
STM32F105RBT6: 72MHz, 64-LQFP, Pinout and Datasheet25 February 20225250
ULN2003A Seven Darlington Array: Pinout, Features and Datasheet18 May 202121225
CD4511BE BCD to 7 Segment Decoder: Datasheet, Equivalent, Pinout, and Uses12 April 202217319
RS3000-AP Rectifier Diode: Features, Alternatives, Comparison26 July 2021332
What are the Applications of Filters?17 January 202616841
Comparison of Advantages and Disadvantages of Common Switch Mode Power Supply(SMPS)21 January 20228177
Multiplexers: Types, Functionality, and Applications21 April 20252420
Rectangular Connectors vs Circular Connectors: Which fits your Project Best04 July 20252611
How Nvidia Became a Chip Industry Giant14 April 20221027
Vibration Isolator: Types and Applications13 January 202112619
What is Optical Module?08 December 20217133
A New Way of Thinking About the "Trolley Problem" of Artificial Intelligence27 May 20221716
SIMCom Wireless Solutions
In Stock
United States
China
Canada
Japan
Russia
Germany
United Kingdom
Singapore
Italy
Hong Kong(China)
Taiwan(China)
France
Korea
Mexico
Netherlands
Malaysia
Austria
Spain
Switzerland
Poland
Thailand
Vietnam
India
United Arab Emirates
Afghanistan
Åland Islands
Albania
Algeria
American Samoa
Andorra
Angola
Anguilla
Antigua & Barbuda
Argentina
Armenia
Aruba
Australia
Azerbaijan
Bahamas
Bahrain
Bangladesh
Barbados
Belarus
Belgium
Belize
Benin
Bermuda
Bhutan
Bolivia
Bonaire, Sint Eustatius and Saba
Bosnia & Herzegovina
Botswana
Brazil
British Indian Ocean Territory
British Virgin Islands
Brunei
Bulgaria
Burkina Faso
Burundi
Cabo Verde
Cambodia
Cameroon
Cayman Islands
Central African Republic
Chad
Chile
Christmas Island
Cocos (Keeling) Islands
Colombia
Comoros
Congo
Congo (DRC)
Cook Islands
Costa Rica
Côte d’Ivoire
Croatia
Cuba
Curaçao
Cyprus
Czechia
Denmark
Djibouti
Dominica
Dominican Republic
Ecuador
Egypt
El Salvador
Equatorial Guinea
Eritrea
Estonia
Eswatini
Ethiopia
Falkland Islands
Faroe Islands
Fiji
Finland
French Guiana
French Polynesia
Gabon
Gambia
Georgia
Ghana
Gibraltar
Greece
Greenland
Grenada
Guadeloupe
Guam
Guatemala
Guernsey
Guinea
Guinea-Bissau
Guyana
Haiti
Honduras
Hungary
Iceland
Indonesia
Iran
Iraq
Ireland
Isle of Man
Israel
Jamaica
Jersey
Jordan
Kazakhstan
Kenya
Kiribati
Kosovo
Kuwait
Kyrgyzstan
Laos
Latvia
Lebanon
Lesotho
Liberia
Libya
Liechtenstein
Lithuania
Luxembourg
Macao(China)
Madagascar
Malawi
Maldives
Mali
Malta
Marshall Islands
Martinique
Mauritania
Mauritius
Mayotte
Micronesia
Moldova
Monaco
Mongolia
Montenegro
Montserrat
Morocco
Mozambique
Myanmar
Namibia
Nauru
Nepal
New Caledonia
New Zealand
Nicaragua
Niger
Nigeria
Niue
Norfolk Island
North Korea
North Macedonia
Northern Mariana Islands
Norway
Oman
Pakistan
Palau
Palestinian Authority
Panama
Papua New Guinea
Paraguay
Peru
Philippines
Pitcairn Islands
Portugal
Puerto Rico
Qatar
Réunion
Romania
Rwanda
Samoa
San Marino
São Tomé & Príncipe
Saudi Arabia
Senegal
Serbia
Seychelles
Sierra Leone
Sint Maarten
Slovakia
Slovenia
Solomon Islands
Somalia
South Africa
South Sudan
Sri Lanka
St Helena, Ascension, Tristan da Cunha
St. Barthélemy
St. Kitts & Nevis
St. Lucia
St. Martin
St. Pierre & Miquelon
St. Vincent & Grenadines
Sudan
Suriname
Svalbard & Jan Mayen
Sweden
Syria
Tajikistan
Tanzania
Timor-Leste
Togo
Tokelau
Tonga
Trinidad & Tobago
Tunisia
Turkey
Turkmenistan
Turks & Caicos Islands
Tuvalu
U.S. Outlying Islands
U.S. Virgin Islands
Uganda
Ukraine
Uruguay
Uzbekistan
Vanuatu
Vatican City
Venezuela
Wallis & Futuna
Yemen
Zambia
Zimbabwe


Product
Brand
Articles
Tools