The Guide to BFW10 30V N-Channel JFET [Datasheet]

UTMEL

Published: 30 March 2022 | Last Updated: 30 March 2022

23696

BFW10

BFW10

TEXAS INSTRUMENTS INC

BFW10 datasheet pdf and Unclassified product details from TEXAS INSTRUMENTS INC stock available at Utmel

Purchase Guide

The BFW10 is an N-Channel JFET Transistor that is used to amplify or switch electronic signals as well as electrical power. This article will cover guide details for your reference.

This video demonstrates how to identify the terminals of BFW 10/11.

TRICK To Identify Terminals of BFW 10/11 || Best and Easy Way

What is BFW10?

The BFW10 is an N-Channel JFET Transistor that is used to amplify or switch electronic signals as well as electrical power. It's made of semiconductor material and has at least three terminals for connecting to a circuit outside of it. The current  through another pair of terminals  is controlled by a voltage  or current  applied to one pair of transistor   terminals

transistor can magnify a signal because the regulated (output) power can be higher than the controlling (input) power,  Some transistors are still packaged separately nowadays, but many more are included in integrated circuits.


BFW10 Pinout

BFW10 PINOUT.jpg

BFW10 Pinout

BFW10 Maximum Ratings

  • Drain-Source Voltage  : Vds = 30 Vdc

  • Drain-Gate Voltage  : Vdg = 30 Vdc

  • Reverse Gate-Source Voltage  : Vgsr = -30 Vdc

  • Forward Gate Current  : Igf = 10 mADC


Specifications

TEXAS INSTRUMENTS INC BFW10 technical specifications, attributes, parameters and parts with similar specifications to TEXAS INSTRUMENTS INC BFW10.
  • Type
    Parameter
  • Surface Mount

    having leads that are designed to be soldered on the side of a circuit board that the body of the component is mounted on.

    NO
  • Operating Temperature (Max.)
    175°C
  • Reach Compliance Code

    Reach Compliance Code refers to a designation indicating that electronic components meet the requirements set by the Registration, Evaluation, Authorization, and Restriction of Chemicals (REACH) regulation in the European Union. It signifies that the manufacturer has assessed and managed the chemical substances within the components to ensure safety and environmental protection. This code is vital for compliance with regulations aimed at minimizing risks associated with hazardous substances in electronic products.

    not_compliant
  • Polarity/Channel Type

    In electronic components, the parameter "Polarity/Channel Type" refers to the characteristic that determines the direction of current flow or the type of signal that can be accommodated by the component. For components like diodes and transistors, polarity indicates the direction in which current can flow through the component, such as forward bias or reverse bias for diodes. For components like MOSFETs or JFETs, the channel type refers to whether the component is an N-channel or P-channel device, which determines the type of charge carriers that carry current through the component. Understanding the polarity or channel type of a component is crucial for proper circuit design and ensuring that the component is connected correctly to achieve the desired functionality.

    N-CHANNEL
  • FET Technology

    Field-Effect Transistor (FET) technology is a type of semiconductor device commonly used in electronic components such as transistors and integrated circuits. FETs operate by controlling the flow of current through a semiconductor channel using an electric field. There are several types of FETs, including Metal-Oxide-Semiconductor FETs (MOSFETs) and Junction FETs (JFETs), each with its own characteristics and applications. FET technology offers advantages such as high input impedance, low power consumption, and fast switching speeds, making it suitable for a wide range of electronic devices and circuits. Overall, FET technology plays a crucial role in modern electronics by enabling efficient and reliable signal processing and amplification.

    JUNCTION
  • Power Dissipation-Max (Abs)

    Power Dissipation-Max (Abs) refers to the maximum amount of power that an electronic component can dissipate without undergoing thermal damage or degradation. This value is crucial for ensuring reliable operation, as exceeding it can result in overheating and failure. It is typically specified in watts and serves as a critical parameter for designers to determine proper heat management strategies in circuits. Properly managing the power dissipation is essential for the longevity and performance of electronic devices.

    0.25W
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    Non-RoHS Compliant
0 Similar Products Remaining

BFW10 Features

  • Type Designator: BFW10 

  • Type of TransistorJFET 

  • Type of Control Channel: N -Channel 

  • Maximum Power Dissipation (Pd): 0.3 W

  • Maximum Drain-Source Voltage  |Vds|: 30 V

  • Maximum Gate-Source Voltage  |Vgs|: 30 V

  • Maximum Drain Current |Id|: 0.01 A

  • Maximum Junction Temperature  (Tj): 150 °C

  • Maximum Drain-Source On-State Resistance (Rds): 500 Ohm

  • Package: TO-72


BFW10 Applications

BFW10 is employed as voltage-variable resistors (WRs) in operational amplifiers  (op-amps), tone controls, and logic circuits, as well as for mixer operation on FM  and TV receivers.

BFW10 Circuit Diagram

bfw10 circuit diagram.jpg

BFW10 Circuit Diagram

BFW10 Equivalents

PTF10149 , RJK0234DNS , SPP100N06S2-05 , SPB100N06S2-05 , SSM5N03FE , STK0260D , SWD5N65K , VN10KLS , BS170 , BFW11 , CS3N20ATH , FHP3205 , FS10KM-12 , FS10KM-2 , FTP50N20R , JCS12N65T , JCS12N65CT

What are JFET transistors used for?

JFET stands for "junction field-effect transistor.  " and it can be utilized for anything that a standard MOSFET can do. The JFET, on the other hand, lacks a gate oxide and hence operates more like a bipolar junction device, with a higher gate current than a MOSFET.

JFETs are commonly used as low noise amplifiers in the front ends of extremely sensitive circuits. The 1/f noise is smaller because they don't have gate oxide. They're also sometimes utilized as big resistors, like MOSFET  s in depletion mode.

 


BFW10 Dimensions

BFW10 dimensions.jpg

BFW10 Dimensions

BFW10 Manufacturer

Texas Instruments Incorporated (TI) is an American technology company headquartered in Dallas,  Texas, that designs and manufactures semiconductors and various integrated circuits, which it sells to electronics designers and manufacturers globally.

BFW10 Datasheet

BFW10 Datasheet for your reference

Frequently Asked Questions

What is the use of BFW10?

BFW10 is a semiconductor device used to amplify or switch electronic signals and electrical power.

What type of transistor is the BFW10?

N-Channel JFET Transistor

N-Channel JFET Transistor

The BFW10 Drain Current-Max is 0.02 A.

What is the max operating temperature of BFW10?

175°C

What is the size of BFW10?

TO-72
BFW10

TEXAS INSTRUMENTS INC

In Stock