TLP521-4XGBSM Optocoupler: Isocom, Datasheet, Applications [FAQ]

Sophie

Published: 12 January 2023 | Last Updated: 12 January 2023

716

TLP521-4XGBSM

TLP521-4XGBSM

Isocom Components

TransistorOptocouplers 4 5300Vrms SMD-16 Optocouplers RoHS

Purchase Guide

TransistorOptocouplers 4 5300Vrms SMD-16 Optocouplers RoHS

This article will cover the datasheet, pinout, applications and more detailed information about TLP521-4XGBSM.

TLP521-4XGBSM Pinout

TLP521-4XGBSM Pinout.jpg

TLP521-4XGBSM Pinout

TLP521-4XGBSM CAD Model

Symbol


TLP521-4XGBSM Symbol.jpg

TLP521-4XGBSM Symbol

Footprint

TLP521-4XGBSM Footprint.jpg

TLP521-4XGBSM Symbol

3D Model

TLP521-4XGBSM 3D Model.jpg

TLP521-4XGBSM 3D Model

TLP521-4XGBSM Brief Introduction

Isocom's TLP521-4XGBSM is a through-hole optically coupled isolator in a DIP 16-pin package. The isolation device is made up of infrared light-emitting diodes and an NPN silicon phototransistor. This isolator is commonly used in computer terminals, industrial system controllers, and signal transmission between systems with varying potentials and impedances.


TLP521-4XGBSM Applications

  • Computer Terminals

  • Industrial System Controllers

  • Measuring Instruments

  • Signal Transmission between Systems of Different Potentials and Impedances


TLP521-4XGBSM Package

TLP521-4XGBSM Package.jpg

TLP521-4XGBSM Package

TLP521-4XGBSM Manufacturer

ISOCOM Components is a leader in high-performance infrared optoelectronic devices among global manufacturers. We are focused on providing optocouplers and optoswitches. During its 25-year development, Isocom insists on delivering in excess of its customer's expectations. Therefore, we become one of the most respected brands in the optoelectronic industry around the world. Due to our high-quality products and superior customer service, we win the praise of our long-term customers. ISOCOM Components provides a natural alternative to the industry standard type of commercial optocouplers. At the same time, in order to meet the customer's specific circuit design requirements, we have carried out special parameter selection. Our products are in compliance with leading recognized industry standards.


More Similar Article:

The Comprehensive Introduction to TLP521-1XGBSMT&R [Video]

TLP521-2XGB Optocoupler: TLP521 Series, Datasheet, Pinout [FAQ]

Specifications

Isocom Components TLP521-4XGBSM technical specifications, attributes, parameters and parts with similar specifications to Isocom Components TLP521-4XGBSM.
  • Type
    Parameter
  • Package / Case

    refers to the protective housing that encases an electronic component, providing mechanical support, electrical connections, and thermal management.

    SMD-16
  • Packaging

    Semiconductor package is a carrier / shell used to contain and cover one or more semiconductor components or integrated circuits. The material of the shell can be metal, plastic, glass or ceramic.

    Tube-packed
  • Voltage - Isolation

    Voltage - Isolation is a parameter in electronic components that refers to the maximum voltage that can be safely applied between two isolated points without causing electrical breakdown or leakage. It is a crucial specification for components such as transformers, optocouplers, and capacitors that require isolation to prevent electrical interference or safety hazards. The voltage isolation rating ensures that the component can withstand the specified voltage without compromising its performance or safety. It is typically measured in volts and is an important consideration when designing circuits that require isolation between different parts of the system.

    5300Vrms
  • Number of Channels
    4
  • Output Current-Max

    Output Current-Max is a parameter in electronic components that specifies the maximum amount of current that can be safely drawn from the output of the component without causing damage. It is an important specification to consider when designing circuits to ensure that the component can handle the required current without overheating or failing. Exceeding the maximum output current can lead to performance issues, component damage, or even complete failure of the circuit. It is crucial to adhere to the specified maximum output current to ensure the reliable operation of the electronic component and the overall circuit.

    100nA
  • Output Voltage-Max

    Output Voltage-Max is a parameter in electronic components that specifies the maximum voltage level that can be safely output by the component under normal operating conditions. This parameter is crucial for ensuring the proper functioning and longevity of the component, as exceeding the maximum output voltage can lead to damage or failure. Designers and engineers must carefully consider this specification when selecting components for a circuit to prevent overloading and potential hazards. It is important to adhere to the specified maximum output voltage to maintain the reliability and performance of the electronic system.

    55V
  • RoHS Status

    RoHS means “Restriction of Certain Hazardous Substances” in the “Hazardous Substances Directive” in electrical and electronic equipment.

    RoHS Compliant
0 Similar Products Remaining

Datasheet PDF

Download datasheets and manufacturer documentation for Isocom Components TLP521-4XGBSM.
Frequently Asked Questions

What is TLP521-4XGBSM ?

The TLP521-4XGBSM from Isocom is a through hole optically coupled isolator in DIP 16 pin package. 

What is the operating temperature of TLP521-4XGBSM?

-30°C to +100°C
TLP521-4XGBSM

Isocom Components

In Stock: 2000
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
Related Parts More